![]() |
![]() |
TI-OpenThread
1.08.06.06
|
#include <openthread-core-config.h>
#include <stdint.h>
#include <openthread/config.h>
#include <openthread/instance.h>
Go to the source code of this file.
Functions | |
otError | otPlatUartFlush (void) |
void | otSysInit (int argc, char *argv[]) |
void | platformAlarmInit (void) |
void | platformAlarmMicroInit (void) |
void | platformAlarmMicroProcess (otInstance *aInstance) |
void | platformAlarmMicroSignal (void) |
void | platformAlarmProcess (otInstance *aInstance) |
void | platformAlarmSignal (void) |
void | platformDebugUartInit (void) |
void | platformRadioInit (void) |
void | platformRadioProcess (otInstance *aInstance, uintptr_t arg) |
void | platformRadioSignal (uintptr_t arg) |
void | platformRandomInit (void) |
void | platformRandomProcess (void) |
void | platformRandomSignal (void) |
void | platformSpiProcess (void) |
void | platformSpiSignal (void) |
void | platformUartProcess (uintptr_t arg) |
void | platformUartSignal (uintptr_t arg) |
Variables | |
otInstance * | sInstance |
void otSysInit | ( | int | argc, |
char * | argv[] | ||
) |
Initialize the platform support modules.
Function documented in system.h
void platformDebugUartInit | ( | void | ) |
Initialize the debug uart
void platformAlarmInit | ( | void | ) |
This method initializes the alarm service used by OpenThread.
Function documented in system.h
void platformAlarmSignal | ( | ) |
Signal the processing loop to process the alarm module.
Callback from the alarm module indicating need for processing.
void platformAlarmProcess | ( | otInstance * | aInstance | ) |
This method performs alarm driver processing.
Function documented in system.h
void platformAlarmMicroInit | ( | void | ) |
This method initializes the alarm service used by OpenThread.
Function documented in system.h
void platformAlarmMicroSignal | ( | ) |
Signal the processing loop to process the alarm module.
Callback from the alarm module indicating need for processing.
void platformAlarmMicroProcess | ( | otInstance * | aInstance | ) |
This method performs alarm driver processing.
Function documented in system.h
void platformRadioInit | ( | void | ) |
This method initializes the radio service used by OpenThread.
Function documented in system.h
void platformRadioSignal | ( | uintptr_t | arg | ) |
Callback from the radio module indicating need for processing.
void platformRadioProcess | ( | otInstance * | aInstance, |
uintptr_t | arg | ||
) |
This method performs radio driver processing.
Function documented in system.h This is called from the main process loop.
void platformRandomInit | ( | void | ) |
This method initializes the random number service used by OpenThread.
Function documented in system.h
void platformRandomSignal | ( | void | ) |
Callback from random module indicating need for processing.
Callback from the random generator module indicating need for processing.
void platformRandomProcess | ( | void | ) |
This method performs random driver processing.
Function documented in system.h
void platformUartSignal | ( | uintptr_t | arg | ) |
Signal the processing loop to process the uart module.
Callback from the alarm module indicating need for processing.
void platformUartProcess | ( | uintptr_t | arg | ) |
This method performs uart driver processing.
Function documented in system.h
void platformSpiSignal | ( | ) |
Signal the processing loop to process the spi module.
Callback from the spi module indicating need for processing.
void platformSpiProcess | ( | void | ) |
This method performs spi driver processing.
otError otPlatUartFlush | ( | void | ) |
This method performs UART Flush.
Function documented in system.h
otInstance* sInstance |