TI-OpenThread  1.08.06.06
Data Structures | Macros | Typedefs | Enumerations | Functions | Variables
LP_EM_CC1354P10_6/thread/shade/platform/radio.h File Reference
#include <ti/devices/DeviceFamily.h>
#include <DeviceFamily_constructPath(driverlib/rf_ieee_cmd.h)>
#include <openthread/instance.h>
+ Include dependency graph for LP_EM_CC1354P10_6/thread/shade/platform/radio.h:
+ This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  ext_src_match_data_s
 
struct  short_src_match_data_s
 

Macros

#define DATA_ENTRY_LENSZ_BYTE   1
 
#define IEEE802154_A_TURNAROUND_TIME   (12)
 
#define IEEE802154_A_UINT_BACKOFF_PERIOD   (20)
 
#define IEEE802154_ACK_LENGTH   (5)
 
#define IEEE802154_ACK_REQUEST   (1<<5)
 
#define IEEE802154_DSN_OFFSET   (2)
 
#define IEEE802154_FRAME_PENDING   (1<<4)
 
#define IEEE802154_FRAME_PENDING_MASK   (0x40)
 
#define IEEE802154_FRAME_TYPE_ACK   (0x2)
 
#define IEEE802154_FRAME_TYPE_MASK   (0x7)
 
#define IEEE802154_MAC_ACK_WAIT_DURATION
 
#define IEEE802154_MAC_MAX_BE   (5)
 
#define IEEE802154_MAC_MAX_CSMA_BACKOFFS   (4)
 
#define IEEE802154_MAC_MAX_FRAMES_RETRIES   (3)
 
#define IEEE802154_MAC_MIN_BE   (3)
 
#define IEEE802154_PHY_SHR_DURATION   (10)
 
#define IEEE802154_PHY_SYMBOLS_PER_OCTET   (2)
 
#define IEEE802154_SYMBOLS_PER_SEC   (62500)
 
#define PLATFORM_RADIO_EXTADD_SRC_MATCH_NUM   10
 
#define PLATFORM_RADIO_INVALID_RSSI   (127)
 
#define PLATFORM_RADIO_RAT_TICKS_PER_SEC   (4000000)
 
#define PLATFORM_RADIO_SHORTADD_SRC_MATCH_NUM   10
 
#define PLATFORM_RADIO_SRC_MATCH_NONE   0xFF
 
#define RF_DRIVER_ABORT   0
 
#define RF_EVENT_BUF_FULL   (1U << 5)
 
#define RF_EVENT_ED_SCAN_DONE   (1U << 1)
 
#define RF_EVENT_RX_ACK_DONE   (1U << 3)
 
#define RF_EVENT_RX_CMD_STOP   (1U << 6)
 
#define RF_EVENT_RX_DONE   (1U << 2)
 
#define RF_EVENT_SLEEP_YIELD   (1U << 4)
 
#define RF_EVENT_TX_CMD_PREEMPTED   (1U << 7)
 
#define RF_EVENT_TX_DONE   (1U << 0)
 
#define RX_BUF_SIZE   148
 

Typedefs

typedef struct __RFC_STRUCT ext_src_match_data_s ext_src_match_data_t
 
typedef enum platformRadio_address platformRadio_address
 
typedef enum platformRadio_phyState platformRadio_phyState
 
typedef struct __RFC_STRUCT short_src_match_data_s short_src_match_data_t
 

Enumerations

enum  platformRadio_address {
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1,
  platformRadio_address_short = 0, platformRadio_address_ext = 1, platformRadio_address_short = 0, platformRadio_address_ext = 1
}
 
enum  platformRadio_phyState {
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit,
  platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan,
  platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep, platformRadio_phyState_Receive,
  platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0, platformRadio_phyState_Sleep,
  platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit, platformRadio_phyState_Disabled = 0,
  platformRadio_phyState_Sleep, platformRadio_phyState_Receive, platformRadio_phyState_EdScan, platformRadio_phyState_Transmit
}
 

Functions

otError otPlatDiagRadioToneStart (otInstance *aInstance, bool aModulated)
 
otError otPlatDiagRadioToneStop (otInstance *aInstance)
 
void rfCoreDiagChannelDisable (uint8_t aChannel)
 
void rfCoreDiagChannelEnable (uint8_t aChannel)
 
void rfCorePriorityCoex (bool aEnable)
 
void rfCoreRequestCoex (bool aEnable)
 

Variables

struct __RFC_STRUCT ext_src_match_data_s __RFC_STRUCT_ATTR
 

Macro Definition Documentation

§ RX_BUF_SIZE

#define RX_BUF_SIZE   148

Size of the receive buffers in the receive queue.

§ RF_DRIVER_ABORT

#define RF_DRIVER_ABORT   0

Value to pass to RF_cancelCmd to signify aborting the command.

documented in source/ti/drivers/rf/RF.h

§ PLATFORM_RADIO_SRC_MATCH_NONE

#define PLATFORM_RADIO_SRC_MATCH_NONE   0xFF

Return value used when searching the source match array.

Returned if an address could not be found or if an empty element could not be found.

§ PLATFORM_RADIO_EXTADD_SRC_MATCH_NUM

#define PLATFORM_RADIO_EXTADD_SRC_MATCH_NUM   10

Number of extended addresses in ext_src_match_data_t.

§ PLATFORM_RADIO_SHORTADD_SRC_MATCH_NUM

#define PLATFORM_RADIO_SHORTADD_SRC_MATCH_NUM   10

Number of short addresses in short_src_match_data_t.

§ DATA_ENTRY_LENSZ_BYTE

#define DATA_ENTRY_LENSZ_BYTE   1

size of length field in receive struct.

defined in Table 23-10 of the cc13xx and cc26xx TRM.

§ RF_EVENT_TX_DONE

#define RF_EVENT_TX_DONE   (1U << 0)

Event flags for the radio process function

§ RF_EVENT_ED_SCAN_DONE

#define RF_EVENT_ED_SCAN_DONE   (1U << 1)

§ RF_EVENT_RX_DONE

#define RF_EVENT_RX_DONE   (1U << 2)

§ RF_EVENT_RX_ACK_DONE

#define RF_EVENT_RX_ACK_DONE   (1U << 3)

§ RF_EVENT_SLEEP_YIELD

#define RF_EVENT_SLEEP_YIELD   (1U << 4)

§ RF_EVENT_BUF_FULL

#define RF_EVENT_BUF_FULL   (1U << 5)

§ RF_EVENT_RX_CMD_STOP

#define RF_EVENT_RX_CMD_STOP   (1U << 6)

§ RF_EVENT_TX_CMD_PREEMPTED

#define RF_EVENT_TX_CMD_PREEMPTED   (1U << 7)

§ IEEE802154_FRAME_TYPE_MASK

#define IEEE802154_FRAME_TYPE_MASK   (0x7)

(IEEE 802.15.4-2006) PSDU.FCF.frameType.

§ IEEE802154_FRAME_PENDING_MASK

#define IEEE802154_FRAME_PENDING_MASK   (0x40)

(IEEE 802.15.4-2006) PSDU.FCF.framePending.

§ IEEE802154_FRAME_TYPE_ACK

#define IEEE802154_FRAME_TYPE_ACK   (0x2)

(IEEE 802.15.4-2006) frame type: ACK.

§ IEEE802154_FRAME_PENDING

#define IEEE802154_FRAME_PENDING   (1<<4)

(IEEE 802.15.4-2006) PSDU.FCF.bFramePending.

§ IEEE802154_ACK_LENGTH

#define IEEE802154_ACK_LENGTH   (5)

(IEEE 802.15.4-2006) Length of an ack frame.

§ IEEE802154_ACK_REQUEST

#define IEEE802154_ACK_REQUEST   (1<<5)

(IEEE 802.15.4-2006) PSDU.FCF.bAR.

§ IEEE802154_DSN_OFFSET

#define IEEE802154_DSN_OFFSET   (2)

(IEEE 802.15.4-2006) PSDU.sequenceNumber.

§ IEEE802154_MAC_MIN_BE

#define IEEE802154_MAC_MIN_BE   (3)

(IEEE 802.15.4-2006) macMinBE.

§ IEEE802154_MAC_MAX_BE

#define IEEE802154_MAC_MAX_BE   (5)

(IEEE 802.15.4-2006) macMaxBE.

§ IEEE802154_MAC_MAX_CSMA_BACKOFFS

#define IEEE802154_MAC_MAX_CSMA_BACKOFFS   (4)

(IEEE 802.15.4-2006) macMaxCSMABackoffs.

§ IEEE802154_MAC_MAX_FRAMES_RETRIES

#define IEEE802154_MAC_MAX_FRAMES_RETRIES   (3)

(IEEE 802.15.4-2006) macMaxFrameRetries.

§ IEEE802154_A_UINT_BACKOFF_PERIOD

#define IEEE802154_A_UINT_BACKOFF_PERIOD   (20)

(IEEE 802.15.4-2006 7.4.1) MAC constants.

§ IEEE802154_A_TURNAROUND_TIME

#define IEEE802154_A_TURNAROUND_TIME   (12)

(IEEE 802.15.4-2006 6.4.1) PHY constants.

§ IEEE802154_PHY_SHR_DURATION

#define IEEE802154_PHY_SHR_DURATION   (10)

(IEEE 802.15.4-2006 6.4.2) PHY PIB attribute, specifically the O-QPSK PHY.

§ IEEE802154_PHY_SYMBOLS_PER_OCTET

#define IEEE802154_PHY_SYMBOLS_PER_OCTET   (2)

(IEEE 802.15.4-2006 6.4.2) PHY PIB attribute, specifically the O-QPSK PHY.

§ IEEE802154_MAC_ACK_WAIT_DURATION

#define IEEE802154_MAC_ACK_WAIT_DURATION
Value:
#define IEEE802154_A_UINT_BACKOFF_PERIOD
Definition: LP_EM_CC1354P10_6/thread/shade/platform/radio.h:163
#define IEEE802154_PHY_SYMBOLS_PER_OCTET
Definition: LP_EM_CC1354P10_6/thread/shade/platform/radio.h:178
#define IEEE802154_PHY_SHR_DURATION
Definition: LP_EM_CC1354P10_6/thread/shade/platform/radio.h:173
#define IEEE802154_A_TURNAROUND_TIME
Definition: LP_EM_CC1354P10_6/thread/shade/platform/radio.h:168

(IEEE 802.15.4-2006 7.4.2) macAckWaitDuration PIB attribute.

§ IEEE802154_SYMBOLS_PER_SEC

#define IEEE802154_SYMBOLS_PER_SEC   (62500)

(IEEE 802.15.4-2006 6.5.3.2) O-QPSK symbol rate.

§ PLATFORM_RADIO_RAT_TICKS_PER_SEC

#define PLATFORM_RADIO_RAT_TICKS_PER_SEC   (4000000)

Frequency of the Radio Timer module.

4MHz clock.

§ PLATFORM_RADIO_INVALID_RSSI

#define PLATFORM_RADIO_INVALID_RSSI   (127)

Invalid RSSI value returned from an ED scan.

Typedef Documentation

§ ext_src_match_data_t

typedef struct __RFC_STRUCT ext_src_match_data_s ext_src_match_data_t

Structure for source matching extended addresses.

Defined in Table 23-73 of the cc13xx and cc26xx TRM.

§ short_src_match_data_t

typedef struct __RFC_STRUCT short_src_match_data_s short_src_match_data_t

Structure for source matching short addresses.

Defined in Table 23-74 of the cc13xx and cc26xx TRM.

§ platformRadio_address

Enum for specifying short/ext address type

§ platformRadio_phyState

This enum represents the state of a radio.

Initially, a radio is in the Disabled state.

The following are valid radio state transitions for the platform

+----------+ Enable() +-------+ Receive() +---------+ Transmit() +----------+
| |----------->| |------------->| |-------------->| |
| Disabled | | Sleep | | Receive | | Transmit |
| |<-----------| |<-------------| |<--------------| |
+----------+ Disable() | | Sleep() +---------+ Receive() or +----------+
^ | | | ^ Transmit complete
| | | EnergyScan() | |
| | | V | Scan Complete
| | | EnergyScan() +--------+
Init() | |-------------->| EdScan |
+-------+ +--------+

These states slightly differ from the states in include/openthread/platform/radio.h from OpenThread. The additional states the phy can be in are due to the asynchronous nature of the CM0 radio core.

state description
Disabled The rfcore powerdomain is off and the RFCPE is off
Sleep The RFCORE PD is on, and the RFCPE is in IEEE mode
Receive The RFCPE is running a CMD_IEEE_RX
EdScan The RFCPE is running a CMD_IEEE_ED_SCAN
Transmit The RFCPE is running a transmit command string

Enumeration Type Documentation

§ platformRadio_address

Enum for specifying short/ext address type

Enumerator
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 
platformRadio_address_short 
platformRadio_address_ext 

§ platformRadio_phyState

This enum represents the state of a radio.

Initially, a radio is in the Disabled state.

The following are valid radio state transitions for the platform

+----------+ Enable() +-------+ Receive() +---------+ Transmit() +----------+
| |----------->| |------------->| |-------------->| |
| Disabled | | Sleep | | Receive | | Transmit |
| |<-----------| |<-------------| |<--------------| |
+----------+ Disable() | | Sleep() +---------+ Receive() or +----------+
^ | | | ^ Transmit complete
| | | EnergyScan() | |
| | | V | Scan Complete
| | | EnergyScan() +--------+
Init() | |-------------->| EdScan |
+-------+ +--------+

These states slightly differ from the states in include/openthread/platform/radio.h from OpenThread. The additional states the phy can be in are due to the asynchronous nature of the CM0 radio core.

state description
Disabled The rfcore powerdomain is off and the RFCPE is off
Sleep The RFCORE PD is on, and the RFCPE is in IEEE mode
Receive The RFCPE is running a CMD_IEEE_RX
EdScan The RFCPE is running a CMD_IEEE_ED_SCAN
Transmit The RFCPE is running a transmit command string
Enumerator
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 
platformRadio_phyState_Disabled 
platformRadio_phyState_Sleep 
platformRadio_phyState_Receive 
platformRadio_phyState_EdScan 
platformRadio_phyState_Transmit 

Function Documentation

§ otPlatDiagRadioToneStart()

otError otPlatDiagRadioToneStart ( otInstance *  aInstance,
bool  aModulated 
)

The diagnostic module calls this function to begin transmitting a continuous tone. The tone will be transmitted on the current receive channel.

Parameters
[in]aInstanceThe OpenThread instance structure.
[in]aModulatedIndicates whether or not the tone was modulated or not.
Return values
OT_ERROR_NONESuccessfully started sending the RF tone.
OT_ERROR_NOT_IMPLEMENTEDThe radio doesn't support sending a test tone.

Function documented in platform/radio.h

§ otPlatDiagRadioToneStop()

otError otPlatDiagRadioToneStop ( otInstance *  aInstance)

The diagnostic module calls this to stop transmitting a continuous tone.

Parameters
[in]aInstanceThe OpenThread instance structure.
Return values
OT_ERROR_NONESuccessfully stopped sending the RF tone.
OT_ERROR_NOT_IMPLEMENTEDThe radio doesn't support sending a test tone.

Function documented in platform/radio.h

§ rfCoreDiagChannelDisable()

void rfCoreDiagChannelDisable ( uint8_t  aChannel)

The diagnostic module calls this to set the channel and disable channel switching.

This function was added to support automated Thread Test Harness execution. It is intended to simulate the device being placed within a shield box by switching the radio to an unused channel and disallowing the stack switching back to the set channel.

Parameters
[in]aChannelThe new (empty) channel.

Function documented in radio.h

§ rfCoreDiagChannelEnable()

void rfCoreDiagChannelEnable ( uint8_t  aChannel)

The diagnostic module calls this to reset the channel and re-enable channel switching.

See also
rfCoreDiagChannelDisable
Parameters
[in]aChannelThe original channel.

Function documented in radio.h

§ rfCorePriorityCoex()

void rfCorePriorityCoex ( bool  aEnable)

Set the priority value used for CoEx operation.

Enable or Disable the priority signal for RF operations in the coexistence module. This will set the global option for all RF commands to assert the priority line. Assertion polarity is defined by the RF Library module. These options are only used in 3-wire and greater configuration.

Parameters
[in]aEnablesets the Priority signal; true is asserted, false is de-asserted.

Function documented in radio.h

§ rfCoreRequestCoex()

void rfCoreRequestCoex ( bool  aEnable)

Set the request value used for CoEx operation.

Receive operations do not normally assert the request line for CoEx operations. This API sets the global enable/disable of the request during RX. Assertion polarity is defined by the RF Library module. These options are only used in 2-wire and greater configuration.

Parameters
[in]aEnablesets the behavior of the Request signal

Function documented in radio.h

Variable Documentation

§ __RFC_STRUCT_ATTR

struct __RFC_STRUCT short_src_match_data_s __RFC_STRUCT_ATTR
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale