System Performance and Limitations¶
The typical use case for DMM is a smart phone being used to interface with a multi-protocol TI device, such as a CC13xx or CC26xx device, and an application on the smart phone to control or configure the device or a network of devices. Typically the BLE connection is not used for streaming content, but only intermittent information exchange.
DMM Current Limitations¶
The current DMM implementation has the following limitations:
The DMM only supports 2 simultaneous stacks.
The DMM scheduler does NOT pause a stack regardless of the policy settings. When a policy enters a pause state, an application callback is invoked to notify the stack that it should pause its activity. The pause policy should only be used if the application callback has been implemented and registered with DMM.
The DMM has only been tested/characterized with the stack and role combinations covered by the examples provided in the SimpleLink CC13xx/CC26xx SDK.
The DMM does not perform arbitration of peripherals or hardware other than the RF Core. The high level applications must be written in such a way that conflicting access to peripherals is avoided.
The DMM BLE examples are tested for up to four concurrent BLE connections. Please note that connecting to multiple peers over BLE requires more resources (SRAM, radio time).
Protocol Stack Limitations¶
The DMM will attempt to maximize the time domain utilization of the radio while still respecting the constraints of the protocol stacks that are using it. However, unlike CPU scheduling RF commands cannot resume once they have been canceled or preempted. Combining two protocol stacks means that there must be application defined limits of the parameters that can be used by each stack based on what the application needs to operate. Time-synchronous protocols such as BLE further increase these limitations.
For example, assuming a low-priority BLE connection in connected state, the application must make sure that the BLE-Stack is able to operate within the supervision timeout of the connection(s) to avoid disconnecting from the peer device(s).
TI has characterized a subset of possible protocol stack combinations. TI does not guarantee proper operations for other stack combinations. Below is a list of the characterized stack combinations:
BLE5 Peripheral + WSN (EasyLink) Sensor
BLE5 Peripheral + TI 15.4 Collector (all modes)
BLE5 Peripheral + TI 15.4 Sensor (all modes)
BLE5 Peripheral + Zigbee Coordinator
BLE5 Peripheral + Zigbee Router
BLE5 Peripheral + Zigbee End Device
The TI-characterized use cases are available as example projects in the SimpleLink CC13xx/CC26xx SDK. While only a limited subset has been characterized by TI, possible protocol stack combinations are not limited to these.
Before using DMM to combine two arbitrary protocol stacks, a basic analysis should be done to determine the feasibility of said combination:
Do both stacks support DMM, i.e. implement the DMM RF mapping table?
If two instances of one stack are needed, does the stack support multiple instances?
What are the radio requirements of the stack application? Is there enough free radio time to accommodate both stacks?
How will the stacks handle being rejected radio access? What level of rejection is acceptable?
Following the initial feasibility analysis, the use case of each stack should be considered to determine what application states exist for each stack. An initial policy table should then be created based on the defined application states.
In order to optimize the DMM performance for a given set of stacks, the individual stack parameters also need to be tweaked to improve the co-existence of the two stacks. An example of this would be the connection interval and supervision timeout of a BLE5 connection, or the report interval of a WSN Sensor example.
Bit Rate and Transmission Time¶
When choosing a PHY for your stack, the bit rate of that PHY will directly impact the feasibility of the DMM system. The bit rate is proportional to the amount of time required to complete the transmissions, which means a lower bit rate requires the DMM device to use the radio more to complete the transmission.
In some cases it can be useful to calculate the amount of radio time is required to complete a transmission of a given length based on the selected PHY. This could for instance help to decide how long intervals need to be.
Calculating the transmission time requires you to know the PHY protocol data unit (PPDU), which is PHY dependent. In most cases, this includes knowing the preamble length, syncword length, PHY header length, packet length and CRC length. The transmission time is then calculated as the PPDU divided by the bit rate.
End-to-End Stack Reliance and Latency¶
When looking at a given DMM stack combination, it is important to consider the DMM impact on the network’s end-to-end reliance and latency. These factors vary between protocols, stacks and even roles within a stack. Many protocols such as BLE and Zigbee features for example retry logic to prevent data loss due to network instability. The same applies to the TI 15.4-Stack offering.
These features mean that even in the DMM use-case, where for example a BLE peripheral could be starved radio access and suffer in terms if throughput, the end-to-end reliance should remain stable and the packet loss at 0% (as long as the connection is maintained).
While retries might solve potential packet losses when running a DMM system, they will also introduce a (potential) end-to-end latency depending on how many times a packet has to be retried in order to be successful. Please note this latency increase is the same for all packet loss reasons, it is not particular to using DMM.
While, as mentioned above, many protocols and stacks include features to mitigate network issues, it can still be important to consider impact of these in the complete system. In cases where a protocol or stack do not support any such logic, the user is responsible for resending data in case of a DMM preemption or packet loss.
Estimating Throughput¶
Knowing the bit rate and transmission times of the stacks in use, simple calculations can be made to estimate the theoretical throughput for a given stack.
Note
The following section provides equations to calculate a theoretical estimation of the expected throughput. The real-life scenario numbers could be varying depending on factors not included in the theoretical equations.
Internal testing shows that the equations below yields results in line with what is measured with an error margin of roughly 2 %. As such, they can be considered a good way to get an initial overview of how well a certain DMM system might perform.
The following section will assume two stacks, stack A and stack B, are being coordinated by DMM.
The Simple Estimate¶
A simplified average throughput estimation, , for stack A, assumed to be operating at maximum throughput, could be defined as follows:
This assumes that stack B is only sending periodic messages and thus takes up a given part of the available radio bandwidth () given in percent. The radio bandwidth requirement for a particular type of packet is given by the round trip time () of that packet type divided by the packet interval ().
Note
assumes the packet is set to a higher priority than the running stack A command. If the packet is not of higher priority then there will be no impact to the throughput of stack A.
The average throughput of stack A is defined as the ratio of the throughput of the standalone application and the theoretically available radio bandwidth in the DMM use-case. The available radio bandwidth is the remaining radio bandwidth after subtracting the sum of the bandwidth requirement for each packet type in stack B that is of a higher priority than stack A.
This simple estimate has some limitations as it assumes non-absolute scheduling. Non-absolute scheduling corresponds to radio commands that could be delayed by the DMM scheduler as they have no given fixed time to be sent out. In a real use-case, it is likely that both stacks use absolute timing to some degree of the commands.
The Absolute Timing Case¶
In the case of an absolute time conflict between two stacks, there would be an unrecoverable loss of bandwidth that we need to factor into the equation of the radio bandwidth. For this the following assumptions is made:
Stack A, in order to maximize throughput, would resume operations as soon as possible after getting interrupted by an absolute command from stack B
There is an equal chance that stack A is interrupted at any given time of the operation
With these assumptions made, the round trip time of stack A’s interrupted packet is factored in:
The new definition of radio bandwidth assumes that stack A would maximize for throughput. This might not always be the case due to power consumption restrictions. For many protocols, such as BLE, communication is performed on a periodic event basis which allow for lower power consumption of the devices.
The Periodic Event Case¶
Taking BLE as an example, data exchange is limited to the periodic connection events only. To get an estimate in this case, we redefine the radio bandwidth as number of missed events () for stack A divided by the total number of events () that would occur during a conflicting stack B packet. Again, the assumption that only non-absolute scheduling is used which means that stack B would never interrupt an ongoing event:
Note
The use of and refers to the ceiling and floor functions respectively. In this case the ceil value of is used. This means that any partially missed event is counted against the maximum bandwidth.
As previously noted, non-absolute timing might not always be an option and the absolute time would ideally have to be factored in as well. This is however a bit more complicated in the periodic event case as the following needs to be considered:
Stack B finishes the operation before the next periodic event of stack A.
Stack B finish just after stack A has missed the event.
By calculating the probability () of case one and two occurring, the average bandwidth cost could be estimated. This is then used to calculate the average time lost () where the and subscript refers to the cases mentioned above:
In the case of partially missed events, , are not counted towards the time lost. Since stack B is assumed to be finished before stack A’s next event, only the events that are guaranteed to fall inside the period where stack B is active would be missed. For , the partially missed events is counted towards the time lost. This since stack B is assumed to finish after the start of the next stack A event.
As the final average time lost, , is the same as the time not available for stack A, the radio bandwidth is given by:
The expected throughput is then given by our first equation:
Note
As gets smaller, the difference between the non-absolute and absolute versions of the radio bandwidth equation approaches each other.
Warning
All of the equations above are theoretical and some simplification to a stack’s assumed scheduling behavior has been made. In reality there are more limitations then possible to mention as the ultimate behavior depends on the actual behavior of the stacks used as well as the DMM priorities defined in the system.
Because of this, they should ONLY serve as a guideline for what could be expected by a certain stack combination.
Example¶
Assume stack A is working alongside a stack B that sends two type of packets: * 20 byte long packets sent out once every second. * 200 byte long packets sent out once every 10 seconds.
Depending on the scheduling nature of stack A and stack B, different equations would be used. These examples showcase the “simple estimate” and the “periodic event case”. In the “periodic event case” examples are given for both non-absolute and absolute stack B scheduling. In all cases, stack B is considered to be of higher priority having a bit rate of 50 kbps.
In the “simple estimate” example, stack A is assumed to constantly be working to send data out, effectively filling up any remaining bandwidth. It is also assumed that stack B is using non-absolute scheduling:
For the “periodic event case” examples, it is assumed that stack A is instead the BLE stack with a connection event interval set to 100 ms. In the first example it is assumed that stack B is using non-absolute scheduling:
The second “periodic event case” example assumes that stack B is using absolute scheduling. Stack A is assumed to be the same as in the first “periodic event case”:
In all the examples, it is clear that stack B is not interfering to much with stack A as it does not use up much of the radio bandwidth. It can however be seen that the expected throughput goes down as the assumption on how stack A access the radio changes from freely polling the radio to be bound to a given interval.
Long Range Mode (LRM) PHY Considerations¶
When a stack operates with the SimpleLink LRM PHY, the radio timing often increases significantly as the bit rate is much lower. For example, the TI 15.4 default sensor data + MAC Ack require approximately 200 ms of radio time to complete.
If the stack operating in LRM is considered lower priority in the context of DMM, this has to be taking into considerations when setting up the radio interval of the high priority stack to avoid starving the stack using LRM.
A practical example is when combining TI 15.4 together with the BLE-Stack, where the advertising and connection interval must be chosen to allow time slots big enough for the TI 15.4-Stack to operate.
Adjusting the BLE Connection Interval¶
The BLE peripheral is not able to directly control the connection interval; it may, however, request a connection parameter update to the central device.
For more information about the connection parameter update process, refer to the Generic Access Profile (GAP) Section in the BLE5-Stack User’s Guide. In the GAP chapter there is a section that covers the connection parameter update process and the APIs needed to perform one.
Multiple BLE Connections¶
The maximum number of BLE connections can be set in SysConfig -> RF STACKS -> BLE -> General Configuration -> Max Number of Connections. DMM examples are tested with up to four BLE connections.
In the BLE5-Stack User’s Guide you can read more about how the BLE-Stack handles and prioritizes multiple connections. Please see the Link Layer chapter.
It is recommended to set the Max Number of Connections
as low as possible.
This is because the BLE-Stack will allocate a unique Rx/Tx packet buffer per
connection from the ICall heap. Per default this buffer is around 1 kB. You can
read about these buffers in the BLE5-Stack User’s Guide, in the Link Layer
Buffers section.
If you choose to use multiple BLE connections, please remember that each connection takes the same amount of resources as the first one. The DMM scheduler will have to schedule twice as many BLE connection events etc. Please consider how this will affect the other RF protocol stack running in your project.