DMM API Reference  4.10.00.01
DMMPolicy_CurrentInfo Struct Reference

Policy Information dynamically updated. More...

#include <dmm_policy.h>

Public Attributes

uint32_t stackID
 ID to define the stack using current policy.
 
uint8_t currentWeight
 The current weight value of the policy.
 
uint8_t defaultPriority
 The default priority of the policy.
 

Detailed Description

Policy Information dynamically updated.


The documentation for this struct was generated from the following file: