Data Fields
EDDSACC26X2_Workspace Struct Reference

EDDSACC26X2 Workspace. More...

#include <EDDSACC26X2.h>

Data Fields

uint8_t digestResult [SHA2_DIGEST_LENGTH_BYTES_512]
 
uint8_t digestResult2 [SHA2_DIGEST_LENGTH_BYTES_512]
 
uint8_t publicKey [32]
 
uint8_t secretScalar [32]
 
uint8_t xResult [32]
 
uint8_t yResult [32]
 
uint8_t x_0
 

Detailed Description

EDDSACC26X2 Workspace.

Holds intermediate memory to perform Ed25519 operations. Unlike PKA SRAM, these values can be easily accessed or modified.

Field Documentation

§ digestResult

uint8_t EDDSACC26X2_Workspace::digestResult[SHA2_DIGEST_LENGTH_BYTES_512]

§ digestResult2

uint8_t EDDSACC26X2_Workspace::digestResult2[SHA2_DIGEST_LENGTH_BYTES_512]

§ publicKey

uint8_t EDDSACC26X2_Workspace::publicKey[32]

§ secretScalar

uint8_t EDDSACC26X2_Workspace::secretScalar[32]

§ xResult

uint8_t EDDSACC26X2_Workspace::xResult[32]

§ yResult

uint8_t EDDSACC26X2_Workspace::yResult[32]

§ x_0

uint8_t EDDSACC26X2_Workspace::x_0

The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale