![]() |
![]() |
Z-Stack API Reference
6.10.00.04
|
#include <zstack.h>
Data Fields | |
uint32_t | bdbSecondaryChannelSet |
bool | has_bdbSecondaryChannelSet |
uint32_t | bdbPrimaryChannelSet |
bool | has_bdbPrimaryChannelSet |
uint16_t | bdbCommissioningGroupID |
bool | has_bdbCommissioningGroupID |
uint8_t | bdbScanDuration |
bool | has_bdbScanDuration |
Structure to send a BDB Set Attributes Request. Each config field has 2 parts to it, the actual value field and its "has_" field. The "has_" field must be set to "true" for the value field to be valid. For example, the pollRate field is valid only if the has_pollRate field is set to true.
uint16_t bdbCommissioningGroupID |
Group ID for Finding and Binding
uint32_t bdbPrimaryChannelSet |
Primary Channel Set
uint8_t bdbScanDuration |
Scan Duration
uint32_t bdbSecondaryChannelSet |
Secondary Channel Set
bool has_bdbCommissioningGroupID |
Set to true if bdbCommissioningGroupID is available, false if not
bool has_bdbPrimaryChannelSet |
Set to true if bdbPrimaryChannelSet is available, false if not
bool has_bdbScanDuration |
Set to true if bdbScanDuration is available, false if not
bool has_bdbSecondaryChannelSet |
Set to true if bdbSecondaryChannelSet is available, false if not