Z-Stack API Reference  6.10.00.04
_zstack_zdodeviceannounceind_t Struct Reference

#include <zstack.h>

Data Fields

uint16_t srcAddr
 Source address.
 
uint16_t devAddr
 Device short address.
 
zstack_LongAddr_t devExtAddr
 Devices IEEE Address (64-bit)
 
zstack_CapabilityInfo_t capInfo
 Device's Capabilities.
 

Detailed Description

Structure to send a ZDO Device Announce Indication.


The documentation for this struct was generated from the following file: