Z-Stack API Reference  6.10.00.04
_zstack_zdomgmtnwkdiscrspind_t Struct Reference

#include <zstack.h>

Data Fields

uint16_t srcAddr
 Source address.
 
zstack_ZdpStatus status
 Response status.
 
uint8_t networkCount
 The total number of networks reported.
 
uint8_t startIndex
 The starting point in the networkList.
 
uint8_t n_netList
 Number of items in the netList.
 
zstack_nwkDiscItem_tpNetList
 Array of networks.
 

Detailed Description

Structure to send a ZDO Mgmt Network Discovery Response Indication.


The documentation for this struct was generated from the following file: