Z-Stack API Reference  6.10.00.04
gpCommissioningNotificationCmd_t Struct Reference

Data Fields

uint16_t options
 Notification command. More...
 
uint32_t gpdId
 ID of the GPD.
 
uint8_t gpdIEEE [Z_EXTADDR_LEN]
 IEEE of the GPD if application ID is 0b010.
 
uint8_t ep
 Endpoint of the GP if application ID is 0b010.
 
uint32_t gpdSecCounter
 The security frame counter.
 
uint8_t cmdId
 Command ID.
 
uint8_t payloadLen
 Command payload length.
 
uint8_t * cmdPayload
 Command payolad.
 
uint16_t gppShortAddr
 Notification. More...
 
uint8_t gppGpdLink
 Link quality of between the GPD and GPP.
 
uint32_t mic
 Security MIC.
 

Field Documentation

§ gppShortAddr

uint16_t gppShortAddr

Notification.

Address of the GPP that generates the

§ options

uint16_t options

Notification command.

Options field of the GP Commissioning


The documentation for this struct was generated from the following file: