![]() |
![]() |
Z-Stack API Reference
6.10.00.04
|
Data Fields | |
uint8_t | zoneStatusComplete |
uint8_t | numberOfZones |
Number of zones in the payload. | |
zclACEZoneStatus_t * | zoneInfo |
List of zones. The number of zones is defined by numberOfZones. | |
uint8_t zoneStatusComplete |
Indicates whether there are additional Zone IDs managed by the IAS ACE Server with Zone Status information to be obtained.