Z-Stack API Reference  6.10.00.04
zclACEPanelStatusChanged_t Struct Reference

Data Fields

uint8_t panelStatus
 Panel Status enumeration.
 
uint8_t secondsRemaining
 Remaining time in seconds.
 
uint8_t audibleNotification
 
uint8_t alarmStatus
 

Field Documentation

§ alarmStatus

uint8_t alarmStatus

Provides the ACE client with information on the type of alarm the panel is in if its Panel Status field indicates it is "in alarm."

§ audibleNotification

uint8_t audibleNotification

Provide the ACE client with information on which type of audible notification it SHOULD make for the zone status change.


The documentation for this struct was generated from the following file: