![]() |
![]() |
Z-Stack API Reference
6.10.00.04
|
Client Commands Received: Operation Event Notification. More...
#include <zcl_closures.h>
Data Fields | |
uint8_t | operationEventSource |
This field indicates where the event was triggered from. | |
uint8_t | operationEventCode |
significant operational event on the lock. | |
uint16_t | userID |
The User ID who performed the event. | |
uint8_t | pin |
ID who performed the event. More... | |
uint32_t | zigBeeLocalTime |
The LocalTime that indicates when the event is triggered. | |
uint8_t * | pData |
The operation event notification command contains a variable string. | |
Client Commands Received: Operation Event Notification.
uint8_t pin |
ID who performed the event.
The PIN that is associated with the User .