Z-Stack API Reference  6.10.00.04
zclLocation_t Struct Reference

Data Fields

afAddrType_t * srcAddr
 requestor's address
 
uint8_t cmdID
 COMMAND_LOCATION_GET_DEV_CFG or COMMAND_LOCATION_GET_DATA. More...
 
union {
   zclLocationAbsolute_t   absLoc
 Absolute Location info (only valid for COMMAND_LOCATION_SET_ABSOLUTE)
 
   zclLocationGetData_t   loc
 Get Location info (only valid for COMMAND_LOCATION_GET_DATA)
 
   zclLocationDevCfg_t   devCfg
 Device Config info (only valid for COMMAND_LOCATION_SET_DEV_CFG)
 
   uint8_t *   ieeeAddr
 Device's IEEE Addr (only valid for COMMAND_LOCATION_GET_DEV_CFG)
 
un
 
uint8_t seqNum
 Sequence number received with the message (only valid for GET commands)
 

Field Documentation

§ cmdID

uint8_t cmdID

COMMAND_LOCATION_GET_DEV_CFG or COMMAND_LOCATION_GET_DATA.

COMMAND_LOCATION_SET_ABSOLUTE, COMMAND_LOCATION_SET_DEV_CFG,


The documentation for this struct was generated from the following file: