Z-Stack API Reference  6.10.00.04
zclZoneEnrollReq_t Struct Reference

Data Fields

afAddrType_t * srcAddr
 initiator's address
 
uint8_t zoneID
 allocated zone ID
 
uint16_t zoneType
 current value of Zone Type attribute
 
uint16_t manufacturerCode
 manufacturer Code from node descriptor for the device
 

The documentation for this struct was generated from the following file: