SimpleLink CC13xx/CC26xx SDK Overview¶
The SimpleLink™ CC13xx and CC26xx Software Development Kit provides a complete package for the development of BLE, Sub-1 GHz,Zigbee, Thread, and IEEE™ 802.15.4 based applications for the CC13xx or CC26xx wireless microcontroller.
Introduction to the CC13xx and CC26xx¶
This kit is based on the SimpleLink CC13xx and CC26xx which is optimized for ultra-low power while providing fast and capable MCU systems to enable short processing times and high integration. The CC13xx or CC26xx device combines a sub-1/2.4 GHz RF transceiver with a full range of peripherals and the following memory options.
Device |
Flash (kB) |
SRAM (kB) |
CC2672x3, CC13x2x1, or CC26x2x1 |
352 |
80 |
CC13x2x7 or CC26x2x7 |
704 |
144 |
CC13x1x3 or CC26x1x3 |
352 |
40 |
The CC13xx or CC26xx device is centered on an Arm® Cortex®-M4F series processor, that executes the user application and stack code, and an autonomous radio core centered on an Arm Cortex-M0 processor, which handles all the low-level radio control. The sensor controller block provides additional flexibility by allowing autonomous data acquisition and control independent of the Cortex-M4F processor core, which further extends the low-power capabilities of the CC13xx or CC26xx device.
The CC13xx or CC26xx LaunchPad kit supports programming and debugging from CCS and IAR Embedded Workbench® integrated development environments (IDEs).
Introduction to the SimpleLink CC13xx/CC26xx SDK¶
TI’s royalty-free SimpleLink CC13xx/CC26xx SDK is a complete software platform for developing applications that require low-power, security, reliability, and mesh networking. The CC13xx and CC26xx devices are part of the SimpleLink™ MCU platform which consists of Wi-Fi®, Bluetooth® Low Energy, Sub-1 GHz, Thread, Zigbee, IEEE 802.15.4 and host MCUs, which all share a common, easy-to-use development environment and rich tool set. A one-time integration of the SimpleLink™ platform enables you to add any combination of the portfolio’s devices into your design, allowing 100 percent code reuse when your design requirements change. For more information, visit the SimpleLink™ Solutions Overview.
Solution Platform¶
This section describes the various components that are installed with the SimpleLink CC13xx/CC26xx SDK, the directory structure of the protocol stack, and any tools required for development.
The following components are included in the solution platform:
Real-time operating system (RTOS) with the TI-RTOS™ SYS/BIOS kernel, optimized power management support, and peripheral drivers.
The driverLib provides a register abstraction layer that is used by software and drivers to control the CC13xx or CC26xx MCU.
TI-Drivers are a set of RTOS aware drivers designed to allow seemless use of CC13xx or CC26xx peripherals inside your application.
Example applications make the beginning stages of development easier. Example applications are provided for the CC13xx or CC26xx platform
Directory Structure¶
The SimpleLink CC13xx/CC26xx SDK directory structure is broken down into a few major directories at the root to allow easy differentiation between documentation, examples, kernel source, and other source code. From the root directory, the sub-directories are:
- docs
Contains HTML and PDF documentation for the SimpleLink CC13xx/CC26xx SDK.
- examples
Contains the example projects and example source for this SimpleLink CC13xx/CC26xx SDK.
- kernel
Contains the source and build tools for the kernels supported by this SimpleLink CC13xx/CC26xx SDK.
- source
Contains the source code for the larger components of the SimpleLink CC13xx/CC26xx SDK. A more detailed description of this directory follows.
- tools
Scripts and definition files used by the SimpleLink CC13xx/CC26xx SDK. Contains scripts referenced by the SimpleLink CC13xx/CC26xx SDK documentation.
The source directory is split into major categories based on where the source
code came from. All of the source code within the third_party
directory
comes from vendors other than Texas Instruments. All of the source code within
the ti
directory comes from Texas Instruments.
- ti\boards
Contains the board hardware configurations.
- ti\devices
Contains the board support source code.
- ti\display
Contains the source code for the display libraries.
- ti\drivers
Contains the source code for the TI-RTOS drivers.
- ti\grlib
Contains the source code for the graphics libraries.
End Production Development Architecture Choices¶
Protocol Stack and Application Configurations¶
Figure 21. shows the two different system architectures enabled by Z-Stack.
A single device is shown in Figure 21. (left). The application and protocol stack are both implemented on the CC13xx or CC26xx as a true single-chip solution. This configuration is the simplest and most common when using the CC13xx or CC26xx for network nodes and also using the CC13xx or CC26xx as a personal area network (PAN) coordinator node. This configuration is the most cost-effective technique and provides the best power performance.
A coprocessor is shown in Figure 21. (right). The protocol stack runs on the CC13xx or CC26xx while the application is executed on an external MPU or MCU. The application interfaces with the CC13xx or CC26xx using the network protocol interface (NPI) over a serial universal asynchronous receiver/transmitter (UART) connection. The description of the API interface is provided in the ZNP Interface Guide. This configuration is useful for applications that require long-range wireless connectivity or peripheral applications, which execute on another device (such as an external MCU) or on a PC without the requirement to implement the complexities associated with a wireless networking protocol. As well for implementing the Feature rich gateway applications e.g. on Linux host. In these cases, the application can be developed externally on a host processor while running Z-Stack on the CC13xx or CC26xx, which provides ease of development and quickly adds Zigbee wireless connectivity to existing products.