AESCBCCC26X4_s.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2022 Texas Instruments Incorporated - http://www.ti.com
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33 #ifndef ti_drivers_aescbc_AESCBCCC26X4_s__include
34 #define ti_drivers_aescbc_AESCBCCC26X4_s__include
35 
36 #include <stdint.h>
37 
39 #include <ti/drivers/AESCBC.h>
40 
41 #include <ti/sysbios/psa/SecureCB.h>
42 
43 #include <third_party/tfm/interface/include/psa/crypto_types.h>
44 #include <third_party/tfm/interface/include/psa/service.h>
45 
46 #include "ti_drivers_config.h" /* Sysconfig generated header */
47 
48 #ifdef __cplusplus
49 extern "C" {
50 #endif
51 
52 /*
53  * AES CBC secure message types
54  *
55  * Non-secure clients must register their callback after opening or
56  * constructing a driver instance with blocking or callback return behavior.
57  */
58 #define AESCBC_S_MSG_TYPE_CONSTRUCT (CRYPTO_S_MSG_TYPE_INDEX_AESCBC | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 0U)))
59 #define AESCBC_S_MSG_TYPE_OPEN (CRYPTO_S_MSG_TYPE_INDEX_AESCBC | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 1U)))
60 #define AESCBC_S_MSG_TYPE_REGISTER_CALLBACK \
61  (CRYPTO_S_MSG_TYPE_INDEX_AESCBC | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 2U)))
62 #define AESCBC_S_MSG_TYPE_CLOSE (CRYPTO_S_MSG_TYPE_INDEX_AESCBC | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 3U)))
63 #define AESCBC_S_MSG_TYPE_ONE_STEP_ENCRYPT \
64  (CRYPTO_S_MSG_TYPE_INDEX_AESCBC | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 4U)))
65 #define AESCBC_S_MSG_TYPE_ONE_STEP_DECRYPT \
66  (CRYPTO_S_MSG_TYPE_INDEX_AESCBC | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 5U)))
67 #define AESCBC_S_MSG_TYPE_SETUP_ENCRYPT \
68  (CRYPTO_S_MSG_TYPE_INDEX_AESCBC | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 6U)))
69 #define AESCBC_S_MSG_TYPE_SETUP_DECRYPT \
70  (CRYPTO_S_MSG_TYPE_INDEX_AESCBC | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 7U)))
71 #define AESCBC_S_MSG_TYPE_SET_IV (CRYPTO_S_MSG_TYPE_INDEX_AESCBC | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 8U)))
72 #define AESCBC_S_MSG_TYPE_ADD_DATA (CRYPTO_S_MSG_TYPE_INDEX_AESCBC | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 9U)))
73 #define AESCBC_S_MSG_TYPE_FINALIZE (CRYPTO_S_MSG_TYPE_INDEX_AESCBC | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 10U)))
74 #define AESCBC_S_MSG_TYPE_CANCEL_OPERATION \
75  (CRYPTO_S_MSG_TYPE_INDEX_AESCBC | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 11U)))
76 
77 /*
78  * Config pool size determines how many dynamic driver instances can be created
79  * by the non-secure client using AESCBC_construct().
80  */
81 #ifndef CONFIG_AESCBC_S_CONFIG_POOL_SIZE
82  #define CONFIG_AESCBC_S_CONFIG_POOL_SIZE 1
83 #endif
84 
85 #define AESCBC_SECURE_CALLBACK_COUNT (CONFIG_TI_DRIVERS_AESCBC_COUNT + CONFIG_AESCBC_S_CONFIG_POOL_SIZE)
86 
87 /*
88  * ========= AES CBC Secure Callback struct =========
89  */
90 typedef struct
91 {
92  SecureCB_Object object;
93  /* AES CBC callback fxn parameters */
95  int_fast16_t returnValue;
99 
100 /*
101  * ========= AES CBC Secure Message Structs =========
102  * These secure message structs correspond to the secure message types defined
103  * above. Together, they are used by non-secure client to make PSA calls to the
104  * AES CBC secure service. There is a single input vector for the PSA call
105  * which is a pointer to secure message struct. If the underlying function
106  * has a return value, there is a single output vector which is a pointer to
107  * storage for the return value.
108  */
109 typedef struct
110 {
114 
115 typedef struct
116 {
117  uint_least8_t index;
120 
121 typedef struct
122 {
126 
127 typedef struct
128 {
131 
132 typedef struct
133 {
137 
138 typedef struct
139 {
141  const CryptoKey *key;
143 
144 typedef struct
145 {
147  const uint8_t *iv;
148  size_t ivLength;
150 
151 typedef struct
152 {
156 
158 
159 typedef struct
160 {
163 
174 psa_status_t AESCBC_s_handlePsaMsg(psa_msg_t *msg);
175 
181 void AESCBC_s_init(void);
182 
183 #ifdef __cplusplus
184 }
185 #endif
186 
187 #endif /* ti_drivers_aescbc_AESCBCCC26X4_s__include */
AESCBC driver header.
AESCBC_Handle handle
Definition: AESCBCCC26X4_s.h:161
Definition: AESCBCCC26X4_s.h:132
Definition: AESCBCCC26X4_s.h:151
AESCBC_Handle handle
Definition: AESCBCCC26X4_s.h:146
AES Global configuration.
Definition: AESCommon.h:154
const CryptoKey * key
Definition: AESCBCCC26X4_s.h:141
CryptoKey datastructure.
Definition: CryptoKey.h:192
size_t ivLength
Definition: AESCBCCC26X4_s.h:148
Definition: AESCBCCC26X4_s.h:121
AESCBC_Handle handle
Definition: AESCBCCC26X4_s.h:140
AESCBC_Config * config
Definition: AESCBCCC26X4_s.h:111
SecureCB_Object object
Definition: AESCBCCC26X4_s.h:92
Definition: AESCBCCC26X4_s.h:90
const uint8_t * iv
Definition: AESCBCCC26X4_s.h:147
AESCBC_s_AddDataMsg AESCBC_s_FinalizeMsg
Definition: AESCBCCC26X4_s.h:157
Struct containing the parameters required for encrypting/decrypting a message in a segmented operatio...
Definition: AESCBC.h:770
Secure Crypto Service.
AESCBC_Handle handle
Definition: AESCBCCC26X4_s.h:153
Struct containing the parameters required for encrypting/decrypting a message in a single-step operat...
Definition: AESCBC.h:730
Definition: AESCBCCC26X4_s.h:159
AESCBC_s_SecureCallback * callback
Definition: AESCBCCC26X4_s.h:124
AESCBC_Handle handle
Definition: AESCBCCC26X4_s.h:94
Definition: AESCBCCC26X4_s.h:115
int_fast16_t returnValue
Definition: AESCBCCC26X4_s.h:95
Definition: AESCBCCC26X4_s.h:109
AESCBC_OperationUnion * operation
Definition: AESCBCCC26X4_s.h:96
Definition: AESCBCCC26X4_s.h:127
const AESCBC_Params * params
Definition: AESCBCCC26X4_s.h:118
AESCBC_OperationType
Enum for the operation types supported by the driver.
Definition: AESCBC.h:815
AESCBC_OperationType operationType
Definition: AESCBCCC26X4_s.h:97
Union containing a reference to a one step or segmented operation.
Definition: AESCBC.h:806
uint_least8_t index
Definition: AESCBCCC26X4_s.h:117
AESCBC_Handle handle
Definition: AESCBCCC26X4_s.h:134
void AESCBC_s_init(void)
Initializes the AES CBC secure driver.
psa_status_t AESCBC_s_handlePsaMsg(psa_msg_t *msg)
Handles PSA messages for AES CBC secure driver.
AESCBC_Handle handle
Definition: AESCBCCC26X4_s.h:129
AESCBC_OneStepOperation * operation
Definition: AESCBCCC26X4_s.h:135
Definition: AESCBCCC26X4_s.h:138
CBC Parameters.
Definition: AESCBC.h:856
Definition: AESCBCCC26X4_s.h:144
AESCBC_Handle handle
Definition: AESCBCCC26X4_s.h:123
AESCBC_SegmentedOperation * operation
Definition: AESCBCCC26X4_s.h:154
const AESCBC_Params * params
Definition: AESCBCCC26X4_s.h:112
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale