![]() |
![]() |
Holder of common helper functions for the Timer driver.
============================================================================
Go to the source code of this file.
Functions | |
void | TimerSupport_timerDisable (Timer_Handle handle) |
Function to disable the timer peripheral. More... | |
void | TimerSupport_timerEnable (Timer_Handle handle) |
Function to enable the timer peripheral. More... | |
bool | TimerSupport_timerFullWidth (Timer_Handle handle) |
Function to determine if timer is full-width. More... | |
void | TimerSupport_timerLoad (Timer_Handle handle) |
Function to load timer peripheral. More... | |
void TimerSupport_timerDisable | ( | Timer_Handle | handle | ) |
Function to disable the timer peripheral.
[in] | handle | A Timer_Handle returned from Timer_open() |
void TimerSupport_timerEnable | ( | Timer_Handle | handle | ) |
Function to enable the timer peripheral.
[in] | handle | A Timer_Handle returned from Timer_open() |
bool TimerSupport_timerFullWidth | ( | Timer_Handle | handle | ) |
Function to determine if timer is full-width.
[in] | handle | A Timer_Handle returned from Timer_open() |
void TimerSupport_timerLoad | ( | Timer_Handle | handle | ) |
Function to load timer peripheral.
[in] | handle | A Timer_Handle returned from Timer_open() |