![]() |
![]() |
ECDSACC26X2 Object. More...
#include <ECDSACC26X2.h>
Data Fields | |
TRNG_Config | trngConfig |
TRNGCC26XX_Object | trngObject |
TRNGCC26XX_HWAttrs | trngHwAttrs |
TRNG_Handle | trngHandle |
bool | isOpen |
bool | operationInProgress |
bool | operationCanceled |
int_fast16_t | operationStatus |
ECDSA_Operation | operation |
ECDSA_OperationType | operationType |
ECDSA_CallbackFxn | callbackFxn |
ECDSACC26X2_stateMachineFxn | fsmFxn |
ECDSA_ReturnBehavior | returnBehavior |
ECDSACC26X2_FsmState | fsmState |
uint32_t | semaphoreTimeout |
uint32_t | resultAddress |
uint32_t * | scratchNumber1 |
uint32_t * | scratchNumber2 |
CryptoKey | pmsnKey |
ECDSACC26X2 Object.
The application must not access any member variables of this structure!
TRNG_Config ECDSACC26X2_Object::trngConfig |
TRNGCC26XX_Object ECDSACC26X2_Object::trngObject |
TRNGCC26XX_HWAttrs ECDSACC26X2_Object::trngHwAttrs |
TRNG_Handle ECDSACC26X2_Object::trngHandle |
bool ECDSACC26X2_Object::isOpen |
bool ECDSACC26X2_Object::operationInProgress |
bool ECDSACC26X2_Object::operationCanceled |
int_fast16_t ECDSACC26X2_Object::operationStatus |
ECDSA_Operation ECDSACC26X2_Object::operation |
ECDSA_OperationType ECDSACC26X2_Object::operationType |
ECDSA_CallbackFxn ECDSACC26X2_Object::callbackFxn |
ECDSACC26X2_stateMachineFxn ECDSACC26X2_Object::fsmFxn |
ECDSA_ReturnBehavior ECDSACC26X2_Object::returnBehavior |
ECDSACC26X2_FsmState ECDSACC26X2_Object::fsmState |
uint32_t ECDSACC26X2_Object::semaphoreTimeout |
uint32_t ECDSACC26X2_Object::resultAddress |
uint32_t* ECDSACC26X2_Object::scratchNumber1 |
uint32_t* ECDSACC26X2_Object::scratchNumber2 |
CryptoKey ECDSACC26X2_Object::pmsnKey |