Data Fields
PDMCC26XX_HWAttrs Struct Reference

PDMCC26XX Hardware attributes. More...

#include <PDMCC26XX.h>

Data Fields

uint32_t micPower
 
int taskPriority
 

Detailed Description

PDMCC26XX Hardware attributes.

These fields are used by the PDM driver

Field Documentation

§ micPower

uint32_t PDMCC26XX_HWAttrs::micPower

Microphone power pin

§ taskPriority

int PDMCC26XX_HWAttrs::taskPriority

PDM task priority pin


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale