rflib
Data Fields
rfc_CMD_DISABLE_RAT_CH_s Struct Reference

Disable Radio Timer Channel. More...

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0408. More...
 
uint8_t ratCh
 The radio timer channel number. More...
 

Detailed Description

Disable Radio Timer Channel.

Field Documentation

§ commandNo

uint16_t rfc_CMD_DISABLE_RAT_CH_s::commandNo

The command ID number 0x0408.

§ ratCh

uint8_t rfc_CMD_DISABLE_RAT_CH_s::ratCh

The radio timer channel number.


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale