rflib
Data Fields
rfc_CMD_SET_TX20_POWER_s Struct Reference

Set Transmit Power for 20-dBm PA. More...

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0014. More...
 
uint16_t __dummy0
 
uint32_t tx20Power
 New TX power setting. More...
 

Detailed Description

Set Transmit Power for 20-dBm PA.

Field Documentation

§ commandNo

uint16_t rfc_CMD_SET_TX20_POWER_s::commandNo

The command ID number 0x0014.

§ __dummy0

uint16_t rfc_CMD_SET_TX20_POWER_s::__dummy0

§ tx20Power

uint32_t rfc_CMD_SET_TX20_POWER_s::tx20Power

New TX power setting.


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale