Set New Synthesizer Frequency without Recalibration (Deprecated; use CMD_MODIFY_FS)
More...
#include <rf_common_cmd.h>
Set New Synthesizer Frequency without Recalibration (Deprecated; use CMD_MODIFY_FS)
§ commandNo
uint16_t rfc_CMD_UPDATE_FS_s::commandNo |
The command ID number 0x0011.
§ __dummy0
uint16_t rfc_CMD_UPDATE_FS_s::__dummy0 |
§ __dummy1
uint32_t rfc_CMD_UPDATE_FS_s::__dummy1 |
§ __dummy2
uint32_t rfc_CMD_UPDATE_FS_s::__dummy2 |
§ __dummy3
uint16_t rfc_CMD_UPDATE_FS_s::__dummy3 |
§ frequency
uint16_t rfc_CMD_UPDATE_FS_s::frequency |
The frequency in MHz to tune to.
§ fractFreq
uint16_t rfc_CMD_UPDATE_FS_s::fractFreq |
Fractional part of the frequency to tune to.
The documentation for this struct was generated from the following file: