CC26xx Driver Library
[aux_adc.h] AUX Analog to Digital Converter

Functions

void AUXADCDisable (void)
 Disables the ADC. More...
 
void AUXADCEnableAsync (uint32_t refSource, uint32_t trigger)
 Enables the ADC for asynchronous operation. More...
 
void AUXADCEnableSync (uint32_t refSource, uint32_t sampleTime, uint32_t trigger)
 Enables the ADC for synchronous operation. More...
 
void AUXADCEnableSyncNoBugWorkaround (uint32_t refSource, uint32_t sampleTime, uint32_t trigger)
 Enables the ADC for synchronous operation. More...
 
void AUXADCDisableInputScaling (void)
 Disables scaling of the ADC input. More...
 
void AUXADCFlushFifo (void)
 Flushes the ADC FIFO. More...
 
static void AUXADCGenManualTrigger (void)
 Generates a single manual ADC trigger. More...
 
static uint32_t AUXADCGetFifoStatus (void)
 Returns flags indicating the status of the ADC FIFO. More...
 
uint32_t AUXADCReadFifo (void)
 Waits for and returns the first sample in the ADC FIFO. More...
 
uint32_t AUXADCPopFifo (void)
 Returns the first sample in the ADC FIFO, without waiting. More...
 
static void AUXADCSelectInput (uint32_t input)
 Selects internal or external input for the ADC. More...
 
int32_t AUXADCGetAdjustmentGain (uint32_t refSource)
 Returns the gain value used when adjusting for ADC gain/offset. More...
 
int32_t AUXADCGetAdjustmentOffset (uint32_t refSource)
 Returns the offset value used when adjusting for ADC gain/offset. More...
 
int32_t AUXADCValueToMicrovolts (int32_t fixedRefVoltage, int32_t adcValue)
 Converts an "adjusted" ADC value to microvolts. More...
 
int32_t AUXADCMicrovoltsToValue (int32_t fixedRefVoltage, int32_t microvolts)
 Converts a number of microvolts to corresponding "adjusted" ADC value. More...
 
int32_t AUXADCAdjustValueForGainAndOffset (int32_t adcValue, int32_t gain, int32_t offset)
 Performs ADC value gain and offset adjustment. More...
 
int32_t AUXADCUnadjustValueForGainAndOffset (int32_t adcValue, int32_t gain, int32_t offset)
 Performs the inverse of the ADC value gain and offset adjustment. More...
 

Detailed Description

Function Documentation

§ AUXADCAdjustValueForGainAndOffset()

int32_t AUXADCAdjustValueForGainAndOffset ( int32_t  adcValue,
int32_t  gain,
int32_t  offset 
)

Performs ADC value gain and offset adjustment.

This function takes a measured ADC value compensates for the internal gain and offset in the ADC.

Parameters
adcValue12-bit ADC unadjusted value
gainGain adjustment value provided by AUXADCGetAdjustmentGain()
offsetOffset adjustment value provided by AUXADCGetAdjustmentOffset()
Returns
12-bit ADC adjusted value

Referenced by AUXADCSelectInput().

337 {
338  // Apply gain and offset adjustment
339  adcValue = (((adcValue + offset) * gain) + 16384) / 32768;
340 
341  // Saturate
342  if (adcValue < 0) {
343  return 0;
344  } else if (adcValue > 4095) {
345  return 4095;
346  } else {
347  return adcValue;
348  }
349 }

§ AUXADCDisable()

void AUXADCDisable ( void  )

Disables the ADC.

This function must be called:

88 {
89  // Disable the ADC reference
90  ADI8BitsClear(AUX_ADI4_BASE, ADI_4_AUX_O_ADCREF0, ADI_4_AUX_ADCREF0_EN_M | ADI_4_AUX_ADCREF0_REF_ON_IDLE_M | ADI_4_AUX_ADCREF0_SRC_M);
91 
92  // Assert reset and disable the ADC
93  ADI8BitsClear(AUX_ADI4_BASE, ADI_4_AUX_O_ADC0, ADI_4_AUX_ADC0_EN_M | ADI_4_AUX_ADC0_RESET_N_M | ADI_4_AUX_ADC0_SMPL_MODE_M | ADI_4_AUX_ADC0_SMPL_CYCLE_EXP_M);
94 
95  // Ensure that scaling is enabled by default before next use of the ADC
96  ADI8BitsClear(AUX_ADI4_BASE, ADI_4_AUX_O_ADC1, ADI_4_AUX_ADC1_SCALE_DIS_M);
97 
98  // Flush the FIFO before disabling the clocks
99  HWREGBITW(AUX_ANAIF_BASE + AUX_ANAIF_O_ADCCTL, 1) = 1; // CMD: EN(1) -> FLUSH(3)
100  HWREGBITW(AUX_ANAIF_BASE + AUX_ANAIF_O_ADCCTL, 1) = 0; // CMD: FLUSH(3) -> EN(1)
101 
102  // Disable the ADC clock (no need to wait since IOB_WUC_ADCCLKCTL_ACK goes low immediately)
103  HWREG(AUX_SYSIF_BASE + AUX_SYSIF_O_ADCCLKCTL) = 0;
104 
105  // Disable the ADC data interface
106  HWREG(AUX_ANAIF_BASE + AUX_ANAIF_O_ADCCTL) = 0;
107 }
static void ADI8BitsClear(uint32_t ui32Base, uint32_t ui32Reg, uint8_t ui8Val)
Clear specific bits in an 8 bit ADI register.
Definition: adi.h:512
Here is the call graph for this function:

§ AUXADCDisableInputScaling()

void AUXADCDisableInputScaling ( void  )

Disables scaling of the ADC input.

By default, the ADC operates internally on a version of the input signal that has been scaled down by a factor 1408 / 4095. This function disables that scaling, allowing for a trade-off between dynamic range and and resolution.

Note
This function must only be called while the ADC is disabled, before calling AUXADCEnableSync() or AUXADCEnableAsync().
Different input maximum ratings apply when input scaling is disabled. Violating these may damage the device.
221 {
222  ADI8BitsSet(AUX_ADI4_BASE, ADI_4_AUX_O_ADC1, ADI_4_AUX_ADC1_SCALE_DIS_M);
223 }
static void ADI8BitsSet(uint32_t ui32Base, uint32_t ui32Reg, uint8_t ui8Val)
Set specific bits in a single 8 bit ADI register.
Definition: adi.h:371
Here is the call graph for this function:

§ AUXADCEnableAsync()

void AUXADCEnableAsync ( uint32_t  refSource,
uint32_t  trigger 
)

Enables the ADC for asynchronous operation.

In asynchronous operation, the ADC samples continuously between conversions.

The ADC trigger starts the conversion. Note that the first conversion may be invalid if the sampling period is too short.

ADC input scaling is enabled by default after device reset, and is also re- enabled by AUXADCDisable(). To disable input scaling, call AUXADCDisableInputScaling() before calling AUXADCEnableAsync().

Parameters
refSourceADC reference source:
triggerADC conversion trigger:
116 {
117  // Enable the ADC reference, with the following options:
118  // - SRC: Set when using relative reference
119  // - REF_ON_IDLE: Always cleared since there is no idle state in asynchronous operation
120  ADI8BitsSet(AUX_ADI4_BASE, ADI_4_AUX_O_ADCREF0, refSource | ADI_4_AUX_ADCREF0_EN_M);
121 
122  // Enable the ADC clock
123  HWREG(AUX_SYSIF_BASE + AUX_SYSIF_O_ADCCLKCTL) = AUX_SYSIF_ADCCLKCTL_REQ_M;
124  while (!(HWREG(AUX_SYSIF_BASE + AUX_SYSIF_O_ADCCLKCTL) & AUX_SYSIF_ADCCLKCTL_ACK_M));
125 
126  // Enable the ADC data interface
127  if (trigger == AUXADC_TRIGGER_MANUAL) {
128  // Manual trigger: No need to configure event routing from GPT
129  HWREG(AUX_ANAIF_BASE + AUX_ANAIF_O_ADCCTL) = AUX_ANAIF_ADCCTL_START_SRC_NO_EVENT | AUX_ANAIF_ADCCTL_CMD_EN;
130  } else {
131  // GPT trigger: Configure event routing via MCU_EV to the AUX domain
132  HWREG(EVENT_BASE + EVENT_O_AUXSEL0) = trigger;
133  HWREG(AUX_ANAIF_BASE + AUX_ANAIF_O_ADCCTL) = AUX_ANAIF_ADCCTL_START_SRC_MCU_EV | AUX_ANAIF_ADCCTL_CMD_EN;
134  }
135 
136  // Configure the ADC
137  ADI8BitsSet(AUX_ADI4_BASE, ADI_4_AUX_O_ADC0, ADI_4_AUX_ADC0_SMPL_MODE_M);
138 
139  // Release reset and enable the ADC
140  ADI8BitsSet(AUX_ADI4_BASE, ADI_4_AUX_O_ADC0, ADI_4_AUX_ADC0_EN_M | ADI_4_AUX_ADC0_RESET_N_M);
141 }
static void ADI8BitsSet(uint32_t ui32Base, uint32_t ui32Reg, uint8_t ui8Val)
Set specific bits in a single 8 bit ADI register.
Definition: adi.h:371
#define AUXADC_TRIGGER_MANUAL
Definition: aux_adc.h:125
Here is the call graph for this function:

§ AUXADCEnableSync()

void AUXADCEnableSync ( uint32_t  refSource,
uint32_t  sampleTime,
uint32_t  trigger 
)

Enables the ADC for synchronous operation.

In synchronous operation, the ADC is idle between a conversion and subsequent samplings.

The ADC trigger starts sampling with specified duration, followed by the conversion. Note that the first conversion may be invalid if the initial sampling period is too short.

ADC input scaling is enabled by default after device reset, and is also re- enabled by AUXADCDisable(). To disable input scaling, call AUXADCDisableInputScaling() before calling AUXADCEnableSync().

Parameters
refSourceADC reference source:
sampleTimeADC sampling time:
triggerADC conversion trigger:
190 {
191  // The original AUXADCEnableSync() implementation requires a workaround,
192  // consisting of a delay, after its invocation. This delay is implemented by
193  // repeating the last ADI write operation three times.
194  //
195  // We need to make a call to the ROM symbol directly. Otherwise, the
196  // current build process will call the implementation in flash instead even
197  // if a ROM version is available.
198 #if defined(ROM_AUXADCEnableSyncNoBugWorkaround) && !defined(DRIVERLIB_NOROM) && !defined(DOXYGEN)
199  ROM_AUXADCEnableSyncNoBugWorkaround(refSource, sampleTime, trigger);
200 #else
201  AUXADCEnableSyncNoBugWorkaround(refSource, sampleTime, trigger);
202 #endif
203 
204 
205  // Repeat this write another three times to add a delay. This is required
206  // to prevent the device from hanging if we generate a manual ADC trigger
207  // immediately after enabling the ADC and the Sensor Controller turns on
208  // or off the XOSC_HF as a reference for the TDC at the same time.
209  ADI8BitsSet(AUX_ADI4_BASE, ADI_4_AUX_O_ADC0, ADI_4_AUX_ADC0_EN_M | ADI_4_AUX_ADC0_RESET_N_M);
210  ADI8BitsSet(AUX_ADI4_BASE, ADI_4_AUX_O_ADC0, ADI_4_AUX_ADC0_EN_M | ADI_4_AUX_ADC0_RESET_N_M);
211  ADI8BitsSet(AUX_ADI4_BASE, ADI_4_AUX_O_ADC0, ADI_4_AUX_ADC0_EN_M | ADI_4_AUX_ADC0_RESET_N_M);
212 }
static void ADI8BitsSet(uint32_t ui32Base, uint32_t ui32Reg, uint8_t ui8Val)
Set specific bits in a single 8 bit ADI register.
Definition: adi.h:371
void AUXADCEnableSyncNoBugWorkaround(uint32_t refSource, uint32_t sampleTime, uint32_t trigger)
Enables the ADC for synchronous operation.
Definition: aux_adc.c:151
#define ROM_AUXADCEnableSyncNoBugWorkaround
Definition: rom.h:718
Here is the call graph for this function:

§ AUXADCEnableSyncNoBugWorkaround()

void AUXADCEnableSyncNoBugWorkaround ( uint32_t  refSource,
uint32_t  sampleTime,
uint32_t  trigger 
)

Enables the ADC for synchronous operation.

The device can hang if we generate a manual ADC trigger immediately after enabling the ADC with this function and the Sensor Controller turns on or off the XOSC_HF as a reference for the TDC at the same time.

An application should be calling AUXADCEnableSync() instead.

In synchronous operation, the ADC is idle between a conversion and subsequent samplings.

The ADC trigger starts sampling with specified duration, followed by the conversion. Note that the first conversion may be invalid if the initial sampling period is too short.

ADC input scaling is enabled by default after device reset, and is also re- enabled by AUXADCDisable(). To disable input scaling, call AUXADCDisableInputScaling() before calling AUXADCEnableSync().

Parameters
refSourceADC reference source:
sampleTimeADC sampling time:
triggerADC conversion trigger:

Referenced by AUXADCEnableSync().

152 {
153  // Enable the ADC reference, with the following options:
154  // - SRC: Set when using relative reference
155  // - REF_ON_IDLE: Set when using fixed reference and sample time < 21.3 us
156  uint8_t adcref0 = refSource | ADI_4_AUX_ADCREF0_EN_M;
157  if (!refSource && (sampleTime < AUXADC_SAMPLE_TIME_21P3_US)) {
158  adcref0 |= ADI_4_AUX_ADCREF0_REF_ON_IDLE_M;
159  }
160  ADI8BitsSet(AUX_ADI4_BASE, ADI_4_AUX_O_ADCREF0, adcref0);
161 
162  // Enable the ADC clock
163  HWREG(AUX_SYSIF_BASE + AUX_SYSIF_O_ADCCLKCTL) = AUX_SYSIF_ADCCLKCTL_REQ_M;
164  while (!(HWREG(AUX_SYSIF_BASE + AUX_SYSIF_O_ADCCLKCTL) & AUX_SYSIF_ADCCLKCTL_ACK_M));
165 
166  // Enable the ADC data interface
167  if (trigger == AUXADC_TRIGGER_MANUAL) {
168  // Manual trigger: No need to configure event routing from GPT
169  HWREG(AUX_ANAIF_BASE + AUX_ANAIF_O_ADCCTL) = AUX_ANAIF_ADCCTL_START_SRC_NO_EVENT | AUX_ANAIF_ADCCTL_CMD_EN;
170  } else {
171  // GPT trigger: Configure event routing via MCU_EV to the AUX domain
172  HWREG(EVENT_BASE + EVENT_O_AUXSEL0) = trigger;
173  HWREG(AUX_ANAIF_BASE + AUX_ANAIF_O_ADCCTL) = AUX_ANAIF_ADCCTL_START_SRC_MCU_EV | AUX_ANAIF_ADCCTL_CMD_EN;
174  }
175 
176  // Configure the ADC
177  ADI8BitsSet(AUX_ADI4_BASE, ADI_4_AUX_O_ADC0, sampleTime << ADI_4_AUX_ADC0_SMPL_CYCLE_EXP_S);
178 
179  // Release reset and enable the ADC
180  ADI8BitsSet(AUX_ADI4_BASE, ADI_4_AUX_O_ADC0, ADI_4_AUX_ADC0_EN_M | ADI_4_AUX_ADC0_RESET_N_M);
181 }
#define AUXADC_SAMPLE_TIME_21P3_US
Definition: aux_adc.h:151
static void ADI8BitsSet(uint32_t ui32Base, uint32_t ui32Reg, uint8_t ui8Val)
Set specific bits in a single 8 bit ADI register.
Definition: adi.h:371
#define AUXADC_TRIGGER_MANUAL
Definition: aux_adc.h:125
Here is the call graph for this function:

§ AUXADCFlushFifo()

void AUXADCFlushFifo ( void  )

Flushes the ADC FIFO.

This empties the FIFO and clears the underflow/overflow flags.

Note: This function must only be called while the ADC is enabled.

232 {
233  HWREGBITW(AUX_ANAIF_BASE + AUX_ANAIF_O_ADCCTL, 1) = 1; // CMD: EN(1) -> FLUSH(3)
234  HWREGBITW(AUX_ANAIF_BASE + AUX_ANAIF_O_ADCCTL, 1) = 0; // CMD: FLUSH(3) -> EN(1)
235 }

§ AUXADCGenManualTrigger()

static void AUXADCGenManualTrigger ( void  )
inlinestatic

Generates a single manual ADC trigger.

For synchronous mode, the trigger starts sampling followed by conversion. For asynchronous mode, the trigger starts conversion.

367 {
368  HWREG(AUX_ANAIF_BASE + AUX_ANAIF_O_ADCTRIG) = 0;
369 }

§ AUXADCGetAdjustmentGain()

int32_t AUXADCGetAdjustmentGain ( uint32_t  refSource)

Returns the gain value used when adjusting for ADC gain/offset.

The function returns the gain value to be used with AUXADCAdjustValueForGainAndOffset() or AUXADCUnadjustValueForGainAndOffset(). The gain value is found during chip manufacturing and is stored in the factory configuration, FCFG1.

Parameters
refSourceADC reference source:
Returns
The gain value to be used in adjustments

Referenced by AUXADCSelectInput().

272 {
273  int32_t gain;
274  if (refSource == AUXADC_REF_FIXED) {
275  // AUXADC_REF_FIXED ==> ABS_GAIN
276  gain = (HWREG(FCFG1_BASE + FCFG1_O_SOC_ADC_ABS_GAIN) & FCFG1_SOC_ADC_ABS_GAIN_SOC_ADC_ABS_GAIN_TEMP1_M) >> FCFG1_SOC_ADC_ABS_GAIN_SOC_ADC_ABS_GAIN_TEMP1_S;
277  } else {
278  // AUXADC_REF_VDDS_REL ==> REL_GAIN
279  gain = (HWREG(FCFG1_BASE + FCFG1_O_SOC_ADC_REL_GAIN) & FCFG1_SOC_ADC_REL_GAIN_SOC_ADC_REL_GAIN_TEMP1_M) >> FCFG1_SOC_ADC_REL_GAIN_SOC_ADC_REL_GAIN_TEMP1_S;
280  }
281  return gain;
282 }
#define AUXADC_REF_FIXED
Definition: aux_adc.h:106

§ AUXADCGetAdjustmentOffset()

int32_t AUXADCGetAdjustmentOffset ( uint32_t  refSource)

Returns the offset value used when adjusting for ADC gain/offset.

The function returns the offset value to be used with AUXADCAdjustValueForGainAndOffset() or AUXADCUnadjustValueForGainAndOffset(). The offset value is found during chip manufacturing and is stored in the factory configuration, FCFG1.

Parameters
refSourceADC reference source:
Returns
The offset value to be used in adjustments

Referenced by AUXADCSelectInput().

291 {
292  int8_t offset;
293  if ( refSource == AUXADC_REF_FIXED ) {
294  // AUXADC_REF_FIXED ==> ABS_OFFSET
295  offset = HWREG(FCFG1_BASE + FCFG1_O_SOC_ADC_OFFSET_INT) >> FCFG1_SOC_ADC_OFFSET_INT_SOC_ADC_ABS_OFFSET_TEMP1_S;
296  } else {
297  // AUXADC_REF_VDDS_REL ==> REL_OFFSET
298  offset = HWREG(FCFG1_BASE + FCFG1_O_SOC_ADC_OFFSET_INT) >> FCFG1_SOC_ADC_OFFSET_INT_SOC_ADC_REL_OFFSET_TEMP1_S;
299  }
300  return offset;
301 }
#define AUXADC_REF_FIXED
Definition: aux_adc.h:106

§ AUXADCGetFifoStatus()

static uint32_t AUXADCGetFifoStatus ( void  )
inlinestatic

Returns flags indicating the status of the ADC FIFO.

The flags indicate FIFO empty, full and almost full, and whether overflow/underflow has occurred.

Returns
A combination (bitwise OR) of the following flags:
389 {
390  return HWREG(AUX_ANAIF_BASE + AUX_ANAIF_O_ADCFIFOSTAT);
391 }
Here is the call graph for this function:

§ AUXADCMicrovoltsToValue()

int32_t AUXADCMicrovoltsToValue ( int32_t  fixedRefVoltage,
int32_t  microvolts 
)

Converts a number of microvolts to corresponding "adjusted" ADC value.

This function can only be used when measuring with fixed ADC reference (AUXADC_REF_FIXED). The specified reference voltage accounts for whether the sampled ADC input is scaled down before conversion or not.

Parameters
fixedRefVoltageFixed reference voltage, in microvolts
microvoltsThe number of microvolts
Returns
The corresponding expected ADC value (adjusted for ADC gain/offset)

Referenced by AUXADCSelectInput().

323 {
324  // Chop off 4 bits during calculations to avoid 32-bit overflow
325  fixedRefVoltage >>= 4;
326  microvolts >>= 4;
327  return ((microvolts * 4095) + (fixedRefVoltage / 2)) / fixedRefVoltage;
328 }

§ AUXADCPopFifo()

uint32_t AUXADCPopFifo ( void  )

Returns the first sample in the ADC FIFO, without waiting.

This function does not wait, and must only be called when there is at least one sample in the ADC FIFO. Otherwise the call will generate FIFO underflow (AUXADC_FIFO_UNDERFLOW_M).

Returns
The first (12-bit) sample from the ADC FIFO, or an undefined value if the FIFO is empty

Referenced by AUXADCGetFifoStatus().

258  {
259 
260  // Return the first sample from the FIFO. If the FIFO is empty, this
261  // generates ADC FIFO underflow
262  return HWREG(AUX_ANAIF_BASE + AUX_ANAIF_O_ADCFIFO);
263 }

§ AUXADCReadFifo()

uint32_t AUXADCReadFifo ( void  )

Waits for and returns the first sample in the ADC FIFO.

This function waits until there is at least one sample in the ADC FIFO. It then pops and returns the first sample from the FIFO.

Note
This procedure will deadlock if called without setting up ADC trigger generation in advance. The trigger can either be manual or periodical (using a GPT).
Returns
The first (12-bit) sample from the ADC FIFO

Referenced by AUXADCGetFifoStatus().

243  {
244 
245  // Wait until there is at least one sample in the FIFO
246  while (HWREG(AUX_ANAIF_BASE + AUX_ANAIF_O_ADCFIFOSTAT) & AUX_ANAIF_ADCFIFOSTAT_EMPTY_M);
247 
248  // Return the first sample from the FIFO
249  return HWREG(AUX_ANAIF_BASE + AUX_ANAIF_O_ADCFIFO);
250 }

§ AUXADCSelectInput()

static void AUXADCSelectInput ( uint32_t  input)
inlinestatic

Selects internal or external input for the ADC.

Note that calling this function also selects the same input for AUX_COMPB.

Parameters
inputInternal/external input selection:
446 {
448 }
#define HapiSelectADCCompBInput(a)
Definition: rom.h:155
Here is the call graph for this function:

§ AUXADCUnadjustValueForGainAndOffset()

int32_t AUXADCUnadjustValueForGainAndOffset ( int32_t  adcValue,
int32_t  gain,
int32_t  offset 
)

Performs the inverse of the ADC value gain and offset adjustment.

This function finds the expected measured ADC value, without gain and offset compensation, for a given "ideal" ADC value. The function can for example be used to find ADC value thresholds to be used in Sensor Controller task configurations.

Parameters
adcValue12-bit ADC adjusted value
gainGain adjustment value provided by AUXADCGetAdjustmentGain()
offsetOffset adjustment value provided by AUXADCGetAdjustmentOffset()
Returns
12-bit ADC unadjusted value

Referenced by AUXADCSelectInput().

358 {
359  // Apply inverse gain and offset adjustment
360  adcValue = (((adcValue * 32768) + (gain / 2)) / gain) - offset;
361 
362  // Saturate
363  if (adcValue < 0) {
364  return 0;
365  } else if (adcValue > 4095) {
366  return 4095;
367  } else {
368  return adcValue;
369  }
370 }

§ AUXADCValueToMicrovolts()

int32_t AUXADCValueToMicrovolts ( int32_t  fixedRefVoltage,
int32_t  adcValue 
)

Converts an "adjusted" ADC value to microvolts.

This function can only be used when measuring with fixed ADC reference (AUXADC_REF_FIXED). The specified reference voltage accounts for whether the sampled ADC input is scaled down before conversion or not.

Parameters
fixedRefVoltageFixed reference voltage, in microvolts
adcValueThe ADC value
Returns
The corresponding number of microvolts

Referenced by AUXADCSelectInput().

310 {
311  // Chop off 4 bits during calculations to avoid 32-bit overflow
312  fixedRefVoltage >>= 4;
313  return (((adcValue * fixedRefVoltage) + 2047) / 4095) << 4;
314 }

Macro Definition Documentation

§ AUXADC_FIFO_ALMOST_FULL_M

#define AUXADC_FIFO_ALMOST_FULL_M   (AUX_ANAIF_ADCFIFOSTAT_ALMOST_FULL_M)

§ AUXADC_FIFO_EMPTY_M

#define AUXADC_FIFO_EMPTY_M   (AUX_ANAIF_ADCFIFOSTAT_EMPTY_M)

§ AUXADC_FIFO_FULL_M

#define AUXADC_FIFO_FULL_M   (AUX_ANAIF_ADCFIFOSTAT_FULL_M)

§ AUXADC_FIFO_OVERFLOW_M

#define AUXADC_FIFO_OVERFLOW_M   (AUX_ANAIF_ADCFIFOSTAT_OVERFLOW_M)

§ AUXADC_FIFO_UNDERFLOW_M

#define AUXADC_FIFO_UNDERFLOW_M   (AUX_ANAIF_ADCFIFOSTAT_UNDERFLOW_M)

§ AUXADC_FIXED_REF_VOLTAGE_NORMAL

#define AUXADC_FIXED_REF_VOLTAGE_NORMAL   4300000

§ AUXADC_FIXED_REF_VOLTAGE_UNSCALED

#define AUXADC_FIXED_REF_VOLTAGE_UNSCALED   1478500

§ AUXADC_REF_FIXED

#define AUXADC_REF_FIXED   (0 << ADI_4_AUX_ADCREF0_SRC_S)

§ AUXADC_REF_VDDS_REL

#define AUXADC_REF_VDDS_REL   (1 << ADI_4_AUX_ADCREF0_SRC_S)

§ AUXADC_SAMPLE_TIME_10P6_US

#define AUXADC_SAMPLE_TIME_10P6_US   5

§ AUXADC_SAMPLE_TIME_10P9_MS

#define AUXADC_SAMPLE_TIME_10P9_MS   15

§ AUXADC_SAMPLE_TIME_170_US

#define AUXADC_SAMPLE_TIME_170_US   9

§ AUXADC_SAMPLE_TIME_1P37_MS

#define AUXADC_SAMPLE_TIME_1P37_MS   12

§ AUXADC_SAMPLE_TIME_21P3_US

#define AUXADC_SAMPLE_TIME_21P3_US   6

§ AUXADC_SAMPLE_TIME_2P73_MS

#define AUXADC_SAMPLE_TIME_2P73_MS   13

§ AUXADC_SAMPLE_TIME_2P7_US

#define AUXADC_SAMPLE_TIME_2P7_US   3

§ AUXADC_SAMPLE_TIME_341_US

#define AUXADC_SAMPLE_TIME_341_US   10

§ AUXADC_SAMPLE_TIME_42P6_US

#define AUXADC_SAMPLE_TIME_42P6_US   7

§ AUXADC_SAMPLE_TIME_5P3_US

#define AUXADC_SAMPLE_TIME_5P3_US   4

§ AUXADC_SAMPLE_TIME_5P46_MS

#define AUXADC_SAMPLE_TIME_5P46_MS   14

§ AUXADC_SAMPLE_TIME_682_US

#define AUXADC_SAMPLE_TIME_682_US   11

§ AUXADC_SAMPLE_TIME_85P3_US

#define AUXADC_SAMPLE_TIME_85P3_US   8

§ AUXADC_TRIGGER_GPT0A

#define AUXADC_TRIGGER_GPT0A   (EVENT_AUXSEL0_EV_GPT0A)

§ AUXADC_TRIGGER_GPT0A_CMP

#define AUXADC_TRIGGER_GPT0A_CMP   (EVENT_AUXSEL0_EV_GPT0A_CMP)

§ AUXADC_TRIGGER_GPT0B

#define AUXADC_TRIGGER_GPT0B   (EVENT_AUXSEL0_EV_GPT0B)

§ AUXADC_TRIGGER_GPT0B_CMP

#define AUXADC_TRIGGER_GPT0B_CMP   (EVENT_AUXSEL0_EV_GPT0B_CMP)

§ AUXADC_TRIGGER_GPT1A

#define AUXADC_TRIGGER_GPT1A   (EVENT_AUXSEL0_EV_GPT1A)

§ AUXADC_TRIGGER_GPT1A_CMP

#define AUXADC_TRIGGER_GPT1A_CMP   (EVENT_AUXSEL0_EV_GPT1A_CMP)

§ AUXADC_TRIGGER_GPT1B

#define AUXADC_TRIGGER_GPT1B   (EVENT_AUXSEL0_EV_GPT1B)

§ AUXADC_TRIGGER_GPT1B_CMP

#define AUXADC_TRIGGER_GPT1B_CMP   (EVENT_AUXSEL0_EV_GPT1B_CMP)

§ AUXADC_TRIGGER_GPT2A

#define AUXADC_TRIGGER_GPT2A   (EVENT_AUXSEL0_EV_GPT2A)

§ AUXADC_TRIGGER_GPT2A_CMP

#define AUXADC_TRIGGER_GPT2A_CMP   (EVENT_AUXSEL0_EV_GPT2A_CMP)

§ AUXADC_TRIGGER_GPT2B

#define AUXADC_TRIGGER_GPT2B   (EVENT_AUXSEL0_EV_GPT2B)

§ AUXADC_TRIGGER_GPT2B_CMP

#define AUXADC_TRIGGER_GPT2B_CMP   (EVENT_AUXSEL0_EV_GPT2B_CMP)

§ AUXADC_TRIGGER_GPT3A

#define AUXADC_TRIGGER_GPT3A   (EVENT_AUXSEL0_EV_GPT3A)

§ AUXADC_TRIGGER_GPT3A_CMP

#define AUXADC_TRIGGER_GPT3A_CMP   (EVENT_AUXSEL0_EV_GPT3A_CMP)

§ AUXADC_TRIGGER_GPT3B

#define AUXADC_TRIGGER_GPT3B   (EVENT_AUXSEL0_EV_GPT3B)

§ AUXADC_TRIGGER_GPT3B_CMP

#define AUXADC_TRIGGER_GPT3B_CMP   (EVENT_AUXSEL0_EV_GPT3B_CMP)

§ AUXADC_TRIGGER_MANUAL

#define AUXADC_TRIGGER_MANUAL   (EVENT_AUXSEL0_EV_NONE)