Developing a Bluetooth LE Application

To develop a custom Bluetooth Low Energy Application with the CC13xx or CC26xx family of devices, a system designer must have a firm grasp on the general system architecture, application, and Bluetooth Low Energy stack framework. This section provides guidance on how to implement a custom application based on information presented in the previous sections (Introduction and BLE5-Stack) as well as knowledge of RTOS and CC13xx or CC26xx.

First, the user shoud decide what role and purpose the custom application should have. If an application is tied to a specific service or profile, start with that sample application. A project’s role can be essentially be placed in one of the five (5) categories as described by GAP Roles. Once the role has been selected, the user may need to alter the application code, the memory map, the building and linking options and more to turn their example project into a custom application.

Application Layer

In this section, we take as an example the simple_peripheral project and describe for you the application portion. This section includes the following topics:

Memory Management

This section aims to describe the various memory regions available on the device as well as how they are used by the stack and application. The chapter starts with an overview of the memory map of the device, and then each section goes into detail on how this memory region is used.

Compiler and Linker Options

The following section details the building and linking options for development with CCS.

Production Test Mode and Direct Test Mode

This section discusses how Production Test Mode and Direct Test Mode can be incorporated into a project to allow users to automatically test their products before they ship.

Bluetooth LE Network Processor

The BLE Network Processor section describes a configuration where most of the programming logic happens on a separate controller, which communicates with the CC13xx or CC26xx device over wired communication.