TI BLE5-Stack API Documentation  2.02.07.00
Data Structures | Macros | Typedefs | Functions
sm.h File Reference

Detailed Description

This file contains the interface to the SM.

Go to the source code of this file.

Data Structures

struct  authReq_t
 
struct  keyDist_t
 
struct  smDhKeyEvt_t
 
struct  smEccKeys_t
 
struct  smEccKeysEvt_t
 
struct  smEventHdr_t
 
struct  smIdentityInfo_t
 
struct  smLinkSecurityReq_t
 
struct  smNewRandKeyEvent_t
 
struct  smSecurityInfo_t
 
struct  smSigningInfo_t
 

Macros

#define DISPLAY_ONLY   0x00
 Display Only Device.
 
#define DISPLAY_YES_NO   0x01
 Display and Yes and No Capable.
 
#define KEYBOARD_DISPLAY   0x04
 Both Keyboard and Display Capable.
 
#define KEYBOARD_ONLY   0x02
 Keyboard Only.
 
#define NO_INPUT_NO_OUTPUT   0x03
 No Display or Input Device.
 
#define PASSKEY_LEN   6
 Passkey Character Length (ASCII Characters)
 
#define SM_AUTH_MITM_MASK(a)   (((a) & 0x04) >> 2)
 MITM Mask.
 
#define SM_AUTH_REQ_BONDING   0x01
 Bonding.
 
#define SM_AUTH_REQ_NO_BONDING   0x00
 No bonding.
 
#define SM_AUTH_STATE_AUTHENTICATED   0x04
 Authenticate requested.
 
#define SM_AUTH_STATE_BONDING   0x01
 Bonding requested.
 
#define SM_AUTH_STATE_SECURECONNECTION   0x08
 Secure Connection requested.
 
#define SM_DH_KEY_EVENT   0x01
 Diffie-Hellman key.
 
#define SM_ECC_KEY_LEN   32
 ECC Key length in bytes.
 
#define SM_ECC_KEYS_EVENT   0x00
 ECC Keys.
 
#define SM_ECC_KEYS_NOT_AVAILABLE   0xFF
 Initial state of recycled keys before they exist.
 
#define SM_ECC_KEYS_REGENERATE_ALWAYS   0x00
 Always regenerate the keys.
 
#define SM_ECC_KEYS_REGNENERATE_NEVER   0xFF
 Never regenerate the keys.
 
#define SM_PASSKEY_TYPE_DISPLAY   0x02
 Display the passkey.
 
#define SM_PASSKEY_TYPE_INPUT   0x01
 Input the passkey.
 

Typedefs

typedef void(* smCB_t) (uint8 *secretKey, uint8 *publicKeyX, uint8 *publicKeyY)
 

Functions

bStatus_t SM_Encrypt (uint8 *pKey, uint8 *pPlainText, uint8 *pResult)
 Encrypt the plain text data with the key.. More...
 
bStatus_t SM_GenerateAuthenSig (uint8 *pData, uint16 len, uint8 *pAuthenSig, uint16 connHandle)
 
void SM_GenerateRandBuf (uint8 *random, uint8 len)
 
uint8 SM_GetAllowDebugKeysMode (void)
 Get the device debug keys allownce policy. If not allowed, the pairing will be rejected with code of invalid parameters. If allowed, pairing will continue noramlly. More...
 
uint8 SM_GetAuthenPairingOnlyMode (void)
 Get the device into Authenticated Pairing Only Mode. If enabled and the key generation method does not result in a key that provides Authenticated MITM protection then the device will send the Pairing Failed command with the error code Authentication Requirements. More...
 
bStatus_t SM_GetDHKey (uint8 *secretKey, uint8 *publicKeyX, uint8 *publicKeyY)
 Request a Diffie-Hellman key from the ECC engine. Key is returned through the callback registered in SM_RegisterCb, in the first parameter. More...
 
bStatus_t SM_GetEccKeys (void)
 Get ECC private and public keys. Keys are returned through the callback registered in SM_RegisterCb. More...
 
bStatus_t SM_GetScConfirmOob (uint8 *publicKey, uint8 *oob, uint8 *pOut)
 Generate a confirm value for OOB data. More...
 
bStatus_t SM_InitiatorInit (void)
 Initialize SM Initiator on a master device. More...
 
bStatus_t SM_NewRandKey (uint8 taskID)
 Generate a key with a random value. More...
 
bStatus_t SM_PasskeyUpdate (uint8 *pPasskey, uint16 connectionHandle)
 Update the passkey for the pairing process. More...
 
void SM_RegisterTask (uint8 taskID)
 Register Task with the Security Manager to receive ECC keys or a ECDH shared secret. More...
 
bStatus_t SM_ResponderInit (void)
 Initialize SM Responder on a slave device. More...
 
void SM_SetAllowDebugKeysMode (uint8 state)
 
void SM_SetAuthenPairingOnlyMode (uint8 state)
 
void SM_SetECCRegenerationCount (uint8 count)
 Update the regeneration count for ECC key re-usage. More...
 
bStatus_t SM_StartEncryption (uint16 connHandle, uint8 *pLTK, uint16 div, uint8 *pRandNum, uint8 keyLen)
 Send Start Encrypt through HCI. More...
 
bStatus_t SM_StartPairing (uint8 initiator, uint8 taskID, uint16 connectionHandle, smLinkSecurityReq_t *pSecReqs)
 Start the pairing process. More...
 
bStatus_t SM_VerifyAuthenSig (uint16 connHandle, uint8 authentication, uint8 *pData, uint16 len, uint8 *pAuthenSig)
 Verify an Authentication Signature. More...
 

Typedef Documentation

§ smCB_t

typedef void(* smCB_t) (uint8 *secretKey, uint8 *publicKeyX, uint8 *publicKeyY)

Application callback to the SM for ECC keys and Diffie-Hellman Shared Secret (ECDH).

Function Documentation

§ SM_Encrypt()

bStatus_t SM_Encrypt ( uint8 *  pKey,
uint8 *  pPlainText,
uint8 *  pResult 
)

Encrypt the plain text data with the key..

Parameters
pKey- key data
pPlainText- Plain text data
pResult- place to put the encrypted result
Returns
SUCCESS - if started
INVALIDPARAMETER - one of the parameters are NULL
bleAlreadyInRequestedMode
bleMemAllocError

§ SM_GenerateAuthenSig()

bStatus_t SM_GenerateAuthenSig ( uint8 *  pData,
uint16  len,
uint8 *  pAuthenSig,
uint16  connHandle 
)

Generate an outgoing Authentication Signature.

Parameters
pDatamessage data
lenlength of pData
pAuthenSigplace to put new signature
connHandleconnection handle
Returns
SUCCESS - signature authentication generated
INVALIDPARAMETER - pData or pAuthenSig is NULL
bleMemAllocError

§ SM_GetAllowDebugKeysMode()

SM_GetAllowDebugKeysMode ( void  )

Get the device debug keys allownce policy. If not allowed, the pairing will be rejected with code of invalid parameters. If allowed, pairing will continue noramlly.

Parameters
none
Returns
state - TRUE debug keys as peer public keys are allowed FALSE when disallowed

§ SM_GetAuthenPairingOnlyMode()

SM_GetAuthenPairingOnlyMode ( void  )

Get the device into Authenticated Pairing Only Mode. If enabled and the key generation method does not result in a key that provides Authenticated MITM protection then the device will send the Pairing Failed command with the error code Authentication Requirements.

Parameters
none
Returns
state - TRUE Authenticated Pairing Only Mode is enabled FALSE when disabled

§ SM_GetDHKey()

bStatus_t SM_GetDHKey ( uint8 *  secretKey,
uint8 *  publicKeyX,
uint8 *  publicKeyY 
)

Request a Diffie-Hellman key from the ECC engine. Key is returned through the callback registered in SM_RegisterCb, in the first parameter.

Parameters
secretKey- the local private key
publicKeyX- the remote public key, X-Coordinate.
publicKeyY- the remote public key, Y-Coordinate.
Returns
SUCCESS if processing
FAILURE if SM is pairing
HCI_ERROR_CODE_MEM_CAP_EXCEEDED if out of heap memory.

§ SM_GetEccKeys()

bStatus_t SM_GetEccKeys ( void  )

Get ECC private and public keys. Keys are returned through the callback registered in SM_RegisterCb.

Returns
SUCCESS if processing
FAILURE if SM is pairing
HCI_ERROR_CODE_MEM_CAP_EXCEEDED if out of heap memory.

§ SM_GetScConfirmOob()

bStatus_t SM_GetScConfirmOob ( uint8 *  publicKey,
uint8 *  oob,
uint8 *  pOut 
)

Generate a confirm value for OOB data.

Parameters
publicKey- the local public key X-coordinate
oob- the random string to be sent to the remote device via oob
pOut- pointer to the generated confirm value. The calling application must copy this data into its own buffer.
Returns
SUCCESS
INVALIDPARAMETER
bleMemAllocError

§ SM_InitiatorInit()

bStatus_t SM_InitiatorInit ( void  )

Initialize SM Initiator on a master device.

Warning
Only use this API on a master device
Returns
SUCCESS

§ SM_NewRandKey()

bStatus_t SM_NewRandKey ( uint8  taskID)

Generate a key with a random value.

Parameters
taskID- task ID to send results.
Returns
SUCCESS
bleNotReady
bleMemAllocError
FAILURE

§ SM_PasskeyUpdate()

bStatus_t SM_PasskeyUpdate ( uint8 *  pPasskey,
uint16  connectionHandle 
)

Update the passkey for the pairing process.

Parameters
pPasskey- pointer to the 6 digit passkey
connectionHandle- connection handle to link.
Returns
SUCCESS
bleIncorrectMode - Not pairing
INVALIDPARAMETER - link is incorrect

§ SM_RegisterTask()

void SM_RegisterTask ( uint8  taskID)

Register Task with the Security Manager to receive ECC keys or a ECDH shared secret.

Parameters
taskID- Application's task ID.

§ SM_ResponderInit()

bStatus_t SM_ResponderInit ( void  )

Initialize SM Responder on a slave device.

Warning
Only use this API on a slave device
Returns
SUCCESS

§ SM_SetECCRegenerationCount()

void SM_SetECCRegenerationCount ( uint8  count)

Update the regeneration count for ECC key re-usage.

Parameters
count- number of times a keypair can be reused before regeneration.

§ SM_StartEncryption()

bStatus_t SM_StartEncryption ( uint16  connHandle,
uint8 *  pLTK,
uint16  div,
uint8 *  pRandNum,
uint8  keyLen 
)

Send Start Encrypt through HCI.

Warning
Only use this API on a master device
Parameters
connHandle- Connection Handle
pLTK- pointer to 16 byte lkt
div- div or ediv
pRandNum- pointer to 8 byte random number
keyLen- length of LTK (bytes)
Returns
SUCCESS
INVALIDPARAMETER

§ SM_StartPairing()

bStatus_t SM_StartPairing ( uint8  initiator,
uint8  taskID,
uint16  connectionHandle,
smLinkSecurityReq_t pSecReqs 
)

Start the pairing process.

This function is also called if the device is already bound.

Note
Only one pairing process at a time per device.
Warning
Only use this API on a master device
Parameters
initiator- TRUE to start pairing as Initiator.
taskID- task ID to send results.
connectionHandle- Link's connection handle
pSecReqs- Security parameters for pairing
Returns
SUCCESS
INVALIDPARAMETER
bleAlreadyInRequestedMode

§ SM_VerifyAuthenSig()

bStatus_t SM_VerifyAuthenSig ( uint16  connHandle,
uint8  authentication,
uint8 *  pData,
uint16  len,
uint8 *  pAuthenSig 
)

Verify an Authentication Signature.

Parameters
connHandle- connection to verify against.
authentication- TRUE if requires an authenticated CSRK, FALSE if not
pData- message data
len- length of pData
pAuthenSig- message signature to verify
Returns
SUCCESS - signature authentication verified
FAILURE - if not verified
bleNotConnected - Connection not found
INVALIDPARAMETER - pData or pAuthenSig is NULL, or signCounter is invalid
bleMemAllocError
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale