TI BLE5-Stack API Documentation
2.02.07.00
|
Data type returned with GAP_EVT_SCAN_REQ_RECEIVED event. More...
Data Fields | |
uint8 | channel |
Channel when the scan req was received. | |
uint8 | handle |
Advertising handle. | |
int8 | rssi |
RSSI of the scan req. | |
uint8 | scanAddr [B_ADDR_LEN] |
Address of scanning device. | |
uint8 | scanAddrType |
Address type of scanning device. | |
Data type returned with GAP_EVT_SCAN_REQ_RECEIVED event.