TI BLE5-Stack API Documentation  2.02.07.00
Data Fields
GapScan_Evt_AdvRpt_t Struct Reference

Event for advertising report. More...

Data Fields

uint8_t addr [B_ADDR_LEN]
 Address of the advertising device.
 
GAP_Addr_Types_t addrType
 Public, random, public ID, random ID, or anonymous.
 
uint8_t advSid
 SID (0x00-0x0f) of the advertising PDU. 0xFF means no ADI field in the PDU.
 
uint16_t dataLen
 Length of the data.
 
uint8_t directAddr [B_ADDR_LEN]
 TargetA address.
 
GAP_Addr_Types_t directAddrType
 Type of TargetA address in the directed advertising PDU.
 
uint8_t evtType
 
uint8_t * pData
 Pointer to advertising or scan response data.
 
uint16_t periodicAdvInt
 Periodic advertising interval. 0 means no periodic advertising.
 
GapScan_ScannedPhy_t primPhy
 PHY of the primary advertising channel.
 
int8_t rssi
 -127 dBm <= RSSI <= 20 dBm
 
GapScan_ScannedPhy_t secPhy
 PHY of the secondary advertising channel.
 
int8_t txPower
 -127 dBm <= TX power <= 126 dBm
 

Detailed Description

Event for advertising report.

Field Documentation

§ evtType

uint8_t evtType

Bits 0 to 4 indicate connectable, scannable, directed, scan response, and legacy respectively


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale