TI BLE5-Stack API Documentation  2.02.07.00
Data Fields
gapPairingReq_t Struct Reference

Data Fields

uint8_t authReq
 Pairing Request Auth Req field.
 
uint8_t ioCap
 Pairing Request ioCap field.
 
keyDist_t keyDist
 Pairing Request Key Distribution field.
 
uint8_t maxEncKeySize
 Pairing Request Maximum Encryption Key Size field.
 
uint8_t oobDataFlag
 Pairing Request OOB Data Flag field.
 

Detailed Description

Pairing Request fields for GAP_Authenticate which should only be used if the gapbondmgr does not exist


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale