![]() |
![]() |
|
SYS/BIOS
7.00
|
Runtime error manager.
The Error module provides mechanisms for raising, checking, and handling errors in a program. At the configuration time, you can use the parameters Error.policy and Error.raiseHook to specify what happens when an error takes place. You can control how much debugging information is available in that case, while also controlling the memory footprint that the `Error' module adds to the program.
The Error.policy configuration parameter defines what happens when an error is raised. If Error.policy is set to "Error_UNWIND", the error will be captured in the error block and control will be returned to the caller. If Error.policy is set to "Error_TERMINATE", System_abort() will be called when an error is raised.
The Error.raiseHook configuration parameter allows a configured function to be invoked when an error is raised. This function is passed a pointer to the error's error block and makes it easy to manage all errors from a common point. For example, you can trap any error (fatal or not) by simply setting a breakpoint in this function. You can use Error_getMsg() to extract information from an error block.
Example 1: The following C code shows that you may pass a special constant Error_IGNORE in place of an error block to a function requiring an error block. The purpose of this constant is to avoid allocating an error block on stack in the use case where the caller is not checking the error block after the call returns. In this example, the caller only checks the returned value but not the error block. If the function raises an error, the program will return to the caller, assuming Error.policy is set to "Error_UNWIND".
Example 2: The following C code shows that you may pass a special constant Error_ABORT (NULL) in place of an error block to a function requiring an error block. In this case, if the function raises an error, the program is aborted (via System_abort()), thus execution control will never return to the caller.
Example 3: The following C code supplies an error block to a function that requires one and tests the error block to see if the function raised an error. Note that an error block must be initialized before it can be used and same error block may be passed to several functions.
#include <stdbool.h>#include <stddef.h>#include <stdint.h>

Go to the source code of this file.
Data Structures | |
| struct | Error_Block |
| Error block. More... | |
Macros | |
| #define | Error_E_memory "out of memory: heap=0x%x, size=%u" |
| Out of memory error. More... | |
| #define | Error_E_generic "error %s" |
| Generic error. More... | |
| #define | Error_IGNORE (&Error_ignore) |
| A pointer to a special Error_Block used when the caller does not want to check Error_Block. More... | |
| #define | Error_ABORT NULL |
| A special Error_Block pointer that terminates the application in case of an error. More... | |
Typedefs | |
| typedef struct Error_Block | Error_Block |
| Error block. More... | |
| typedef void(* | Error_HookFxn) (Error_Block *eb) |
Functions | |
| bool | Error_check (Error_Block *eb) |
| Return true if an error was raised. More... | |
| void | Error_init (Error_Block *eb) |
| Initialize an error block. More... | |
| void | Error_print (Error_Block *eb) |
| Print error using System.printf() More... | |
| #define Error_E_memory "out of memory: heap=0x%x, size=%u" |
Out of memory error.
The first parameter must be the heap instance handle. The second parameter is the size of the object for which the allocation failed.
| #define Error_E_generic "error %s" |
Generic error.
This error takes advantage of the $S specifier to allow for recursive formatting of the error message passed to error raise.
For example, the following is possible:
| #define Error_IGNORE (&Error_ignore) |
A pointer to a special Error_Block used when the caller does not want to check Error_Block.
This constant should be used when the caller does not plan to check Error_Block after the call returns, but wants the call to return even in the case when an error is raised. The configuration parameter, Error.policy, is still in effect and the application will still terminate when an error is raised if Error.policy is not set to "Error_UNWIND".
| #define Error_ABORT NULL |
A special Error_Block pointer that terminates the application in case of an error.
This constant has the same effect as passing NULL in place of an Error_Block. If an error is raised when Error_ABORT is passed, the application terminates regardless of the Error.policy configuration parameter setting.
| typedef struct Error_Block Error_Block |
Error block.
An opaque structure used to store information about errors once raised. This structure must be initialized via Error_init before being used for the first time.
| typedef void(* Error_HookFxn) (Error_Block *eb) |
| bool Error_check | ( | Error_Block * | eb | ) |
Return true if an error was raised.
If eb is non-NULL and Error.policy is set to Error_UNWIND and an error was raised on eb, this function returns true. Otherwise, it returns false.
| eb | pointer to an Error_Block, Error_ABORT or Error_IGNORE |
| true | if an error was raised, false if no error raised |
| void Error_init | ( | Error_Block * | eb | ) |
Initialize an error block.
If eb is non-NULL, initialize the fields in the error block to 0.
| eb | pointer to an Error_Block |
| void Error_print | ( | Error_Block * | eb | ) |
Print error using System.printf()
This function prints the error using System_printf(). The output is on a single line terminated with a new line character and has the following form:
where "{file}" and "{line} are the file and line at the Error_raise() call site, and "{err_msg}" is the error message rendered with the arguments associated with the error.
If "eb" is "Error_ABORT" or "Error_IGNORE", this function simply returns with no output.
Gate_enter/Gate_leave pair or simply ensure that only one thread in the system ever calls this method.| eb | pointer to an "Error_Block", "Error_ABORT" or "Error_IGNORE" |