TI BLE5-Stack API Documentation  2.02.08.00
Modules | Files | Macros | Functions
GATTServApp

This module implements the GATT Server App. More...

Modules

 GATT Server App Callbacks
 
 GATT Server App Constants
 
 GATT Server App Structures
 

Files

file  gattservapp.h
 GATTServApp layer interface.
 

Macros

#define GATT_ATT(type, permission, value)
 GATT Custom Attribute. More...
 
#define GATT_ATT_BT_UUID_TYPE(type)   {ATT_BT_UUID_SIZE,type}
 GATT BT Attribute Type format.
 
#define GATT_ATT_UUID_TYPE(type)   {ATT_UUID_SIZE,type}
 GATT Custom Attribute Type format.
 
#define GATT_BT_ATT(type, permission, value)
 GATT BT Attribute. More...
 
#define GATT_BT_UUID(name, UUID)
 GATT BT UUID. More...
 
#define GATT_CCC_TBL(pValue)   ( (gattCharCfg_t *)(*((PTR_TYPE)(pValue))) )
 Client Characteristic Configuration table (from CCC attribute value pointer)
 
#define GATT_INCLUDED_HANDLE(attrs, i)   ( *((uint16 *)((attrs)[(i)].pValue)) )
 The handle of the first included service (i = 1) is the value of the second attribute.
 
#define GATT_NUM_ATTRS(attrs)   ( sizeof( attrs ) / sizeof( gattAttribute_t ) )
 The number of attribute records in a given attribute table.
 
#define GATT_SERVICE_HANDLE(attrs)   ( (attrs)[0].handle )
 The handle of a service is the handle of the first attribute.
 
#define GATT_UUID(name, UUID)
 GATT Custom UUID. More...
 

Functions

bStatus_t GATTServApp_AddService (uint32 services)
 Add function for the GATT Service. More...
 
bStatus_t GATTServApp_DelService (uint32 services)
 Delete function for the GATT Service. More...
 
bStatus_t GATTServApp_DeregisterService (uint16 handle, gattAttribute_t **p2pAttrs)
 Deregister a service's attribute list and callback functions from the GATT Server Application. More...
 
gattAttribute_tGATTServApp_FindAttr (gattAttribute_t *pAttrTbl, uint16 numAttrs, uint8 *pValue)
 Find the attribute record within a service attribute table for a given attribute value pointer. More...
 
bStatus_t GATTServApp_GetParameter (uint8 param, void *pValue)
 Get a GATT Server parameter. More...
 
uint16 GATTServApp_GetParamValue (void)
 Get a GATT Server Application Parameter value. More...
 
void GATTServApp_InitCharCfg (uint16 connHandle, gattCharCfg_t *charCfgTbl)
 Initialize the client characteristic configuration table. More...
 
bStatus_t GATTServApp_ProcessCCCWriteReq (uint16 connHandle, gattAttribute_t *pAttr, uint8 *pValue, uint16 len, uint16 offset, uint16 validCfg)
 Process the client characteristic configuration write request for a given client. More...
 
bStatus_t GATTServApp_ProcessCharCfg (gattCharCfg_t *charCfgTbl, uint8 *pValue, uint8 authenticated, gattAttribute_t *attrTbl, uint16 numAttrs, uint8 taskId, pfnGATTReadAttrCB_t pfnReadAttrCB)
 Process Client Characteristic Configuration change. More...
 
uint8 GATTServApp_ReadAttr (uint16 connHandle, gattAttribute_t *pAttr, uint16 service, uint8 *pValue, uint16 *pLen, uint16 offset, uint16 maxLen, uint8 method)
 Read an attribute. If the format of the attribute value is unknown to GATT Server, use the callback function provided by the Service. More...
 
uint16 GATTServApp_ReadCharCfg (uint16 connHandle, gattCharCfg_t *charCfgTbl)
 Read the client characteristic configuration for a given client. More...
 
bStatus_t GATTServApp_ReadRsp (uint16 connHandle, uint8 *pValue, uint16 pLen, uint16 offset)
 If a service returns blePending to the read attribute call back invoked from GATTServApp, the service can later respond to with the value to be read using this API. More...
 
void GATTServApp_RegisterForMsg (uint8 taskID)
 Register your task ID to receive event messages from the GATT Server Application. More...
 
bStatus_t GATTServApp_RegisterService (gattAttribute_t *pAttrs, uint16 numAttrs, uint8 encKeySize, CONST gattServiceCBs_t *pServiceCBs)
 Register a service's attribute list and callback functions with the GATT Server Application. More...
 
void GATTServApp_SendCCCUpdatedEvent (uint16 connHandle, uint16 attrHandle, uint16 value)
 Build and send the GATT_CLIENT_CHAR_CFG_UPDATED_EVENT to the application. More...
 
bStatus_t GATTServApp_SendServiceChangedInd (uint16 connHandle, uint8 taskId)
 Send out a Service Changed Indication. More...
 
bStatus_t GATTServApp_SetParameter (uint8 param, uint8 len, void *pValue)
 Set a GATT Server parameter. More...
 
void GATTServApp_SetParamValue (uint16 value)
 Set a GATT Server Application Parameter value. Use this function to change the default GATT parameter values. More...
 
bStatus_t GATTServApp_UpdateCharCfg (uint16 connHandle, uint16 attrHandle, uint16 value)
 Update the Client Characteristic Configuration for a given Client. More...
 
uint8 GATTServApp_WriteAttr (uint16 connHandle, uint16 handle, uint8 *pValue, uint16 len, uint16 offset, uint8 method)
 Write attribute data. More...
 
uint8 GATTServApp_WriteCharCfg (uint16 connHandle, gattCharCfg_t *charCfgTbl, uint16 value)
 Write the client characteristic configuration for a given client. More...
 

Detailed Description

This module implements the GATT Server App.

Macro Definition Documentation

§ GATT_ATT

#define GATT_ATT (   type,
  permission,
  value 
)
Value:
{\
GATT_ATT_UUID_TYPE(type),\
permission,\
0,\
value\
}

GATT Custom Attribute.

§ GATT_BT_ATT

#define GATT_BT_ATT (   type,
  permission,
  value 
)
Value:
{\
GATT_ATT_BT_UUID_TYPE(type),\
permission,\
0,\
value\
}

GATT BT Attribute.

§ GATT_BT_UUID

#define GATT_BT_UUID (   name,
  UUID 
)
Value:
CONST uint8 name[ATT_BT_UUID_SIZE] =\
{\
LO_UINT16(UUID), HI_UINT16(UUID)\
}
#define ATT_BT_UUID_SIZE
Size of 16-bit Bluetooth UUID.
Definition: att.h:115

GATT BT UUID.

§ GATT_UUID

#define GATT_UUID (   name,
  UUID 
)
Value:
CONST uint8 name[ATT_UUID_SIZE] =\
{\
TI_BASE_UUID_128(UUID)\
}
#define ATT_UUID_SIZE
Size of 128-bit UUID.
Definition: att.h:117

GATT Custom UUID.

Function Documentation

§ GATTServApp_AddService()

bStatus_t GATTServApp_AddService ( uint32  services)

Add function for the GATT Service.

Parameters
services- services to add. This is a bit map and can contain more than one service.
Returns
SUCCESS : Service added successfully.
INVALIDPARAMETER : Invalid service field.
FAILURE : Not enough attribute handles available.
bleMemAllocError

§ GATTServApp_DelService()

bStatus_t GATTServApp_DelService ( uint32  services)

Delete function for the GATT Service.

Parameters
services- services to delete. This is a bit map and can contain more than one service.
Returns
SUCCESS : Service deleted successfully.
FAILURE : Service not found.

§ GATTServApp_DeregisterService()

bStatus_t GATTServApp_DeregisterService ( uint16  handle,
gattAttribute_t **  p2pAttrs 
)

Deregister a service's attribute list and callback functions from the GATT Server Application.

Note
It's the caller's responsibility to free the service attribute list returned from this API.
Parameters
handle- handle of service to be deregistered
p2pAttrs- pointer to array of attribute records (to be returned)
Returns
SUCCESS : Service deregistered successfully.
FAILURE : Service not found.

§ GATTServApp_FindAttr()

gattAttribute_t* GATTServApp_FindAttr ( gattAttribute_t pAttrTbl,
uint16  numAttrs,
uint8 *  pValue 
)

Find the attribute record within a service attribute table for a given attribute value pointer.

Parameters
pAttrTbl- pointer to attribute table
numAttrs- number of attributes in attribute table
pValue- pointer to attribute value
Returns
Pointer to attribute record
NULL, if not found

§ GATTServApp_GetParameter()

bStatus_t GATTServApp_GetParameter ( uint8  param,
void *  pValue 
)

Get a GATT Server parameter.

Parameters
param- GATT Server Parameters
pValue- pointer to data to put. This is dependent on the parameter ID and WILL be cast to the appropriate data type (example: data type of uint16 will be cast to uint16 pointer).
Returns
SUCCESS : Parameter get successful
INVALIDPARAMETER : Invalid parameter

§ GATTServApp_GetParamValue()

uint16 GATTServApp_GetParamValue ( void  )

Get a GATT Server Application Parameter value.

Returns
GATT Parameter value

§ GATTServApp_InitCharCfg()

void GATTServApp_InitCharCfg ( uint16  connHandle,
gattCharCfg_t charCfgTbl 
)

Initialize the client characteristic configuration table.

Note
Each client has its own instantiation of the Client Characteristic Configuration. Reads/Writes of the Client Characteristic Configuration only only affect the configuration of that client.
Parameters
connHandle- connection handle (0xFFFF for all connections).
charCfgTbl- client characteristic configuration table.

§ GATTServApp_ProcessCCCWriteReq()

bStatus_t GATTServApp_ProcessCCCWriteReq ( uint16  connHandle,
gattAttribute_t pAttr,
uint8 *  pValue,
uint16  len,
uint16  offset,
uint16  validCfg 
)

Process the client characteristic configuration write request for a given client.

Parameters
connHandle- connection message was received on.
pAttr- pointer to attribute.
pValue- pointer to data to be written.
len- length of data.
offset- offset of the first octet to be written.
validCfg- valid configuration.
Returns
SUCCESS
FAILURE
ATT_ERR_INVALID_VALUE : an invalid value for a CCC
ATT_ERR_INVALID_VALUE_SIZE : an invalid size for a CCC
ATT_ERR_ATTR_NOT_LONG : offset needs to be 0
ATT_ERR_INSUFFICIENT_RESOURCES : CCC not found

§ GATTServApp_ProcessCharCfg()

bStatus_t GATTServApp_ProcessCharCfg ( gattCharCfg_t charCfgTbl,
uint8 *  pValue,
uint8  authenticated,
gattAttribute_t attrTbl,
uint16  numAttrs,
uint8  taskId,
pfnGATTReadAttrCB_t  pfnReadAttrCB 
)

Process Client Characteristic Configuration change.

Parameters
charCfgTbl- characteristic configuration table.
pValue- pointer to attribute value.
authenticated- whether an authenticated link is required.
attrTbl- attribute table.
numAttrs- number of attributes in attribute table.
taskId- task to be notified of confirmation.
pfnReadAttrCB- read callback function pointer.
Returns
SUCCESS
FAILURE
bleTimeout : ATT timeout occurred
blePending : another ATT request is pending
LINKDB_ERR_INSUFFICIENT_AUTHEN : authentication is required but link is not authenticated
bleMemAllocError : memory allocation failure occurred when allocating buffer

§ GATTServApp_ReadAttr()

uint8 GATTServApp_ReadAttr ( uint16  connHandle,
gattAttribute_t pAttr,
uint16  service,
uint8 *  pValue,
uint16 *  pLen,
uint16  offset,
uint16  maxLen,
uint8  method 
)

Read an attribute. If the format of the attribute value is unknown to GATT Server, use the callback function provided by the Service.

Parameters
connHandle- connection message was received on
pAttr- pointer to attribute
service- handle of owner service
pValue- pointer to data to be read
pLen- length of data to be read
offset- offset of the first octet to be read
maxLen- maximum length of data to be read
method- type of read
Returns
SUCCESS
FAILURE

§ GATTServApp_ReadCharCfg()

uint16 GATTServApp_ReadCharCfg ( uint16  connHandle,
gattCharCfg_t charCfgTbl 
)

Read the client characteristic configuration for a given client.

Note
Each client has its own instantiation of the Client Characteristic Configuration. Reads of the Client Characteristic Configuration only shows the configuration for that client.
Parameters
connHandle- connection handle.
charCfgTbl- client characteristic configuration table.
Returns
attribute value

§ GATTServApp_ReadRsp()

bStatus_t GATTServApp_ReadRsp ( uint16  connHandle,
uint8 *  pValue,
uint16  pLen,
uint16  offset 
)

If a service returns blePending to the read attribute call back invoked from GATTServApp, the service can later respond to with the value to be read using this API.

Parameters
connHandle- connection read request was received on
pValue- pointer to data to be read (to be returned)
pLen- length of data (to be returned)
offset- offset of the first octet to be read
Returns
SUCCESS : Read was successfully added to response.
bleNotConnected : Connection associated with read req is down.

§ GATTServApp_RegisterForMsg()

void GATTServApp_RegisterForMsg ( uint8  taskID)

Register your task ID to receive event messages from the GATT Server Application.

Parameters
taskID- Default task ID to send events.

§ GATTServApp_RegisterService()

bStatus_t GATTServApp_RegisterService ( gattAttribute_t pAttrs,
uint16  numAttrs,
uint8  encKeySize,
CONST gattServiceCBs_t pServiceCBs 
)

Register a service's attribute list and callback functions with the GATT Server Application.

Parameters
pAttrs- Array of attribute records to be registered
numAttrs- Number of attributes in array
encKeySize- Minimum encryption key size required by service (7-16 bytes)
pServiceCBs- Service callback function pointers
Returns
SUCCESS : Service registered successfully.
INVALIDPARAMETER : Invalid service fields.
FAILURE : Not enough attribute handles available.
bleMemAllocError
bleInvalidRange :Encryption key size's out of range.

§ GATTServApp_SendCCCUpdatedEvent()

void GATTServApp_SendCCCUpdatedEvent ( uint16  connHandle,
uint16  attrHandle,
uint16  value 
)

Build and send the GATT_CLIENT_CHAR_CFG_UPDATED_EVENT to the application.

Parameters
connHandle- connection handle
attrHandle- attribute handle
value- attribute new value

§ GATTServApp_SendServiceChangedInd()

bStatus_t GATTServApp_SendServiceChangedInd ( uint16  connHandle,
uint8  taskId 
)

Send out a Service Changed Indication.

Parameters
connHandle- connection to use
taskId- task to be notified of confirmation
Returns
SUCCESS : Indication was sent successfully.
FAILURE : Service Changed attribute not found.
INVALIDPARAMETER
MSG_BUFFER_NOT_AVAIL
bleNotConnected
blePending : A confirmation is pending with this client.

§ GATTServApp_SetParameter()

bStatus_t GATTServApp_SetParameter ( uint8  param,
uint8  len,
void *  pValue 
)

Set a GATT Server parameter.

Parameters
param- GATT Server Parameters
len- length of data to right
pValue- pointer to data to write. This is dependent on the parameter ID and WILL be cast to the appropriate data type (example: data type of uint16 will be cast to uint16 pointer).
Returns
SUCCESS : Parameter set successful
FAILURE : Parameter in use
INVALIDPARAMETER : Invalid parameter
bleInvalidRange :Invalid value
bleMemAllocError : Memory allocation failed

§ GATTServApp_SetParamValue()

void GATTServApp_SetParamValue ( uint16  value)

Set a GATT Server Application Parameter value. Use this function to change the default GATT parameter values.

Parameters
value- new param value

§ GATTServApp_UpdateCharCfg()

bStatus_t GATTServApp_UpdateCharCfg ( uint16  connHandle,
uint16  attrHandle,
uint16  value 
)

Update the Client Characteristic Configuration for a given Client.

Note
This API should only be called from the Bond Manager.
Parameters
connHandle- connection handle.
attrHandle- attribute handle.
value- characteristic configuration value.
Returns
SUCCESS : Parameter get successful
INVALIDPARAMETER : Invalid parameter

§ GATTServApp_WriteAttr()

uint8 GATTServApp_WriteAttr ( uint16  connHandle,
uint16  handle,
uint8 *  pValue,
uint16  len,
uint16  offset,
uint8  method 
)

Write attribute data.

Parameters
connHandle- connection message was received on
handle- attribute handle
pValue- pointer to data to be written
len- length of data
offset- offset of the first octet to be written
method- type of write
Returns
SUCCESS
FAILURE

§ GATTServApp_WriteCharCfg()

uint8 GATTServApp_WriteCharCfg ( uint16  connHandle,
gattCharCfg_t charCfgTbl,
uint16  value 
)

Write the client characteristic configuration for a given client.

Note: Each client has its own instantiation of the Client Characteristic Configuration. Writes of the Client Characteristic Configuration only only affect the configuration of that client.

Parameters
connHandle- connection handle.
charCfgTbl- client characteristic configuration table.
value- attribute new value.
Returns
SUCCESS
FAILURE
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale