TI BLE5-Stack API Documentation
2.02.08.01
|
Macros | |
#define | RTLSSRV_ANTENNA_INFORMATION_EVT 2 |
#define | RTLSSRV_CL_AOA_ENABLE_EVT 12 |
#define | RTLSSRV_CL_CTE_EVT 5 |
#define | RTLSSRV_CL_CTE_IQ_REPORT_EVT 10 |
#define | RTLSSRV_CONNECTION_CTE_IQ_REPORT_EVT 1 |
#define | RTLSSRV_CTE_REQUEST_FAILED_EVT 3 |
#define | RTLSSRV_ERROR_EVT 4 |
#define | RTLSSRV_PERIODIC_ADV_RPT 9 |
#define | RTLSSRV_PERIODIC_ADV_TERMINATE_SYNC 11 |
#define | RTLSSRV_READ_PERIODIC_LIST_SIZE_EVT 6 |
#define | RTLSSRV_SYNC_EST_EVT 7 |
#define | RTLSSRV_SYNC_LOST_EVT 8 |
Event types are used to parse various messages produced by RTLS Services Events are passed using RTLS Services callbacks
#define RTLSSRV_ANTENNA_INFORMATION_EVT 2 |
Antenna information event is received Used to identify rtlsSrv_antennaInfo_t
#define RTLSSRV_CL_AOA_ENABLE_EVT 12 |
Genetated when sampling enable command complete event was received from the controller
#define RTLSSRV_CL_CTE_EVT 5 |
Genetated when CL CTE cmd complete returns
#define RTLSSRV_CL_CTE_IQ_REPORT_EVT 10 |
Genetated when connectionless IQ report was received from the controller
#define RTLSSRV_CONNECTION_CTE_IQ_REPORT_EVT 1 |
CTE I/Q report is received Used to identify rtlsSrv_connectionIQReport_t
#define RTLSSRV_CTE_REQUEST_FAILED_EVT 3 |
Generated when a CTE request fails
#define RTLSSRV_ERROR_EVT 4 |
Generated when an async error occurs
#define RTLSSRV_PERIODIC_ADV_RPT 9 |
Genetated when a periodic advertising packet was received
#define RTLSSRV_PERIODIC_ADV_TERMINATE_SYNC 11 |
Generated when termminate sync command complete event was received from the controller
#define RTLSSRV_READ_PERIODIC_LIST_SIZE_EVT 6 |
Genetated when read adv list size command complete returns
#define RTLSSRV_SYNC_EST_EVT 7 |
Genetated when the controller receives the first periodic advertising packet
#define RTLSSRV_SYNC_LOST_EVT 8 |
Genetated when the controller has not received a periodic advertising packets