|
void | uDMAChannelAttributeEnable (uint32_t ui32Base, uint32_t ui32ChannelNum, uint32_t ui32Attr) |
| Enables attributes of a uDMA channel. More...
|
|
void | uDMAChannelAttributeDisable (uint32_t ui32Base, uint32_t ui32ChannelNum, uint32_t ui32Attr) |
| Disables attributes of an uDMA channel. More...
|
|
uint32_t | uDMAChannelAttributeGet (uint32_t ui32Base, uint32_t ui32ChannelNum) |
| Gets the enabled attributes of a uDMA channel. More...
|
|
void | uDMAChannelControlSet (uint32_t ui32Base, uint32_t ui32ChannelStructIndex, uint32_t ui32Control) |
| Sets the control parameters for a uDMA channel control structure. More...
|
|
void | uDMAChannelTransferSet (uint32_t ui32Base, uint32_t ui32ChannelStructIndex, uint32_t ui32Mode, void *pvSrcAddr, void *pvDstAddr, uint32_t ui32TransferSize) |
| Sets the transfer parameters for a uDMA channel control structure. More...
|
|
void | uDMAChannelScatterGatherSet (uint32_t ui32Base, uint32_t ui32ChannelNum, uint32_t ui32TaskCount, void *pvTaskList, uint32_t ui32IsPeriphSG) |
| Configures a uDMA channel for scatter-gather mode. More...
|
|
uint32_t | uDMAChannelSizeGet (uint32_t ui32Base, uint32_t ui32ChannelStructIndex) |
| Gets the current transfer size for a uDMA channel control structure. More...
|
|
uint32_t | uDMAChannelModeGet (uint32_t ui32Base, uint32_t ui32ChannelStructIndex) |
| Gets the transfer mode for a uDMA channel control structure. More...
|
|