67 #ifndef ti_drivers_sha2_SHA2CC26X1__include 68 #define ti_drivers_sha2_SHA2CC26X1__include 75 #include <ti/devices/DeviceFamily.h> 76 #include DeviceFamily_constructPath(driverlib/rom_sha256.h) 106 SHA256_Workzone workzone;
uint8_t dummy
Definition: SHA2CC26X1.h:90
SHA2_ReturnBehavior
The way in which SHA2 function calls return after performing an operation.
Definition: SHA2.h:374
Hardware-specific configuration attributes.
Definition: SHA2CC26X1.h:88
void(* SHA2_CallbackFxn)(SHA2_Handle handle, int_fast16_t returnStatus)
The definition of a callback function used by the SHA2 driver when used in SHA2_RETURN_BEHAVIOR_CALLB...
Definition: SHA2.h:470