Hardware-specific configuration attributes. More...
#include <SHA2CC26X1.h>
Data Fields | |
uint8_t | dummy |
Hardware-specific configuration attributes.
SHA2CC26X1 hardware attributes are used in the board file by the SHA2_Config struct.
uint8_t SHA2CC26X1_HWAttrs::dummy |