CCM Parameters. More...
#include <AESCCM.h>
Data Fields | |
AESCCM_ReturnBehavior | returnBehavior |
AESCCM_CallbackFxn | callbackFxn |
uint32_t | timeout |
void * | custom |
CCM Parameters.
CCM Parameters used with the AESCCM_open() call. Default values for these parameters are set using AESCCM_Params_init().
AESCCM_ReturnBehavior AESCCM_Params::returnBehavior |
Blocking, callback, or polling return behavior
AESCCM_CallbackFxn AESCCM_Params::callbackFxn |
Callback function pointer
uint32_t AESCCM_Params::timeout |
Timeout before the driver returns an error in AESCCM_RETURN_BEHAVIOR_BLOCKING
void* AESCCM_Params::custom |
Custom argument used by driver implementation