TI BLE5-Stack API Documentation
2.02.08.01
|
Macros | |
#define | GAPBOND_ALLOW_DEBUG_KEYS 0x416 |
#define | GAPBOND_AUTHEN_PAIRING_ONLY 0x41B |
#define | GAPBOND_AUTO_SYNC_WL 0x40D |
#define | GAPBOND_BOND_COUNT 0x40E |
#define | GAPBOND_BOND_FAIL_ACTION 0x40F |
#define | GAPBOND_BONDING_ENABLED 0x406 |
#define | GAPBOND_ECC_KEYS 0x413 |
#define | GAPBOND_ECCKEY_REGEN_POLICY 0x412 |
#define | GAPBOND_ERASE_ALLBONDS 0x409 |
#define | GAPBOND_ERASE_BOND_IN_CONN 0x415 |
#define | GAPBOND_ERASE_LOCAL_INFO 0x41A |
#define | GAPBOND_ERASE_SINGLEBOND 0x410 |
#define | GAPBOND_IO_CAPABILITIES 0x403 |
#define | GAPBOND_KEY_DIST_LIST 0x407 |
#define | GAPBOND_KEYSIZE 0x40C |
#define | GAPBOND_LRU_BOND_REPLACEMENT 0x418 |
#define | GAPBOND_MITM_PROTECTION 0x402 |
#define | GAPBOND_OOB_DATA 0x405 |
#define | GAPBOND_OOB_ENABLED 0x404 |
#define | GAPBOND_PAIRING_MODE 0x400 |
#define | GAPBOND_SAME_IRK_OPTION 0x41C |
#define | GAPBOND_SC_HOST_DEBUG 0x414 |
#define | GAPBOND_SECURE_CONNECTION 0x411 |
Parameters set via GAPBondMgr_SetParameter
#define GAPBOND_ALLOW_DEBUG_KEYS 0x416 |
Allows to receive debug keys during pairing, in the public keys exchange phase.
If TRUE, receiving debug keys is allowed. If FALSE, receiving debug keys is not allowed, pairing will fail with invalid paramters code.
size: uint8_t
default: TRUE
range: TRUE (allow receiving debug keys). FALSE(reject debug keys).
#define GAPBOND_AUTHEN_PAIRING_ONLY 0x41B |
Whether to enfore authenticated pairing (Read/Write)
size: uint8_t
default: FALSE
range: TRUE (enforce) or FALSE (do not enforce)
#define GAPBOND_AUTO_SYNC_WL 0x40D |
Synchronize the whitelist with bonded devices (Read/Write)
If TRUE, the whitelist will first be cleared. Then, each unique address stored by bonds in SNV will be synched with the whitelist indefinitely or until this is set to FALSE
size: uint8_t
default: FALSE
range: TRUE (sync) or FALSE (don't sync)
#define GAPBOND_BOND_COUNT 0x40E |
Gets the total number of bonds stored in NV (Read-only)
size: uint8_t
range: 0 255
#define GAPBOND_BOND_FAIL_ACTION 0x40F |
The action that the device takes after an unsuccessful bonding attempt (Read / Write)
size: uint8_t
default: GAPBOND_FAIL_TERMINATE_ERASE_SINGLE_BOND
range: Bonding Failure Actions
#define GAPBOND_BONDING_ENABLED 0x406 |
Whether to bond after pairing (Read/Write)
size: uint8_t
default: FALSE
range: TRUE (request) or FALSE (do not request)
#define GAPBOND_ECC_KEYS 0x413 |
The private and public keys to use for Secure Connections pairing (Read/Write)
Only applicable for Secure Connections. Allows the application to specify the private and public keys to use pairing. When this is set, the keys are used indefinitely even if a regeneration policy was set with GAPBOND_ECCKEY_REGEN_POLICY. To make the Bond Manager stop using these keys, pass a 1 byte value of 0x00. These keys are stored in RAM and are not retained in non-volatile memory. These keys can be defined by the application, or the application can request them using the SM_GetEccKeys command.
size: gapBondEccKeys_t
default: by default, the keys are generated using GAPBOND_ECCKEY_REGEN_POLICY
range: A valid gapBondEccKeys_t structure
0x00: previously passed keys will no longer be used
#define GAPBOND_ECCKEY_REGEN_POLICY 0x412 |
ECC Key Regeneration Policy (Write Only)
Only applicable for Secure Connections. Define reuse of the private and public ECC keys for multiple pairings.The default is to always regenerate the keys upon each new pairing. This parameter has no effect when the application specifies the keys using the GAPBOND_ECC_KEYS parameter. The behavior is that upon each pairing the number of recycles remaining is decremented by 1, but if the pairing fails the count is decremented by 3. The specification recommends that this value be set to no higher than 10 to avoid an attacker from learning too much about a private key before it is regenerated.
size: uint8_t
default: 2
range: 0 256
#define GAPBOND_ERASE_ALLBONDS 0x409 |
Erase all bonds from SNV and remove all bonded devices (Write)
#define GAPBOND_ERASE_BOND_IN_CONN 0x415 |
Allows to erase a bond even if there are active connections
If TRUE, a bond can be erased even if there are active connections. If FALSE, a bond can be erased only when there are no active connections.
size: uint8_t
default: FALSE
range: TRUE (erase a bond when there are active connections). FALSE(erase a bond when there are no active connections).
#define GAPBOND_ERASE_LOCAL_INFO 0x41A |
Erase Local NV Info (Write-only)
Erase local IRK, CSRK, address mode, LRU list, random address.
#define GAPBOND_ERASE_SINGLEBOND 0x410 |
Erase a single bonded device (Write-only)
size: uint8_t[B_ADDR_LEN]
range: A one-byte address type followed by a 6 byte address
#define GAPBOND_IO_CAPABILITIES 0x403 |
The I/O capabilities of the local device (Read/Write)
size: uint8_t
default: GAPBOND_IO_CAP_DISPLAY_ONLY
#define GAPBOND_KEY_DIST_LIST 0x407 |
Key distribution list for pairing (Read/Write)
Multiple values can be used via bitwise ORing
size: uint8_t
default: GAPBOND_KEYDIST_SENCKEY | GAPBOND_KEYDIST_SIDKEY | GAPBOND_KEYDIST_MIDKEY | GAPBOND_KEYDIST_MSIGN
#define GAPBOND_KEYSIZE 0x40C |
Key Size used in pairing. (Read/Write)
size: uint8_t
default: 16
#define GAPBOND_LRU_BOND_REPLACEMENT 0x418 |
Enable / Disable LRU Bond Replacement Scheme (Read/Write)
Whether to enable the least recently used bond scheme so that, when a newly bonded device is added and all the entries are full, the least recently used device’s bond is deleted to make room.
size: uint8_t
default: FALSE
range: TRUE (enable) or FALSE (disable)
#define GAPBOND_MITM_PROTECTION 0x402 |
Whether to use authenticated pairing (Read/Write)
size: uint8_t
default: TRUE
range: TRUE (use) or FALSE (do not use)
#define GAPBOND_OOB_DATA 0x405 |
OOB data to use for pairing (Read/Write)
size: uint8_t[16]
default: 0x00000000000000000000000000000000 -
range: 0x00000000000000000000000000000000 - 0xFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF
#define GAPBOND_OOB_ENABLED 0x404 |
Whether to use OOB for pairing (Read/Write)
size: uint8_t
default: FALSE
range: TRUE (use) or FALSE (do not use)
#define GAPBOND_PAIRING_MODE 0x400 |
Whether to allow pairing, and if so, whether to initiate pairing. (Read/Write)
size: uint8_t
default: GAPBOND_PAIRING_MODE_WAIT_FOR_REQ
#define GAPBOND_SAME_IRK_OPTION 0x41C |
The action that the device takes after receiving an IRK that is already exists in the resolving list
size: uint8_t
default: GAPBOND_SAME_IRK_UPDATE_BOND_REC
#define GAPBOND_SC_HOST_DEBUG 0x414 |
Whether to enable SC_HOST_DEBUG
size: uint8_t
default: FALSE
range: TRUE (enabled) or FALSE (do not enabled)
#define GAPBOND_SECURE_CONNECTION 0x411 |
Define Secure Connections Usage during Pairing (Read/Write)
size: uint8_t
default: GAPBOND_SECURE_CONNECTION_ALLOW