Data Structures | Macros | Typedefs | Enumerations | Functions | Variables
AESCMAC.h File Reference

Detailed Description

AESCMAC (CMAC and CBC-MAC) driver header.

Overview

The Cipher-based Message Authentication Code (CMAC) and Cipher Block Chaining Message Authentication Code (CBC-MAC) are generic block cipher modes of operation. They can be used with any block cipher but this driver implementation uses AES.

Both CMAC and CBC-MAC create a message authentication code from a message of any practical length to provide authenticity and integrity assurances. CMAC is recommended over CBC-MAC because CBC-MAC is not secure for variable length messages.

CBC-MAC Drawbacks

CBC-MAC is only secure for fixed-length messages. Any single key must only be used for messages of a fixed and known length. The CMAC algorithm, which is based on a variation of CBC-MAC at its core, was developed to address that security deficiency and is the MAC algorithm recommended by NIST.

CMAC Usage

Before starting a CMAC operation

Before starting a CMAC operation, the application must do the following:

Starting a CMAC operation

The AESCMAC_oneStepSign and AESCMAC_oneStepVerify functions perform a CMAC operation in a single call. They will always be the most highly optimized routines with the least overhead and the fastest runtime. However, they require all plaintext or ciphertext to be available to the function at the start of the call. All devices support single call operations.

After the CMAC operation completes

After the CMAC operation completes, the application should either start another operation or close the driver by calling AESCMAC_close().

Synopsis

// Import CMAC Driver definitions
#include <ti/drivers/CMAC.h>
// Define name for CMAC channel index
#define AESCMAC_INSTANCE 0
handle = AESCMAC_open(AESCMAC_INSTANCE, NULL);
// Initialize symmetric key
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
// Initialize the operation
operation.input = input;
operation.inputLength = sizeof(input);
operation.mac = mac;
operation.macLength = sizeof(mac);
signResult = AESCMAC_oneStepSign(handle, &operation, &cryptoKey);
AESCMAC_close(handle);

Examples

### Single call CMAC authentication with plaintext CryptoKey in blocking return mode #

...
uint8_t message[16] = {0x6B, 0xC1, 0xBE, 0xE2, 0x2E, 0x40, 0x9F, 0x96,
0xE9, 0x3D, 0x7E, 0x11, 0x73, 0x93, 0x17, 0x2A};
uint8_t keyingMaterial[16] = {0x2B, 0x7E, 0x15, 0x16, 0x28, 0xAE, 0xD2, 0xA6,
0xAB, 0xF7, 0x15, 0x88, 0x09, 0xCF, 0x4F, 0x3C};
uint8_t mac[16];
...
CryptoKey cryptoKey;
AESCMAC_Handle handle = AESCMAC_open(0, NULL);
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
operation.input = input;
operation.inputLength = sizeof(input);
operation.mac = mac;
operation.macLength = sizeof(mac);
int_fast16_t result = AESCMAC_oneStepSign(handle, &operation, &cryptoKey);
if (result != AESCMAC_STATUS_SUCCESS) {
// handle error
}
// The resulting MAC should equal the following after the operation:
// 0x07, 0x0A, 0x16, 0xB4, 0x6B, 0x4D, 0x41, 0x44,
// 0xF7, 0x9B, 0xDD, 0x9D, 0xD0, 0x4A, 0x28, 0x7C
AESCMAC_close(handle);

### Single call CMAC verification with plaintext CryptoKey in callback return mode #

...
uint8_t message[16] = {0x6B, 0xC1, 0xBE, 0xE2, 0x2E, 0x40, 0x9F, 0x96,
0xE9, 0x3D, 0x7E, 0x11, 0x73, 0x93, 0x17, 0x2A};
uint8_t keyingMaterial[16] = {0x2B, 0x7E, 0x15, 0x16, 0x28, 0xAE, 0xD2, 0xA6,
0xAB, 0xF7, 0x15, 0x88, 0x09, 0xCF, 0x4F, 0x3C};
uint8_t expectedMac[16] = {0x07, 0x0A, 0x16, 0xB4, 0x6B, 0x4D, 0x41, 0x44,
0xF7, 0x9B, 0xDD, 0x9D, 0xD0, 0x4A, 0x28, 0x7C};
void cmacCallback(AESCMAC_Handle handle,
int_fast16_t returnValue) {
if (returnValue != AESCMAC_STATUS_SUCCESS) {
// handle error
}
}
void cmacStartFunction(void) {
AESCMAC_Operation operation;
CryptoKey cryptoKey;
int_fast16_t verificationResult;
params.callbackFxn = cmacCallback;
handle = AESCMAC_open(0, &params);
if (handle == NULL) {
// handle error
}
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
operation.input = input;
operation.inputLength = sizeof(input);
operation.mac = expectedMac;
operation.macLength = sizeof(expectedMac);
verificationResult = AESCMAC_oneStepVerify(handle, &operation, &cryptoKey);
if (verificationResult != AESCMAC_STATUS_SUCCESS) {
// handle error
}
// do other things while CMAC operation completes in the background
}

### Multi-step CMAC signature with plaintext CryptoKey in blocking return mode #

#define AES_BLOCK_SIZE 16 // bytes
...
uint8_t keyingMaterial[32] = {0x60, 0x3d, 0xeb, 0x10, 0x15, 0xca, 0x71, 0xbe,
0x2b, 0x73, 0xae, 0xf0, 0x85, 0x7d, 0x77, 0x81,
0x1f, 0x35, 0x2c, 0x07, 0x3b, 0x61, 0x08, 0xd7,
0x2d, 0x98, 0x10, 0xa3, 0x09, 0x14, 0xdf, 0xf4};
uint8_t message[40] = {0x6b, 0xc1, 0xbe, 0xe2, 0x2e, 0x40, 0x9f, 0x96,
0xe9, 0x3d, 0x7e, 0x11, 0x73, 0x93, 0x17, 0x2a,
0xae, 0x2d, 0x8a, 0x57, 0x1e, 0x03, 0xac, 0x9c,
0x9e, 0xb7, 0x6f, 0xac, 0x45, 0xaf, 0x8e, 0x51,
0x30, 0xc8, 0x1c, 0x46, 0xa3, 0x5c, 0xe4, 0x11};
uint8_t mac[16];
CryptoKey cryptoKey;
AESCMAC_Operation operation;
AESCMAC_Handle handle = AESCMAC_open(0, NULL);
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
// Set up multi-step sign.
int_fast16_t result = AESCMAC_setupSign(handle, &cryptoKey);
if (result != AESCMAC_STATUS_SUCCESS) {
// handle error
}
size_t initialSegmentSize = AES_BLOCK_SIZE;
// Add first segment of data.
operation.input = input;
operation.inputLength = initialSegmentSize; // Must be a non-zero multiple of the block size (16-bytes) unless
finalizing. result = AESCMAC_addData(handle, &operation);
if (result != AESCMAC_STATUS_SUCCESS) {
// handle error
}
// Finalize with the last segment of data.
operation.input = &input[initialSegmentSize];
operation.inputLength = sizeof(input) - initialSegmentSize;
operation.mac = mac;
operation.macLength = sizeof(mac);
result = AESCMAC_finalize(handle, &operation);
if (result != AESCMAC_STATUS_SUCCESS) {
// handle error
}
// The resulting MAC should equal the following after the operation:
// 0xaa, 0xf3, 0xd8, 0xf1, 0xde, 0x56, 0x40, 0xc2,
// 0x32, 0xf5, 0xb1, 0x69, 0xb9, 0xc9, 0x11, 0xe6
...
AESCMAC_close(handle);

CBC-MAC Usage

Before starting a CBC-MAC operation

Before starting a CBC-MAC operation, the application must do the following:

Starting a CBC-MAC operation

The AESCMAC_oneStepSign and AESCMAC_oneStepVerify functions perform a CBC-MAC operation in a single call. They will always be the most highly optimized routines with the least overhead and the fastest runtime. However, they require all plaintext or ciphertext to be available to the function at the start of the call. All devices support single call operations.

After the CBC-MAC operation completes

After the CBC-MAC operation completes, the application should either start another operation or close the driver by calling AESCMAC_close().

Synopsis

// Import AESCMAC Driver definitions
// Define name for AESCMAC channel index
#define AESCMAC_INSTANCE 0
handle = AESCMAC_open(AESCMAC_INSTANCE, &params);
// Initialize symmetric key
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
// Set up AESCMAC_Operation
operation.input = plaintext;
operation.inputLength = sizeof(plaintext);
operation.mac = mac;
operation.macLength = sizeof(mac);
signResult = AESCMAC_oneStepSign(handle, &operation);
AESCMAC_close(handle);

Examples

### One step AES CBC-MAC signature with plaintext CryptoKey in blocking return mode #

...
AESCMAC_Params params;
CryptoKey cryptoKey;
int_fast16_t signResult;
// For example purposes only.
// Test vector derived from RFC 3602 Case #2
uint8_t plaintext[32] = {0x56, 0x2F, 0x15, 0x9A, 0x69, 0x0C, 0x3B, 0x2F,
0xD5, 0xBA, 0xB0, 0x62, 0x56, 0x23, 0x61, 0x57,
0x10, 0x11, 0x12, 0x13, 0x14, 0x15, 0x16, 0x17,
0x18, 0x19, 0x1A, 0x1B, 0x1C, 0x1D, 0x1E, 0x1F};
uint8_t mac[16];
uint8_t keyingMaterial[16] = {0xC2, 0x86, 0x69, 0x6D, 0x88, 0x7C, 0x9A, 0xA0,
0x61, 0x1B, 0xBB, 0x3E, 0x20, 0x25, 0xA4, 0x5A};
// The MAC should equal the following after the operation:
// 0x75, 0x86, 0x60, 0x2D, 0x25, 0x3C, 0xFF, 0xF9,
// 0x1B, 0x82, 0x66, 0xBE, 0xA6, 0xD6, 0x1A, 0xB1
handle = AESCMAC_open(0, &params);
if (handle == NULL) {
// handle error
}
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
AESCMAC_Operation_init(&operation); // Optional as all struct members will be set before use.
operation.input = plaintext;
operation.inputLength = sizeof(plaintext);
operation.mac = mac;
operation.macLength = sizeof(mac);
signResult = AESCMAC_oneStepSign(handle, &operation, &cryptoKey);
if (signResult == AESCMAC_STATUS_SUCCESS) {
// signature is available in mac[] buffer.
}
else {
// handle error
}
AESCMAC_close(handle);

Multi-step AES CBC-MAC verify with plaintext CryptoKey in polling return mode

#include <ti/drivers/types/cryptoKey/CryptoKey_Plaintext.h>
#define AES_BLOCK_SIZE 16 // bytes
...
CryptoKey cryptoKey;
int_fast16_t retVal;
// For example purposes only.
// Test vector derived from RFC 3602 Case #2
uint8_t plaintext[32] = {0x56, 0x2F, 0x15, 0x9A, 0x69, 0x0C, 0x3B, 0x2F,
0xD5, 0xBA, 0xB0, 0x62, 0x56, 0x23, 0x61, 0x57,
0x10, 0x11, 0x12, 0x13, 0x14, 0x15, 0x16, 0x17,
0x18, 0x19, 0x1A, 0x1B, 0x1C, 0x1D, 0x1E, 0x1F};
uint8_t mac[16] = {0x75, 0x86, 0x60, 0x2D, 0x25, 0x3C, 0xFF, 0xF9,
0x1B, 0x82, 0x66, 0xBE, 0xA6, 0xD6, 0x1A, 0xB1}
uint8_t keyingMaterial[16] = {0xC2, 0x86, 0x69, 0x6D, 0x88, 0x7C, 0x9A, 0xA0,
0x61, 0x1B, 0xBB, 0x3E, 0x20, 0x25, 0xA4, 0x5A};
params.returnBehavior = AESCMAC_RETURN_BEHAVIOR_POLLING;
params.operationalMode = AESCMAC_OPMODE_CBCMAC;
handle = AESCMAC_open(0, &params);
if (handle == NULL) {
// handle error
}
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
AESCMAC_Operation operation;
AESCMAC_Operation_init(&operation); // Optional as all struct members will be set before use.
retVal = AESCMAC_setupVerify(handle, &cryptoKey);
if (retVal != AESCMAC_STATUS_SUCCESS) {
// handle error
}
operation.input = plaintext;
operation.inputLength = AES_BLOCK_SIZE; // Must be a non-zero multiple of the block size (16-bytes) unless
finalizing.
// Note: MAC pointer only needs to be set when finalizing operation.
retVal = AESCMAC_addData(handle, &operation);
if (retVal != AESCMAC_STATUS_SUCCESS) {
// handle error
}
operation.input = plaintext + AES_BLOCK_SIZE;
operation.inputLength = AES_BLOCK_SIZE;
operation.mac = mac;
operation.macLength = sizeof(mac);
retVal = AESCMAC_finalize(handle, &operation);
// retVal should be AESCMAC_STATUS_SUCCESS to indicate that the signature
// verification passed.
if (retVal == AESCMAC_STATUS_MAC_INVALID) {
// handle invalid MAC
}
else if (retVal != AESCMAC_STATUS_SUCCESS) {
// handle error
}
AESCMAC_close(handle);
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/drivers/AESCommon.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKey.h>
Include dependency graph for AESCMAC.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  AESCMAC_Operation
 Struct containing the parameters required for signing or verifying a message. More...
 
struct  AESCMAC_Params
 AESCMAC Parameters. More...
 

Macros

#define AESCMAC_STATUS_RESERVED   AES_STATUS_RESERVED
 
#define AESCMAC_STATUS_SUCCESS   AES_STATUS_SUCCESS
 Successful status code. More...
 
#define AESCMAC_STATUS_ERROR   AES_STATUS_ERROR
 Generic error status code. More...
 
#define AESCMAC_STATUS_RESOURCE_UNAVAILABLE   AES_STATUS_RESOURCE_UNAVAILABLE
 An error status code returned if the hardware or software resource is currently unavailable. More...
 
#define AESCMAC_STATUS_MAC_INVALID   AES_STATUS_MAC_INVALID
 The MAC verification failed. More...
 
#define AESCMAC_STATUS_CANCELED   AES_STATUS_CANCELED
 The ongoing operation was canceled. More...
 
#define AESCMAC_STATUS_KEYSTORE_INVALID_ID   AES_STATUS_KEYSTORE_INVALID_ID
 The operation tried to load a key from the keystore using an invalid key ID. More...
 
#define AESCMAC_STATUS_KEYSTORE_GENERIC_ERROR   AES_STATUS_KEYSTORE_GENERIC_ERROR
 The key store module returned a generic error. See key store documentation for additional details. More...
 
#define AESCMAC_STATUS_UNALIGNED_IO_NOT_SUPPORTED   AES_STATUS_UNALIGNED_IO_NOT_SUPPORTED
 The operation does not support non-word-aligned input. More...
 
#define AESCMAC_OP_CODE_MASK   0x0F /* bits 0-3 */
 Mask for the operation code. More...
 
#define AESCMAC_OP_FLAG_SIGN   0x10 /* bit 4 */
 Flag indicating a sign operation. If this bit is not set, then it is a verify operation. More...
 
#define AESCMAC_OP_FLAGS_MASK   (AESCMAC_OP_FLAG_SIGN | AESCMAC_OP_FLAG_VERIFY)
 Mask for all valid operation flags. More...
 

Typedefs

typedef AESCommon_Config AESCMAC_Config
 CMAC Global configuration. More...
 
typedef AESCMAC_ConfigAESCMAC_Handle
 A handle that is returned from an AESCMAC_open() call. More...
 
typedef void(* AESCMAC_CallbackFxn) (AESCMAC_Handle handle, int_fast16_t returnValue, AESCMAC_Operation *operation, AESCMAC_OperationType operationType)
 The definition of a callback function used by the AESCMAC driver when used in AESCMAC_RETURN_BEHAVIOR_CALLBACK. More...
 

Enumerations

enum  AESCMAC_ReturnBehavior { AESCMAC_RETURN_BEHAVIOR_CALLBACK = AES_RETURN_BEHAVIOR_CALLBACK, AESCMAC_RETURN_BEHAVIOR_BLOCKING = AES_RETURN_BEHAVIOR_BLOCKING, AESCMAC_RETURN_BEHAVIOR_POLLING = AES_RETURN_BEHAVIOR_POLLING }
 The return behavior of AESCMAC functions. More...
 
enum  AESCMAC_OperationalMode { AESCMAC_OPMODE_CMAC = 1, AESCMAC_OPMODE_CBCMAC = 2 }
 Defines the operation modes for the AESCMAC driver. More...
 
enum  AESCMAC_OperationCode { AESCMAC_OP_CODE_ONE_STEP = 0, AESCMAC_OP_CODE_SEGMENTED, AESCMAC_OP_CODE_FINALIZE }
 Enum for the operation codes supported by the driver. More...
 
enum  AESCMAC_OperationType {
  AESCMAC_OP_TYPE_SIGN = AESCMAC_OP_CODE_ONE_STEP | 0x10, AESCMAC_OP_TYPE_VERIFY = AESCMAC_OP_CODE_ONE_STEP, AESCMAC_OP_TYPE_SEGMENTED_SIGN = AESCMAC_OP_CODE_SEGMENTED | 0x10, AESCMAC_OP_TYPE_SEGMENTED_VERIFY = AESCMAC_OP_CODE_SEGMENTED,
  AESCMAC_OP_TYPE_FINALIZE_SIGN = AESCMAC_OP_CODE_FINALIZE | 0x10, AESCMAC_OP_TYPE_FINALIZE_VERIFY = AESCMAC_OP_CODE_FINALIZE
}
 Enum for the operation types supported by the driver. More...
 

Functions

void AESCMAC_init (void)
 Initializes the CMAC module. More...
 
void AESCMAC_Params_init (AESCMAC_Params *params)
 Initializes the AESCMAC_Params struct to its defaults. More...
 
void AESCMAC_Operation_init (AESCMAC_Operation *operation)
 Initializes an AESCMAC_Operation struct to its defaults. More...
 
AESCMAC_Handle AESCMAC_open (uint_least8_t index, const AESCMAC_Params *params)
 Opens a given AESCMAC peripheral. More...
 
void AESCMAC_close (AESCMAC_Handle handle)
 Closes a AESCMAC peripheral specified by the CMAC handle. More...
 
int_fast16_t AESCMAC_setupSign (AESCMAC_Handle handle, const CryptoKey *key)
 Prepares a segmented AESCMAC sign operation. More...
 
int_fast16_t AESCMAC_setupVerify (AESCMAC_Handle handle, const CryptoKey *key)
 Prepares a segmented AESCMAC verify operation. More...
 
int_fast16_t AESCMAC_addData (AESCMAC_Handle handle, AESCMAC_Operation *operation)
 Adds data to the current segmented operation. More...
 
int_fast16_t AESCMAC_finalize (AESCMAC_Handle handle, AESCMAC_Operation *operation)
 Finalizes the current segmented operation. More...
 
int_fast16_t AESCMAC_oneStepSign (AESCMAC_Handle handle, AESCMAC_Operation *operation, CryptoKey *key)
 Performs a AESCMAC signature in one call. More...
 
int_fast16_t AESCMAC_oneStepVerify (AESCMAC_Handle handle, AESCMAC_Operation *operation, CryptoKey *key)
 Performs a AESCMAC verification in one call. More...
 
int_fast16_t AESCMAC_cancelOperation (AESCMAC_Handle handle)
 Cancels an ongoing AESCMAC operation. More...
 
AESCMAC_Handle AESCMAC_construct (AESCMAC_Config *config, const AESCMAC_Params *params)
 Constructs a new AESCMAC object. More...
 

Variables

const AESCMAC_Params AESCMAC_defaultParams
 Default AESCMAC_Params structure. More...
 

Macro Definition Documentation

§ AESCMAC_STATUS_RESERVED

#define AESCMAC_STATUS_RESERVED   AES_STATUS_RESERVED

Common CMAC status code reservation offset. CMAC driver implementations should offset status codes with AESCMAC_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

#define AESCMACXYZ_STATUS_ERROR0 AESCMAC_STATUS_RESERVED - 0
#define AESCMACXYZ_STATUS_ERROR1 AESCMAC_STATUS_RESERVED - 1
#define AESCMACXYZ_STATUS_ERROR2 AESCMAC_STATUS_RESERVED - 2

§ AESCMAC_STATUS_SUCCESS

#define AESCMAC_STATUS_SUCCESS   AES_STATUS_SUCCESS

Successful status code.

Functions return AESCMAC_STATUS_SUCCESS if the function was executed successfully.

§ AESCMAC_STATUS_ERROR

#define AESCMAC_STATUS_ERROR   AES_STATUS_ERROR

Generic error status code.

Functions return AESCMAC_STATUS_ERROR if the function was not executed successfully and no more pertinent error code could be returned.

§ AESCMAC_STATUS_RESOURCE_UNAVAILABLE

#define AESCMAC_STATUS_RESOURCE_UNAVAILABLE   AES_STATUS_RESOURCE_UNAVAILABLE

An error status code returned if the hardware or software resource is currently unavailable.

CMAC driver implementations may have hardware or software limitations on how many clients can simultaneously perform operations. This status code is returned if the mutual exclusion mechanism signals that an operation cannot currently be performed.

§ AESCMAC_STATUS_MAC_INVALID

#define AESCMAC_STATUS_MAC_INVALID   AES_STATUS_MAC_INVALID

The MAC verification failed.

Functions return AESCMAC_STATUS_MAC_INVALID if the MAC computed for the provided (key, message) pair did not match the MAC provided.

§ AESCMAC_STATUS_CANCELED

#define AESCMAC_STATUS_CANCELED   AES_STATUS_CANCELED

The ongoing operation was canceled.

§ AESCMAC_STATUS_KEYSTORE_INVALID_ID

#define AESCMAC_STATUS_KEYSTORE_INVALID_ID   AES_STATUS_KEYSTORE_INVALID_ID

The operation tried to load a key from the keystore using an invalid key ID.

§ AESCMAC_STATUS_KEYSTORE_GENERIC_ERROR

#define AESCMAC_STATUS_KEYSTORE_GENERIC_ERROR   AES_STATUS_KEYSTORE_GENERIC_ERROR

The key store module returned a generic error. See key store documentation for additional details.

§ AESCMAC_STATUS_UNALIGNED_IO_NOT_SUPPORTED

#define AESCMAC_STATUS_UNALIGNED_IO_NOT_SUPPORTED   AES_STATUS_UNALIGNED_IO_NOT_SUPPORTED

The operation does not support non-word-aligned input.

AESCMAC driver implementations may have restrictions on the alignment of input data due to performance limitations of the hardware.

§ AESCMAC_OP_CODE_MASK

#define AESCMAC_OP_CODE_MASK   0x0F /* bits 0-3 */

Mask for the operation code.

§ AESCMAC_OP_FLAG_SIGN

#define AESCMAC_OP_FLAG_SIGN   0x10 /* bit 4 */

Flag indicating a sign operation. If this bit is not set, then it is a verify operation.

§ AESCMAC_OP_FLAGS_MASK

#define AESCMAC_OP_FLAGS_MASK   (AESCMAC_OP_FLAG_SIGN | AESCMAC_OP_FLAG_VERIFY)

Mask for all valid operation flags.

Typedef Documentation

§ AESCMAC_Config

CMAC Global configuration.

The AESCMAC_Config structure contains a set of pointers used to characterize the CMAC driver implementation.

This structure needs to be defined before calling AESCMAC_init() and it must not be changed thereafter.

See also
AESCMAC_init()

§ AESCMAC_Handle

A handle that is returned from an AESCMAC_open() call.

§ AESCMAC_CallbackFxn

typedef void(* AESCMAC_CallbackFxn) (AESCMAC_Handle handle, int_fast16_t returnValue, AESCMAC_Operation *operation, AESCMAC_OperationType operationType)

The definition of a callback function used by the AESCMAC driver when used in AESCMAC_RETURN_BEHAVIOR_CALLBACK.

Parameters
handleHandle of the client that started the AESCMAC operation.
returnValueThe result of the AESCMAC operation. May contain an error code. Informs the application of why the callback function was called.
operationPointer to an operation struct.
operationTypeIndicates which operation the callback refers to.

Enumeration Type Documentation

§ AESCMAC_ReturnBehavior

The return behavior of AESCMAC functions.

Not all AESCMAC operations exhibit the specified return behavior. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specified return behavior is not implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.

AESCMAC functions exhibiting the specified return behavior have restrictions on the context from which they may be called.

Task Hwi Swi
AESCMAC_RETURN_BEHAVIOR_CALLBACK X X X
AESCMAC_RETURN_BEHAVIOR_BLOCKING X
AESCMAC_RETURN_BEHAVIOR_POLLING X X X
Enumerator
AESCMAC_RETURN_BEHAVIOR_CALLBACK 

The function call will return immediately while the MAC operation goes on in the background. The registered callback function is called after the operation completes. The context the callback function is called (task, HWI, SWI) is implementation-dependent.

AESCMAC_RETURN_BEHAVIOR_BLOCKING 

The function call will block while the MAC operation goes on in the background. MAC operation results are available after the function returns.

AESCMAC_RETURN_BEHAVIOR_POLLING 

The function call will continuously poll a flag while MAC operation goes on in the background. MAC operation results are available after the function returns.

§ AESCMAC_OperationalMode

Defines the operation modes for the AESCMAC driver.

By default, the driver will use CMAC to sign and verify messages. To use CBC-MAC instead of CMAC, set the operationalMode in AESCMAC_Params accordingly before calling AESCMAC_open or AESCMAC_construct. The operational mode persists throughout the existance of the driver instance.

Enumerator
AESCMAC_OPMODE_CMAC 

CMAC operational mode

AESCMAC_OPMODE_CBCMAC 

CBC-MAC operational mode

§ AESCMAC_OperationCode

Enum for the operation codes supported by the driver.

Enumerator
AESCMAC_OP_CODE_ONE_STEP 
AESCMAC_OP_CODE_SEGMENTED 
AESCMAC_OP_CODE_FINALIZE 

§ AESCMAC_OperationType

Enum for the operation types supported by the driver.

Enumerator
AESCMAC_OP_TYPE_SIGN 
AESCMAC_OP_TYPE_VERIFY 
AESCMAC_OP_TYPE_SEGMENTED_SIGN 
AESCMAC_OP_TYPE_SEGMENTED_VERIFY 
AESCMAC_OP_TYPE_FINALIZE_SIGN 
AESCMAC_OP_TYPE_FINALIZE_VERIFY 

Function Documentation

§ AESCMAC_init()

void AESCMAC_init ( void  )

Initializes the CMAC module.

Precondition
The AESCMAC_config structure must exist and be persistent before this function can be called. This function must also be called before any other CMAC driver APIs. This function call does not modify any peripheral registers.

§ AESCMAC_Params_init()

void AESCMAC_Params_init ( AESCMAC_Params params)

Initializes the AESCMAC_Params struct to its defaults.

Parameters
[in]paramsPointer to AESCMAC_Params structure for initialization

Defaults values are: returnBehavior = AESCMAC_RETURN_BEHAVIOR_BLOCKING operationalMode = AESCMAC_OPMODE_CMAC callbackFxn = NULL timeout = SemaphoreP_WAIT_FOREVER custom = NULL

§ AESCMAC_Operation_init()

void AESCMAC_Operation_init ( AESCMAC_Operation operation)

Initializes an AESCMAC_Operation struct to its defaults.

Parameters
[in]operationPointer to an AESCMAC_Operation structure for initialization

Defaults values are all zeros.

§ AESCMAC_open()

AESCMAC_Handle AESCMAC_open ( uint_least8_t  index,
const AESCMAC_Params params 
)

Opens a given AESCMAC peripheral.

Note
AESCMAC_Params operationalMode may be set to enable CBC-MAC mode but the default is CMAC mode
Precondition
AESCMAC driver has been initialized using AESCMAC_init()
Parameters
[in]indexLogical peripheral number for the CMAC indexed into the AESCMAC_config table
[in]paramsPointer to a parameter block, if NULL it will use default values
Returns
An AESCMAC_Handle on success or a NULL on an error or if it has been opened already.
See also
AESCMAC_init()
AESCMAC_close()

§ AESCMAC_close()

void AESCMAC_close ( AESCMAC_Handle  handle)

Closes a AESCMAC peripheral specified by the CMAC handle.

Precondition
AESCMAC_open() or AESCMAC_construct()
Parameters
handleAESCMAC handle
See also
AESCMAC_open()
AESCMAC_construct()

§ AESCMAC_setupSign()

int_fast16_t AESCMAC_setupSign ( AESCMAC_Handle  handle,
const CryptoKey key 
)

Prepares a segmented AESCMAC sign operation.

This function sets up a segmented AESCMAC sign operation. After a segmented operation is setup, it must be completed with AESCMAC_finalize or cancelled with AESCMAC_cancelOperation before another operation can be started.

Precondition
AESCMAC_open() or AESCMAC_construct()
Parameters
[in]handleAESCMAC handle
[in]keyPointer to a previously initialized CryptoKey.
Return values
AESCMAC_STATUS_SUCCESSThe operation succeeded. Segmented data may now be added.
AESCMAC_STATUS_ERRORThe operation failed.
Postcondition
AESCMAC_addData() or AESCMAC_finalize()
See also
AESCMAC_setupVerify()

§ AESCMAC_setupVerify()

int_fast16_t AESCMAC_setupVerify ( AESCMAC_Handle  handle,
const CryptoKey key 
)

Prepares a segmented AESCMAC verify operation.

This function sets up a segmented AESCMAC verify operation. After a segmented operation is setup, it must be completed with AESCMAC_finalize or cancelled with AESCMAC_cancelOperation before another operation can be started.

Precondition
AESCMAC_open() or AESCMAC_construct()
Parameters
[in]handleAESCMAC handle
[in]keyPointer to a previously initialized CryptoKey.
Return values
AESCMAC_STATUS_SUCCESSThe operation succeeded. Segmented data may now be added.
AESCMAC_STATUS_ERRORThe operation failed.
Postcondition
AESCMAC_addData() or AESCMAC_finalize()
See also
AESCMAC_setupSign()

§ AESCMAC_addData()

int_fast16_t AESCMAC_addData ( AESCMAC_Handle  handle,
AESCMAC_Operation operation 
)

Adds data to the current segmented operation.

The inputLength must be a non-zero multiple of the block size (16-bytes). AESCMAC_addData() may be called an arbitrary number of times before finishing the operation with AESCMAC_finalize().

This function blocks until the final MAC been computed. It returns immediately when AESCMAC_RETURN_BEHAVIOR_CALLBACK is set.

Note
None of the buffers provided as arguments may be altered by the application during an ongoing operation. Doing so can yield corrupted plaintext.
Precondition
AESCMAC_setupSign() or AESCMAC_setupVerify()
Parameters
[in]handleAESCMAC handle
[in]operationPointer to CMAC operation structure()
Return values
AESCMAC_STATUS_SUCCESSThe operation succeeded.
AESCMAC_STATUS_ERRORThe operation failed.
AESCMAC_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
AESCMAC_STATUS_UNALIGNED_IO_NOT_SUPPORTEDThe input buffer was not word-aligned.
Postcondition
AESCMAC_addData() or AESCMAC_finalize()

§ AESCMAC_finalize()

int_fast16_t AESCMAC_finalize ( AESCMAC_Handle  handle,
AESCMAC_Operation operation 
)

Finalizes the current segmented operation.

For sign operations: This function computes and writes back the final MAC mac of length macLength.

For verify operations: This function uses the provided MAC mac to authenticate an input message. The return value indicates whether the authentication was successful.

Note
Finalizing without additional input data is not supported. If finalization is attempted with inputLength of zero, AESCMAC_STATUS_ERROR will be returned and the caller must either retry finalization with data or terminate the segmented operation by calling AESCMAC_cancelOperation.
None of the buffers provided as arguments may be altered by the application during an ongoing operation. Doing so can yield corrupted plaintext.
Precondition
AESCMAC_addData() or AESCMAC_setupSign() or AESCMAC_setupVerify()
Parameters
[in]handleAESCMAC handle
[in]operationPointer to CMAC operation structure()
Return values
AESCMAC_STATUS_SUCCESSIn AESCMAC_RETURN_BEHAVIOR_BLOCKING and AESCMAC_RETURN_BEHAVIOR_POLLING, this means the MAC was generated successfully. In AESCMAC_RETURN_BEHAVIOR_CALLBACK, this means the operation started successfully.
AESCMAC_STATUS_ERRORThe operation failed.
AESCMAC_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
AESCMAC_STATUS_MAC_INVALIDThe provided MAC did not match the generated MAC. This return value is only valid for verify operations.
AESCMAC_STATUS_UNALIGNED_IO_NOT_SUPPORTEDThe input buffer was not word-aligned.

§ AESCMAC_oneStepSign()

int_fast16_t AESCMAC_oneStepSign ( AESCMAC_Handle  handle,
AESCMAC_Operation operation,
CryptoKey key 
)

Performs a AESCMAC signature in one call.

This function uses the provided key to authenticate an input message. The resulting output is a message authentication code.

Note
None of the buffers provided as arguments may be altered by the application during an ongoing operation. Doing so can yield corrupted plaintext.
Precondition
AESCMAC_open() or AESCMAC_construct()
Parameters
[in]handleAESCMAC handle
[in]operationPointer to AESCMAC operation structure
[in]keyPointer to a previously initialized CryptoKey
Return values
AESCMAC_STATUS_SUCCESSIn AESCMAC_RETURN_BEHAVIOR_BLOCKING and AESCMAC_RETURN_BEHAVIOR_POLLING, this means the MAC was generated successfully. In AESCMAC_RETURN_BEHAVIOR_CALLBACK, this means the operation started successfully.
AESCMAC_STATUS_ERRORThe operation failed.
AESCMAC_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
AESCMAC_STATUS_UNALIGNED_IO_NOT_SUPPORTEDThe input buffer was not word-aligned.
See also
AESCMAC_oneStepVerify()

§ AESCMAC_oneStepVerify()

int_fast16_t AESCMAC_oneStepVerify ( AESCMAC_Handle  handle,
AESCMAC_Operation operation,
CryptoKey key 
)

Performs a AESCMAC verification in one call.

This function verifies that the provided message authentication code matches the one generated by the provided key and input message.

Note
None of the buffers provided as arguments may be altered by the application during an ongoing operation. Doing so can yield corrupted plaintext.
Precondition
AESCMAC_open() or AESCMAC_construct()
Parameters
[in]handleAESCMAC handle
[in]operationPointer to AESCMAC operation structure
[in]keyPointer to a previously initialized CryptoKey
Return values
AESCMAC_STATUS_SUCCESSIn AESCMAC_RETURN_BEHAVIOR_BLOCKING and AESCMAC_RETURN_BEHAVIOR_POLLING, this means the MAC was verified successfully. In AESCMAC_RETURN_BEHAVIOR_CALLBACK, this means the operation started successfully.
AESCMAC_STATUS_ERRORThe operation failed.
AESCMAC_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
AESCMAC_STATUS_MAC_INVALIDThe provided MAC did not match the generated MAC. This return value is only valid for verify operations.
AESCMAC_STATUS_UNALIGNED_IO_NOT_SUPPORTEDThe input buffer was not word-aligned.
See also
AESCMAC_oneStepSign()

§ AESCMAC_cancelOperation()

int_fast16_t AESCMAC_cancelOperation ( AESCMAC_Handle  handle)

Cancels an ongoing AESCMAC operation.

Asynchronously cancels an AESCMAC operation. Only available when using AESCMAC_RETURN_BEHAVIOR_CALLBACK. The operation will terminate as though an error occurred. The return status code of the operation will be AESCMAC_STATUS_CANCELED.

Note
Only the same thread that started an operation is permitted to cancel it. This function cannot be be called from an interrupt context or callback.
Parameters
[in]handleHandle of the operation to cancel
Return values
AESCMAC_STATUS_SUCCESSThe operation was canceled or the operation had already completed.

§ AESCMAC_construct()

AESCMAC_Handle AESCMAC_construct ( AESCMAC_Config config,
const AESCMAC_Params params 
)

Constructs a new AESCMAC object.

Unlike AESCMAC_open(), AESCMAC_construct() does not require the hwAttrs and object to be allocated in a AESCMAC_Config array that is indexed into. Instead, the AESCMAC_Config, hwAttrs, and object can be allocated at any location. This allows for relatively simple run-time allocation of temporary driver instances on the stack or the heap. The drawback is that this makes it more difficult to write device-agnostic code. If you use an ifdef with DeviceFamily, you can choose the correct object and hwAttrs to allocate. That compilation unit will be tied to the device it was compiled for at this point. To change devices, recompilation of the application with a different DeviceFamily setting is necessary.

Note
AESCMAC_Params operationalMode may be set to enable CBC-MAC mode but the default is CMAC mode
Precondition
The object struct config points to must be zeroed out prior to calling this function. Otherwise, unexpected behavior may ensue.
Parameters
[in]configAESCMAC_Config describing the location of the object and hwAttrs.
[in]paramsAESCMAC_Params to configure the driver instance.
Returns
Returns a AESCMAC_Handle on success or NULL on failure.

Variable Documentation

§ AESCMAC_defaultParams

const AESCMAC_Params AESCMAC_defaultParams

Default AESCMAC_Params structure.

See also
AESCMAC_Params_init()
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale