Data Structures | Macros | Typedefs | Enumerations | Functions | Variables
AESCTR.h File Reference

Detailed Description

AESCTR driver header.


Overview

The Counter (CTR) mode of operation is a generic block cipher mode of operation that can be used with any block cipher including AES which is used in this implementation.

CTR mode encrypts and decrypts messages. It is not required for the message length to be evenly divisible by the cipher block size. This also means that padding the message is not required.

Operation

CTR encryption and decryption perform the following steps:

  1. Set the counter value to the initial counter value
  2. Encrypt the counter value under the symmetric key
  3. XOR the encrypted counter value with the input block (plaintext or ciphertext)
  4. Increment the counter value. Interpret the byte array as a big-endian number.
  5. Repeat steps 2 to 4 until the input is completely processed. If the input is not evenly divisible by the block size, XOR the last (u = input length % block size) input bytes with the most significant u bytes of the last encrypted counter value.

CTR performs the same steps regardless of whether it is used to encrypt or decrypt a message. The input merely changes.

Choosing Initial Counter Values

CTR requires that each counter value used to encrypt a block of a message is unique for each key used. If this requirement is not kept, the confidentiality of that message block may be compromised.

There are two general strategies when choosing the initial counter value of a CTR operation to ensure this requirement holds.

The first is to choose an initial counter value for the first message and increment the initial counter value for a subsequent message by by message length % block length (16-bytes for AES). This effectively turns a sequence of messages into one long message. If 0 is chosen as the initial counter value, up to 2^128 - 1 blocks may be encrypted before key rotation is mandatory.

The second is to split the initial counter value into a nonce and counter section. The nonce of length n bits must be unique per message. This allows for up to 2^n - 1 messages to be encrypted before key rotation is required. The counter section of length c is incremented as usual. This limits messages to a length of at most 2^c - 1 blocks. n and c must be chosen such that n + c = block length in bits (128 bits for AES) holds.

Usage

Before starting a CTR operation

Before starting a CTR operation, the application must do the following:

Starting a CTR operation

The AESCTR_oneStepEncrypt() and AESCTR_oneStepDecrypt() functions perform a CTR operation in a single call.

After the CTR operation completes

After the CTR operation completes, the application should either start another operation or close the driver by calling AESCTR_close().

Synopsis

// Import AESCTR Driver definitions
// Define name for AESCTR channel index
#define AESCTR_INSTANCE 0
handle = AESCTR_open(AESCTR_INSTANCE, NULL);
// Initialize symmetric key
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
// Set up AESCTR_Operation
operation.key = &cryptoKey;
operation.input = plaintext;
operation.output = ciphertext;
operation.inputLength = sizeof(plaintext);
operation.initialCounter = initialCounter;
encryptionResult = AESCTR_oneStepEncrypt(handle, &operation);
AESCTR_close(handle);

Examples

One step CTR encryption with plaintext CryptoKey in blocking return mode
...
AESCTR_Handle handle;
CryptoKey cryptoKey;
int_fast16_t encryptionResult;
// For example purposes only. Generate IVs in a non-static way in practice.
// Test vector from NIST SP 800-38A
uint8_t initialCounter[16] = {0xf0, 0xf1, 0xf2, 0xf3, 0xf4, 0xf5, 0xf6, 0xf7,
0xf8, 0xf9, 0xfa, 0xfb, 0xfc, 0xfd, 0xfe, 0xff};
uint8_t plaintext[64] = {0x6b, 0xc1, 0xbe, 0xe2, 0x2e, 0x40, 0x9f, 0x96,
0xe9, 0x3d, 0x7e, 0x11, 0x73, 0x93, 0x17, 0x2a,
0xae, 0x2d, 0x8a, 0x57, 0x1e, 0x03, 0xac, 0x9c,
0x9e, 0xb7, 0x6f, 0xac, 0x45, 0xaf, 0x8e, 0x51,
0x30, 0xc8, 0x1c, 0x46, 0xa3, 0x5c, 0xe4, 0x11,
0xe5, 0xfb, 0xc1, 0x19, 0x1a, 0x0a, 0x52, 0xef,
0xf6, 0x9f, 0x24, 0x45, 0xdf, 0x4f, 0x9b, 0x17,
0xad, 0x2b, 0x41, 0x7b, 0xe6, 0x6c, 0x37, 0x10};
uint8_t ciphertext[sizeof(plaintext)];
uint8_t keyingMaterial[16] = {0x2b, 0x7e, 0x15, 0x16, 0x28, 0xae, 0xd2, 0xa6,
0xab, 0xf7, 0x15, 0x88, 0x09, 0xcf, 0x4f, 0x3c};
handle = AESCTR_open(0, NULL);
if (handle == NULL) {
// handle error
while(1);
}
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
operation.key = &cryptoKey;
operation.input = plaintext;
operation.output = ciphertext;
operation.inputLength = sizeof(plaintext);
operation.initialCounter = initialCounter;
encryptionResult = AESCTR_oneStepEncrypt(handle, &operation);
if (encryptionResult != AESCTR_STATUS_SUCCESS) {
// handle error
while(1);
}
// The ciphertext should be the following after the encryption operation:
// 0x87, 0x4d, 0x61, 0x91, 0xb6, 0x20, 0xe3, 0x26,
// 0x1b, 0xef, 0x68, 0x64, 0x99, 0x0d, 0xb6, 0xce,
// 0x98, 0x06, 0xf6, 0x6b, 0x79, 0x70, 0xfd, 0xff,
// 0x86, 0x17, 0x18, 0x7b, 0xb9, 0xff, 0xfd, 0xff,
// 0x5a, 0xe4, 0xdf, 0x3e, 0xdb, 0xd5, 0xd3, 0x5e,
// 0x5b, 0x4f, 0x09, 0x02, 0x0d, 0xb0, 0x3e, 0xab,
// 0x1e, 0x03, 0x1d, 0xda, 0x2f, 0xbe, 0x03, 0xd1,
// 0x79, 0x21, 0x70, 0xa0, 0xf3, 0x00, 0x9c, 0xee
AESCTR_close(handle);
One step CTR decryption with plaintext CryptoKey in callback return mode
...
void ctrCallback(AESCTR_Handle handle,
int_fast16_t returnValue,
AESCTR_OperationType operationType) {
if (returnValue != AESCTR_STATUS_SUCCESS) {
// handle error
while(1);
}
}
AESCTR_Operation operation;
void ctrStartFunction(void) {
uint8_t initialCounter[16] = {0x00, 0xE0, 0x01, 0x7B, 0x27, 0x77, 0x7F, 0x3F,
0x4A, 0x17, 0x86, 0xF0, 0x00, 0x00, 0x00, 0x01};
uint8_t ciphertext[] = {0xC1, 0xCF, 0x48, 0xA8, 0x9F, 0x2F, 0xFD, 0xD9,
0xCF, 0x46, 0x52, 0xE9, 0xEF, 0xDB, 0x72, 0xD7,
0x45, 0x40, 0xA4, 0x2B, 0xDE, 0x6D, 0x78, 0x36,
0xD5, 0x9A, 0x5C, 0xEA, 0xAE, 0xF3, 0x10, 0x53,
0x25, 0xB2, 0x07, 0x2F};
uint8_t keyingMaterial[] = {0x76, 0x91, 0xBE, 0x03, 0x5E, 0x50, 0x20, 0xA8,
0xAC, 0x6E, 0x61, 0x85, 0x29, 0xF9, 0xA0, 0xDC};
uint8_t plaintext[sizeof(ciphertext)];
AESCTR_Handle handle;
CryptoKey cryptoKey;
int_fast16_t decryptionResult;
params.callbackFxn = ctrCallback;
handle = AESCTR_open(0, &params);
if (handle == NULL) {
// handle error
while(1);
}
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
AESCTR_OneStepOperation_init(&operation); // Optional as all struct members will be set before use.
operation.key = &cryptoKey;
operation.input = ciphertext;
operation.output = plaintext;
operation.inputLength = sizeof(ciphertext);
operation.initialCounter = initialCounter;
decryptionResult = AESCTR_oneStepDecrypt(handle, &operation);
if (decryptionResult != AESCTR_STATUS_SUCCESS) {
// handle error
while(1);
}
// do other things while CTR operation completes in the background
// After the operation completes and the callback is invoked, the resultant
// plaintext should be:
// 0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07,
// 0x08, 0x09, 0x0A, 0x0B, 0x0C, 0x0D, 0x0E, 0x0F,
// 0x10, 0x11, 0x12, 0x13, 0x14, 0x15, 0x16, 0x17,
// 0x18, 0x19, 0x1A, 0x1B, 0x1C, 0x1D, 0x1E, 0x1F,
// 0x20, 0x21, 0x22, 0x23
AESCTR_close(handle);
}
Multi-step AES CTR encrypt with plaintext CryptoKey in polling return mode
#define AES_BLOCK_SIZE 16 // bytes
...
AESCTR_Handle handle;
CryptoKey cryptoKey;
int_fast16_t retVal;
// For example purposes only.
uint8_t plaintext[36] = {0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07,
0x08, 0x09, 0x0A, 0x0B, 0x0C, 0x0D, 0x0E, 0x0F,
0x10, 0x11, 0x12, 0x13, 0x14, 0x15, 0x16, 0x17,
0x18, 0x19, 0x1A, 0x1B, 0x1C, 0x1D, 0x1E, 0x1F,
0x20, 0x21, 0x22, 0x23};
uint8_t initialCounter[] = {0x00, 0xE0, 0x01, 0x7B, 0x27, 0x77, 0x7F, 0x3F,
0x4A, 0x17, 0x86, 0xF0, 0x00, 0x00, 0x00, 0x01};
uint8_t keyingMaterial[] = {0x76, 0x91, 0xBE, 0x03, 0x5E, 0x50, 0x20, 0xA8,
0xAC, 0x6E, 0x61, 0x85, 0x29, 0xF9, 0xA0, 0xDC};
uint8_t ciphertext[sizeof(plaintext)];
params.returnBehavior = AESCTR_RETURN_BEHAVIOR_POLLING;
handle = AESCTR_open(0, &params);
if (handle == NULL) {
// handle error
}
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
AESCTR_SegmentedOperation_init(&operation); // Optional as all struct members will be set before use.
retVal = AESCTR_setupEncrypt(handle, &cryptoKey, initialCounter);
if (retVal != AESCTR_STATUS_SUCCESS) {
// handle error
}
operation.input = plaintext;
operation.inputLength = AES_BLOCK_SIZE; // Only block multiple lengths are permitted when adding data.
operation.output = ciphertext;
retVal = AESCTR_addData(handle, &operation);
if (retVal != AESCTR_STATUS_SUCCESS) {
// handle error
}
operation.input = plaintext + AES_BLOCK_SIZE;
operation.inputLength = sizeof(plaintext) - AES_BLOCK_SIZE; // Non-block multiple length permitted during
finalization. operation.output = ciphertext + AES_BLOCK_SIZE;
retVal = AESCTR_finalize(handle, &operation);
if (retVal != AESCTR_STATUS_SUCCESS) {
// handle error
}
// Upon successful return, the resulting ciphertext should be:
// 0xC1, 0xCF, 0x48, 0xA8, 0x9F, 0x2F, 0xFD, 0xD9,
// 0xCF, 0x46, 0x52, 0xE9, 0xEF, 0xDB, 0x72, 0xD7,
// 0x45, 0x40, 0xA4, 0x2B, 0xDE, 0x6D, 0x78, 0x36,
// 0xD5, 0x9A, 0x5C, 0xEA, 0xAE, 0xF3, 0x10, 0x53,
// 0x25, 0xB2, 0x07, 0x2F
AESCTR_close(handle);
#include <stddef.h>
#include <stdint.h>
#include <ti/drivers/AESCommon.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKey.h>
Include dependency graph for AESCTR.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  AESCTR_OneStepOperation
 Struct containing the parameters required for encrypting/decrypting a message using a one-step operation. More...
 
struct  AESCTR_SegmentedOperation
 Struct containing the parameters required for encrypting/decrypting a message using a segmented operation. This struct must be updated for each "add data" and "finalize" step. Modifying the structure and any buffers that it points to while an operation is in progress is prohibited. More...
 
union  AESCTR_OperationUnion
 Union containing a reference to a one-step and segmented operation structure. More...
 
struct  AESCTR_Params
 CTR Parameters. More...
 

Macros

#define AESCTR_STATUS_RESERVED   AES_STATUS_RESERVED
 
#define AESCTR_STATUS_SUCCESS   AES_STATUS_SUCCESS
 Successful status code. More...
 
#define AESCTR_STATUS_ERROR   AES_STATUS_ERROR
 Generic error status code. More...
 
#define AESCTR_STATUS_RESOURCE_UNAVAILABLE   AES_STATUS_RESOURCE_UNAVAILABLE
 An error status code returned if the hardware or software resource is currently unavailable. More...
 
#define AESCTR_STATUS_CANCELED   AES_STATUS_CANCELED
 The ongoing operation was canceled. More...
 
#define AESCTR_STATUS_FEATURE_NOT_SUPPORTED   AES_STATUS_FEATURE_NOT_SUPPORTED
 The operation requested is not supported. More...
 
#define AESCTR_STATUS_KEYSTORE_INVALID_ID   AES_STATUS_KEYSTORE_INVALID_ID
 The operation tried to load a key from the keystore using an invalid key ID. More...
 
#define AESCTR_STATUS_KEYSTORE_GENERIC_ERROR   AES_STATUS_KEYSTORE_GENERIC_ERROR
 The key store module returned a generic error. See key store documentation for additional details. More...
 
#define AESCTR_STATUS_UNALIGNED_IO_NOT_SUPPORTED   AES_STATUS_UNALIGNED_IO_NOT_SUPPORTED
 The operation does not support non-word-aligned input and/or output. More...
 
#define AESCTR_OP_MODE_MASK   0x0F
 Mask for the operation mode. More...
 
#define AESCTR_OP_FLAG_SEGMENTED   0x10 /* bit 4 */
 Flag indicating a segmented operation. More...
 
#define AESCTR_OP_FLAG_FINALIZE   0x20 /* bit 5 */
 Flag indicating a finalize operation. More...
 
#define AESCTR_OP_FLAGS_MASK   (AESCTR_OP_FLAG_SEGMENTED | AESCTR_OP_FLAG_FINALIZE)
 Mask for all valid operation flags. More...
 

Typedefs

typedef AESCTR_OneStepOperation AESCTR_Operation
 
typedef AESCommon_Config AESCTR_Config
 AESCTR Global configuration. More...
 
typedef AESCTR_ConfigAESCTR_Handle
 A handle that is returned from an AESCTR_open() call. More...
 
typedef void(* AESCTR_CallbackFxn) (AESCTR_Handle handle, int_fast16_t returnValue, AESCTR_OperationUnion *operation, AESCTR_OperationType operationType)
 The definition of a callback function used by the AESCTR driver when used in AESCTR_RETURN_BEHAVIOR_CALLBACK. More...
 

Enumerations

enum  AESCTR_ReturnBehavior { AESCTR_RETURN_BEHAVIOR_CALLBACK = AES_RETURN_BEHAVIOR_CALLBACK, AESCTR_RETURN_BEHAVIOR_BLOCKING = AES_RETURN_BEHAVIOR_BLOCKING, AESCTR_RETURN_BEHAVIOR_POLLING = AES_RETURN_BEHAVIOR_POLLING }
 The way in which CTR function calls return after performing an encryption or decryption operation. More...
 
enum  AESCTR_Mode { AESCTR_MODE_ENCRYPT = 1, AESCTR_MODE_DECRYPT = 2 }
 Enum for the direction of the CTR operation. More...
 
enum  AESCTR_OperationType {
  AESCTR_OPERATION_TYPE_ENCRYPT = AESCTR_MODE_ENCRYPT, AESCTR_OPERATION_TYPE_DECRYPT = AESCTR_MODE_DECRYPT, AESCTR_OPERATION_TYPE_ENCRYPT_SEGMENTED = (AESCTR_MODE_ENCRYPT | 0x10 ), AESCTR_OPERATION_TYPE_DECRYPT_SEGMENTED = (AESCTR_MODE_DECRYPT | 0x10 ),
  AESCTR_OPERATION_TYPE_ENCRYPT_FINALIZE = (AESCTR_MODE_ENCRYPT | 0x20 ), AESCTR_OPERATION_TYPE_DECRYPT_FINALIZE = (AESCTR_MODE_DECRYPT | 0x20 )
}
 Enum for the operation types supported by the driver. More...
 

Functions

void AESCTR_init (void)
 This function initializes the CTR module. More...
 
void AESCTR_Params_init (AESCTR_Params *params)
 Function to initialize the AESCTR_Params struct to its defaults. More...
 
AESCTR_Handle AESCTR_open (uint_least8_t index, const AESCTR_Params *params)
 This function opens a given AESCTR peripheral. More...
 
void AESCTR_close (AESCTR_Handle handle)
 Function to close a CTR peripheral specified by the AESCTR handle. More...
 
int_fast16_t AESCTR_setupEncrypt (AESCTR_Handle handle, const CryptoKey *key, const uint8_t *initialCounter)
 Function to prepare a segmented AESCTR encryption operation. More...
 
int_fast16_t AESCTR_setupDecrypt (AESCTR_Handle handle, const CryptoKey *key, const uint8_t *initialCounter)
 Function to prepare a segmented AESCTR decryption operation. More...
 
int_fast16_t AESCTR_addData (AESCTR_Handle handle, AESCTR_SegmentedOperation *operation)
 Encrypts or decrypts a segment of data with a length. More...
 
int_fast16_t AESCTR_finalize (AESCTR_Handle handle, AESCTR_SegmentedOperation *operation)
 Finalize the AES operation. If new data needs to be added, inputLength will be used to govern how many bytes will be written. More...
 
void AESCTR_Operation_init (AESCTR_Operation *operation)
 Function to initialize an AESCTR_Operation struct to its defaults (all zeroes) More...
 
void AESCTR_OneStepOperation_init (AESCTR_OneStepOperation *operation)
 Function to initialize an AESCTR_OneStepOperation struct to its defaults (all zeroes) More...
 
void AESCTR_SegmentedOperation_init (AESCTR_SegmentedOperation *operation)
 Function to initialize an AESCTR_SegmentedOperation struct to its defaults (all zeroes) More...
 
int_fast16_t AESCTR_oneStepEncrypt (AESCTR_Handle handle, AESCTR_OneStepOperation *operation)
 Function to perform an AESCTR encryption operation in one call. More...
 
int_fast16_t AESCTR_oneStepDecrypt (AESCTR_Handle handle, AESCTR_OneStepOperation *operation)
 Function to perform an AESCTR decryption operation in one call. More...
 
int_fast16_t AESCTR_cancelOperation (AESCTR_Handle handle)
 Cancels an ongoing AESCTR operation. More...
 
AESCTR_Handle AESCTR_construct (AESCTR_Config *config, const AESCTR_Params *params)
 Constructs a new AESCTR object. More...
 

Variables

const AESCTR_Params AESCTR_defaultParams
 Default AESCTR_Params structure. More...
 

Macro Definition Documentation

§ AESCTR_STATUS_RESERVED

#define AESCTR_STATUS_RESERVED   AES_STATUS_RESERVED

Common AESCTR status code reservation offset. AESCTR driver implementations should offset status codes with AESCTR_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

#define AESCTRXYZ_STATUS_ERROR0 AESCTR_STATUS_RESERVED - 0
#define AESCTRXYZ_STATUS_ERROR1 AESCTR_STATUS_RESERVED - 1
#define AESCTRXYZ_STATUS_ERROR2 AESCTR_STATUS_RESERVED - 2

§ AESCTR_STATUS_SUCCESS

#define AESCTR_STATUS_SUCCESS   AES_STATUS_SUCCESS

Successful status code.

Functions return AESCTR_STATUS_SUCCESS if the function was executed successfully.

§ AESCTR_STATUS_ERROR

#define AESCTR_STATUS_ERROR   AES_STATUS_ERROR

Generic error status code.

Functions return AESCTR_STATUS_ERROR if the function was not executed successfully and no more pertinent error code could be returned.

§ AESCTR_STATUS_RESOURCE_UNAVAILABLE

#define AESCTR_STATUS_RESOURCE_UNAVAILABLE   AES_STATUS_RESOURCE_UNAVAILABLE

An error status code returned if the hardware or software resource is currently unavailable.

AESCTR driver implementations may have hardware or software limitations on how many clients can simultaneously perform operations. This status code is returned if the mutual exclusion mechanism signals that an operation cannot currently be performed.

§ AESCTR_STATUS_CANCELED

#define AESCTR_STATUS_CANCELED   AES_STATUS_CANCELED

The ongoing operation was canceled.

§ AESCTR_STATUS_FEATURE_NOT_SUPPORTED

#define AESCTR_STATUS_FEATURE_NOT_SUPPORTED   AES_STATUS_FEATURE_NOT_SUPPORTED

The operation requested is not supported.

§ AESCTR_STATUS_KEYSTORE_INVALID_ID

#define AESCTR_STATUS_KEYSTORE_INVALID_ID   AES_STATUS_KEYSTORE_INVALID_ID

The operation tried to load a key from the keystore using an invalid key ID.

§ AESCTR_STATUS_KEYSTORE_GENERIC_ERROR

#define AESCTR_STATUS_KEYSTORE_GENERIC_ERROR   AES_STATUS_KEYSTORE_GENERIC_ERROR

The key store module returned a generic error. See key store documentation for additional details.

§ AESCTR_STATUS_UNALIGNED_IO_NOT_SUPPORTED

#define AESCTR_STATUS_UNALIGNED_IO_NOT_SUPPORTED   AES_STATUS_UNALIGNED_IO_NOT_SUPPORTED

The operation does not support non-word-aligned input and/or output.

AESCTR driver implementations may have restrictions on the alignment of input/output data due to performance limitations of the hardware.

§ AESCTR_OP_MODE_MASK

#define AESCTR_OP_MODE_MASK   0x0F

Mask for the operation mode.

§ AESCTR_OP_FLAG_SEGMENTED

#define AESCTR_OP_FLAG_SEGMENTED   0x10 /* bit 4 */

Flag indicating a segmented operation.

§ AESCTR_OP_FLAG_FINALIZE

#define AESCTR_OP_FLAG_FINALIZE   0x20 /* bit 5 */

Flag indicating a finalize operation.

§ AESCTR_OP_FLAGS_MASK

#define AESCTR_OP_FLAGS_MASK   (AESCTR_OP_FLAG_SEGMENTED | AESCTR_OP_FLAG_FINALIZE)

Mask for all valid operation flags.

Typedef Documentation

§ AESCTR_Operation

Deprecated:
Define a typedef for deprecated operation AESCTR_Operation. Existing code should be refactored to use AESCTR_OneStepOperation. This reference may be removed at some point in the future.

§ AESCTR_Config

AESCTR Global configuration.

The AESCTR_Config structure contains a set of pointers used to characterize the AESCTR driver implementation.

This structure needs to be defined before calling AESCTR_init() and it must not be changed thereafter.

See also
AESCTR_init()

§ AESCTR_Handle

A handle that is returned from an AESCTR_open() call.

§ AESCTR_CallbackFxn

typedef void(* AESCTR_CallbackFxn) (AESCTR_Handle handle, int_fast16_t returnValue, AESCTR_OperationUnion *operation, AESCTR_OperationType operationType)

The definition of a callback function used by the AESCTR driver when used in AESCTR_RETURN_BEHAVIOR_CALLBACK.

Parameters
handleHandle of the client that started the CTR operation.
returnValueThe result of the CTR operation. May contain an error code. Informs the application of why the callback function was called.
operationPointer to the operation union struct.
operationTypeThis parameter determines which operation the callback refers to.

Enumeration Type Documentation

§ AESCTR_ReturnBehavior

The way in which CTR function calls return after performing an encryption or decryption operation.

Not all CTR operations exhibit the specified return behavior. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specified return behavior is not implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.

AESCTR functions exhibiting the specified return behavior have restrictions on the context from which they may be called.

Task Hwi Swi
AESCTR_RETURN_BEHAVIOR_CALLBACK X X X
AESCTR_RETURN_BEHAVIOR_BLOCKING X
AESCTR_RETURN_BEHAVIOR_POLLING X X X
Enumerator
AESCTR_RETURN_BEHAVIOR_CALLBACK 

The function call will return immediately while the CTR operation goes on in the background. The registered callback function is called after the operation completes. The context the callback function is called (task, HWI, SWI) is implementation-dependent.

AESCTR_RETURN_BEHAVIOR_BLOCKING 

The function call will block while the CTR operation goes on in the background. CTR operation results are available after the function returns.

AESCTR_RETURN_BEHAVIOR_POLLING 

The function call will continuously poll a flag while CTR operation goes on in the background. CTR operation results are available after the function returns.

§ AESCTR_Mode

Enum for the direction of the CTR operation.

Enumerator
AESCTR_MODE_ENCRYPT 
AESCTR_MODE_DECRYPT 

§ AESCTR_OperationType

Enum for the operation types supported by the driver.

Enumerator
AESCTR_OPERATION_TYPE_ENCRYPT 
AESCTR_OPERATION_TYPE_DECRYPT 
AESCTR_OPERATION_TYPE_ENCRYPT_SEGMENTED 
AESCTR_OPERATION_TYPE_DECRYPT_SEGMENTED 
AESCTR_OPERATION_TYPE_ENCRYPT_FINALIZE 
AESCTR_OPERATION_TYPE_DECRYPT_FINALIZE 

Function Documentation

§ AESCTR_init()

void AESCTR_init ( void  )

This function initializes the CTR module.

Precondition
The AESCTR_config structure must exist and be persistent before this function can be called. This function must also be called before any other CTR driver APIs. This function call does not modify any peripheral registers.

§ AESCTR_Params_init()

void AESCTR_Params_init ( AESCTR_Params params)

Function to initialize the AESCTR_Params struct to its defaults.

Parameters
[in]paramsPointer to AESCTR_Params structure for initialization

Defaults values are: returnBehavior = AESCTR_RETURN_BEHAVIOR_BLOCKING callbackFxn = NULL timeout = SemaphoreP_WAIT_FOREVER custom = NULL

§ AESCTR_open()

AESCTR_Handle AESCTR_open ( uint_least8_t  index,
const AESCTR_Params params 
)

This function opens a given AESCTR peripheral.

Precondition
AESCTR driver has been initialized using AESCTR_init()
Parameters
[in]indexLogical peripheral number for the CTR indexed into the AESCTR_config table
[in]paramsPointer to a parameter block, if NULL it will use default values.
Returns
A AESCTR_Handle on success or a NULL on an error or if it has been opened already.
See also
AESCTR_init()
AESCTR_close()

§ AESCTR_close()

void AESCTR_close ( AESCTR_Handle  handle)

Function to close a CTR peripheral specified by the AESCTR handle.

Precondition
AESCTR_open() or AESCTR_construct()
Parameters
[in]handleAESCTR handle
See also
AESCTR_open()

§ AESCTR_setupEncrypt()

int_fast16_t AESCTR_setupEncrypt ( AESCTR_Handle  handle,
const CryptoKey key,
const uint8_t *  initialCounter 
)

Function to prepare a segmented AESCTR encryption operation.

This function sets up a segmented AESCTR encryption operation.

Precondition
AESCTR_open() or AESCTR_construct()
Parameters
[in]handleAESCTR handle
[in]keyPointer to a previously initialized CryptoKey
[in]initialCounterPointer to initial counter value. The buffer size must be at least 16-bytes. If NULL, zero will be used for the initial counter value.
Return values
AESCTR_STATUS_SUCCESSThe operation succeeded.
AESCTR_STATUS_ERRORThe operation failed.
Postcondition
AESCTR_addData()

§ AESCTR_setupDecrypt()

int_fast16_t AESCTR_setupDecrypt ( AESCTR_Handle  handle,
const CryptoKey key,
const uint8_t *  initialCounter 
)

Function to prepare a segmented AESCTR decryption operation.

This function sets up a segmented AESCTR decryption operation.

Precondition
AESCTR_open() or AESCTR_construct()
Parameters
[in]handleAESCTR handle
[in]keyPointer to a previously initialized CryptoKey.
[in]initialCounterPointer to initial counter value. The buffer size must be at least 16-bytes. If NULL, zero will be used for the initial counter value.
Return values
AESCTR_STATUS_SUCCESSThe operation succeeded.
AESCTR_STATUS_ERRORThe operation failed.
Postcondition
AESCTR_addData()

§ AESCTR_addData()

int_fast16_t AESCTR_addData ( AESCTR_Handle  handle,
AESCTR_SegmentedOperation operation 
)

Encrypts or decrypts a segment of data with a length.

The inputLength must be a non-zero multiple of the block size (16-bytes). AESCTR_addData() may be called an arbitrary number of times before finishing the operation with AESCTR_finalize().

This function blocks until the final stream bytes have been computed. It returns immediately when AESCTR_RETURN_BEHAVIOR_CALLBACK is set.

Precondition
A segmented operation has been setup using AESCTR_setupEncrypt() or AESCTR_setupDecrypt()
Parameters
[in]handleAESCTR handle
[in]operationPointer to AESCTR_SegmentedOperation structure containing the parameters required to perform the operation.
Return values
AESCTR_STATUS_SUCCESSThe operation succeeded.
AESCTR_STATUS_ERRORThe operation failed.
AESCTR_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
AESCTR_STATUS_UNALIGNED_IO_NOT_SUPPORTEDThe input and/or output buffer were not word-aligned.
Postcondition
AESCTR_addData() or AESCTR_finalize()

§ AESCTR_finalize()

int_fast16_t AESCTR_finalize ( AESCTR_Handle  handle,
AESCTR_SegmentedOperation operation 
)

Finalize the AES operation. If new data needs to be added, inputLength will be used to govern how many bytes will be written.

Note
To finalize an operation without any additional data, set inputLength to zero. The input and output buffers will not be used in this scenario.
Precondition
AESCTR_setupEncrypt() or AESCTR_setupDecrypt()
AESCTR_addData()
Parameters
[in]handleAESCTR handle
[in]operationPointer to AESCTR_SegmentedOperation structure containing the parameters required to perform the operation.
Return values
AESCTR_STATUS_SUCCESSIn AESCTR_RETURN_BEHAVIOR_BLOCKING and AESCTR_RETURN_BEHAVIOR_POLLING, this means the CTR was generated successfully. In AESCTR_RETURN_BEHAVIOR_CALLBACK, this means the operation started successfully.
AESCTR_STATUS_ERRORThe operation failed.
AESCTR_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
AESCTR_STATUS_UNALIGNED_IO_NOT_SUPPORTEDThe input and/or output buffer were not word-aligned.

§ AESCTR_Operation_init()

void AESCTR_Operation_init ( AESCTR_Operation operation)

Function to initialize an AESCTR_Operation struct to its defaults (all zeroes)

Deprecated:
Use AESCTR_OneStepOperation_init() or AESCTR_SegmentedOperation_init() based on whether it is a one-step or a segmented AESCTR operation.
Parameters
operationPointer to an AESCTR_Operation structure for initialization

§ AESCTR_OneStepOperation_init()

void AESCTR_OneStepOperation_init ( AESCTR_OneStepOperation operation)

Function to initialize an AESCTR_OneStepOperation struct to its defaults (all zeroes)

Parameters
[in]operationPointer to an AESCTR_OneStepOperation structure for initialization

§ AESCTR_SegmentedOperation_init()

void AESCTR_SegmentedOperation_init ( AESCTR_SegmentedOperation operation)

Function to initialize an AESCTR_SegmentedOperation struct to its defaults (all zeroes)

Parameters
[in]operationPointer to an AESCTR_SegmentedOperation structure for initialization

§ AESCTR_oneStepEncrypt()

int_fast16_t AESCTR_oneStepEncrypt ( AESCTR_Handle  handle,
AESCTR_OneStepOperation operation 
)

Function to perform an AESCTR encryption operation in one call.

Note
None of the buffers provided as arguments may be altered by the application during an ongoing operation. Doing so can yield corrupted ciphertext.
Precondition
AESCTR_open() or AESCTR_construct()
Parameters
[in]handleAESCTR handle
[in]operationPointer to a struct containing the parameters required to perform the operation.
Return values
AESCTR_STATUS_SUCCESSThe operation succeeded.
AESCTR_STATUS_ERRORThe operation failed.
AESCTR_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
AESCTR_STATUS_UNALIGNED_IO_NOT_SUPPORTEDThe input and/or output buffer were not word-aligned.
See also
AESCTR_oneStepDecrypt()

§ AESCTR_oneStepDecrypt()

int_fast16_t AESCTR_oneStepDecrypt ( AESCTR_Handle  handle,
AESCTR_OneStepOperation operation 
)

Function to perform an AESCTR decryption operation in one call.

Note
None of the buffers provided as arguments may be altered by the application during an ongoing operation. Doing so can yield corrupted plaintext.
Precondition
AESCTR_open() or AESCTR_construct()
Parameters
[in]handleAESCTR handle
[in]operationPointer to a struct containing the parameters required to perform the operation.
Return values
AESCTR_STATUS_SUCCESSThe operation succeeded.
AESCTR_STATUS_ERRORThe operation failed.
AESCTR_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
AESCTR_STATUS_UNALIGNED_IO_NOT_SUPPORTEDThe input and/or output buffer were not word-aligned.
See also
AESCTR_oneStepEncrypt()

§ AESCTR_cancelOperation()

int_fast16_t AESCTR_cancelOperation ( AESCTR_Handle  handle)

Cancels an ongoing AESCTR operation.

Asynchronously cancels an AESCTR operation. Only available when using AESCTR_RETURN_BEHAVIOR_CALLBACK. The operation will terminate as though an error occurred. The return status code of the operation will be AESCTR_STATUS_CANCELED.

Parameters
[in]handleAESCTR handle
Return values
AESCTR_STATUS_SUCCESSThe operation was canceled or the operation had already completed.

§ AESCTR_construct()

AESCTR_Handle AESCTR_construct ( AESCTR_Config config,
const AESCTR_Params params 
)

Constructs a new AESCTR object.

Unlike AESCTR_open(), AESCTR_construct() does not require the hwAttrs and object to be allocated in a AESCTR_Config array that is indexed into. Instead, the AESCTR_Config, hwAttrs, and object can be allocated at any location. This allows for relatively simple run-time allocation of temporary driver instances on the stack or the heap. The drawback is that this makes it more difficult to write device-agnostic code. If you use an ifdef with DeviceFamily, you can choose the correct object and hwAttrs to allocate. That compilation unit will be tied to the device it was compiled for at this point. To change devices, recompilation of the application with a different DeviceFamily setting is necessary.

Precondition
The object struct config points to must be zeroed out prior to calling this function. Otherwise, unexpected behavior may occur.
Parameters
[in]configAESCTR_Config describing the location of the object and hwAttrs.
[in]paramsAESCTR_Params to configure the driver instance.
Returns
Returns a AESCTR_Handle on success or NULL on failure.

Variable Documentation

§ AESCTR_defaultParams

const AESCTR_Params AESCTR_defaultParams

Default AESCTR_Params structure.

See also
AESCTR_Params_init()
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale