Data Structures | Macros | Typedefs | Enumerations | Functions | Variables
AESGCM.h File Reference

Detailed Description

AESGCM driver header.


Overview

The Galois Counter Mode (GCM) mode of operation is a generic authenticated encryption with associated data (AEAD) block cipher mode. It can be implemented with any block cipher. AESGCM combines GHASH with the AES block cipher in CTR mode of operation.

This combination of block cipher modes enables GCM to encrypt messages of any length and not only multiples of the block cipher block size.

CTR provides confidentiality. The using GHASH and encrypting the result provides message integrity and authentication.

The AES key is a shared secret between the two parties and has a length of 128, 192, or 256 bits.

The IV is generated by the party performing the authenticated encryption operation. Within the scope of any authenticated encryption key, the IV value must be unique. That is, the set of IV values used with any given key must not contain any duplicate values. Using the same IV for two different messages encrypted with the same key destroys the security properties of GCM.

The optional additional authentication data (AAD) is authenticated but not encrypted. Thus, the AAD is not included in the AES-GCM output. It can be used to authenticate packet headers, timestamps and other metadata.

After the encryption operation, the ciphertext contains the encrypted data and the message authentication code (MAC).

GCM is highly performant for an AEAD mode. Counter with CBC-MAC requires one invocation per block of AAD and two invocations of the block cipher per proccessed block of input; one to compute the CBC-MAC and one to perform CTR. GCM substitutes the block cipher invocation during CBC-MAC computation with computing GHASH over the same input. GHASH is significantly faster per block than AES. In turn, this gives GCM a performance edge over CCM.

Security Considerations

In each operation, GCM limits the length of the input and AAD to guarantee its security properties:

The security properties of GCM rely on the MAC size. While MAC lengths of [4, 8, 12, 13, 14, 15, 16] bytes are permitted, it is recommended to use the full 16-byte MAC.

See NIST SP 800-38D for more a more detailed discussion of security considerations.

Usage

Before starting a GCM operation

Before starting a GCM operation, the application must do the following:

Starting a GCM operation

The AESGCM_oneStepEncrypt() and AESGCM_oneStepDecrypt() functions perform a GCM operation in a single call.

When performing a decryption operation with AESGCM_oneStepDecrypt(), the MAC is automatically verified.

After the GCM operation completes

After the GCM operation completes, the application should either start another operation or close the driver by calling AESGCM_close()

Synopsis

// Import AESGCM Driver definitions
// Define name for AESGCM channel index
#define AESGCM_INSTANCE 0
handle = AESGCM_open(AESGCM_INSTANCE, NULL);
// Initialize symmetric key
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
// Set up AESGCM_OneStepOperation
operation.key = &cryptoKey;
operation.aad = aad;
operation.aadLength = sizeof(aad);
operation.input = plaintext;
operation.output = ciphertext;
operation.inputLength = sizeof(plaintext);
operation.iv = iv;
operation.ivLength = sizeof(iv);
operation.mac = mac;
operation.macLength = sizeof(mac);
encryptionResult = AESGCM_oneStepEncrypt(handle, &operation);
AESGCM_close(handle);

Examples

Single call GCM encryption + authentication with plaintext CryptoKey in blocking return mode
...
AESGCM_Handle handle;
CryptoKey cryptoKey;
int_fast16_t encryptionResult;
uint8_t iv[12] = "12-byte IV ";
uint8_t aad[] = "This string will be authenticated but not encrypted.";
uint8_t plaintext[] = "This string will be encrypted and authenticated.";
uint8_t mac[16];
uint8_t ciphertext[sizeof(plaintext)];
uint8_t keyingMaterial[32] = {0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07,
0x08, 0x09, 0x0A, 0x0B, 0x0C, 0x0D, 0x0E, 0x0F,
0x10, 0x11, 0x12, 0x13, 0x14, 0x15, 0x16, 0x17,
0x18, 0x19, 0x1A, 0x1B, 0x1C, 0x1D, 0x1E, 0x1F};
handle = AESGCM_open(0, NULL);
if (handle == NULL) {
// handle error
}
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
operation.key = &cryptoKey;
operation.aad = aad;
operation.aadLength = sizeof(aad);
operation.input = plaintext;
operation.output = ciphertext;
operation.inputLength = sizeof(plaintext);
operation.iv = iv;
operation.ivLength = 12;
operation.mac = mac;
operation.macLength = sizeof(mac);
encryptionResult = AESGCM_oneStepEncrypt(handle, &operation);
if (encryptionResult != AESGCM_STATUS_SUCCESS) {
// handle error
}
AESGCM_close(handle);
Single call GCM decryption + verification with plaintext CryptoKey in callback return mode
...
// The following test vector is Packet Vector 1 from RFC 3610 of the IETF.
uint8_t iv[] = {0x1f, 0x80, 0x3c, 0x52, 0xca, 0xc4, 0x97, 0xe1,
0x55, 0xaa, 0x55, 0x2d};
uint8_t aad[] = {0x3b, 0xba, 0x31, 0x28, 0x9d, 0x05, 0xf5, 0x0f,
0xed, 0x6c, 0x53, 0x35, 0x3c, 0x1f, 0x74, 0xd8,
0x28, 0xa9, 0x96, 0xb8, 0xd6, 0x84, 0xfe, 0x64,
0x7f, 0x7c, 0x40, 0xc0, 0xd5, 0x68, 0x8c, 0x89,
0x68, 0x1a, 0x33, 0xb1, 0x0c, 0xb7, 0x14, 0xb6,
0x49, 0x0b, 0xdf, 0x1f, 0x16, 0x60, 0x60, 0xa7};
uint8_t mac[] = {0x39, 0x03, 0xe4, 0xdc, 0xa4, 0xe7, 0xc8, 0x21,
0x62, 0x1a, 0xbb, 0xb2, 0x37, 0x2c, 0x97};
uint8_t ciphertext[] = {0xf8, 0x7e, 0xf7, 0x99, 0x4a, 0x86, 0xf3, 0xe9,
0xa3, 0xab, 0x6a, 0x6f, 0x2d, 0x34, 0x3b, 0xbd};
uint8_t keyingMaterial[] = {0x4f, 0xd7, 0xf2, 0x09, 0xdf, 0xb0, 0xdf, 0xbd,
0xd9, 0x8d, 0x2d, 0xb4, 0x98, 0x66, 0x4c, 0x88};
uint8_t plaintext[sizeof(ciphertext)];
// The plaintext should be the following after the decryption operation:
// 0x17, 0x9d, 0xcb, 0x79, 0x5c, 0x09, 0x8f, 0xc5, 0x31, 0x4b, 0xde, 0x0d, 0x39, 0x9d, 0x7a, 0x10
void gcmCallback(AESGCM_Handle handle,
int_fast16_t returnValue,
AESGCM_OperationType operationType) {
if (returnValue != AESGCM_STATUS_SUCCESS) {
// handle error
}
}
CryptoKey cryptoKey;
void gcmStartFunction(void) {
AESGCM_Handle handle;
int_fast16_t decryptionResult;
params.callbackFxn = gcmCallback;
handle = AESGCM_open(0, &params);
if (handle == NULL) {
// handle error
}
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
operation.key = &cryptoKey;
operation.aad = aad;
operation.aadLength = sizeof(aad);
operation.input = ciphertext;
operation.output = plaintext;
operation.inputLength = sizeof(ciphertext);
operation.iv = iv;
operation.ivLength = sizeof(iv);
operation.mac = mac;
operation.macLength = sizeof(mac);
decryptionResult = AESGCM_oneStepDecrypt(handle, &operation);
if (decryptionResult != AESGCM_STATUS_SUCCESS) {
// handle error
}
// do other things while GCM operation completes in the background
}

### Multi-step GCM encryption + authentication with plaintext CryptoKey in blocking return mode #

...
#define AES_BLOCK_SIZE 16 // bytes
CryptoKey cryptoKey;
int_fast16_t encryptionResult;
uint8_t keyingMaterial[32] = {0x58, 0x53, 0xc0, 0x20, 0x94, 0x6b, 0x35, 0xf2,
0xc5, 0x8e, 0xc4, 0x27, 0x15, 0x2b, 0x84, 0x04,
0x20, 0xc4, 0x00, 0x29, 0x63, 0x6a, 0xdc, 0xbb,
0x02, 0x74, 0x71, 0x37, 0x8c, 0xfd, 0xde, 0x0f};
uint8_t aad[20] = {0x13, 0x89, 0xb5, 0x22, 0xc2, 0x4a, 0x77, 0x41,
0x81, 0x70, 0x05, 0x53, 0xf0, 0x24, 0x6b, 0xba,
0xbd, 0xd3, 0x8d, 0x6f};
uint8_t plaintext[32] = {0xce, 0x74, 0x58, 0xe5, 0x6a, 0xef, 0x90, 0x61,
0xcb, 0x0c, 0x42, 0xec, 0x23, 0x15, 0x56, 0x5e,
0x61, 0x68, 0xf5, 0xa6, 0x24, 0x9f, 0xfd, 0x31,
0x61, 0x0b, 0x6d, 0x17, 0xab, 0x64, 0x93, 0x5e};
uint8_t iv[12] = {0xee, 0xc3, 0x13, 0xdd, 0x07, 0xcc, 0x1b, 0x3e,
0x6b, 0x06, 0x8a, 0x47};
uint8_t mac[16];
uint8_t ciphertext[sizeof(plaintext)];
// The ciphertext should be the following after the encryption operation:
// {0xea, 0xdc, 0x3b, 0x87, 0x66, 0xa7, 0x7d, 0xed,
// 0x1a, 0x58, 0xcb, 0x72, 0x7e, 0xca, 0x2a, 0x97,
// 0x90, 0x49, 0x6c, 0x29, 0x86, 0x54, 0xcd, 0xa7,
// 0x8f, 0xeb, 0xf0, 0xda, 0x16, 0xb6, 0x90, 0x3b}
handle = AESGCM_open(0, NULL);
if (handle == NULL) {
// handle error
}
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
encryptionResult = AESGCM_setupEncrypt(handle, &cryptoKey, sizeof(aad), sizeof(plaintext));
if (decryptionResult != AESGCM_STATUS_SUCCESS) {
// handle error
}
encryptionResult = AESGCM_setIV(handle, iv, sizeof(iv));
if (encryptionResult != AESGCM_STATUS_SUCCESS) {
// handle error
}
AESGCM_SegmentedAADOperation segmentedAADOperation;
AESGCM_SegmentedAADOperation_init(&segmentedAADOperation);
segmentedAADOperation.aad = aad;
// One should pass in data that is a block-sized multiple length
// until passing in the last segment of data.
// In that case, the input length simply needs to be a non-zero value.
segmentedAADOperation.aadLength = sizeof(aad);
encryptionResult = AESGCM_addAAD(handle, &segmentedAADOperation);
if (encryptionResult != AESGCM_STATUS_SUCCESS) {
// handle error
}
AESGCM_SegmentedDataOperation segmentedDataOperation;
AESGCM_SegmentedDataOperation_init(&segmentedDataOperation);
segmentedDataOperation.input = plaintext;
segmentedDataOperation.output = ciphertext;
// One should pass in data that is a block-sized multiple length
// until passing in the last segment of data.
// In that case, the input length simply needs to be a non-zero value.
segmentedDataOperation.inputLength = AES_BLOCK_SIZE;
encryptionResult = AESGCM_addData(handle, &segmentedDataOperation);
if (encryptionResult != AESGCM_STATUS_SUCCESS) {
// handle error
}
AESGCM_SegmentedFinalizeOperation segmentedFinalizeOperation;
AESGCM_SegmentedFinalizeOperation_init(&egmentedFinalizeOperation);
segmentedFinalizeOperation.input = plaintext + AES_BLOCK_SIZE;
segmentedFinalizeOperation.output = ciphertext + AES_BLOCK_SIZE;
segmentedFinalizeOperation.inputLength = AES_BLOCK_SIZE;
segmentedFinalizeOperation.mac = mac;
segmentedFinalizeOperation.macLength = sizeof(mac);
encryptionResult = AESGCM_finalizeEncrypt(handle, &segmentedFinalizeOperation);
if (encryptionResult != AESGCM_STATUS_SUCCESS) {
// handle error
}
AESGCM_close(handle);

Multi-step GCM decryption + verification with plaintext CryptoKey in callback return mode

...
#define AES_BLOCK_SIZE 16 // bytes
uint8_t iv[] = {0x7f, 0xc2, 0x5c, 0x0c, 0x7a, 0x65, 0xb9, 0x50,
0x00, 0x23, 0xd0, 0x58};
uint8_t aad[] = {0x9e, 0xca, 0x27, 0x10, 0xbc, 0x1c, 0xaa, 0x99,
0x50, 0x2d, 0xe3, 0x0f, 0x08, 0x94, 0x30, 0x69,
0x7a, 0xee, 0xfc, 0x03};
uint8_t mac[] = {0x77, 0xb6, 0x4e, 0x40};
uint8_t ciphertext[] = {0xbd, 0xb4, 0x3f, 0x90, 0xf1, 0x6e, 0x26, 0xdc,
0xff, 0x60, 0xdb, 0x92, 0xb9, 0x6c, 0x4a, 0x2f};
uint8_t keyingMaterial[] = {0xfb, 0x96, 0x31, 0x2b, 0xdb, 0x8a, 0x22, 0xf1,
0x6f, 0xad, 0xc4, 0x23, 0x69, 0x4f, 0x45, 0x70};
uint8_t plaintext[sizeof(ciphertext)];
// The plaintext should be the following after the decryption operation:
// {0xae, 0xe4, 0x16, 0xa2, 0x1f, 0x0e, 0x98, 0x3f,
// 0xd7, 0x05, 0x20, 0xb8, 0xce, 0xdb, 0x24, 0xe5}
void gcmCallback(AESGCM_Handle handle,
int_fast16_t returnValue,
AESGCM_OperationType operationType) {
if (returnValue != AESGCM_STATUS_SUCCESS) {
// handle error
}
if(operationType == AESGCM_OPERATION_TYPE_DECRYPT ||
{
// Callback fxn only used for one-shot operations
// Use operation->oneStepOperation
}
else if(operationType == AESGCM_OP_TYPE_AAD_DECRYPT ||
operationType == AESGCM_OP_TYPE_AAD_ENCRYPT)
{
// Callback fxn only used for segmented AAD operations
// Use operation->segmentedAADOperation
}
else if(operationType == AESGCM_OP_TYPE_DATA_DECRYPT ||
operationType == AESGCM_OP_TYPE_DATA_ENCRYPT)
{
// Callback fxn only used for segmented data operations
// Use operation->segmentedDataOperation
}
else
{
// Callback fxn only used for segmented finalize operations
// Use operation->segmentedFinalizeOperation
}
}
void gcmStartFunction(void) {
AESGCM_Handle handle;
CryptoKey cryptoKey;
int_fast16_t decryptionResult;
params.callbackFxn = gcmCallback;
handle = AESGCM_open(0, &params);
if (handle == NULL) {
// handle error
}
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
decryptionResult = AESGCM_setupDecrypt(handle, &cryptoKey, 0, 0);
if (decryptionResult != AESGCM_STATUS_SUCCESS) {
// handle error
}
// setLengths must be called if the AAD and input lengths aren't provided in setupXXXX.
decryptionResult = AESGCM_setLengths(handle, sizeof(aad), sizeof(ciphertext));
if (decryptionResult != AESGCM_STATUS_SUCCESS) {
// handle error
}
decryptionResult = AESGCM_setIV(handle, iv, sizeof(iv));
if (decryptionResult != AESGCM_STATUS_SUCCESS) {
// handle error
}
AESGCM_SegmentedAADOperation segmentedAADOperation;
AESGCM_SegmentedAADOperation_init(&segmentedAADOperation);
segmentedAADOperation.aad = aad;
segmentedAADOperation.aadLength = sizeof(aad);
decryptionResult = AESGCM_addAAD(handle, &segmentedAADOperation);
if (decryptionResult != AESGCM_STATUS_SUCCESS) {
// handle error
}
AESGCM_SegmentedDataOperation segmentedDataOperation;
AESGCM_SegmentedDataOperation_init(&segmentedDataOperation);
segmentedDataOperation.input = ciphertext;
segmentedDataOperation.output = plaintext;
segmentedDataOperation.inputLength = AES_BLOCK_SIZE;
decryptionResult = AESGCM_addData(handle, &segmentedDataOperation);
if (decryptionResult != AESGCM_STATUS_SUCCESS) {
// handle error
}
AESGCM_SegmentedFinalizeOperation segmentedFinalizeOperation;
AESGCM_SegmentedFinalizeOperation_init(&egmentedFinalizeOperation);
segmentedFinalizeOperation.input = ciphertext;
segmentedFinalizeOperation.output = plaintext;
// You can finalize with no new data
segmentedFinalizeOperation.inputLength = 0;
segmentedFinalizeOperation.mac = mac;
segmentedFinalizeOperation.macLength = sizeof(mac);
decryptionResult = AESGCM_finalizeDecrypt(handle, &segmentedFinalizeOperation);
if (decryptionResult != AESGCM_STATUS_SUCCESS) {
// handle error
}
// do other things while GCM operation completes in the background
}
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/drivers/AESCommon.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKey.h>
Include dependency graph for AESGCM.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  AESGCM_OneStepOperation
 Struct containing the parameters required for encrypting/decrypting and authenticating/verifying a message for one-step operations. More...
 
struct  AESGCM_SegmentedAADOperation
 Struct containing the parameters required for authenticating/verifying additional data in a segmented operation. Must be updated for each add AAD step of a segmented operation. More...
 
struct  AESGCM_SegmentedDataOperation
 Struct containing the parameters required for encrypting/decrypting a message in a segmented operation. Must be updated between each add data step of a segmented operation. More...
 
struct  AESGCM_SegmentedFinalizeOperation
 Struct containing the parameters required for finalizing an encryption/decryption and authentication/verification of a message in a segmented operation. More...
 
union  AESGCM_OperationUnion
 Union containing a reference to a one step, segmented AAD, segmented data, or segmented finalize operation. More...
 
struct  AESGCM_Params
 GCM Parameters. More...
 

Macros

#define AESGCM_IV_LENGTH_BYTES   12
 
#define AESGCM_STATUS_RESERVED   AES_STATUS_RESERVED
 
#define AESGCM_STATUS_SUCCESS   AES_STATUS_SUCCESS
 Successful status code. More...
 
#define AESGCM_STATUS_ERROR   AES_STATUS_ERROR
 Generic error status code. More...
 
#define AESGCM_STATUS_RESOURCE_UNAVAILABLE   AES_STATUS_RESOURCE_UNAVAILABLE
 An error status code returned if the hardware or software resource is currently unavailable. More...
 
#define AESGCM_STATUS_CANCELED   AES_STATUS_CANCELED
 The ongoing operation was canceled. More...
 
#define AESGCM_STATUS_MAC_INVALID   AES_STATUS_MAC_INVALID
 An error status code returned if the MAC provided by the application for a decryption operation does not match the one calculated during the operation. More...
 
#define AESGCM_STATUS_FEATURE_NOT_SUPPORTED   AES_STATUS_FEATURE_NOT_SUPPORTED
 The operation requested is not supported on the target hardware. More...
 
#define AESGCM_STATUS_KEYSTORE_INVALID_ID   AES_STATUS_KEYSTORE_INVALID_ID
 The operation tried to load a key from the keystore using an invalid key ID. More...
 
#define AESGCM_STATUS_KEYSTORE_GENERIC_ERROR   AES_STATUS_KEYSTORE_GENERIC_ERROR
 The key store module returned a generic error. See key store documentation for additional details. More...
 

Typedefs

typedef AESCommon_Config AESGCM_Config
 AESGCM Global configuration. More...
 
typedef AESGCM_ConfigAESGCM_Handle
 A handle that is returned from an AESGCM_open() call. More...
 
typedef AESGCM_OneStepOperation AESGCM_Operation
 
typedef union AESGCM_OperationUnion AESGCM_OperationUnion
 Union containing a reference to a one step, segmented AAD, segmented data, or segmented finalize operation. More...
 
typedef void(* AESGCM_CallbackFxn) (AESGCM_Handle handle, int_fast16_t returnValue, AESGCM_OperationUnion *operation, AESGCM_OperationType operationType)
 The definition of a callback function used by the AESGCM driver when used in AESGCM_RETURN_BEHAVIOR_CALLBACK. More...
 

Enumerations

enum  AESGCM_ReturnBehavior { AESGCM_RETURN_BEHAVIOR_CALLBACK = AES_RETURN_BEHAVIOR_CALLBACK, AESGCM_RETURN_BEHAVIOR_BLOCKING = AES_RETURN_BEHAVIOR_BLOCKING, AESGCM_RETURN_BEHAVIOR_POLLING = AES_RETURN_BEHAVIOR_POLLING }
 The way in which GCM function calls return after performing an encryption + authentication or decryption + verification operation. More...
 
enum  AESGCM_Mode { AESGCM_MODE_ENCRYPT = 1, AESGCM_MODE_DECRYPT = 2 }
 Enum for the direction of the GCM operation. More...
 
enum  AESGCM_OperationType {
  AESGCM_OPERATION_TYPE_ENCRYPT = 1, AESGCM_OPERATION_TYPE_DECRYPT = 2, AESGCM_OP_TYPE_ONESTEP_ENCRYPT = 1, AESGCM_OP_TYPE_ONESTEP_DECRYPT = 2,
  AESGCM_OP_TYPE_AAD_ENCRYPT = 3, AESGCM_OP_TYPE_AAD_DECRYPT = 4, AESGCM_OP_TYPE_DATA_ENCRYPT = 5, AESGCM_OP_TYPE_DATA_DECRYPT = 6,
  AESGCM_OP_TYPE_FINALIZE_ENCRYPT = 7, AESGCM_OP_TYPE_FINALIZE_DECRYPT = 8
}
 Enum for the operation types supported by the driver. More...
 

Functions

void AESGCM_init (void)
 This function initializes the GCM module. More...
 
void AESGCM_Params_init (AESGCM_Params *params)
 Function to initialize the AESGCM_Params struct to its defaults. More...
 
AESGCM_Handle AESGCM_open (uint_least8_t index, const AESGCM_Params *params)
 This function opens a given GCM peripheral. More...
 
void AESGCM_close (AESGCM_Handle handle)
 Function to close a GCM peripheral specified by the GCM handle. More...
 
int_fast16_t AESGCM_setupEncrypt (AESGCM_Handle handle, const CryptoKey *key, size_t totalAADLength, size_t totalPlaintextLength)
 Function to prepare a segmented AESGCM encryption operation. More...
 
int_fast16_t AESGCM_setupDecrypt (AESGCM_Handle handle, const CryptoKey *key, size_t totalAADLength, size_t totalPlaintextLength)
 Function to prepare a segmented AESGCM decryption operation. More...
 
int_fast16_t AESGCM_setLengths (AESGCM_Handle handle, size_t aadLength, size_t plaintextLength)
 Function to set the lengths of the message and additional data. More...
 
int_fast16_t AESGCM_setIV (AESGCM_Handle handle, const uint8_t *iv, size_t ivLength)
 Function to set the initialization vector (IV) for an AES GCM segmented operation. More...
 
int_fast16_t AESGCM_generateIV (AESGCM_Handle handle, uint8_t *iv, size_t ivSize, size_t *ivLength)
 Function to generate an IV for an AES GCM segmented encryption operation. More...
 
int_fast16_t AESGCM_addAAD (AESGCM_Handle handle, AESGCM_SegmentedAADOperation *operation)
 Adds a segment of aad with a length in bytes to the generated MAC. More...
 
int_fast16_t AESGCM_addData (AESGCM_Handle handle, AESGCM_SegmentedDataOperation *operation)
 Adds a segment of data with a length that is a multiple of an AES block-size (16 bytes) to the plaintext/ciphertext output and generated MAC. The length does not have to be a block-size multiple if passing in the last chunk of data. More...
 
int_fast16_t AESGCM_finalizeEncrypt (AESGCM_Handle handle, AESGCM_SegmentedFinalizeOperation *operation)
 Finalize the MAC and ciphertext. More...
 
int_fast16_t AESGCM_finalizeDecrypt (AESGCM_Handle handle, AESGCM_SegmentedFinalizeOperation *operation)
 Finalize the MAC and plaintext and verify it. More...
 
void AESGCM_Operation_init (AESGCM_Operation *operationStruct)
 Function to initialize an AESGCM_Operation struct to its defaults. More...
 
void AESGCM_OneStepOperation_init (AESGCM_OneStepOperation *operationStruct)
 Function to initialize an AESGCM_OneStepOperation struct to its defaults. More...
 
void AESGCM_SegmentedAADOperation_init (AESGCM_SegmentedAADOperation *operationStruct)
 Function to initialize an AESGCM_SegmentedAADOperation struct to its defaults. More...
 
void AESGCM_SegmentedDataOperation_init (AESGCM_SegmentedDataOperation *operationStruct)
 Function to initialize an AESGCM_SegmentedDataOperation struct to its defaults. More...
 
void AESGCM_SegmentedFinalizeOperation_init (AESGCM_SegmentedFinalizeOperation *operationStruct)
 Function to initialize an AESGCM_SegmentedFinalizeOperation struct to its defaults. More...
 
int_fast16_t AESGCM_oneStepEncrypt (AESGCM_Handle handle, AESGCM_OneStepOperation *operationStruct)
 Function to perform an AESGCM encryption + authentication operation in one call. More...
 
int_fast16_t AESGCM_oneStepDecrypt (AESGCM_Handle handle, AESGCM_OneStepOperation *operationStruct)
 Function to perform an AESGCM decryption + verification operation in one call. More...
 
int_fast16_t AESGCM_cancelOperation (AESGCM_Handle handle)
 Cancels an ongoing AESGCM operation. More...
 
AESGCM_Handle AESGCM_construct (AESGCM_Config *config, const AESGCM_Params *params)
 Constructs a new AESGCM object. More...
 

Variables

const AESGCM_Params AESGCM_defaultParams
 Default AESGCM_Params structure. More...
 

Macro Definition Documentation

§ AESGCM_IV_LENGTH_BYTES

#define AESGCM_IV_LENGTH_BYTES   12

§ AESGCM_STATUS_RESERVED

#define AESGCM_STATUS_RESERVED   AES_STATUS_RESERVED

Common AESGCM status code reservation offset. AESGCM driver implementations should offset status codes with AESGCM_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

#define AESGCMXYZ_STATUS_ERROR0 AESGCM_STATUS_RESERVED - 0
#define AESGCMXYZ_STATUS_ERROR1 AESGCM_STATUS_RESERVED - 1
#define AESGCMXYZ_STATUS_ERROR2 AESGCM_STATUS_RESERVED - 2

§ AESGCM_STATUS_SUCCESS

#define AESGCM_STATUS_SUCCESS   AES_STATUS_SUCCESS

Successful status code.

Functions return AESGCM_STATUS_SUCCESS if the function was executed successfully.

§ AESGCM_STATUS_ERROR

#define AESGCM_STATUS_ERROR   AES_STATUS_ERROR

Generic error status code.

Functions return AESGCM_STATUS_ERROR if the function was not executed successfully and no more pertinent error code could be returned.

§ AESGCM_STATUS_RESOURCE_UNAVAILABLE

#define AESGCM_STATUS_RESOURCE_UNAVAILABLE   AES_STATUS_RESOURCE_UNAVAILABLE

An error status code returned if the hardware or software resource is currently unavailable.

AESGCM driver implementations may have hardware or software limitations on how many clients can simultaneously perform operations. This status code is returned if the mutual exclusion mechanism signals that an operation cannot currently be performed.

§ AESGCM_STATUS_CANCELED

#define AESGCM_STATUS_CANCELED   AES_STATUS_CANCELED

The ongoing operation was canceled.

§ AESGCM_STATUS_MAC_INVALID

#define AESGCM_STATUS_MAC_INVALID   AES_STATUS_MAC_INVALID

An error status code returned if the MAC provided by the application for a decryption operation does not match the one calculated during the operation.

This code is returned by AESGCM_oneStepDecrypt() or AESGCM_finalizeDecrypt() if the verification of the MAC fails.

§ AESGCM_STATUS_FEATURE_NOT_SUPPORTED

#define AESGCM_STATUS_FEATURE_NOT_SUPPORTED   AES_STATUS_FEATURE_NOT_SUPPORTED

The operation requested is not supported on the target hardware.

This code is returned by AES GCM segmented data operations when attempting to use them on device families that do not support segmented operations.

§ AESGCM_STATUS_KEYSTORE_INVALID_ID

#define AESGCM_STATUS_KEYSTORE_INVALID_ID   AES_STATUS_KEYSTORE_INVALID_ID

The operation tried to load a key from the keystore using an invalid key ID.

§ AESGCM_STATUS_KEYSTORE_GENERIC_ERROR

#define AESGCM_STATUS_KEYSTORE_GENERIC_ERROR   AES_STATUS_KEYSTORE_GENERIC_ERROR

The key store module returned a generic error. See key store documentation for additional details.

Typedef Documentation

§ AESGCM_Config

AESGCM Global configuration.

The AESGCM_Config structure contains a set of pointers used to characterize the AESGCM driver implementation.

This structure needs to be defined before calling AESGCM_init() and it must not be changed thereafter.

See also
AESGCM_init()

§ AESGCM_Handle

A handle that is returned from an AESGCM_open() call.

§ AESGCM_Operation

Deprecated:
Define a typedef for deprecated operation AESGCM_Operation. Existing code should be refactored to use AESGCM_OneStepOperation. This reference may be removed at some point in the future

§ AESGCM_OperationUnion

Union containing a reference to a one step, segmented AAD, segmented data, or segmented finalize operation.

§ AESGCM_CallbackFxn

typedef void(* AESGCM_CallbackFxn) (AESGCM_Handle handle, int_fast16_t returnValue, AESGCM_OperationUnion *operation, AESGCM_OperationType operationType)

The definition of a callback function used by the AESGCM driver when used in AESGCM_RETURN_BEHAVIOR_CALLBACK.

Parameters
handleHandle of the client that started the GCM operation.
returnValueThe result of the GCM operation. May contain an error code. Informs the application of why the callback function was called.
operationUnionA pointer to an operation union.
operationTypeThis parameter determines which operation the callback refers to.

Enumeration Type Documentation

§ AESGCM_ReturnBehavior

The way in which GCM function calls return after performing an encryption + authentication or decryption + verification operation.

Not all GCM operations exhibit the specified return behavior. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specified return behavior is not implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.

AESGCM functions exhibiting the specified return behavior have restrictions on the context from which they may be called.

Task Hwi Swi
AESGCM_RETURN_BEHAVIOR_CALLBACK X X X
AESGCM_RETURN_BEHAVIOR_BLOCKING X
AESGCM_RETURN_BEHAVIOR_POLLING X X X
Enumerator
AESGCM_RETURN_BEHAVIOR_CALLBACK 

The function call will return immediately while the GCM operation goes on in the background. The registered callback function is called after the operation completes. The context the callback function is called (task, HWI, SWI) is implementation-dependent.

AESGCM_RETURN_BEHAVIOR_BLOCKING 

The function call will block while the GCM operation goes on in the background. GCM operation results are available after the function returns.

AESGCM_RETURN_BEHAVIOR_POLLING 

The function call will continuously poll a flag while GCM operation goes on in the background. GCM operation results are available after the function returns.

§ AESGCM_Mode

Enum for the direction of the GCM operation.

Enumerator
AESGCM_MODE_ENCRYPT 
AESGCM_MODE_DECRYPT 

§ AESGCM_OperationType

Enum for the operation types supported by the driver.

Enumerator
AESGCM_OPERATION_TYPE_ENCRYPT 
AESGCM_OPERATION_TYPE_DECRYPT 
AESGCM_OP_TYPE_ONESTEP_ENCRYPT 
AESGCM_OP_TYPE_ONESTEP_DECRYPT 
AESGCM_OP_TYPE_AAD_ENCRYPT 
AESGCM_OP_TYPE_AAD_DECRYPT 
AESGCM_OP_TYPE_DATA_ENCRYPT 
AESGCM_OP_TYPE_DATA_DECRYPT 
AESGCM_OP_TYPE_FINALIZE_ENCRYPT 
AESGCM_OP_TYPE_FINALIZE_DECRYPT 

Function Documentation

§ AESGCM_init()

void AESGCM_init ( void  )

This function initializes the GCM module.

Precondition
The AESGCM_config structure must exist and be persistent before this function can be called. This function must also be called before any other GCM driver APIs. This function call does not modify any peripheral registers.

§ AESGCM_Params_init()

void AESGCM_Params_init ( AESGCM_Params params)

Function to initialize the AESGCM_Params struct to its defaults.

Parameters
paramsAn pointer to AESGCM_Params structure for initialization

Defaults values are: returnBehavior = AESGCM_RETURN_BEHAVIOR_BLOCKING callbackFxn = NULL timeout = SemaphoreP_WAIT_FOREVER custom = NULL

§ AESGCM_open()

AESGCM_Handle AESGCM_open ( uint_least8_t  index,
const AESGCM_Params params 
)

This function opens a given GCM peripheral.

Precondition
GCM controller has been initialized using AESGCM_init()
Parameters
[in]indexLogical peripheral number for the GCM indexed into the AESGCM_config table
[in]paramsPointer to an parameter block, if NULL it will use default values.
Returns
An AESGCM_Handle on success or a NULL on an error or if it has been opened already.
See also
AESGCM_init()
AESGCM_close()

§ AESGCM_close()

void AESGCM_close ( AESGCM_Handle  handle)

Function to close a GCM peripheral specified by the GCM handle.

Precondition
AESGCM_open() or AESGCM_construct()
Parameters
[in]handleA GCM handle
See also
AESGCM_open()

§ AESGCM_setupEncrypt()

int_fast16_t AESGCM_setupEncrypt ( AESGCM_Handle  handle,
const CryptoKey key,
size_t  totalAADLength,
size_t  totalPlaintextLength 
)

Function to prepare a segmented AESGCM encryption operation.

This function sets up a segmented AESGCM encryption operation.

Precondition
AESGCM_open() or AESGCM_construct()
Parameters
[in]handleA GCM handle returned from AESGCM_open() or AESGCM_construct()
[in]keyPointer to a previously initialized CryptoKey.
[in]totalAADLengthTotal size of the AAD in bytes. This value can be 0 and later provided by AESGCM_setLengths().
[in]totalPlaintextLengthTotal size of the plaintext in bytes. This value can be 0 and later provided by AESGCM_setLengths().
Return values
AESGCM_STATUS_SUCCESSThe operation succeeded.
AESGCM_STATUS_ERRORThe operation failed.
AESGCM_STATUS_FEATURE_NOT_SUPPORTEDThe operation is not supported in this device.
Postcondition
AESGCM_addAAD()
AESGCM_addData()

§ AESGCM_setupDecrypt()

int_fast16_t AESGCM_setupDecrypt ( AESGCM_Handle  handle,
const CryptoKey key,
size_t  totalAADLength,
size_t  totalPlaintextLength 
)

Function to prepare a segmented AESGCM decryption operation.

This function sets up a segmented AESGCM decryption operation.

Precondition
AESGCM_open() or AESGCM_construct()
Parameters
[in]handleA GCM handle returned from AESGCM_open() or AESGCM_construct()
[in]keyPointer to a previously initialized CryptoKey.
[in]totalAADLengthTotal size of the AAD in bytes. This value can be 0 and later provided by AESGCM_setLengths().
[in]totalPlaintextLengthTotal size of the plaintext in bytes This value can be 0 and later provided by AESGCM_setLengths().
Return values
AESGCM_STATUS_SUCCESSThe operation succeeded.
AESGCM_STATUS_ERRORThe operation failed.
AESGCM_STATUS_FEATURE_NOT_SUPPORTEDThe operation is not supported in this device.
Postcondition
AESGCM_addAAD()
AESGCM_addData()

§ AESGCM_setLengths()

int_fast16_t AESGCM_setLengths ( AESGCM_Handle  handle,
size_t  aadLength,
size_t  plaintextLength 
)

Function to set the lengths of the message and additional data.

This function declares the lengths of the message and additional authenticated data (AAD).

Note
This function doesn't have to be called if the lengths above were specified in AESGCM_setupEncrypt() or AESGCM_setupDecrypt().
Precondition
AESGCM_setupEncrypt() or AESGCM_setupDecrypt()
Parameters
[in]handleA GCM handle returned from AESGCM_open() or AESGCM_construct()
[in]aadLengthSize of the non-encrypted AAD in bytes
[in]plaintextLengthSize of the plaintext to encrypt or the ciphertext to decrypt in bytes
Return values
AESGCM_STATUS_SUCCESSThe operation succeeded.
AESGCM_STATUS_ERRORThe operation failed.
AESGCM_STATUS_FEATURE_NOT_SUPPORTEDThe operation is not supported in this device.
Postcondition
AESGCM_setIV()
AESGCM_generateIV()

§ AESGCM_setIV()

int_fast16_t AESGCM_setIV ( AESGCM_Handle  handle,
const uint8_t *  iv,
size_t  ivLength 
)

Function to set the initialization vector (IV) for an AES GCM segmented operation.

Precondition
AESGCM_setupEncrypt(), AESGCM_setupDecrypt(), or AESGCM_setLengths()
Parameters
[in]handleA GCM handle returned from AESGCM_open() or AESGCM_construct()
[in]ivPointer to the buffer containing the IV
[in]ivLengthThe length of the IV in bytes
Return values
AESGCM_STATUS_SUCCESSThe operation succeeded.
AESGCM_STATUS_ERRORThe operation failed.
AESGCM_STATUS_FEATURE_NOT_SUPPORTEDThe operation is not supported in this device.
Postcondition
AESGCM_addAAD()
AESGCM_addData()

§ AESGCM_generateIV()

int_fast16_t AESGCM_generateIV ( AESGCM_Handle  handle,
uint8_t *  iv,
size_t  ivSize,
size_t *  ivLength 
)

Function to generate an IV for an AES GCM segmented encryption operation.

Precondition
AESGCM_setupEncrypt() or AESGCM_setLengths()
Parameters
[in]handleA GCM handle returned from AESGCM_open() or AESGCM_construct()
[in]ivPointer to the buffer where the generated IV is to be written to
[in]ivSizeThe length of the IV buffer in bytes
[out]ivLengthThe length of the IV actually written if the operation was successful
Return values
AESGCM_STATUS_SUCCESSThe operation succeeded.
AESGCM_STATUS_ERRORThe operation failed.
AESGCM_STATUS_FEATURE_NOT_SUPPORTEDThe operation is not supported in this device.
Postcondition
AESGCM_addAAD()
AESGCM_addData()

§ AESGCM_addAAD()

int_fast16_t AESGCM_addAAD ( AESGCM_Handle  handle,
AESGCM_SegmentedAADOperation operation 
)

Adds a segment of aad with a length in bytes to the generated MAC.

AESGCM_addAAD() may be called an arbitrary number of times before continuing the operation with AESGCM_addData(), AESGCM_finalizeEncrypt() or AESGCM_finalizeDecrypt().

This function returns according to the return behavior set when opening the driver.

Note
This function must not be called after passing data to encrypt or decrypt with AESGCM_addData().
Warning
When decrypting, do not use the output until AESGCM_finalizeDecrypt() succeeds.
Precondition
AESGCM_setIV() or AESGCM_generateIV()
Parameters
[in]handleA GCM handle returned from AESGCM_open() or AESGCM_construct()
[in]operationPointer to segmented AAD GCM operation structure
Return values
AESGCM_STATUS_SUCCESSThe operation succeeded.
AESGCM_STATUS_ERRORThe operation failed.
AESGCM_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
AESGCM_STATUS_FEATURE_NOT_SUPPORTEDThe operation is not supported in this device.
Postcondition
AESGCM_addAAD()
AESGCM_addData()
AESGCM_finalizeEncrypt()
AESGCM_finalizeDecrypt()

§ AESGCM_addData()

int_fast16_t AESGCM_addData ( AESGCM_Handle  handle,
AESGCM_SegmentedDataOperation operation 
)

Adds a segment of data with a length that is a multiple of an AES block-size (16 bytes) to the plaintext/ciphertext output and generated MAC. The length does not have to be a block-size multiple if passing in the last chunk of data.

AESGCM_addData() may be called an arbitrary number of times before finishing the operation with AESGCM_finalizeEncrypt() or AESGCM_finalizeDecrypt().

This function returns according to the return behavior set when opening the driver.

Warning
When decrypting, do not use the output until AESGCM_finalizeDecrypt() succeeds.
Precondition
AESGCM_setIV() or AESGCM_generateIV()
Parameters
[in]handleA GCM handle returned from AESGCM_open() or AESGCM_construct()
[in]operationPointer to segmented data GCM operation structure
Return values
AESGCM_STATUS_SUCCESSThe operation succeeded.
AESGCM_STATUS_ERRORThe operation failed.
AESGCM_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
AESGCM_STATUS_FEATURE_NOT_SUPPORTEDThe operation is not supported in this device.
Postcondition
AESGCM_addData()
AESGCM_finalizeEncrypt()
AESGCM_finalizeDecrypt()

§ AESGCM_finalizeEncrypt()

int_fast16_t AESGCM_finalizeEncrypt ( AESGCM_Handle  handle,
AESGCM_SegmentedFinalizeOperation operation 
)

Finalize the MAC and ciphertext.

This function finalizes the encryption of a dataset earlier provided by calls to AESGCM_addAAD() and AESGCM_addData() and creates a message authentication code. If additional data needs to be encrypted and verified as part of this call, set the operation structure inputLength accordingly.

The resulting output is a message authentication code and ciphertext.

Precondition
AESGCM_addAAD() or AESGCM_addData()
Parameters
[in]handleA GCM handle returned from AESGCM_open() or AESGCM_construct()
[in]operationPointer to segmented finalize GCM operation structure
Return values
AESGCM_STATUS_SUCCESSIn AESGCM_RETURN_BEHAVIOR_BLOCKING and AESGCM_RETURN_BEHAVIOR_POLLING, this means the MAC was generated successfully. In AESGCM_RETURN_BEHAVIOR_CALLBACK, this means the operation started successfully.
AESGCM_STATUS_ERRORThe operation failed.
AESGCM_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
AESGCM_STATUS_FEATURE_NOT_SUPPORTEDThe operation is not supported in this device.

§ AESGCM_finalizeDecrypt()

int_fast16_t AESGCM_finalizeDecrypt ( AESGCM_Handle  handle,
AESGCM_SegmentedFinalizeOperation operation 
)

Finalize the MAC and plaintext and verify it.

This function finalizes the decryption of a dataset earlier provided by calls to AESGCM_addAAD() and AESGCM_addData() and verifies a provided message authentication code. If additional data needs to be decrypted and verified as part of this call, set the operation structure inputLength accordingly.

The resulting output is a verification return code and plaintext.

Note
None of the buffers provided as arguments may be altered by the application during an ongoing operation. Doing so can yield a corrupted MAC comparison.
Precondition
AESGCM_addAAD() or AESGCM_addData()
Parameters
[in]handleA GCM handle returned from AESGCM_open() or AESGCM_construct()
[in]operationPointer to segmented finalize GCM operation structure
Return values
AESGCM_STATUS_SUCCESSIn AESGCM_RETURN_BEHAVIOR_BLOCKING and AESGCM_RETURN_BEHAVIOR_POLLING, this means the MAC was verified successfully. In AESGCM_RETURN_BEHAVIOR_CALLBACK, this means the operation started successfully.
AESGCM_STATUS_ERRORThe operation failed.
AESGCM_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
AESGCM_STATUS_MAC_INVALIDThe provided MAC did not match the recomputed one.
AESGCM_STATUS_FEATURE_NOT_SUPPORTEDThe operation is not supported in this device.

§ AESGCM_Operation_init()

void AESGCM_Operation_init ( AESGCM_Operation operationStruct)

Function to initialize an AESGCM_Operation struct to its defaults.

Deprecated:
This function should be replaced by calls to operation-specific init functions.
Parameters
[in]operationStructA pointer to an AESGCM_Operation structure for initialization

Defaults values are all zeros.

§ AESGCM_OneStepOperation_init()

void AESGCM_OneStepOperation_init ( AESGCM_OneStepOperation operationStruct)

Function to initialize an AESGCM_OneStepOperation struct to its defaults.

Parameters
[in]operationStructA pointer to an AESGCM_OneStepOperation structure for initialization

Defaults values are all zeros.

§ AESGCM_SegmentedAADOperation_init()

void AESGCM_SegmentedAADOperation_init ( AESGCM_SegmentedAADOperation operationStruct)

Function to initialize an AESGCM_SegmentedAADOperation struct to its defaults.

Parameters
[in]operationStructA pointer to an AESGCM_SegmentedAADOperation structure for initialization

Defaults values are all zeros.

§ AESGCM_SegmentedDataOperation_init()

void AESGCM_SegmentedDataOperation_init ( AESGCM_SegmentedDataOperation operationStruct)

Function to initialize an AESGCM_SegmentedDataOperation struct to its defaults.

Parameters
[in]operationStructA pointer to an AESGCM_SegmentedDataOperation structure for initialization

Defaults values are all zeros.

§ AESGCM_SegmentedFinalizeOperation_init()

void AESGCM_SegmentedFinalizeOperation_init ( AESGCM_SegmentedFinalizeOperation operationStruct)

Function to initialize an AESGCM_SegmentedFinalizeOperation struct to its defaults.

Parameters
[in]operationStructA pointer to an AESGCM_SegmentedFinalizeOperation structure for initialization

Defaults values are all zeros.

§ AESGCM_oneStepEncrypt()

int_fast16_t AESGCM_oneStepEncrypt ( AESGCM_Handle  handle,
AESGCM_OneStepOperation operationStruct 
)

Function to perform an AESGCM encryption + authentication operation in one call.

Note
None of the buffers provided as arguments may be altered by the application during an ongoing operation. Doing so can yield corrupted ciphertext or incorrect authentication.
Precondition
AESGCM_open() or AESGCM_construct() and AESGCM_Operation_init() have to be called first.
Parameters
[in]handleA GCM handle returned from AESGCM_open() or AESGCM_construct()
[in]operationStructA pointer to a struct containing the parameters required to perform the operation.
Return values
AESGCM_STATUS_SUCCESSThe operation succeeded.
AESGCM_STATUS_ERRORThe operation failed.
AESGCM_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
See also
AESGCM_oneStepDecrypt()

§ AESGCM_oneStepDecrypt()

int_fast16_t AESGCM_oneStepDecrypt ( AESGCM_Handle  handle,
AESGCM_OneStepOperation operationStruct 
)

Function to perform an AESGCM decryption + verification operation in one call.

Note
None of the buffers provided as arguments may be altered by the application during an ongoing operation. Doing so can yield corrupted plaintext or incorrectly failed verification.
Precondition
AESGCM_open() or AESGCM_construct() and AESGCM_Operation_init() have to be called first.
Parameters
[in]handleA GCM handle returned from AESGCM_open() or AESGCM_construct()
[in]operationStructA pointer to a struct containing the parameters required to perform the operation.
Return values
AESGCM_STATUS_SUCCESSThe operation succeeded.
AESGCM_STATUS_ERRORThe operation failed.
AESGCM_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
AESGCM_STATUS_MAC_INVALIDThe provided MAC did no match the recomputed one.
See also
AESGCM_oneStepEncrypt()

§ AESGCM_cancelOperation()

int_fast16_t AESGCM_cancelOperation ( AESGCM_Handle  handle)

Cancels an ongoing AESGCM operation.

Asynchronously cancels an AESGCM operation. Only available when using AESGCM_RETURN_BEHAVIOR_CALLBACK. The operation will terminate as though an error occurred. The return status code of the operation will be AESGCM_STATUS_CANCELED.

Parameters
[in]handleHandle of the operation to cancel
Return values
AESGCM_STATUS_SUCCESSThe operation was canceled, or the operation had already completed.
AESGCM_STATUS_ERRORThe driver was not in callback mode, or the operation's output and generated MAC weren't properly cleared.

§ AESGCM_construct()

AESGCM_Handle AESGCM_construct ( AESGCM_Config config,
const AESGCM_Params params 
)

Constructs a new AESGCM object.

Unlike AESGCM_open(), AESGCM_construct() does not require the hwAttrs and object to be allocated in a AESGCM_Config array that is indexed into. Instead, the AESGCM_Config, hwAttrs, and object can be allocated at any location. This allows for relatively simple run-time allocation of temporary driver instances on the stack or the heap. The drawback is that this makes it more difficult to write device-agnostic code. If you use an ifdef with DeviceFamily, you can choose the correct object and hwAttrs to allocate. That compilation unit will be tied to the device it was compiled for at this point. To change devices, recompilation of the application with a different DeviceFamily setting is necessary.

Parameters
configAESGCM_Config describing the location of the object and hwAttrs.
paramsAESGCM_Params to configure the driver instance.
Returns
Returns a AESGCM_Handle on success or NULL on failure.
Precondition
The object struct config points to must be zeroed out prior to calling this function. Otherwise, unexpected behavior may ensue.

Variable Documentation

§ AESGCM_defaultParams

const AESGCM_Params AESGCM_defaultParams

Default AESGCM_Params structure.

See also
AESGCM_Params_init()
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale