Data Structures | Macros | Typedefs | Enumerations | Functions | Variables
ECDH.h File Reference

Detailed Description

TI Driver for Elliptic Curve Diffie-Hellman key agreement scheme.


Overview

Elliptic Curve Diffie-Hellman (ECDH) is a key agreement scheme between two parties based on the Diffie-Hellman key exchange protocol.

It provides a means of generating a shared secret and derived symmetric key between the two parties over an insecure channel.

It does not provide authentication. As such, it does not guarantee that the party you are exchanging keys with is truly the party you wish to establish a secured channel with.

The two parties each generate a private key and a public key. The private key is a random integer in the interval [1, n - 1], where n is the order of a previously agreed upon curve. The public key is generated by multiplying the private key by the generator point of a previously agreed upon elliptic curve such as NISTP256 or Curve 25519. The public key is itself a point upon the elliptic curve. Each public key is then transmitted to the other party over a potentially insecure channel. The other party's public key is then multiplied with the private key, generating a shared secret. This shared secret is also a point on the curve. However, the entropy in the secret is not spread evenly throughout the shared secret. In order to generate one or more shared symmetric keys, the shared secret must be run through a key derivation function (KDF) that was previously agreed upon. Usually, only the X coordinate is processed in this way as it contains all the entropy of the shared secret and some curve implementations only provide the X coordinate. The key derivation function can take many forms, from simply hashing the X coordinate of the shared secret with SHA2 and truncating the result to generating multiple symmetric keys with HKDF, an HMAC based KDF.

Key derivation functions in the context of symmetric key generation after elliptic curve based key exchange differ from KDFs used to generate keys from passwords a user provides in a login. Those KDFs such as bcrypt purposefully add additional computation to increase a system's resistance against brute force or dictionary attacks.

Usage

Before starting an ECDH operation

Before starting an ECDH operation, the application must do the following:

Generating your public-private key pair

To generate a public-private key pair for an agreed upon curve, the application must do the following:

Calculating a shared secret

After trading public keys with the other party, the application should do the following to calculate the shared secret:

Creating one or more symmetric keys from the shared secret

After calculating the shared secret between the application and the other party, the entropy in the shared secret must be evened out and stretched as needed. There are uncountable methods and algorithms to stretch an original seed entropy (the share secret) to generate symmetric keys.

After a key exchange

After the ECDH key exchange completes, the application should either start another operation or close the driver by calling ECDH_close()

General usage

The API expects elliptic curves as defined in ti/drivers/cryptoutils/ecc/ECCParams.h. Several commonly used curves are provided. Check the device-specific ECDH documentation for curve type (short Weierstrass, Montgomery, Edwards) support for your device. ECDH support for a curve type on a device does not imply curve-type support for other ECC schemes.

Key Formatting

By default, the ECDH API expects the private and public keys to be formatted in big-endian format. The details of octet string formatting can be found in SEC 1: Elliptic Curve Cryptography.

Private keys can be formatted as big-endian or little-endian integers of the same length as the curve length.

Public keys and shared secrets are points on an elliptic curve. These points can be expressed in several ways. The most common one is in affine coordinates as an X,Y pair. This API uses points expressed in uncompressed affine coordinates by default. The big-endian format requires a formatting byte in the first byte of the public key. When using uncompressed affine coordinates, this is the value 0x04. The point itself is stored as a concatenated array of X followed by Y. X and Y maybe in big-endian or little-endian. Some implementations do not require or yield the Y coordinate for ECDH on certain curves. It is recommended that the full keying material buffer of twice the curve param length is used to facilitate code-reuse. Implementations that do not use the Y coordinate will zero-out the Y-coordinate whenever they write a point to the CryptoKey.

If device-supported, Montgomery curves can be stored as their X-only format based on the RFC-7748 specification. Here, only the X coordinate is packed in little-endian integers of the same length as the curve length.

This API accepts and returns the keying material of public keys according to the following table:

Curve Type Keying Material Array Array Length
Short Weierstrass [0x04, X, Y] 1 + 2 * Curve Param Length
Montgomery [0x04, X, Y] 1 + 2 * Curve Param Length
Montgomery [X] Curve Param Length
Edwards [0x04, X, Y] 1 + 2 * Curve Param Length

Note: This driver will automatically prune the private key according to RFC 7748 for the following curve: X25519

Synopsis

// Import ECDH Driver definitions
// Since we are using default ECDH_Params, we just pass in NULL for that parameter.
ecdhHandle = ECDH_open(0, NULL);
// Initialize myPrivateKey and myPublicKey
CryptoKeyPlaintext_initKey(&myPrivateKey, myPrivateKeyingMaterial, sizeof(myPrivateKeyingMaterial));
CryptoKeyPlaintext_initBlankKey(&myPublicKey, myPublicKeyingMaterial, sizeof(myPublicKeyingMaterial));
ECDH_OperationGeneratePublicKey_init(&operationGeneratePublicKey);
operationGeneratePublicKey.curve = &ECCParams_NISTP256;
operationGeneratePublicKey.myPrivateKey = &myPrivateKey;
operationGeneratePublicKey.myPublicKey = &myPublicKey;
// Generate the keying material for myPublicKey and store it in myPublicKeyingMaterial
operationResult = ECDH_generatePublicKey(ecdhHandle, &operationGeneratePublicKey);
// Now send the content of myPublicKeyingMaterial to the other party,
// receive their public key, and copy their public keying material to theirPublicKeyingMaterial
// Initialize their public CryptoKey and the shared secret CryptoKey
CryptoKeyPlaintext_initKey(&theirPublicKey, theirPublicKeyingMaterial, sizeof(theirPublicKeyingMaterial));
CryptoKeyPlaintext_initBlankKey(&sharedSecret, sharedSecretKeyingMaterial, sizeof(sharedSecretKeyingMaterial));
// The ECC_NISTP256 struct is provided in ti/drivers/types/EccParams.h and the corresponding device-specific
implementation ECDH_OperationComputeSharedSecret_init(&operationComputeSharedSecret);
operationComputeSharedSecret.curve = &ECCParams_NISTP256;
operationComputeSharedSecret.myPrivateKey = &myPrivateKey;
operationComputeSharedSecret.theirPublicKey = &theirPublicKey;
operationComputeSharedSecret.sharedSecret = &sharedSecret;
// Compute the shared secret and copy it to sharedSecretKeyingMaterial
operationResult = ECDH_computeSharedSecret(ecdhHandle, &operationComputeSharedSecret);
// Close the driver
ECDH_close(ecdhHandle);

Synopsis for X25519 X-only key exchange

// Import ECDH Driver definitions
// Since we are using default ECDH_Params, we just pass in NULL for that parameter.
ecdhHandle = ECDH_open(0, NULL);
// Initialize myPrivateKey and myPublicKey
CryptoKeyPlaintext_initKey(&myPrivateKey, myPrivateKeyingMaterial, sizeof(myPrivateKeyingMaterial));
// Note that the public key size is only 32 bytes
CryptoKeyPlaintext_initBlankKey(&myPublicKey, myPublicKeyingMaterial, sizeof(myPublicKeyingMaterial));
ECDH_OperationGeneratePublicKey_init(&operationGeneratePublicKey);
operationGeneratePublicKey.curve = &ECCParams_Curve25519;
operationGeneratePublicKey.myPrivateKey = &myPrivateKey;
operationGeneratePublicKey.myPublicKey = &myPublicKey;
// If generating public key in little-endian format, we use the following format:
operationGeneratePublicKey.keyMaterialEndianness = ECDH_LITTLE_ENDIAN_KEY;
// Generate the keying material for myPublicKey and store it in myPublicKeyingMaterial
operationResult = ECDH_generatePublicKey(ecdhHandle, &operationGeneratePublicKey);
// Now send the content of myPublicKeyingMaterial to the other party,
// receive their public key, and copy their public keying material to theirPublicKeyingMaterial
// Initialize their public CryptoKey and the shared secret CryptoKey
CryptoKeyPlaintext_initKey(&theirPublicKey, theirPublicKeyingMaterial, sizeof(theirPublicKeyingMaterial));
CryptoKeyPlaintext_initBlankKey(&sharedSecret, sharedSecretKeyingMaterial, sizeof(sharedSecretKeyingMaterial));
// The ECC_NISTP256 struct is provided in ti/drivers/types/EccParams.h and the corresponding device-specific
implementation ECDH_OperationComputeSharedSecret_init(&operationComputeSharedSecret);
operationComputeSharedSecret.curve = &ECCParams_Curve25519;
operationComputeSharedSecret.myPrivateKey = &myPrivateKey;
operationComputeSharedSecret.theirPublicKey = &theirPublicKey;
operationComputeSharedSecret.sharedSecret = &sharedSecret;
// If receiving and generating keys in little-endian format, we use the following format:
operationComputeSharedSecret.keyMaterialEndianness = ECDH_LITTLE_ENDIAN_KEY;
// Compute the shared secret and copy it to sharedSecretKeyingMaterial
operationResult = ECDH_computeSharedSecret(ecdhHandle, &operationComputeSharedSecret);
// Close the driver
ECDH_close(ecdhHandle);

Examples

ECDH exchange with plaintext CryptoKeys

#define CURVE_LENGTH 32
...
// Our private key is 0x0000000000000000000000000000000000000000000000000000000000000001
// In practice, this value should come from a TRNG, PRNG, PUF, or device-specific pre-seeded key
uint8_t myPrivateKeyingMaterial[CURVE_LENGTH] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x01};
uint8_t myPublicKeyingMaterial[2 * CURVE_LENGTH + 1] = {0};
uint8_t theirPublicKeyingMaterial[2 * CURVE_LENGTH + 1] = {0};
uint8_t sharedSecretKeyingMaterial[2 * CURVE_LENGTH + 1] = {0};
uint8_t symmetricKeyingMaterial[16] = {0};
CryptoKey myPrivateKey;
CryptoKey myPublicKey;
CryptoKey theirPublicKey;
CryptoKey sharedSecret;
CryptoKey symmetricKey;
ECDH_Handle ecdhHandle;
int_fast16_t operationResult;
ECDH_OperationGeneratePublicKey operationGeneratePublicKey;
// Since we are using default ECDH_Params, we just pass in NULL for that parameter.
ecdhHandle = ECDH_open(0, NULL);
if (!ecdhHandle) {
// Handle error
}
// Initialize myPrivateKey and myPublicKey
CryptoKeyPlaintext_initKey(&myPrivateKey, myPrivateKeyingMaterial, sizeof(myPrivateKeyingMaterial));
CryptoKeyPlaintext_initBlankKey(&myPublicKey, myPublicKeyingMaterial, sizeof(myPublicKeyingMaterial));
ECDH_OperationGeneratePublicKey_init(&operationGeneratePublicKey);
operationGeneratePublicKey.curve = &ECCParams_NISTP256;
operationGeneratePublicKey.myPrivateKey = &myPrivateKey;
operationGeneratePublicKey.myPublicKey = &myPublicKey;
// Generate the keying material for myPublicKey and store it in myPublicKeyingMaterial
operationResult = ECDH_generatePublicKey(ecdhHandle, &operationGeneratePublicKey);
if (operationResult != ECDH_STATUS_SUCCESS) {
// Handle error
}
// Now send the content of myPublicKeyingMaterial to the other party,
// receive their public key, and copy their public keying material and the
// 0x04 byte to theirPublicKeyingMaterial
// Initialise their public CryptoKey and the shared secret CryptoKey
CryptoKeyPlaintext_initKey(&theirPublicKey, theirPublicKeyingMaterial, sizeof(theirPublicKeyingMaterial));
CryptoKeyPlaintext_initBlankKey(&sharedSecret, sharedSecretKeyingMaterial, sizeof(sharedSecretKeyingMaterial));
// The ECC_NISTP256 struct is provided in ti/drivers/types/EccParams.h and the corresponding device-specific
implementation ECDH_OperationComputeSharedSecret_init(&operationComputeSharedSecret);
operationComputeSharedSecret.curve = &ECCParams_NISTP256;
operationComputeSharedSecret.myPrivateKey = &myPrivateKey;
operationComputeSharedSecret.theirPublicKey = &theirPublicKey;
operationComputeSharedSecret.sharedSecret = &sharedSecret;
// Compute the shared secret and copy it to sharedSecretKeyingMaterial
operationResult = ECDH_computeSharedSecret(ecdhHandle, &operationComputeSharedSecret);
if (operationResult != ECDH_STATUS_SUCCESS) {
// Handle error
}
CryptoKeyPlaintext_initBlankKey(&symmetricKey, symmetricKeyingMaterial, sizeof(symmetricKeyingMaterial));
// Set up a KDF such as HKDF and open the requisite cryptographic primitive driver to implement it
// HKDF and SHA2 were chosen as an example and may not be available directly
// At this point, you and the other party have both created the content within symmetricKeyingMaterial without
// someone else listening to your communication channel being able to do so
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKey.h>
#include <ti/drivers/cryptoutils/ecc/ECCParams.h>
Include dependency graph for ECDH.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  ECDH_Config
 ECC Global configuration. More...
 
struct  ECDH_OperationGeneratePublicKey
 Struct containing the parameters required to generate a public key. More...
 
struct  ECDH_OperationComputeSharedSecret
 Struct containing the parameters required to compute the shared secret. More...
 
union  ECDH_Operation
 Union containing pointers to all supported operation structs. More...
 
struct  ECDH_Params
 ECC Parameters. More...
 

Macros

#define ECDH_STATUS_RESERVED   (-32)
 
#define ECDH_STATUS_SUCCESS   (0)
 Successful status code. More...
 
#define ECDH_STATUS_ERROR   (-1)
 Generic error status code. More...
 
#define ECDH_STATUS_RESOURCE_UNAVAILABLE   (-2)
 An error status code returned if the hardware or software resource is currently unavailable. More...
 
#define ECDH_STATUS_POINT_AT_INFINITY   (-3)
 The result of the operation is the point at infinity. More...
 
#define ECDH_STATUS_PRIVATE_KEY_LARGER_EQUAL_ORDER   (-4)
 The private key passed in is larger or equal to the order of the curve. More...
 
#define ECDH_STATUS_PRIVATE_KEY_ZERO   (-5)
 The private key passed in is zero. More...
 
#define ECDH_STATUS_PUBLIC_KEY_NOT_ON_CURVE   (-6)
 The public key of the other party does not lie upon the curve. More...
 
#define ECDH_STATUS_PUBLIC_KEY_LARGER_THAN_PRIME   (-7)
 A coordinate of the public key of the other party is too large. More...
 
#define ECDH_STATUS_CANCELED   (-8)
 The ongoing operation was canceled. More...
 
#define ECDH_STATUS_INVALID_KEY_SIZE   (-9)
 The provided CryptoKey does not match the expected size. More...
 
#define ECDH_STATUS_KEYSTORE_ERROR   (-10)
 Importing generated key into KeyStore failed. More...
 

Typedefs

typedef ECDH_ConfigECDH_Handle
 A handle that is returned from an ECDH_open() call. More...
 
typedef void(* ECDH_CallbackFxn) (ECDH_Handle handle, int_fast16_t returnStatus, ECDH_Operation operation, ECDH_OperationType operationType)
 The definition of a callback function used by the ECDH driver when used in ECDH_RETURN_BEHAVIOR_CALLBACK. More...
 

Enumerations

enum  ECDH_ReturnBehavior { ECDH_RETURN_BEHAVIOR_CALLBACK = 1, ECDH_RETURN_BEHAVIOR_BLOCKING = 2, ECDH_RETURN_BEHAVIOR_POLLING = 4 }
 The way in which ECDH function calls return after performing a public key generation or shared secret compution operation. More...
 
enum  ECDH_KeyMaterialEndianness { ECDH_BIG_ENDIAN_KEY = 0, ECDH_LITTLE_ENDIAN_KEY = 1 }
 
enum  ECDH_OperationType { ECDH_OPERATION_TYPE_GENERATE_PUBLIC_KEY = 1, ECDH_OPERATION_TYPE_COMPUTE_SHARED_SECRET = 2 }
 Enum for the operation types supported by the driver. More...
 

Functions

void ECDH_init (void)
 This function initializes the ECC module. More...
 
void ECDH_Params_init (ECDH_Params *params)
 Function to initialize the ECDH_Params struct to its defaults. More...
 
ECDH_Handle ECDH_open (uint_least8_t index, const ECDH_Params *params)
 This function opens a given ECC peripheral. More...
 
void ECDH_close (ECDH_Handle handle)
 Function to close an ECC peripheral specified by the ECC handle. More...
 
void ECDH_OperationGeneratePublicKey_init (ECDH_OperationGeneratePublicKey *operation)
 Function to initialize an ECDH_OperationGeneratePublicKey struct to its defaults. More...
 
void ECDH_OperationComputeSharedSecret_init (ECDH_OperationComputeSharedSecret *operation)
 Function to initialize an ECDH_OperationComputeSharedSecret struct to its defaults. More...
 
int_fast16_t ECDH_generatePublicKey (ECDH_Handle handle, ECDH_OperationGeneratePublicKey *operation)
 Generates a public key for use in key agreement. More...
 
int_fast16_t ECDH_computeSharedSecret (ECDH_Handle handle, ECDH_OperationComputeSharedSecret *operation)
 Computes a shared secret. More...
 
int_fast16_t ECDH_cancelOperation (ECDH_Handle handle)
 Cancels an ongoing ECDH operation. More...
 
ECDH_Handle ECDH_construct (ECDH_Config *config, const ECDH_Params *params)
 Constructs a new ECDH object. More...
 

Variables

const ECDH_Params ECDH_defaultParams
 Default ECDH_Params structure. More...
 

Macro Definition Documentation

§ ECDH_STATUS_RESERVED

#define ECDH_STATUS_RESERVED   (-32)

Common ECDH status code reservation offset. ECC driver implementations should offset status codes with ECDH_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

#define ECCXYZ_STATUS_ERROR0 ECDH_STATUS_RESERVED - 0
#define ECCXYZ_STATUS_ERROR1 ECDH_STATUS_RESERVED - 1
#define ECCXYZ_STATUS_ERROR2 ECDH_STATUS_RESERVED - 2

§ ECDH_STATUS_SUCCESS

#define ECDH_STATUS_SUCCESS   (0)

Successful status code.

Functions return ECDH_STATUS_SUCCESS if the function was executed successfully.

§ ECDH_STATUS_ERROR

#define ECDH_STATUS_ERROR   (-1)

Generic error status code.

Functions return ECDH_STATUS_ERROR if the function was not executed successfully.

§ ECDH_STATUS_RESOURCE_UNAVAILABLE

#define ECDH_STATUS_RESOURCE_UNAVAILABLE   (-2)

An error status code returned if the hardware or software resource is currently unavailable.

ECC driver implementations may have hardware or software limitations on how many clients can simultaneously perform operations. This status code is returned if the mutual exclusion mechanism signals that an operation cannot currently be performed.

§ ECDH_STATUS_POINT_AT_INFINITY

#define ECDH_STATUS_POINT_AT_INFINITY   (-3)

The result of the operation is the point at infinity.

The operation yielded the point at infinity on this curve. This point is not permitted for further use in ECC operations.

§ ECDH_STATUS_PRIVATE_KEY_LARGER_EQUAL_ORDER

#define ECDH_STATUS_PRIVATE_KEY_LARGER_EQUAL_ORDER   (-4)

The private key passed in is larger or equal to the order of the curve.

Private keys must be integers in the interval [1, n - 1], where n is the order of the curve.

§ ECDH_STATUS_PRIVATE_KEY_ZERO

#define ECDH_STATUS_PRIVATE_KEY_ZERO   (-5)

The private key passed in is zero.

Private keys must be integers in the interval [1, n - 1], where n is the order of the curve.

§ ECDH_STATUS_PUBLIC_KEY_NOT_ON_CURVE

#define ECDH_STATUS_PUBLIC_KEY_NOT_ON_CURVE   (-6)

The public key of the other party does not lie upon the curve.

The public key received from the other party does not lie upon the agreed upon curve.

§ ECDH_STATUS_PUBLIC_KEY_LARGER_THAN_PRIME

#define ECDH_STATUS_PUBLIC_KEY_LARGER_THAN_PRIME   (-7)

A coordinate of the public key of the other party is too large.

A coordinate of the public key received from the other party is larger than the prime of the curve. This implies that the point was not correctly generated on that curve.

§ ECDH_STATUS_CANCELED

#define ECDH_STATUS_CANCELED   (-8)

The ongoing operation was canceled.

§ ECDH_STATUS_INVALID_KEY_SIZE

#define ECDH_STATUS_INVALID_KEY_SIZE   (-9)

The provided CryptoKey does not match the expected size.

The driver expects the private key to have the same length as other curve parameters and the public key to have a length of twice that plus one. If the provided CryptoKeys for the public and private keys do not match this scheme, this error will be returned.

§ ECDH_STATUS_KEYSTORE_ERROR

#define ECDH_STATUS_KEYSTORE_ERROR   (-10)

Importing generated key into KeyStore failed.

Functions return ECDH_STATUS_KEYSTORE_ERROR if the KeyStore_PSA_importKey() did not return KEYSTORE_PSA_STATUS_SUCCESS

Typedef Documentation

§ ECDH_Handle

A handle that is returned from an ECDH_open() call.

§ ECDH_CallbackFxn

typedef void(* ECDH_CallbackFxn) (ECDH_Handle handle, int_fast16_t returnStatus, ECDH_Operation operation, ECDH_OperationType operationType)

The definition of a callback function used by the ECDH driver when used in ECDH_RETURN_BEHAVIOR_CALLBACK.

Parameters
handleHandle of the client that started the ECDH operation.
returnStatusThe result of the ECDH operation. May contain an error code if the result is the point at infinity for example.
operationA union of pointers to operation structs. Only one type of pointer is valid per call to the callback function. Which type is currently valid is determined by /c operationType. The union allows easier access to the struct's fields without the need to typecase the result.
operationTypeThis parameter determined which operation the callback refers to and which type to access through /c operation.

Enumeration Type Documentation

§ ECDH_ReturnBehavior

The way in which ECDH function calls return after performing a public key generation or shared secret compution operation.

Callback return behavior is not supported by software-backed implementations. A NULL handle will be returned when attempting to open or construct a driver instance with an unsupported return behavior.

Not all ECDH operations exhibit the specified return behavior. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specfied return behavior is not implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.

ECDH functions exhibiting the specified return behavior have restrictions on the context from which they may be called.

Task Hwi Swi
ECDH_RETURN_BEHAVIOR_CALLBACK X X X
ECDH_RETURN_BEHAVIOR_BLOCKING X
ECDH_RETURN_BEHAVIOR_POLLING X X X
Enumerator
ECDH_RETURN_BEHAVIOR_CALLBACK 

The function call will return immediately while the ECC operation goes on in the background. The registered callback function is called after the operation completes. The context the callback function is called (task, HWI, SWI) is implementation-dependent.

ECDH_RETURN_BEHAVIOR_BLOCKING 

The function call will block while ECC operation goes on in the background. ECC operation results are available after the function returns.

ECDH_RETURN_BEHAVIOR_POLLING 

The function call will continuously poll a flag while ECC operation goes on in the background. ECC operation results are available after the function returns.

§ ECDH_KeyMaterialEndianness

Enumerator
ECDH_BIG_ENDIAN_KEY 

All ECDH key material (private key, public key, and shared secret (when used)) are in big-endian format

ECDH_LITTLE_ENDIAN_KEY 

All ECDH key material (private key, public key, and shared secret (when used)) are in little-endian format

§ ECDH_OperationType

Enum for the operation types supported by the driver.

Enumerator
ECDH_OPERATION_TYPE_GENERATE_PUBLIC_KEY 
ECDH_OPERATION_TYPE_COMPUTE_SHARED_SECRET 

Function Documentation

§ ECDH_init()

void ECDH_init ( void  )

This function initializes the ECC module.

Precondition
The ECDH_config structure must exist and be persistent before this function can be called. This function must also be called before any other ECC driver APIs. This function call does not modify any peripheral registers.

§ ECDH_Params_init()

void ECDH_Params_init ( ECDH_Params params)

Function to initialize the ECDH_Params struct to its defaults.

Parameters
paramsAn pointer to ECDH_Params structure for initialization

Defaults values are: returnBehavior = ECDH_RETURN_BEHAVIOR_BLOCKING callbackFxn = NULL timeout = SemaphoreP_WAIT_FOREVER custom = NULL

§ ECDH_open()

ECDH_Handle ECDH_open ( uint_least8_t  index,
const ECDH_Params params 
)

This function opens a given ECC peripheral.

Precondition
ECC controller has been initialized using ECDH_init()
Parameters
indexLogical peripheral number for the ECC indexed into the ECDH_config table
paramsPointer to an parameter block, if NULL it will use default values.
Returns
An ECDH_Handle on success or a NULL on an error or if it has been opened already.
See also
ECDH_init()
ECDH_close()

§ ECDH_close()

void ECDH_close ( ECDH_Handle  handle)

Function to close an ECC peripheral specified by the ECC handle.

Precondition
ECDH_open() has to be called first.
Parameters
handleAn ECC handle returned from ECDH_open()
See also
ECDH_open()

§ ECDH_OperationGeneratePublicKey_init()

void ECDH_OperationGeneratePublicKey_init ( ECDH_OperationGeneratePublicKey operation)

Function to initialize an ECDH_OperationGeneratePublicKey struct to its defaults.

Parameters
operationA pointer to ECDH_OperationGeneratePublicKey structure for initialization

Defaults values are all zeros.

§ ECDH_OperationComputeSharedSecret_init()

void ECDH_OperationComputeSharedSecret_init ( ECDH_OperationComputeSharedSecret operation)

Function to initialize an ECDH_OperationComputeSharedSecret struct to its defaults.

Parameters
operationA pointer to ECDH_OperationComputeSharedSecret structure for initialization

Defaults values are all zeros.

§ ECDH_generatePublicKey()

int_fast16_t ECDH_generatePublicKey ( ECDH_Handle  handle,
ECDH_OperationGeneratePublicKey operation 
)

Generates a public key for use in key agreement.

This function can be used to generate a public key from a private key.

Parameters
handleA ECDH handle returned from ECDH_open()
operationA pointer to a struct containing the requisite parameters to execute the function.
Precondition
Call ECDH_OperationGeneratePublicKey_init() on operation.
Postcondition
ECDH_computeSharedSecret()
Return values
ECDH_STATUS_SUCCESSThe operation succeeded.
ECDH_STATUS_ERRORThe operation failed.
ECDH_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
ECDH_STATUS_CANCELEDThe operation was canceled.
ECDH_STATUS_POINT_AT_INFINITYThe computed public key is the point at infinity.
ECDH_STATUS_PRIVATE_KEY_ZEROThe provided private key is zero.
ECDH_STATUS_PRIVATE_KEY_LARGER_EQUAL_ORDERThe provided private key is larger than or equal to the order of the curve.

§ ECDH_computeSharedSecret()

int_fast16_t ECDH_computeSharedSecret ( ECDH_Handle  handle,
ECDH_OperationComputeSharedSecret operation 
)

Computes a shared secret.

This secret can be used to generate shared keys for encryption and authentication.

Parameters
handleA ECDH handle returned from ECDH_open()
operationA pointer to a struct containing the requisite
Precondition
Call ECDH_OperationComputeSharedSecret_init() on operation. Generate a shared secret off-chip or using ECDH_generatePublicKey()
Return values
ECDH_STATUS_SUCCESSThe operation succeeded.
ECDH_STATUS_ERRORThe operation failed.
ECDH_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
ECDH_STATUS_CANCELEDThe operation was canceled.
ECDH_STATUS_PUBLIC_KEY_NOT_ON_CURVEThe foreign public key is not a point on the specified curve.
ECDH_STATUS_PUBLIC_KEY_LARGER_THAN_PRIMEOne of the public key coordinates is larger the the curve's prime.

§ ECDH_cancelOperation()

int_fast16_t ECDH_cancelOperation ( ECDH_Handle  handle)

Cancels an ongoing ECDH operation.

Asynchronously cancels an ECDH operation. Only available when using ECDH_RETURN_BEHAVIOR_CALLBACK or ECDH_RETURN_BEHAVIOR_BLOCKING. The operation will terminate as though an error occurred. The return status code of the operation will be ECDH_STATUS_CANCELED.

Parameters
handleHandle of the operation to cancel
Return values
ECDH_STATUS_SUCCESSThe operation was canceled.
ECDH_STATUS_ERRORThe operation was not canceled. There may be no operation to cancel.

§ ECDH_construct()

ECDH_Handle ECDH_construct ( ECDH_Config config,
const ECDH_Params params 
)

Constructs a new ECDH object.

Unlike ECDH_open(), ECDH_construct() does not require the hwAttrs and object to be allocated in a ECDH_Config array that is indexed into. Instead, the ECDH_Config, hwAttrs, and object can be allocated at any location. This allows for relatively simple run-time allocation of temporary driver instances on the stack or the heap. The drawback is that this makes it more difficult to write device-agnostic code. If you use an ifdef with DeviceFamily, you can choose the correct object and hwAttrs to allocate. That compilation unit will be tied to the device it was compiled for at this point. To change devices, recompilation of the application with a different DeviceFamily setting is necessary.

Parameters
configECDH_Config describing the location of the object and hwAttrs.
paramsECDH_Params to configure the driver instance.
Returns
Returns a ECDH_Handle on success or NULL on failure.
Precondition
The object struct config points to must be zeroed out prior to calling this function. Otherwise, unexpected behavior may ensue.

Variable Documentation

§ ECDH_defaultParams

const ECDH_Params ECDH_defaultParams

Default ECDH_Params structure.

See also
ECDH_Params_init()
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale