Data Structures | Macros | Enumerations | Functions
ITM.h File Reference

Detailed Description

ITM driver header.


Overview

This driver implements APIs to configure and control the ARM Instrumentation Trace Macrocell (ITM), Debug Watchpoint and Trace (DWT), and Trace Port Instrumentation Unit (TPIU) IPs to realize non-intrusive software logging and runtime trace.

Overview

The ITM software module provides application level APIs for the non-invasive debug capabilities of the ARM Cortex-M family. This includes the following hardware modules:

At a high level, the DWT provides watchpoint, data trace, and program counter sampling. The ITM provides memory mapped registers for low-intrusion software profiling. The TPIU provides an external interface for the ITM and DWT. Further details can be found in the ARMv7-M Architecture Reference Manual

Limitations and Constraints

The driver is is designed with the following constraints in mind:

Setup

The ITM is configured via hardware attributes stored in the hardware attributes structure. This structure contains a common portion that is used for all drivers. This structure may be extended for some devices such as CC26XX.

Opening the driver

Unlike other drivers, the ITM is intended to be a singleton. This means that ITM_open can be called multiple times. The ITM will only be configured the first time open is called.

Furthermore, helper functions for features such as PC sampling must coherent across clients. The driver offers no protection against mismatched configuration.

The open call will enable ITM as well as the necessary stimulus ports. It will setup the TPIU for necessary baudrate and serial format.

Pin Muxing

As the ITM driver is primarily interfacing to ARM defined IP, it is almost entirely common across all supported devices. The only specifics are pin muxing of the SWO pin. See the table below for some notes

Device Family Debug Protocol Muxing Configurable?
CC32XX SWD Shared with TDO N
CC13XX/CC26XX JTAG/cJTAG Any pin Y

Device specific pin muxing is done by the device specific ITM backend implementation.

Software Messages

The ITM stimulus ports enable serialization of application data with low overhead. There are multiple ports available, they are selectable via software.

Data written to the software stimulus ports is serialized by the TPIU and wrapped in the SWIT packet format. This packet format is standardized by ARM and described in ARMv7-M Architecture Reference Manual

There are three tiers of access to the stimulus ports. In the table below, polled access means that the API/macro will poll the port's busy flag before writing. This is done to prevent silent data loss that occurs when writing to a port that is not ready. Actual serialization of the data will occur later inside the TPIU.

It is up the the application writer to understand the tradeoff associated with each of these and select the correct one.

DWT Features

The Data Watchpoint and Trace (DWT) module is capable of many instrumentation features such as

Feature ITM API
Exception trace ITM_enableExceptionTrace
Program Counter sampling ITM_enablePCSampling
Event counting ITM_enableEventCounter
Synchronization packets ITM_enableSyncPackets

Data generated by the DWT is serialized via the TPIU. DWT packet formats are defined in the ARMv7-M Architecture Reference Manual referenced above

Flush

The ITM/DWT/TPIU hardware resides in the CPU power domain. This means that whenever the CPU domain is powered down, ITM will power down. Powering down when data is inside in the TPIU can result in lost data. In order to prevent dataloss, the device's power policy will flush the ITM before powering down the CPU domain. When returning from sleep, the power policy will restore the ITM. This is achieved using the ITM_flush and ITM_restore.

These functions are weakly defined as empty functions. This reduces the overhead in the power policy when ITM is not enabled. These weak functions are overridden by syscfg when ITM is enabled.

#include <stddef.h>
#include <stdbool.h>
#include <stdint.h>
#include <ti/devices/DeviceFamily.h>
Include dependency graph for ITM.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  ITM_HWAttrs
 ITM Hardware Attributes. More...
 

Macros

#define ITM_BASE_ADDR   (0xE0000000)
 Base address of the Instrumentation Trace Macrocell (ITM) module. More...
 
#define ITM_DWT_BASE_ADDR   (0xE0001000)
 Base address of the Debug Watchpoint and Trace (DWT) module. More...
 
#define ITM_SCS_BASE_ADDR   (0xE000E000)
 Base address of the CPU_SCS module. More...
 
#define ITM_TPIU_BASE_ADDR   (0xE0040000)
 Base address of the Trace Port Instrumentation Unit (TPIU) module. More...
 
#define ITM_LAR_UNLOCK   (0xC5ACCE55)
 Value to unlock ARM debug modules. This value should be written to the Lock Access Registers (LAR) in order to enable their configuration and use. More...
 
#define ITM_FUNCTION_DISABLED   (0x00)
 Device-specific values that implement the generic ITM-functions in ITM_WatchpointAction. More...
 
#define ITM_FUNCTION_EMIT_PC   (0x30 | 0x4)
 
#define ITM_FUNCTION_EMIT_DATA_ON_READ_WRITE   (0x800 | 0x20 | 0xc)
 
#define ITM_FUNCTION_EMIT_PC_ON_READ_WRITE   (0x800 | 0x30 | 0x2)
 
#define ITM_FUNCTION_EMIT_DATA_ON_READ   (0x800 | 0x20 | 0xe)
 
#define ITM_FUNCTION_EMIT_DATA_ON_WRITE   (0x800 | 0x20 | 0xd)
 
#define ITM_FUNCTION_EMIT_PC_AND_DATA_ON_READ   (0x800 | 0x30 | 0xe)
 
#define ITM_FUNCTION_EMIT_PC_AND_DATA_ON_WRITE   (0x800 | 0x30 | 0xd)
 
#define ITM_port32(n)   (*((volatile unsigned int *)(ITM_BASE_ADDR + 4 * n)))
 Write a 32-bit word to stimulus port n. More...
 
#define ITM_send32Polling(n, x)
 Write a 32-bit word to stimulus port n with polling. More...
 
#define ITM_port16(n)   (*((volatile unsigned short *)(ITM_BASE_ADDR + 4 * n)))
 Write a 16-bit half word to stimulus port n. More...
 
#define ITM_send16Polling(n, x)
 Write a 16-bit word to stimulus port n with polling. More...
 
#define ITM_port8(n)   (*((volatile unsigned char *)(ITM_BASE_ADDR + 4 * n)))
 Write a byte to stimulus port n. More...
 
#define ITM_send8Polling(n, x)
 Write a 8-bit word to stimulus port n with polling. More...
 

Enumerations

enum  ITM_TPIU_PortFormat { ITM_TPIU_SWO_MANCHESTER = 0x00000001, ITM_TPIU_SWO_UART = 0x00000002 }
 
enum  ITM_WatchpointAction {
  ITM_Disabled = (0x00), ITM_EmitPc = (0x30 | 0x4), ITM_EmitDataOnReadWrite = (0x800 | 0x20 | 0xc), ITM_SamplePcAndEmitDataOnReadWrite = (0x800 | 0x30 | 0x2),
  ITM_SampleDataOnRead = (0x800 | 0x20 | 0xe), ITM_SampleDataOnWrite = (0x800 | 0x20 | 0xd), ITM_SamplePcAndDataOnRead = (0x800 | 0x30 | 0xe), ITM_SamplePcAndDataOnWrite = (0x800 | 0x30 | 0xd)
}
 Control the action taken by the DWT on comparator match. More...
 
enum  ITM_TimeStampPrescaler { ITM_TS_DIV_NONE = 0, ITM_TS_DIV_4 = 1, ITM_TS_DIV_16 = 2, ITM_TS_DIV_64 = 3 }
 Prescaler for ITM timestamp generation based on the trace packet reference clock. More...
 
enum  ITM_SyncPacketRate { ITM_SYNC_NONE = 0, ITM_SYNC_TAP_BIT24 = 1, ITM_SYNC_TAP_BIT26 = 2, ITM_SYNC_TAP_BIT28 = 3 }
 Synchronous packet generation rate based on cycles of CYCCNT This controls how often sync packets will be generated. The tap controls which bit transition in the counter triggers a packet. More...
 

Functions

bool ITM_open (void)
 Open and configure the ITM, DWT, and TPIU. This includes muxing pins as needed. More...
 
void ITM_close (void)
 
void ITM_sendBufferAtomic (const uint8_t port, const char *msg, size_t length)
 Write the contents of a buffer to the stimulus port, polling to ensure the port is available. More...
 
void ITM_send32Atomic (uint8_t port, uint32_t value)
 Write a 32-bit word to the given stimulus port, polling to ensure the port is available. More...
 
void ITM_send16Atomic (uint8_t port, uint16_t value)
 Write a 16-bit short to the given stimulus port, polling to ensure the port is available. More...
 
void ITM_send8Atomic (uint8_t port, uint8_t value)
 Write an 8-bit byte to the given stimulus port, polling to ensure the port is available. More...
 
void ITM_enableExceptionTrace (void)
 Enable exception tracing This will trigger the DWT to generate packets when the device enters or leaves an exception. The ITM will forward these packets to the TPIU to be sent to the debugger. More...
 
void ITM_disableExceptionTrace (void)
 Disable exception tracing. More...
 
void ITM_enablePCSampling (bool prescale1024, uint8_t postReset)
 Enable periodic sampling of the program counter using the DWT POSTCNT timer. More...
 
void ITM_enableEventCounter (bool prescale1024, uint8_t postReset)
 Enable generation of event counter packets using the DWT POSTCNT timer. More...
 
void ITM_disablePCAndEventSampling (void)
 Disable program counter and event sampling in the DWT. More...
 
void ITM_enableTimestamps (ITM_TimeStampPrescaler tsPrescale, bool asyncMode)
 Enable the generation of local timestamp packets from the ITM module These are packets sent form the ITM that measure how long it has been since the previous timestamp. More...
 
void ITM_enableSyncPackets (ITM_SyncPacketRate syncPacketRate)
 Enable the generation of synchronization packets from the ITM based on the CYCCNT counter. Synchronization packets can be used to recover bit-to-byte alignment information in a serial data stream. More...
 
bool ITM_enableWatchpoint (ITM_WatchpointAction function, const uintptr_t address)
 Enable the watchpoint functionality using a DWT comparator. More...
 
void ITM_flush (void)
 Flush the ITM in preparation for power off of CPU domain. More...
 
void ITM_restore (void)
 Prepare the ITM hardware to return from power off of CPU domain This will reenable DWT features, re apply the ITM pin mux. More...
 

Macro Definition Documentation

§ ITM_BASE_ADDR

#define ITM_BASE_ADDR   (0xE0000000)

Base address of the Instrumentation Trace Macrocell (ITM) module.

§ ITM_DWT_BASE_ADDR

#define ITM_DWT_BASE_ADDR   (0xE0001000)

Base address of the Debug Watchpoint and Trace (DWT) module.

§ ITM_SCS_BASE_ADDR

#define ITM_SCS_BASE_ADDR   (0xE000E000)

Base address of the CPU_SCS module.

§ ITM_TPIU_BASE_ADDR

#define ITM_TPIU_BASE_ADDR   (0xE0040000)

Base address of the Trace Port Instrumentation Unit (TPIU) module.

§ ITM_LAR_UNLOCK

#define ITM_LAR_UNLOCK   (0xC5ACCE55)

Value to unlock ARM debug modules. This value should be written to the Lock Access Registers (LAR) in order to enable their configuration and use.

§ ITM_FUNCTION_DISABLED

#define ITM_FUNCTION_DISABLED   (0x00)

Device-specific values that implement the generic ITM-functions in ITM_WatchpointAction.

§ ITM_FUNCTION_EMIT_PC

#define ITM_FUNCTION_EMIT_PC   (0x30 | 0x4)

§ ITM_FUNCTION_EMIT_DATA_ON_READ_WRITE

#define ITM_FUNCTION_EMIT_DATA_ON_READ_WRITE   (0x800 | 0x20 | 0xc)

§ ITM_FUNCTION_EMIT_PC_ON_READ_WRITE

#define ITM_FUNCTION_EMIT_PC_ON_READ_WRITE   (0x800 | 0x30 | 0x2)

§ ITM_FUNCTION_EMIT_DATA_ON_READ

#define ITM_FUNCTION_EMIT_DATA_ON_READ   (0x800 | 0x20 | 0xe)

§ ITM_FUNCTION_EMIT_DATA_ON_WRITE

#define ITM_FUNCTION_EMIT_DATA_ON_WRITE   (0x800 | 0x20 | 0xd)

§ ITM_FUNCTION_EMIT_PC_AND_DATA_ON_READ

#define ITM_FUNCTION_EMIT_PC_AND_DATA_ON_READ   (0x800 | 0x30 | 0xe)

§ ITM_FUNCTION_EMIT_PC_AND_DATA_ON_WRITE

#define ITM_FUNCTION_EMIT_PC_AND_DATA_ON_WRITE   (0x800 | 0x30 | 0xd)

§ ITM_port32

#define ITM_port32 (   n)    (*((volatile unsigned int *)(ITM_BASE_ADDR + 4 * n)))

Write a 32-bit word to stimulus port n.

Warning
This does not does not first poll the port for availability.

§ ITM_send32Polling

#define ITM_send32Polling (   n,
 
)
Value:
do \
{ \
while (0 == ITM_port32(n)) \
; \
ITM_port32(n) = x; \
} while (0)
#define ITM_port32(n)
Write a 32-bit word to stimulus port n.
Definition: ITM.h:237

Write a 32-bit word to stimulus port n with polling.

Warning
This macro does not guarantee atomic access between poll and write

§ ITM_port16

#define ITM_port16 (   n)    (*((volatile unsigned short *)(ITM_BASE_ADDR + 4 * n)))

Write a 16-bit half word to stimulus port n.

Warning
This does not does not first poll the port for availability.

§ ITM_send16Polling

#define ITM_send16Polling (   n,
 
)
Value:
do \
{ \
while (0 == ITM_port16(n)) \
; \
ITM_port16(n) = x; \
} while (0)
#define ITM_port16(n)
Write a 16-bit half word to stimulus port n.
Definition: ITM.h:263

Write a 16-bit word to stimulus port n with polling.

Warning
This macro does not guarantee atomic access between poll and write

§ ITM_port8

#define ITM_port8 (   n)    (*((volatile unsigned char *)(ITM_BASE_ADDR + 4 * n)))

Write a byte to stimulus port n.

Warning
This does not does not first poll the port for availability.

§ ITM_send8Polling

#define ITM_send8Polling (   n,
 
)
Value:
do \
{ \
while (0 == ITM_port8(n)) \
; \
ITM_port8(n) = x; \
} while (0)
#define ITM_port8(n)
Write a byte to stimulus port n.
Definition: ITM.h:284

Write a 8-bit word to stimulus port n with polling.

Warning
This macro does not guarantee atomic access between poll and write

Enumeration Type Documentation

§ ITM_TPIU_PortFormat

Enumerator
ITM_TPIU_SWO_MANCHESTER 

Serial format is manchester

ITM_TPIU_SWO_UART 

Serial format is UART

§ ITM_WatchpointAction

Control the action taken by the DWT on comparator match.

Enumerator
ITM_Disabled 

Disabled

ITM_EmitPc 

Emit Program Counter

ITM_EmitDataOnReadWrite 

Emit Data on Read or Write

ITM_SamplePcAndEmitDataOnReadWrite 

Emit Program Counter on Read or Write

ITM_SampleDataOnRead 

Sample Data on Read

ITM_SampleDataOnWrite 

Sample Data on Write

ITM_SamplePcAndDataOnRead 

Sample PC and Data on Read

ITM_SamplePcAndDataOnWrite 

Sample PC and Data on Write

§ ITM_TimeStampPrescaler

Prescaler for ITM timestamp generation based on the trace packet reference clock.

Enumerator
ITM_TS_DIV_NONE 

No division

ITM_TS_DIV_4 

Divide by 4

ITM_TS_DIV_16 

Divide by 16

ITM_TS_DIV_64 

Divide by 64

§ ITM_SyncPacketRate

Synchronous packet generation rate based on cycles of CYCCNT This controls how often sync packets will be generated. The tap controls which bit transition in the counter triggers a packet.

Enumerator
ITM_SYNC_NONE 

Disabled

ITM_SYNC_TAP_BIT24 

Tap the CYCCNT register at bit 24

ITM_SYNC_TAP_BIT26 

Tap the CYCCNT register at bit 26

ITM_SYNC_TAP_BIT28 

Tap the CYCCNT register at bit 28

Function Documentation

§ ITM_open()

bool ITM_open ( void  )

Open and configure the ITM, DWT, and TPIU. This includes muxing pins as needed.

Returns
true - The ITM was successfully configured and the pins were acquired
false - Pin muxing failed and the ITM was not configured

§ ITM_close()

void ITM_close ( void  )

Disable the ITM, when it is no longer in use, it will be shutdown. This will also turn off any additional features that were enabled such as PC sampling or interrupt tracing

See also
ITM_open()

§ ITM_sendBufferAtomic()

void ITM_sendBufferAtomic ( const uint8_t  port,
const char *  msg,
size_t  length 
)

Write the contents of a buffer to the stimulus port, polling to ensure the port is available.

Warning
This API will disable interrupts for the entire buffer duration Use it cautiously to prevent negatively impacting interrupt latency
Parameters
portThe stimulus port to use
msgData to send.
lengthlength of buffer in bytes

§ ITM_send32Atomic()

void ITM_send32Atomic ( uint8_t  port,
uint32_t  value 
)

Write a 32-bit word to the given stimulus port, polling to ensure the port is available.

Parameters
portThe stimulus port to use
valueThe 32-bit value to write

§ ITM_send16Atomic()

void ITM_send16Atomic ( uint8_t  port,
uint16_t  value 
)

Write a 16-bit short to the given stimulus port, polling to ensure the port is available.

Parameters
portThe stimulus port to use
valueThe 16-bit value to write

§ ITM_send8Atomic()

void ITM_send8Atomic ( uint8_t  port,
uint8_t  value 
)

Write an 8-bit byte to the given stimulus port, polling to ensure the port is available.

Parameters
portThe stimulus port to use
valueThe 8-bit value to write

§ ITM_enableExceptionTrace()

void ITM_enableExceptionTrace ( void  )

Enable exception tracing This will trigger the DWT to generate packets when the device enters or leaves an exception. The ITM will forward these packets to the TPIU to be sent to the debugger.

§ ITM_disableExceptionTrace()

void ITM_disableExceptionTrace ( void  )

Disable exception tracing.

See also
ITM_enableExceptionTrace()

§ ITM_enablePCSampling()

void ITM_enablePCSampling ( bool  prescale1024,
uint8_t  postReset 
)

Enable periodic sampling of the program counter using the DWT POSTCNT timer.

Parameters
prescale1024true: divide system clock by 1024 to generate POSTCNT false: divide system clock by 64 to generate POSTCNT
postReset4-bit downcounter that is reloaded on POSTCNT expiration
Note
PC sampling and event counting are mutally exclusive. It is not recommended to call ITM_enableEventCounter() after this API has been called

§ ITM_enableEventCounter()

void ITM_enableEventCounter ( bool  prescale1024,
uint8_t  postReset 
)

Enable generation of event counter packets using the DWT POSTCNT timer.

Parameters
prescale1024true: divide system clock by 1024 to generate POSTCNT false: divide system clock by 64 to generate POSTCNT
postReset4-bit downcounter that is reloaded on POSTCNT expiration
Note
PC sampling and event counting are mutally exclusive. It is not recommended to call ITM_enablePCSampling() after this API has been called

§ ITM_disablePCAndEventSampling()

void ITM_disablePCAndEventSampling ( void  )

Disable program counter and event sampling in the DWT.

See also
ITM_enablePCSampling(), ITM_enableEventCounter

§ ITM_enableTimestamps()

void ITM_enableTimestamps ( ITM_TimeStampPrescaler  tsPrescale,
bool  asyncMode 
)

Enable the generation of local timestamp packets from the ITM module These are packets sent form the ITM that measure how long it has been since the previous timestamp.

Parameters
tsPrescalePrescaler value for the timestamp clock.
asyncModetrue: Synchronous mode - generate timestamps by dividing the system clock. false: Asynchronous mode - generate timestamps by dividing the TPIU clock.

§ ITM_enableSyncPackets()

void ITM_enableSyncPackets ( ITM_SyncPacketRate  syncPacketRate)

Enable the generation of synchronization packets from the ITM based on the CYCCNT counter. Synchronization packets can be used to recover bit-to-byte alignment information in a serial data stream.

Warning
When using the TPIU as a asynchronous serial trace port ARM recommends disabling these packets to reduce stream bandwith.
Parameters
syncPacketRateTap for CYCCNT. Controls the frequency of sync packets.

§ ITM_enableWatchpoint()

bool ITM_enableWatchpoint ( ITM_WatchpointAction  function,
const uintptr_t  address 
)

Enable the watchpoint functionality using a DWT comparator.

Parameters
functionThe DWT_FUNCTION field to be programmed. This controls what data is emitted on comparator match see ITM_WatchpointAction for possible values
addressThe address for the comparator to match on
Returns
true The watchpoint was successfully set
false There was no watchpoint available (all are in use)

§ ITM_flush()

void ITM_flush ( void  )

Flush the ITM in preparation for power off of CPU domain.

This will disable PC sampling, and other DWT features, flush the fifo and (if applicable) setup the PIN as a GPIO.

Warning
This function should not be called from ISR context
Note
This function is invoked by the DPL power policy right before entering IDLE/DEEPSLEEP. By default it is an empty stub so that the power policy doesn't incur the flush overhead when ITM isn't used. When ITM is enabled this function will be strongly defined by SYSCFG.

§ ITM_restore()

void ITM_restore ( void  )

Prepare the ITM hardware to return from power off of CPU domain This will reenable DWT features, re apply the ITM pin mux.

Warning
This function should not be called from ISR context
Note
This function is invoked by the DPL power policy right after leaving IDLE/DEEPSLEEP. By default it is an empty stub so that the power policy doesn't incur the flush overhead when ITM isn't used. When ITM is enabled this function will be strongly defined by SYSCFG.
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale