Data Structures | Typedefs | Variables
PWMTimerCC26XX.h File Reference

Detailed Description

PWM driver implementation for CC26XX/CC13XX.


Overview

The general PWM API should be used in application code, i.e. PWM_open() should be used instead of PWMTimerCC26XX_open(). The board file will define the device specific config, and casting in the general API will ensure that the correct device specific functions are called.

General Behavior

Before using PWM on CC26XX:

Error handling

If unsupported arguments are provided to an API returning an error code, the PWM configuration will not be updated and PWM will stay in the mode it was already configured to.

Power Management

The TI-RTOS power management framework will try to put the device into the most power efficient mode whenever possible. Please see the technical reference manual for further details on each power mode.

The PWMTimerCC26XX.h driver is not explicitly setting a power constraint when the PWM is running to prevent standby as this is assumed to be done in the underlying GPTimer driver. The following statements are valid:

Accuracy

The PWM output period and duty cycle are limited by the underlying timer. In PWM mode the timer is effectively 24 bits which results in a minimum frequency of 48MHz / (2^24-1) = 2.86Hz (349.525ms) The driver will round off the configured duty and period to a value limited by the timer resolution and the application is responsible for selecting duty and period that works with the underlying timer if high accuracy is needed.

The effect of this is most visible when using high output frequencies as the available duty cycle resolution is reduced correspondingly. For a 24MHz PWM only a 0%/50%/100% duty is available as the timer uses only counts 0 and 1. Similarly for a 12MHz period the duty cycle will be limited to a 12.5% resolution.

Note
The PWM signals are generated using the high-frequency clock as a source. The internal RC oscillator is the source of the high frequency clock, but may not be accurate enough for certain applications. If very high-accuracy outputs are needed, the application should request using the external HF crystal:

Limitations

Basic PWM output

The below example will output a 8MHz PWM signal with 50% duty cycle.

PWM_Handle pwmHandle;
PWM_Params_init(&params);
params.periodValue = 8e6;
params.dutyValue = PWM_DUTY_FRACTION_MAX / 2;
pwmHandle = PWM_open(CONFIG_PWM0, &params);
if(pwmHandle == NULL) {
Log_error0("Failed to open PWM");
Task_exit();
}
PWM_start(pwmHandle);
#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/PWM.h>
#include <ti/drivers/timer/GPTimerCC26XX.h>
Include dependency graph for PWMTimerCC26XX.h:

Go to the source code of this file.

Data Structures

struct  PWMTimerCC26XX_HwAttrs
 PWMTimer26XX Hardware attributes. More...
 
struct  PWMTimerCC26XX_Object
 PWMTimer26XX Object. More...
 

Macros

PWMTimerCC26XX specific control commands and arguments
#define PWMTimerCC26XX_CMD_DEBUG_STALL
 
Arguments for PWMTimerCC26XX_CMD_DEBUG_STALL
#define CMD_ARG_DEBUG_STALL_OFF
 
#define CMD_ARG_DEBUG_STALL_ON
 

Typedefs

typedef struct PWMTimerCC26XX_HwAttrs PWMTimerCC26XX_HwAttrs
 PWMTimer26XX Hardware attributes. More...
 
typedef struct PWMTimerCC26XX_Object PWMTimerCC26XX_Object
 PWMTimer26XX Object. More...
 

Variables

const PWM_FxnTable PWMTimerCC26XX_fxnTable
 

Macro Definition Documentation

§ PWMTimerCC26XX_CMD_DEBUG_STALL

#define PWMTimerCC26XX_CMD_DEBUG_STALL

Timer debug stall mode (stop PWM output debugger halts CPU) When enabled, PWM output will be HIGH when CPU is halted

§ CMD_ARG_DEBUG_STALL_OFF

#define CMD_ARG_DEBUG_STALL_OFF

§ CMD_ARG_DEBUG_STALL_ON

#define CMD_ARG_DEBUG_STALL_ON

Typedef Documentation

§ PWMTimerCC26XX_HwAttrs

PWMTimer26XX Hardware attributes.

These fields are used by the driver to set up underlying GPIO and GPTimer driver statically.

§ PWMTimerCC26XX_Object

PWMTimer26XX Object.

These fields are used by the driver to store and modify PWM configuration during run-time. The application must not edit any member variables of this structure. Appplications should also not access member variables of this structure as backwards compatibility is not guaranteed.

Variable Documentation

§ PWMTimerCC26XX_fxnTable

const PWM_FxnTable PWMTimerCC26XX_fxnTable
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale