Data Structures | Macros | Typedefs | Enumerations | Functions
SD.h File Reference

Detailed Description

Secure Digital (SD) Driver.


Overview

The SD driver is designed to serve as an interface to perform basic transfers directly to the SD card.


Usage

This section will cover driver usage.

Synopsis

SD_Handle handle;
uint16_t status;
// Open SD and initialize card
handle = SD_open(CONFIG_SD0, NULL);
status = SD_initialize(handle);
if (handle == NULL || status != SD_STATUS_SUCCESS) {
//Error opening SD driver
while (1);
}
// Write and read back the first sector
status = SD_write(handle, sendBuffer, 0, 1);
if (status == SD_STATUS_SUCCESS) {
status = SD_read(handle, readBuffer, 0 , 1);
}
SD_close(handle);

Examples

Get total capacity of an SD card:

SD_Handle handle;
uint_fast32_t sectorSize, sectorCount;
// Init, open, etc
...
sectorSize = SD_getSectorSize(handle);
sectorCount = SD_getNumSectors(handle);
Display_printf(display, 0, 0,"SD card total capacity is %lu bytes.",
sectorSize * sectorCount);

Configuration

Refer to the Driver's Configuration section for driver configuration information.


#include <stdint.h>
Include dependency graph for SD.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  SD_Params
 SD Parameters. More...
 
struct  SD_FxnTable
 The definition of a SD function table that contains the required set of functions to control a specific SD driver implementation. More...
 
struct  SD_Config_
 SD Global configuration. More...
 

Macros

#define SD_CMD_RESERVED   (32)
 
#define SD_STATUS_RESERVED   (-32)
 
#define SD_STATUS_SUCCESS   (0)
 Successful status code returned by SD_control(). More...
 
#define SD_STATUS_ERROR   (-1)
 Generic error status code returned by SD_control(). More...
 
#define SD_STATUS_UNDEFINEDCMD   (-2)
 An error status code returned by SD_control() for undefined command codes. More...
 

Typedefs

typedef struct SD_Config_SD_Handle
 A handle that is returned from a SD_open() call. More...
 
typedef void(* SD_CloseFxn) (SD_Handle handle)
 A function pointer to a driver specific implementation of SD_CloseFxn(). More...
 
typedef int_fast16_t(* SD_ControlFxn) (SD_Handle handle, uint_fast16_t cmd, void *arg)
 A function pointer to a driver specific implementation of SD_controlFxn(). More...
 
typedef uint_fast32_t(* SD_getNumSectorsFxn) (SD_Handle handle)
 A function pointer to a driver specific implementation of SD_getNumSectorsFxn(). More...
 
typedef uint_fast32_t(* SD_getSectorSizeFxn) (SD_Handle handle)
 A function pointer to a driver specific implementation of SD_getSectorSizeFxn(). More...
 
typedef void(* SD_InitFxn) (SD_Handle handle)
 A function pointer to a driver specific implementation of SD_InitFxn(). More...
 
typedef int_fast16_t(* SD_InitializeFxn) (SD_Handle handle)
 A function pointer to a driver specific implementation of SD_initializeFxn(). More...
 
typedef SD_Handle(* SD_OpenFxn) (SD_Handle handle, SD_Params *params)
 A function pointer to a driver specific implementation of SD_OpenFxn(). More...
 
typedef int_fast16_t(* SD_ReadFxn) (SD_Handle handle, void *buf, int_fast32_t sector, uint_fast32_t secCount)
 A function pointer to a driver specific implementation of SD_readFxn(). More...
 
typedef int_fast16_t(* SD_WriteFxn) (SD_Handle handle, const void *buf, int_fast32_t sector, uint_fast32_t secCount)
 A function pointer to a driver specific implementation of SD_writeFxn(). More...
 
typedef struct SD_Config_ SD_Config
 SD Global configuration. More...
 

Enumerations

enum  SD_CardType { SD_NOCARD = 0, SD_MMC = 1, SD_SDSC = 2, SD_SDHC = 3 }
 SD Card type inserted. More...
 

Functions

void SD_close (SD_Handle handle)
 Function to close a SD peripheral specified by the SD handle. More...
 
int_fast16_t SD_control (SD_Handle handle, uint_fast16_t cmd, void *arg)
 Function performs implementation specific features on a given SD_Handle. More...
 
uint_fast32_t SD_getNumSectors (SD_Handle handle)
 Function to obtain the total number of sectors on the SD card. Note: Total Card capacity is the (NumberOfSectors * SectorSize). More...
 
uint_fast32_t SD_getSectorSize (SD_Handle handle)
 Function to obtain the sector size used to access the SD card. More...
 
void SD_init (void)
 This function initializes the SD driver. More...
 
void SD_Params_init (SD_Params *params)
 Function to initialize the SD_Params struct to its defaults. More...
 
int_fast16_t SD_initialize (SD_Handle handle)
 Function to initialize the SD card. More...
 
SD_Handle SD_open (uint_least8_t index, SD_Params *params)
 Function to open the SD peripheral with the index and parameters specified. More...
 
int_fast16_t SD_read (SD_Handle handle, void *buf, int_fast32_t sector, uint_fast32_t secCount)
 Function that reads the specified sectors from the SD card. The destination is specified by buf. The starting sector is specified by sector and the total number of sectors to read is provided by secCount. More...
 
int_fast16_t SD_write (SD_Handle handle, const void *buf, int_fast32_t sector, uint_fast32_t secCount)
 Function that writes data to the specified sectors of the SD card. The source is specified by buf. The starting sector to write is specified by sector and the total number of sectors to write is provided by secCount. More...
 

Typedef Documentation

§ SD_Handle

typedef struct SD_Config_* SD_Handle

A handle that is returned from a SD_open() call.

§ SD_CloseFxn

typedef void(* SD_CloseFxn) (SD_Handle handle)

A function pointer to a driver specific implementation of SD_CloseFxn().

§ SD_ControlFxn

typedef int_fast16_t(* SD_ControlFxn) (SD_Handle handle, uint_fast16_t cmd, void *arg)

A function pointer to a driver specific implementation of SD_controlFxn().

§ SD_getNumSectorsFxn

typedef uint_fast32_t(* SD_getNumSectorsFxn) (SD_Handle handle)

A function pointer to a driver specific implementation of SD_getNumSectorsFxn().

§ SD_getSectorSizeFxn

typedef uint_fast32_t(* SD_getSectorSizeFxn) (SD_Handle handle)

A function pointer to a driver specific implementation of SD_getSectorSizeFxn().

§ SD_InitFxn

typedef void(* SD_InitFxn) (SD_Handle handle)

A function pointer to a driver specific implementation of SD_InitFxn().

§ SD_InitializeFxn

typedef int_fast16_t(* SD_InitializeFxn) (SD_Handle handle)

A function pointer to a driver specific implementation of SD_initializeFxn().

§ SD_OpenFxn

typedef SD_Handle(* SD_OpenFxn) (SD_Handle handle, SD_Params *params)

A function pointer to a driver specific implementation of SD_OpenFxn().

§ SD_ReadFxn

typedef int_fast16_t(* SD_ReadFxn) (SD_Handle handle, void *buf, int_fast32_t sector, uint_fast32_t secCount)

A function pointer to a driver specific implementation of SD_readFxn().

§ SD_WriteFxn

typedef int_fast16_t(* SD_WriteFxn) (SD_Handle handle, const void *buf, int_fast32_t sector, uint_fast32_t secCount)

A function pointer to a driver specific implementation of SD_writeFxn().

§ SD_Config

typedef struct SD_Config_ SD_Config

SD Global configuration.

The SD_Config structure contains a set of pointers used to characterize the SD driver implementation.

This structure needs to be defined before calling SD_init() and it must not be changed thereafter.

See also
SD_init()

Enumeration Type Documentation

§ SD_CardType

SD Card type inserted.

Enumerator
SD_NOCARD 

Unrecognized Card

SD_MMC 

Multi-media Memory Card (MMC)

SD_SDSC 

Standard SDCard (SDSC)

SD_SDHC 

High Capacity SDCard (SDHC)

Function Documentation

§ SD_close()

void SD_close ( SD_Handle  handle)

Function to close a SD peripheral specified by the SD handle.

Precondition
SD_open() had to be called first.
Parameters
handleA SD_Handle returned from SD_open()
See also
SD_open()

§ SD_control()

int_fast16_t SD_control ( SD_Handle  handle,
uint_fast16_t  cmd,
void *  arg 
)

Function performs implementation specific features on a given SD_Handle.

Commands for SD_control can originate from SD.h or from implementation specific SD*.h files. While commands from SD.h are API portable across driver implementations, not all implementations may support all these commands. Conversely, commands from driver implementation specific SD*.h files add unique driver capabilities but are not API portable across all SD driver implementations.

Commands supported by SD.h follow a SD*_CMD naming convention.

Commands supported by SD*.h follow a SD*_CMD naming convention. Each control command defines arg differently. The types of arg are documented with each command.

See SD_control command codes for command codes.

See SD_control return status codes for status codes.

Precondition
SD_open() has to be called first.
Parameters
handleA SD_Handle returned from SD_open().
cmdSD.h or SD*.h commands.
argAn optional R/W (read/write) command argument accompanied with cmd.
Returns
Implementation specific return codes. Negative values indicate unsuccessful operations.
See also
SD_open()

§ SD_getNumSectors()

uint_fast32_t SD_getNumSectors ( SD_Handle  handle)

Function to obtain the total number of sectors on the SD card. Note: Total Card capacity is the (NumberOfSectors * SectorSize).

Precondition
SD Card has been initialized using SD_initialize().
Parameters
handleA SD_Handle returned from SD_open().
Returns
The total number of sectors on the SD card, or 0 if an error occurred.
See also
SD_initialize()

§ SD_getSectorSize()

uint_fast32_t SD_getSectorSize ( SD_Handle  handle)

Function to obtain the sector size used to access the SD card.

Precondition
SD Card has been initialized using SD_initialize().
Parameters
handleA SD_Handle returned from SD_open().
Returns
The sector size set for use during SD card read/write operations.
See also
SD_initialize()

§ SD_init()

void SD_init ( void  )

This function initializes the SD driver.

Precondition
The SD_config[] array must exist and be persistent before this function can be called. This function must also be called before any other SD driver APIs. This function call does not modify any peripheral registers.

§ SD_Params_init()

void SD_Params_init ( SD_Params params)

Function to initialize the SD_Params struct to its defaults.

Parameters
paramsA pointer to SD_Params structure for initialization.

§ SD_initialize()

int_fast16_t SD_initialize ( SD_Handle  handle)

Function to initialize the SD card.

Precondition
SD controller has been opened by calling SD_open().
Parameters
handleA SD_Handle returned from SD_open().
Returns
SD_STATUS_SUCCESS if no errors occurred during the initialization, SD_STATUS_ERROR otherwise.

§ SD_open()

SD_Handle SD_open ( uint_least8_t  index,
SD_Params params 
)

Function to open the SD peripheral with the index and parameters specified.

Precondition
SD controller has been initialized using SD_init().
Parameters
indexLogical peripheral number for the SD indexed into the SD_config[] table.
paramsPointer to a parameter block, if NULL it will use default values. All the fields in this structure are RO (read-only).
Returns
A SD_Handle on success or a NULL on an error or if it has been opened already.
See also
SD_init()
SD_close()

§ SD_read()

int_fast16_t SD_read ( SD_Handle  handle,
void *  buf,
int_fast32_t  sector,
uint_fast32_t  secCount 
)

Function that reads the specified sectors from the SD card. The destination is specified by buf. The starting sector is specified by sector and the total number of sectors to read is provided by secCount.

Precondition
SD controller has been opened and initialized by calling SD_open() followed by SD_initialize().
Parameters
handleA SD_Handle returned from SD_open().
bufPointer to a buffer to read data into.
sectorStarting sector on the disk to read from.
secCountNumber of sectors to be read.
Returns
SD_STATUS_SUCCESS if no errors occurred during the write, SD_STATUS_ERROR otherwise.
See also
SD_initialize()

§ SD_write()

int_fast16_t SD_write ( SD_Handle  handle,
const void *  buf,
int_fast32_t  sector,
uint_fast32_t  secCount 
)

Function that writes data to the specified sectors of the SD card. The source is specified by buf. The starting sector to write is specified by sector and the total number of sectors to write is provided by secCount.

Precondition
SD controller has been opened and initialized by calling SD_open() followed by SD_initialize().
Parameters
handleA SD_Handle returned from SD_open().
bufPointer to a buffer containing data to write to disk.
sectorStarting sector on the disk to write to.
secCountNumber of sectors to be written.
Returns
SD_STATUS_SUCCESS if no errors occurred during the write, SD_STATUS_ERROR otherwise.
See also
SD_initialize()
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale