Data Structures | Macros | Typedefs | Enumerations | Functions | Variables
SHA2.h File Reference

Detailed Description

SHA2 driver header.


Overview

SHA2 (Secure Hash Algorithm 2) is a cryptographic hashing algorithm that maps an input of arbitrary length to a fixed-length output with negligible probability of collision. A collision would occur when two different inputs map to the same output.

It is not currently technologically feasible to derive an input from the hash digest (output) itself.

Hashes are often used to ensure the integrity of messages. They are also used to as constituent parts of more complicated cryptographic schemes. HMAC is a message authentication code that is based on hash functions such as SHA2 rather than a block cipher. Hashes may themselves be used as or form a part of key derivation functions used to derive symmetric keys from sources of entropy such as an Elliptic Curve Diffie-Helman key exchange (ECDH).

SHA2 is not actually a single algorithm, but a suite of similar algorithms that produce hash digests of different lengths. 224, 256, 384, and 512-bit outputs are available.

"Hash" may refer to either the process of hashing when used as a verb and the output digest when used as a noun.

Usage

Before starting a SHA2 operation, the application must do the following:

There are two general ways to execute a SHA2 operation:

Synopsis

// Import SHA2 Driver definitions
// Define name for SHA2 channel index
#define SHA2_INSTANCE 0
handle = SHA2_open(SHA2_INSTANCE, NULL);
result = SHA2_hashData(handle, message, strlen(message), actualDigest);
SHA2_close(handle);

Examples

One-step hash operation

The SHA2_hashData() function can perform a SHA2 operation in a single call. It will always use the most highly optimized routine with the least overhead and the fastest runtime. However, it requires that the entire input message is available to the function in a contiguous location at the start of the call. The single call operation is required when hashing a message with a length smaller than or equal to one hash-block length. All devices support single call operations.

After a SHA2 operation completes, the application may either start another operation or close the driver by calling SHA2_close().

SHA2_Handle handle;
int_fast16_t result;
char message[] = "A Ferengi without profit is no Ferengi at all.";
uint8_t actualDigest[SHA2_DIGEST_LENGTH_BYTES_256];
uint8_t expectedDigest[] = {
0x93, 0xD6, 0x5C, 0x07,
0xA6, 0x26, 0x88, 0x9C,
0x87, 0xCC, 0x82, 0x24,
0x47, 0xC6, 0xE4, 0x28,
0xC0, 0xBD, 0xC6, 0xED,
0xAA, 0x8C, 0xD2, 0x53,
0x77, 0xAA, 0x73, 0x14,
0xA3, 0xE2, 0xDE, 0x43
};
handle = SHA2_open(0, &params);
assert(handle != NULL);
result = SHA2_hashData(handle, message, strlen(message), actualDigest);
assert(result == SHA2_STATUS_SUCCESS);
result = memcmp(actualDigest, expectedDigest, SHA2_DIGEST_LENGTH_BYTES_256);
assert(result == 0);
SHA2_close(handle);

Partial hash operation

When trying to operate on data that is too large to fit into available memory, partial processing is more advisable. The segments are processed with SHA2_addData() whereas the final digest is computed by SHA2_finalize().

SHA2_Handle handle;
int_fast16_t result;
const char message[] =
"Premature optimization is the root of all evil (or at least most of it) in programming.";
uint8_t actualDigest[SHA2_DIGEST_LENGTH_BYTES_256];
uint8_t expectedDigest[] = {
0xF2, 0x6A, 0xFF, 0x01,
0x11, 0x6B, 0xF6, 0x77,
0x63, 0x91, 0xFE, 0xD9,
0x47, 0x56, 0x99, 0xB2,
0xAD, 0x7D, 0x64, 0x16,
0xF7, 0x40, 0x1A, 0x5B,
0xCC, 0xC7, 0x08, 0x3D,
0xE8, 0x6B, 0x35, 0x6D,
};
handle = SHA2_open(0, &params);
assert(handle != NULL);
// We can configure the driver even after SHA2_open()
assert(result == SHA2_STATUS_SUCCESS);
// Process data in chunks. The driver buffers incomplete blocks internally.
result = SHA2_addData(handle, &message[0], 17);
assert(result == SHA2_STATUS_SUCCESS);
result = SHA2_addData(handle, &message[17], strlen(message) - 17);
assert(result == SHA2_STATUS_SUCCESS);
// Compute the resulting digest
result = SHA2_finalize(handle, actualDigest);
assert(result == SHA2_STATUS_SUCCESS);
// Verify
result = memcmp(actualDigest, expectedDigest, SHA2_DIGEST_LENGTH_BYTES_256);
assert(result == 0);
SHA2_close(handle);

One-step HMAC operation

The SHA2_hmac() function can perform a SHA2 operation in a single call. It will always use the most highly optimized routine with the least overhead and the fastest runtime. It requires that the entire input message is available to the function in a contiguous location at the start of the call.

After a SHA2 operation completes, the application may either start another operation or close the driver by calling SHA2_close().

SHA2_Handle handle;
int_fast16_t result;
CryptoKey hmacKey;
uint8_t message[] = {
0xb1, 0x68, 0x9c, 0x25, 0x91, 0xea, 0xf3, 0xc9,
0xe6, 0x60, 0x70, 0xf8, 0xa7, 0x79, 0x54, 0xff,
0xb8, 0x17, 0x49, 0xf1, 0xb0, 0x03, 0x46, 0xf9,
0xdf, 0xe0, 0xb2, 0xee, 0x90, 0x5d, 0xcc, 0x28,
0x8b, 0xaf, 0x4a, 0x92, 0xde, 0x3f, 0x40, 0x01,
0xdd, 0x9f, 0x44, 0xc4, 0x68, 0xc3, 0xd0, 0x7d,
0x6c, 0x6e, 0xe8, 0x2f, 0xac, 0xea, 0xfc, 0x97,
0xc2, 0xfc, 0x0f, 0xc0, 0x60, 0x17, 0x19, 0xd2,
0xdc, 0xd0, 0xaa, 0x2a, 0xec, 0x92, 0xd1, 0xb0,
0xae, 0x93, 0x3c, 0x65, 0xeb, 0x06, 0xa0, 0x3c,
0x9c, 0x93, 0x5c, 0x2b, 0xad, 0x04, 0x59, 0x81,
0x02, 0x41, 0x34, 0x7a, 0xb8, 0x7e, 0x9f, 0x11,
0xad, 0xb3, 0x04, 0x15, 0x42, 0x4c, 0x6c, 0x7f,
0x5f, 0x22, 0xa0, 0x03, 0xb8, 0xab, 0x8d, 0xe5,
0x4f, 0x6d, 0xed, 0x0e, 0x3a, 0xb9, 0x24, 0x5f,
0xa7, 0x95, 0x68, 0x45, 0x1d, 0xfa, 0x25, 0x8e};
// In this case, keyingMaterial is 40 bytes long. It could also be
// any other length.
uint8_t keyingMaterial[] = {
0x97, 0x79, 0xd9, 0x12, 0x06, 0x42, 0x79, 0x7f,
0x17, 0x47, 0x02, 0x5d, 0x5b, 0x22, 0xb7, 0xac,
0x60, 0x7c, 0xab, 0x08, 0xe1, 0x75, 0x8f, 0x2f,
0x3a, 0x46, 0xc8, 0xbe, 0x1e, 0x25, 0xc5, 0x3b,
0x8c, 0x6a, 0x8f, 0x58, 0xff, 0xef, 0xa1, 0x76};
uint8_t actualHmac[SHA2_DIGEST_LENGTH_BYTES_256];
uint8_t expectedHmac[] = {
0x76, 0x9f, 0x00, 0xd3, 0xe6, 0xa6, 0xcc, 0x1f,
0xb4, 0x26, 0xa1, 0x4a, 0x4f, 0x76, 0xc6, 0x46,
0x2e, 0x61, 0x49, 0x72, 0x6e, 0x0d, 0xee, 0x0e,
0xc0, 0xcf, 0x97, 0xa1, 0x66, 0x05, 0xac, 0x8b
};
handle = SHA2_open(0, &params);
assert(handle != NULL);
keyingMaterial,
sizeof(keyingMaterial));
result = SHA2_hmac(handle,
&hmacKey,
message,
sizeof(message),
actualHmac);
assert(result == SHA2_STATUS_SUCCESS);
result = memcmp(actualHmac, expectedHmac, SHA2_DIGEST_LENGTH_BYTES_256);
assert(result == 0);
SHA2_close(handle);
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKey.h>
Include dependency graph for SHA2.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  SHA2_Config
 SHA2 Global configuration. More...
 
struct  SHA2_Params
 SHA2 Parameters. More...
 

Macros

#define SHA2_STATUS_RESERVED   (-32)
 
#define SHA2_STATUS_SUCCESS   ((int_fast16_t)0)
 Successful status code. More...
 
#define SHA2_STATUS_ERROR   ((int_fast16_t)-1)
 Generic error status code. More...
 
#define SHA2_STATUS_RESOURCE_UNAVAILABLE   ((int_fast16_t)-2)
 An error status code returned if the hardware or software resource is currently unavailable. More...
 
#define SHA2_STATUS_CANCELED   ((int_fast16_t)-3)
 The ongoing operation was canceled. More...
 
#define SHA2_STATUS_UNSUPPORTED   ((int_fast16_t)-4)
 The requested operation or configuration is not supported by the device specific implementation. More...
 
#define SHA2_STATUS_KEYSTORE_ERROR   ((int_fast16_t)-5)
 Importing generated key into KeyStore failed. More...
 

Typedefs

typedef SHA2_ConfigSHA2_Handle
 A handle that is returned from an SHA2_open() call. More...
 
typedef void(* SHA2_CallbackFxn) (SHA2_Handle handle, int_fast16_t returnStatus)
 The definition of a callback function used by the SHA2 driver when used in SHA2_RETURN_BEHAVIOR_CALLBACK. More...
 

Enumerations

enum  SHA2_ReturnBehavior { SHA2_RETURN_BEHAVIOR_CALLBACK = 1, SHA2_RETURN_BEHAVIOR_BLOCKING = 2, SHA2_RETURN_BEHAVIOR_POLLING = 4 }
 The way in which SHA2 function calls return after performing an operation. More...
 
enum  SHA2_HashType { SHA2_HASH_TYPE_224 = 0, SHA2_HASH_TYPE_256 = 1, SHA2_HASH_TYPE_384 = 2, SHA2_HASH_TYPE_512 = 3 }
 Enum for the hash types supported by the driver. More...
 
enum  SHA2_DigestLengthBytes { SHA2_DIGEST_LENGTH_BYTES_224 = 28, SHA2_DIGEST_LENGTH_BYTES_256 = 32, SHA2_DIGEST_LENGTH_BYTES_384 = 48, SHA2_DIGEST_LENGTH_BYTES_512 = 64 }
 Enum for the hash digest lengths in bytes supported by the driver. More...
 
enum  SHA2_BlockSizeBytes { SHA2_BLOCK_SIZE_BYTES_224 = 64, SHA2_BLOCK_SIZE_BYTES_256 = 64, SHA2_BLOCK_SIZE_BYTES_384 = 128, SHA2_BLOCK_SIZE_BYTES_512 = 128 }
 Enum for the block sizes of the algorithms. More...
 

Functions

void SHA2_init (void)
 Initializes the SHA2 driver module. More...
 
void SHA2_Params_init (SHA2_Params *params)
 Initializes params with default values. More...
 
SHA2_Handle SHA2_open (uint_least8_t index, const SHA2_Params *params)
 Initializes a SHA2 driver instance and returns a handle. More...
 
void SHA2_close (SHA2_Handle handle)
 Closes a SHA2 peripheral specified by handle. More...
 
int_fast16_t SHA2_setupHmac (SHA2_Handle handle, CryptoKey *key)
 Starts an HMAC operation on segmented data. More...
 
int_fast16_t SHA2_addData (SHA2_Handle handle, const void *data, size_t length)
 Adds a segment of data with a length in bytes to the cryptographic hash or HMAC. More...
 
int_fast16_t SHA2_finalize (SHA2_Handle handle, void *digest)
 Finishes a hash operation and writes the result to digest. More...
 
int_fast16_t SHA2_finalizeHmac (SHA2_Handle handle, void *hmac)
 Finishes an HMAC operation and writes the result to hmac. More...
 
int_fast16_t SHA2_hashData (SHA2_Handle handle, const void *data, size_t dataLength, void *digest)
 Hashes a segment of data with a size in bytes and writes the resulting hash to digest. More...
 
int_fast16_t SHA2_hmac (SHA2_Handle handle, CryptoKey *key, const void *data, size_t dataLength, void *hmac)
 Creates a keyed hash of data with key. More...
 
void SHA2_reset (SHA2_Handle handle)
 Clears internal buffers and aborts an ongoing SHA2 operation. More...
 
int_fast16_t SHA2_cancelOperation (SHA2_Handle handle)
 Aborts an ongoing SHA2 operation and clears internal buffers. More...
 
int_fast16_t SHA2_setHashType (SHA2_Handle handle, SHA2_HashType type)
 Selects a new hash algorithm type. More...
 
SHA2_Handle SHA2_construct (SHA2_Config *config, const SHA2_Params *params)
 Constructs a new SHA2 object. More...
 

Variables

const SHA2_Config SHA2_config []
 Global SHA2 configuration struct. More...
 
const uint_least8_t SHA2_count
 Global SHA2 configuration count. More...
 
const SHA2_Params SHA2_defaultParams
 Default SHA2_Params structure. More...
 

Macro Definition Documentation

§ SHA2_STATUS_RESERVED

#define SHA2_STATUS_RESERVED   (-32)

Common SHA2 status code reservation offset. SHA2 driver implementations should offset status codes with SHA2_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

#define SHA2XYZ_STATUS_ERROR0 SHA2_STATUS_RESERVED - 0
#define SHA2XYZ_STATUS_ERROR1 SHA2_STATUS_RESERVED - 1
#define SHA2XYZ_STATUS_ERROR2 SHA2_STATUS_RESERVED - 2

§ SHA2_STATUS_SUCCESS

#define SHA2_STATUS_SUCCESS   ((int_fast16_t)0)

Successful status code.

Functions return SHA2_STATUS_SUCCESS if the function was executed successfully.

§ SHA2_STATUS_ERROR

#define SHA2_STATUS_ERROR   ((int_fast16_t)-1)

Generic error status code.

Functions return SHA2_STATUS_ERROR if the function was not executed successfully and no more specific error is applicable.

§ SHA2_STATUS_RESOURCE_UNAVAILABLE

#define SHA2_STATUS_RESOURCE_UNAVAILABLE   ((int_fast16_t)-2)

An error status code returned if the hardware or software resource is currently unavailable.

SHA2 driver implementations may have hardware or software limitations on how many clients can simultaneously perform operations. This status code is returned if the mutual exclusion mechanism signals that an operation cannot currently be performed.

§ SHA2_STATUS_CANCELED

#define SHA2_STATUS_CANCELED   ((int_fast16_t)-3)

The ongoing operation was canceled.

§ SHA2_STATUS_UNSUPPORTED

#define SHA2_STATUS_UNSUPPORTED   ((int_fast16_t)-4)

The requested operation or configuration is not supported by the device specific implementation.

§ SHA2_STATUS_KEYSTORE_ERROR

#define SHA2_STATUS_KEYSTORE_ERROR   ((int_fast16_t)-5)

Importing generated key into KeyStore failed.

Functions return SHA2_STATUS_KEYSTORE_ERROR if the KeyStore_PSA_importKey() did not return KEYSTORE_PSA_STATUS_SUCCESS

Typedef Documentation

§ SHA2_Handle

A handle that is returned from an SHA2_open() call.

§ SHA2_CallbackFxn

typedef void(* SHA2_CallbackFxn) (SHA2_Handle handle, int_fast16_t returnStatus)

The definition of a callback function used by the SHA2 driver when used in SHA2_RETURN_BEHAVIOR_CALLBACK.

Parameters
handleHandle of the client that started the SHA2 operation.
returnStatusThe result of the SHA2 operation. May contain an error code. Informs the application of why the callback function was called.

Enumeration Type Documentation

§ SHA2_ReturnBehavior

The way in which SHA2 function calls return after performing an operation.

Not all SHA2 operations exhibit the specified return behavior. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specified return behavior is not implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.

SHA2 functions exhibiting the specified return behavior have restrictions on the context from which they may be called.

Task Hwi Swi
SHA2_RETURN_BEHAVIOR_CALLBACK X X X
SHA2_RETURN_BEHAVIOR_BLOCKING X
SHA2_RETURN_BEHAVIOR_POLLING X X X
Enumerator
SHA2_RETURN_BEHAVIOR_CALLBACK 

The function call will return immediately while the SHA2 operation goes on in the background. The registered callback function is called after the operation completes. The context the callback function is called (task, HWI, SWI) is implementation-dependent.

SHA2_RETURN_BEHAVIOR_BLOCKING 

The function call will block while the SHA2 operation goes on in the background. SHA2 operation results are available after the function returns.

SHA2_RETURN_BEHAVIOR_POLLING 

The function call will continuously poll a flag while the SHA2 operation goes on in the background. SHA2 operation results are available after the function returns.

§ SHA2_HashType

Enum for the hash types supported by the driver.

Enumerator
SHA2_HASH_TYPE_224 
SHA2_HASH_TYPE_256 
SHA2_HASH_TYPE_384 
SHA2_HASH_TYPE_512 

§ SHA2_DigestLengthBytes

Enum for the hash digest lengths in bytes supported by the driver.

Enumerator
SHA2_DIGEST_LENGTH_BYTES_224 
SHA2_DIGEST_LENGTH_BYTES_256 
SHA2_DIGEST_LENGTH_BYTES_384 
SHA2_DIGEST_LENGTH_BYTES_512 

§ SHA2_BlockSizeBytes

Enum for the block sizes of the algorithms.

SHA2 iteratively consumes segments of the block size and computes intermediate digests which are fed back into the algorithm together with the next segment to compute the next intermediate or final digest. The block sizes of the algorithms differ from their digest lengths. When performing partial hashes, the segment lengths for all but the last segment must be multiples of the relevant block size.

Enumerator
SHA2_BLOCK_SIZE_BYTES_224 
SHA2_BLOCK_SIZE_BYTES_256 
SHA2_BLOCK_SIZE_BYTES_384 
SHA2_BLOCK_SIZE_BYTES_512 

Function Documentation

§ SHA2_init()

void SHA2_init ( void  )

Initializes the SHA2 driver module.

Precondition
The SHA2_config structure must exist and be persistent before this function can be called. This function must also be called before any other SHA2 driver APIs. This function call does not modify any peripheral registers.

§ SHA2_Params_init()

void SHA2_Params_init ( SHA2_Params params)

Initializes params with default values.

Parameters
paramsA pointer to SHA2_Params structure for initialization

Defaults values are: returnBehavior = SHA2_RETURN_BEHAVIOR_BLOCKING callbackFxn = NULL timeout = SemaphoreP_WAIT_FOREVER custom = NULL

§ SHA2_open()

SHA2_Handle SHA2_open ( uint_least8_t  index,
const SHA2_Params params 
)

Initializes a SHA2 driver instance and returns a handle.

Precondition
SHA2 controller has been initialized using SHA2_init()
Parameters
indexLogical peripheral number for the SHA2 indexed into the SHA2_config table
paramsPointer to a parameter block, if NULL it will use default values.
Returns
A SHA2_Handle on success or a NULL on an error or if it has been opened already.
See also
SHA2_init(), SHA2_close()

§ SHA2_close()

void SHA2_close ( SHA2_Handle  handle)

Closes a SHA2 peripheral specified by handle.

Precondition
SHA2_open() has to be called first.
Parameters
handleA SHA2_Handle returned from SHA2_open()
See also
SHA2_open()

§ SHA2_setupHmac()

int_fast16_t SHA2_setupHmac ( SHA2_Handle  handle,
CryptoKey key 
)

Starts an HMAC operation on segmented data.

This function uses key to compute the all intermediate results involving key as specified in FIPS 198-1.

This function blocks until the final digest hash been computed. It returns immediately when SHA2_RETURN_BEHAVIOR_CALLBACK is set.

Precondition
SHA2_open() has to be called first.
Postcondition
Call SHA2_addData() and SHA2_finalizeHmac()
Parameters
handleA SHA2_Handle returned from SHA2_open()
keyThe key with which to sign the message with
Return values
SHA2_STATUS_SUCCESSThe hash operation succeeded.
SHA2_STATUS_ERRORThe hash operation failed.
SHA2_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
SHA2_STATUS_CANCELEDThe hash operation was canceled.
See also
SHA2_reset()

§ SHA2_addData()

int_fast16_t SHA2_addData ( SHA2_Handle  handle,
const void *  data,
size_t  length 
)

Adds a segment of data with a length in bytes to the cryptographic hash or HMAC.

SHA2_addData() may be called arbitrary times before finishing the operation with SHA2_finalize().

This function blocks until the final digest hash been computed. It returns immediately when SHA2_RETURN_BEHAVIOR_CALLBACK is set.

Precondition
SHA2_open() has to be called first.
If computing an HMAC, SHA2_setupHmac() must be called first.
Parameters
handleA SHA2_Handle returned from SHA2_open()
dataPointer to the location to read from. There might be alignment restrictions on different platforms.
lengthLength of the message segment to hash, in bytes.
Return values
SHA2_STATUS_SUCCESSThe hash operation succeeded.
SHA2_STATUS_ERRORThe hash operation failed.
SHA2_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
SHA2_STATUS_CANCELEDThe hash operation was canceled.
See also
SHA2_open(), SHA2_reset(), SHA2_finalize()

§ SHA2_finalize()

int_fast16_t SHA2_finalize ( SHA2_Handle  handle,
void *  digest 
)

Finishes a hash operation and writes the result to digest.

This function finishes a hash operation that has been previously started by SHA2_addData().

This function blocks until the final digest hash been computed. It returns immediately when SHA2_RETURN_BEHAVIOR_CALLBACK is set.

Precondition
SHA2_addData() has to be called first.
Parameters
handleA SHA2_Handle returned from SHA2_open()
digestPointer to the location to write the digest to.
Return values
SHA2_STATUS_SUCCESSThe hash operation succeeded.
SHA2_STATUS_ERRORThe hash operation failed.
SHA2_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
SHA2_STATUS_CANCELEDThe hash operation was canceled.
See also
SHA2_open(), SHA2_addData()

§ SHA2_finalizeHmac()

int_fast16_t SHA2_finalizeHmac ( SHA2_Handle  handle,
void *  hmac 
)

Finishes an HMAC operation and writes the result to hmac.

This function finishes a an HMAC operation that has been previously started by SHA2_setupHmac() and SHA2_addData().

This function blocks until the final digest hash been computed. It returns immediately when SHA2_RETURN_BEHAVIOR_CALLBACK is set.

Precondition
SHA2_setupHmac() must be called prior.
SHA2_addData() should be called after SHA2_setupHmac().
Parameters
handleA SHA2_Handle returned from SHA2_open()
hmacPointer to the location to write the digest to.
Return values
SHA2_STATUS_SUCCESSThe hash operation succeeded.
SHA2_STATUS_ERRORThe hash operation failed.
SHA2_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
SHA2_STATUS_CANCELEDThe hash operation was canceled.
See also
SHA2_open(), SHA2_setupHmac() SHA2_addData()

§ SHA2_hashData()

int_fast16_t SHA2_hashData ( SHA2_Handle  handle,
const void *  data,
size_t  dataLength,
void *  digest 
)

Hashes a segment of data with a size in bytes and writes the resulting hash to digest.

The digest content is computed in one step. Intermediate data from a previous partial operation started with SHA2_addData() is discarded.

This function blocks until the final digest hash been computed. It returns immediately when SHA2_RETURN_BEHAVIOR_CALLBACK is set.

Precondition
SHA2_open() has to be called first.
Parameters
handleA SHA2_Handle returned from SHA2_open()
dataPointer to the location to read from. There might be alignment restrictions on different platforms.
dataLengthLength of the message data, in bytes.
digestPointer to the location to write the digest to. There might be alignment restrictions on different platforms.
Return values
SHA2_STATUS_SUCCESSThe hash operation succeeded.
SHA2_STATUS_ERRORThe hash operation failed.
SHA2_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
SHA2_STATUS_CANCELEDThe hash operation was canceled.
See also
SHA2_open()

§ SHA2_hmac()

int_fast16_t SHA2_hmac ( SHA2_Handle  handle,
CryptoKey key,
const void *  data,
size_t  dataLength,
void *  hmac 
)

Creates a keyed hash of data with key.

This function signs data using key using the keyed-hash message authentication code (HMAC) algorithm specified in FIPS 198-1.

This function expects all of data to be available in contiguous memory.

Intermediate data from a previous partial operation started with SHA2_addData() is discarded.

This function blocks until the final digest hash been computed. It returns immediately when SHA2_RETURN_BEHAVIOR_CALLBACK is set.

Precondition
SHA2_open() has to be called first.
Parameters
handleA SHA2_Handle returned from SHA2_open()
keyThe key with which data is signed
dataPointer to the location to read from. There might be alignment restrictions on different platforms.
dataLengthLength of the message data, in bytes.
hmacPointer to the location to write the HMAC to. There might be alignment restrictions on different platforms.
Return values
SHA2_STATUS_SUCCESSThe hash operation succeeded.
SHA2_STATUS_ERRORThe hash operation failed.
SHA2_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
See also
SHA2_open()

§ SHA2_reset()

void SHA2_reset ( SHA2_Handle  handle)

Clears internal buffers and aborts an ongoing SHA2 operation.

Clears all internal buffers and the intermediate digest of this driver instance. If an asynchronous operation is ongoing, the behavior is the same as for SHA2_cancelOperation().

Parameters
handleA SHA2_Handle returned from SHA2_open()
See also
SHA2_cancelOperation()

§ SHA2_cancelOperation()

int_fast16_t SHA2_cancelOperation ( SHA2_Handle  handle)

Aborts an ongoing SHA2 operation and clears internal buffers.

Aborts an ongoing hash operation of this driver instance. The operation will terminate as though an error occurred and the status code of the operation will be SHA2_STATUS_CANCELED in this case.

Parameters
handleA SHA2_Handle returned from SHA2_open()
Return values
SHA2_STATUS_SUCCESSThe operation was canceled or there was no operation in progress to be canceled.

§ SHA2_setHashType()

int_fast16_t SHA2_setHashType ( SHA2_Handle  handle,
SHA2_HashType  type 
)

Selects a new hash algorithm type.

This function changes the hash algorithm type of the hash digest at run-time. The hash type is usually specified during SHA2_open().

Neither is it allowed to call this function during a running hash operation nor during an incomplete multi-step hash operation. In this case SHA2_STATUS_ERROR would be returned.

Precondition
SHA2_open() has to be called first.
Parameters
handleA SHA2_Handle returned from SHA2_open()
typeNew hash algorithm type
Return values
SHA2_STATUS_SUCCESSHash type set correctly.
SHA2_STATUS_ERRORError. Platform may not support this hash type.

§ SHA2_construct()

SHA2_Handle SHA2_construct ( SHA2_Config config,
const SHA2_Params params 
)

Constructs a new SHA2 object.

Unlike SHA2_open(), SHA2_construct() does not require the hwAttrs and object to be allocated in a SHA2_Config array that is indexed into. Instead, the SHA2_Config, hwAttrs, and object can be allocated at any location. This allows for relatively simple run-time allocation of temporary driver instances on the stack or the heap. The drawback is that this makes it more difficult to write device-agnostic code. If you use an ifdef with DeviceFamily, you can choose the correct object and hwAttrs to allocate. That compilation unit will be tied to the device it was compiled for at this point. To change devices, recompilation of the application with a different DeviceFamily setting is necessary.

Parameters
configSHA2_Config describing the location of the object and hwAttrs.
paramsSHA2_Params to configure the driver instance.
Returns
Returns a SHA2_Handle on success or NULL on failure.
Precondition
The object struct config points to must be zeroed out prior to calling this function. Otherwise, unexpected behavior may ensue.

Variable Documentation

§ SHA2_config

const SHA2_Config SHA2_config[]

Global SHA2 configuration struct.

Specifies context objects and hardware attributes for every driver instance.

This variable is supposed to be defined in the board file.

§ SHA2_count

const uint_least8_t SHA2_count

Global SHA2 configuration count.

Specifies the amount of available SHA2 driver instances.

This variable is supposed to be defined in the board file.

§ SHA2_defaultParams

const SHA2_Params SHA2_defaultParams

Default SHA2_Params structure.

See also
SHA2_Params_init()
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale