Data Structures | Macros | Enumerations | Variables
SPICC26X4DMA.h File Reference

Detailed Description

SPI driver implementation for a CC26X4 SPI controller using the UDMA controller.


Driver include

The SPI header file should be included in an application as follows:

Refer to SPI.h for a complete description of APIs.

Note that the user also needs to include the UDMACC26XX.h driver since the SPI uses uDMA in order to improve throughput.

Overview

The general SPI API should be used in application code, i.e. SPI_open() should be used instead of SPICC26X4DMA_open(). The board file will define the device specific config, and casting in the general API will ensure that the correct device specific functions are called. This is also reflected in the example code in Use Cases.

General Behavior

Before using SPI on CC26X4:

The following is true for peripheral operation:

The following apply for controller operation:

After SPI operation has ended:

The callback function is always called in a SWI context.

Error handling

If an RX overrun occurs during peripheral operation:

Timeout

Timeout can occur in SPI_MODE_BLOCKING, there's no timeout in SPI_MODE_CALLBACK. When in SPI_MODE_CALLBACK, the transfer must be cancelled by calling SPI_transferCancel().
If a timeout happens in either SPI_PERIPHERAL or SPI_CONTROLLER mode, the receive buffer will contain the bytes received up until the timeout occurred. The SPI transaction status will be set to SPI_TRANSFER_FAILED. The SPI transaction count will be set to the number of bytes sent/received before timeout. The remaining bytes will be flushed from the TX FIFO so that the subsequent transfer can be executed correctly. Note that specifying a timeout prevents the driver from performing a polling transfer when in peripheral mode.

Power Management

The TI-RTOS power management framework will try to put the device into the most power efficient mode whenever possible. Please see the technical reference manual for further details on each power mode.

The SPICC26X4DMA.h driver is setting a power constraint during transfers to keep the device out of standby. When the transfer has finished, the power constraint is released. The following statements are valid:

Note
The external hardware connected to the SPI might have some pull configured on the SPI lines. When the SPI is inactive, this might cause leakage on the IO and the current consumption to increase. The application must configure a pull configuration that aligns with the external hardware. See Ensure low power during inactive periods for code example.

SPI details

Chip Select

This SPI controller supports a hardware chip select pin. Refer to the user manual on how this hardware chip select pin behaves in regards to the SPI frame format.

Chip select type SPI_CONTROLLER mode SPI_PERIPHERAL mode
Hardware chip select No action is needed by the application to select the peripheral. See the device documentation on it's chip select requirements.
Software chip select The application is responsible to ensure that correct SPI peripheral is selected before performing a SPI_transfer(). See the device documentation on it's chip select requirements.

Multiple peripherals when operating in controller mode

In a scenario where the SPI module is operating in controller mode with multiple SPI peripherals, the chip select pin can be reallocated at runtime to select the appropriate peripheral device. See Controller Mode With Multiple Peripherals use case below. This is only relevant when chip select is a hardware chip select. Otherwise the application can control the chip select pins directly using the GPIO driver.

Data Frames

When the SPI is configured as SPI controller, the data frame can be any size from 4-bits to 32-bits. When the SPI is configured as SPI peripheral , the minimum data frame is 7-bits and the maximum is 32-bits. If the dataSize in SPI_Params is greater that 8-bits, then the SPICC26X4DMA driver implementation will assume that the SPI_Transaction txBuf and rxBuf point to an array of 16-bit uint16_t elements. Similarly, if the dataSize in SPI_Params is greater than 16-bits, the SPICC26X4DMA driver will assume buffers of uint32_t elements are used.

dataSize buffer element size
4-8 bits uint8_t
9-16 bits uint16_t
17-32 bits uint32_t

Bit Rate

When the SPI is configured as SPI peripheral, the maximum bit rate is 8MHz.

When the SPI is configured as SPI controller, the maximum bit rate is 12MHz.

UDMA

Interrupts

The UDMA module generates IRQs on the SPI interrupt vector. This driver automatically installs a UDMA aware Hwi (interrupt) to service the assigned UDMA channels.

Transfer Size Limit

The UDMA controller only supports data transfers of up to 1024 data frames. A transfer with more than 1024 frames will be transmitted/received in multiple 1024 sized portions until all data has been transmitted/received. A data frame can be 4 to 32 bits in length depending on SPI controller or peripheral mode.

Scratch Buffers

A uint16_t scratch buffer is used to allow SPI_transfers where txBuf or rxBuf are NULL. Rather than requiring txBuf or rxBuf to have a dummy buffer of size of the transfer count, a single-word UDMA accessible uint16_t scratch buffer is used. When rxBuf is NULL, the UDMA will transfer all the received SPI data into the scratch buffer as a "bit-bucket". When txBuf is NULL, the scratch buffer is initialized to defaultTxBufValue so the uDMA will send some known value. Each SPI driver instance uses its own scratch buffer.

TX and RX buffers

Before SPI_transfer, txBuf should be filled with the outgoing SPI data. These data are sent out during the transfer, while the incoming data are received into rxBuf. To save memory space, txBuf and rxBuf can be assigned to the same buffer location. At the beginning of the transfer, this buffer holds outgoing data. At the end of the transfer, the outgoing data are overwritten and the buffer holds the received SPI data.

Polling SPI transfers

When used in blocking mode small SPI transfers are can be done by polling the peripheral & sending data frame-by-frame. A controller device can perform the transfer immediately and return, but a peripheral will block until it receives the number of frames specified in the SPI_Transfer() call. The minDmaTransferSize field in the hardware attributes is the threshold; if the transaction count is below the threshold a polling transfer is performed; otherwise a DMA transfer is done. This is intended to reduce the overhead of setting up a DMA transfer to only send a few data frames.

Notes:

Supported Functions

Generic API function API function Description
SPI_init() SPICC26X4DMA_init() Initialize SPI driver
SPI_open() SPICC26X4DMA_open() Initialize SPI HW and set system dependencies
SPI_close() SPICC26X4DMA_close() Disable SPI and UDMA HW and release system dependencies
SPI_control() SPICC26X4DMA_control() Configure an already opened SPI handle
SPI_transfer() SPICC26X4DMA_transfer() Start transfer from SPI
SPI_transferCancel() SPICC26X4DMA_transferCancel() Cancel ongoing transfer from SPI
Note
All calls should go through the generic API

Unsupported Functionality

The SPI driver is unable to access flash memory in the address range 0x0000 - 0x2000 on devices based on the Cortex M33+ core (CC26X3/CC26X4) due to security constraints.

Use Cases

Basic Peripheral Mode

Receive 100 bytes over SPI in SPI_MODE_BLOCKING.

SPI_Handle handle;
SPI_Transaction transaction;
uint8_t rxBuf[100]; // Receive buffer
// Init SPI and specify non-default parameters
SPI_Params_init(&params);
params.bitRate = 1000000;
// Configure the transaction
transaction.count = 100;
transaction.txBuf = NULL;
transaction.rxBuf = rxBuf;
// Open the SPI and perform the transfer
handle = SPI_open(CONFIG_SPI, &params);
SPI_transfer(handle, &transaction);

Peripheral Mode With Return Partial

This use case will perform a transfer in SPI_MODE_BLOCKING until the wanted amount of bytes is transferred or until chip select is deasserted by the SPI controller. This SPI_transfer() call can be used when unknown amount of bytes shall be transferred.
Note: Partial return is also possible in SPI_MODE_CALLBACK mode. In callback mode, partial transfers can be queued by calling SPI_transfer() multiple times.
Note: Polling transfers are not available when using return partial mode.

SPI_Handle handle;
SPI_Transaction transaction;
uint8_t rxBuf[100]; // Receive buffer
// Init SPI and specify non-default parameters
SPI_Params_init(&params);
params.bitRate = 1000000;
// Configure the transaction
transaction.count = 100;
transaction.txBuf = NULL;
transaction.rxBuf = rxBuf;
// Open the SPI and initiate the partial read
handle = SPI_open(CONFIG_SPI, &params);
// Enable RETURN_PARTIAL
// Begin transfer
SPI_transfer(handle, &transaction);

Continuous Peripheral Transfer In SPI_MODE_CALLBACK

This use case will configure the SPI driver to transfer continuously in SPI_MODE_CALLBACK, 16 bytes at the time and echoing received data after every 16 bytes.

// Callback function
static void transferCallback(SPI_Handle handle, SPI_Transaction *transaction)
{
// Start another transfer
SPI_transfer(handle, transaction);
}
static void taskFxn(uintptr_t a0, uintptr_t a1)
{
SPI_Handle handle;
SPI_Transaction transaction;
uint8_t buf[16]; // Receive and transmit buffer
// Init SPI and specify non-default parameters
SPI_Params_init(&params);
params.bitRate = 1000000;
params.mode = SPI_PERIPHERAL;
params.transferCallbackFxn = transferCallback;
// Configure the transaction
transaction.count = 16;
transaction.txBuf = buf;
transaction.rxBuf = buf;
// Open the SPI and initiate the first transfer
handle = SPI_open(CONFIG_SPI, &params);
SPI_transfer(handle, &transaction);
// Wait forever
while(true);
}

Basic Controller Mode

This use case will configure a SPI controller to send the data in txBuf while receiving data to rxBuf in BLOCKING_MODE.

SPI_Handle handle;
SPI_Transaction transaction;
uint8_t txBuf[] = "Hello World"; // Transmit buffer
uint8_t rxBuf[11]; // Receive buffer
// Init SPI and specify non-default parameters
SPI_Params_init(&params);
params.bitRate = 1000000;
// Configure the transaction
transaction.count = sizeof(txBuf);
transaction.txBuf = txBuf;
transaction.rxBuf = rxBuf;
// Open the SPI and perform the transfer
handle = SPI_open(CONFIG_SPI, &params);
SPI_transfer(handle, &transaction);

Controller Mode With Multiple Peripherals

This use case will configure a SPI controller to send data to one peripheral and then to another in BLOCKING_MODE. It is assumed that SysConfig is configured so that the two chip select pins have a default setting of a high output and that the SPICC26X4DMA_HWAttrs used points to one of them since the SPI driver will revert to this default setting when switching the chip select pin.

// From ti_drivers_config.c
// Use the sysconfig settings to make sure both pins are set to HIGH when not in use
GPIO_PinConfig gpioPinConfigs[31] = {
...
...
}
const SPICC26X4DMA_HWAttrs SPICC26X4DMAHWAttrs[CONFIG_SPI_COUNT] = {
{ // Use SPI0 module with default chip select on CONFIG_CSN_0
.baseAddr = SPI0_BASE,
.intNum = INT_SSI0_COMB,
.intPriority = (~0),
.swiPriority = 0,
.powerMngrId = PowerCC26XX_PERIPH_SSI0,
.defaultTxBufValue = 0xFF,
.rxChannelBitMask = 1<<UDMA_CHAN_SSI0_RX,
.txChannelBitMask = 1<<UDMA_CHAN_SSI0_TX,
.dmaTxTableEntryPri = &dmaSpi0TxControlTableEntry,
.dmaRxTableEntryPri = &dmaSpi0RxControlTableEntry,
.dmaTxTableEntryAlt = &dmaSpi0TxAltControlTableEntry,
.dmaRxTableEntryAlt = &dmaSpi0RxAltControlTableEntry,
.minDmaTransferSize = 10,
.txPinMux = IOC_PORT_MCU_SSI0_TX,
.rxPinMux = IOC_PORT_MCU_SSI0_RX,
.clkPinMux = IOC_PORT_MCU_SSI0_CLK,
.csnPinMux = IOC_PORT_MCU_SSI0_FSS,
.picoPin = CONFIG_GPIO_SPI_CONTROLLER_PICO,
.pociPin = CONFIG_GPIO_SPI_CONTROLLER_POCI,
.clkPin = CONFIG_GPIO_SPI_CONTROLLER_SCLK,
.csnPin = CONFIG_CSN_0
}
// From your_application.c
static void taskFxn(uintptr_t a0, uintptr_t a1)
{
SPI_Handle handle;
SPI_Transaction transaction;
uint_least8_t csnPin1 = CONFIG_CSN_1;
uint8_t txBuf[] = "Hello World"; // Transmit buffer
// Init SPI and specify non-default parameters
SPI_Params_init(&params);
params.bitRate = 1000000;
params.mode = SPI_CONTROLLER;
// Configure the transaction
transaction.count = sizeof(txBuf);
transaction.txBuf = txBuf;
transaction.rxBuf = NULL;
// Open the SPI and perform transfer to the first peripheral
handle = SPI_open(CONFIG_SPI, &params);
SPI_transfer(handle, &transaction);
// Then switch chip select pin and perform transfer to the second peripheral
SPI_transfer(handle, &transaction);
}

Queueing Transactions in Callback Mode

Below is an example of queueing three transactions

// SPI already opened in callback mode
SPI_Transaction t0, t1, t2;
t0.txBuf = txBuff0;
t0.rxBuf = rxBuff0;
t0.count = 2000;
t1.txBuf = txBuff1;
t1.rxBuf = rxBuff1;
t1.count = 1000;
t2.txBuf = txBuff2;
t2.rxBuf = NULL;
t2.count = 1000;
bool transferOk = false;
if (SPI_transfer(spiHandle, &t0)) {
if (SPI_transfer(spiHandle, &t1)) {
transferOk = SPI_transfer(spiHandle, &t2);
}
}
}

Queueing in Manual Start Mode

This example shows a peripheral device queueing two transactions that will complete one after the other. From the controller's perspective there will be one long transfer.

Note
Manual mode also works while the device is in SPI_CONTROLLER mode. The control call to MANUAL_START will start the transfers.
Warning
Manual start mode should not be enabled or disabled while a transaction is in progress.

uint8_t status = SPI_STATUS_SUCCESS;
SPI_Params_init(&params);
spi = SPI_open(CONFIG_SPI, &params);
if (spi == NULL) {
exit(0);
}
// Enable manual start mode
// Queue transactions
t0.txBuf = txBuff0;
t0.rxBuf = rxBuff0;
t0.count = 2000;
if (!SPI_transfer(spi, &t0)) {
status = SPI_STATUS_FAIL;
}
t1.txBuf = txBuff1;
t1.rxBuf = rxBuff1;
t1.count = 1000;
if (!SPI_transfer(spi, &t1)) {
status = SPI_STATUS_FAIL;
}
// Enable the transfers
if (status == SPI_STATUS_SUCCESS) {
}
else {
status = SPI_STATUS_FAILURE;
}
// At this point the peripheral is ready for the controller to start the transfer
// Assume the callback implementation (not shown) posts a semaphore when
// the last transaction completes
sem_wait(&spiSemaphore);
// Disable manual start mode

Ensure low power during inactive periods

External hardware connected on the SPI, i.e. SPI controller/peripheral, might have configured a pull on one or more of the SPI lines. Dependent on the hardware, it might conflict with the pull used for the CC26X4 SPI. To avoid increased leakage and ensure the lowest possible power consumption when the SPI is inactive, the application must configure a matching pull on the SPI IOs. An example of how this can be done is shown below.

SPI_Handle handle;
SPI_Transaction transaction;
uint8_t txBuf[] = "Heartbeat"; // Transmit buffer
uint8_t rxBuf[9]; // Receive buffer
uint32_t standbyDurationMs = 100;
// Init SPI and specify non-default parameters
SPI_Params_init(&params);
params.bitRate = 1000000;
// Configure the transaction
transaction.count = sizeof(txBuf);
transaction.txBuf = txBuf;
transaction.rxBuf = rxBuf;
// Open the SPI and perform the transfer
handle = SPI_open(CONFIG_SPI_0, &params);
// Apply low power sleep pull config for POCI
GPIO_setConfig(CONFIG_GPIO_SPI_0_POCI, GPIO_CFG_IN_PU);
// Do forever
while(1) {
// Transfer data
SPI_transfer(handle, &transaction);
// Sleep
Task_sleep(standbyDurationMs*100);
}

Wake Up On Chip Select Deassertion In Peripheral Mode Using SPI_MODE_CALLBACK

This example demonstrates using a GPIO callback on Chip Select to wake up the device to allow low power modes while waiting for a chip select edge.

In sysconfig or the board file, the CSN GPIO should be configured as input/pull up with an interrupt on falling edge. Otherwise, SPI_close() will reset the pin to the wrong settings and you may see line glitches.

*Note: The SPI controller must allow enough time between deasserting the chip select and the start of the transaction for the SPI peripheral to wake up and open up the SPI driver.

// Global variables
SPI_Handle spiHandle
SPI_Params spiParams;
SPI_Transaction spiTransaction;
const uint8_t transferSize = 8;
uint8_t txBuf[8];
// Chip select callback
static void chipSelectCallback(uint_least8_t)
{
// Open SPI driver, which will override any previous GPIO configuration
spiHandle = SPI_open(CONFIG_SPI, &spiParams);
// Issue the transfer
SPI_transfer(spiHandle, &spiTransaction);
}
// SPI transfer callback
static void transferCallback(SPI_Handle handle, SPI_Transaction *transaction)
{
// Close the SPI driver
SPI_close(handle);
// Note: SPI_close() will reset the pin configuration, so it is important to
// set the default values correctly in sysconfig. We just need to set the
// callback and enable the falling edge interrupt
GPIO_setCallback(CS_PIN_INDEX, chipSelectCallback);
GPIO_enableInt(CS_PIN_INDEX);
}
// From your_application.c
static void taskFxn(uintptr_t a0, uintptr_t a1)
{
uint8_t i;
// Setup SPI params
SPI_Params_init(&spiParams);
spiParams.bitRate = 1000000;
spiParams.frameFormat = SPI_POL1_PHA1;
spiParams.mode = SPI_PERIPHERAL;
spiParams.dataSize = transferSize;
spiParams.transferMode = SPI_MODE_CALLBACK;
spiParams.transferCallbackFxn = transferCallback;
// Setup SPI transaction
spiTransaction.arg = NULL;
spiTransaction.count = transferSize;
spiTransaction.txBuf = txBuf;
spiTransaction.rxBuf = txBuf;
// First echo message
for (i = 0; i < transferSize; i++) {
txBuf[i] = i;
}
// Configure chip select callback
GPIO_setCallback(CS_PIN_INDEX, chipSelectCallback);
GPIO_enableInt(CS_PIN_INDEX);
// Wait forever
while(true);
}

#include <stdint.h>
#include <ti/drivers/SPI.h>
#include <ti/drivers/dma/UDMACC26XX.h>
#include <ti/drivers/Power.h>
#include <ti/drivers/power/PowerCC26XX.h>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/dpl/SemaphoreP.h>
#include <ti/drivers/dpl/SwiP.h>
Include dependency graph for SPICC26X4DMA.h:

Go to the source code of this file.

Data Structures

struct  SPICC26X4DMA_HWAttrs
 SPICC26X4DMA Hardware attributes. More...
 
struct  SPICC26X4DMA_Object
 SPICC26X4DMA Object. More...
 

Macros

#define SPICC26X4DMA_CMD_RETURN_PARTIAL_ENABLE   (SPI_CMD_RESERVED + 0)
 Command used by SPI_control() to enable partial return. More...
 
#define SPICC26X4DMA_CMD_RETURN_PARTIAL_DISABLE   (SPI_CMD_RESERVED + 1)
 Command used by SPI_control() to disable partial return. More...
 
#define SPICC26X4DMA_CMD_SET_CSN_PIN   (SPI_CMD_RESERVED + 2)
 Command used by SPI_control() to re-configure chip select pin. More...
 
#define SPICC26X4DMA_CMD_CLEAR_CSN_PIN   (SPI_CMD_RESERVED + 3)
 Command used by SPI_control() to clear the chip select pin. More...
 
#define SPICC26X4DMA_CMD_SET_MANUAL   (SPI_CMD_RESERVED + 4)
 Command used by SPI_control() to enable manual start mode. More...
 
#define SPICC26X4DMA_CMD_CLR_MANUAL   (SPI_CMD_RESERVED + 5)
 Command used by SPI_control() to disable manual start mode. More...
 
#define SPICC26X4DMA_CMD_MANUAL_START   (SPI_CMD_RESERVED + 6)
 Command used by SPI_control() to enable manual start mode. More...
 
#define SPICC26X4DMA_CMD_SET_SAMPLE_DELAY   (SPI_CMD_RESERVED + 7)
 Command used by SPI_control() to set the sample delay in controller mode. More...
 
#define SPICC26X4DMA_RETURN_PARTIAL_ENABLE   SPICC26X4DMA_CMD_RETURN_PARTIAL_ENABLE
 
#define SPICC26X4DMA_RETURN_PARTIAL_DISABLE   SPICC26X4DMA_CMD_RETURN_PARTIAL_DISABLE
 
#define SPICC26X4DMA_SET_CSN_PIN   SPICC26X4DMA_CMD_SET_CSN_PIN
 

Enumerations

enum  SPICC26X4DMA_FrameSize { SPICC26X4DMA_8bit = 0, SPICC26X4DMA_16bit = 1 }
 
enum  SPICC26X4DMA_ReturnPartial { SPICC26X4DMA_retPartDisabled = 0, SPICC26X4DMA_retPartEnabledIntNotSet = 1, SPICC26X4DMA_retPartEnabledIntSet = 2 }
 

Variables

const SPI_FxnTable SPICC26X4DMA_fxnTable
 

Macro Definition Documentation

§ SPICC26X4DMA_RETURN_PARTIAL_ENABLE

#define SPICC26X4DMA_RETURN_PARTIAL_ENABLE   SPICC26X4DMA_CMD_RETURN_PARTIAL_ENABLE

§ SPICC26X4DMA_RETURN_PARTIAL_DISABLE

#define SPICC26X4DMA_RETURN_PARTIAL_DISABLE   SPICC26X4DMA_CMD_RETURN_PARTIAL_DISABLE

§ SPICC26X4DMA_SET_CSN_PIN

#define SPICC26X4DMA_SET_CSN_PIN   SPICC26X4DMA_CMD_SET_CSN_PIN

Enumeration Type Documentation

§ SPICC26X4DMA_FrameSize

Enumerator
SPICC26X4DMA_8bit 
SPICC26X4DMA_16bit 

§ SPICC26X4DMA_ReturnPartial

Enumerator
SPICC26X4DMA_retPartDisabled 
SPICC26X4DMA_retPartEnabledIntNotSet 
SPICC26X4DMA_retPartEnabledIntSet 

Variable Documentation

§ SPICC26X4DMA_fxnTable

const SPI_FxnTable SPICC26X4DMA_fxnTable
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale