Data Structures | Variables
WatchdogCC26X4.h File Reference

Detailed Description

Watchdog driver implementation for CC13X4/CC26X4.


Driver include

The Watchdog header file should be included in an application as follows:

Refer to Watchdog.h for a complete description of APIs.

Overview

The general Watchdog API should be used in application code, i.e. Watchdog_open() should be used instead of WatchdogCC26X4_open(). The board file will define the device specific config, and casting in the general API will ensure that the correct device specific functions are called.

General Behavior

This Watchdog driver implementation is designed to operate on a CC13X4/CC26X4 device. Before using the Watchdog on CC13X4/CC26X4, the Watchdog driver is initialized by calling Watchdog_init(). The Watchdog HW is configured by calling Watchdog_open(). Once opened, the Watchdog will count down from the reload value specified in WatchdogCC26X4_HWAttrs. If it times out, a reset signal will be generated. To prevent a reset, Watchdog_clear() must be called to reload the timer.

The Watchdog counts down at the rate of the device clock SCLK_LF. SCLK_LF will tick at different rates depending on the SCLK_LF source selected in CCFG, ranging between 31250 Hz and 32768 Hz. The Watchdog driver internally calculates the correct tick value depending on the target SCLK_LF source selected in CCFG. RCOSC_LF is an inherently inaccurate clock source and will present variations around the target 32768 Hz frequency. These inaccuracies have to be taken into consideration at the application level if RSCOC_LF is selected as the source of SCLK_LF.

The reload value from which the Watchdog timer counts down may be changed during runtime using Watchdog_setReload(). This value should be specified in Watchdog clock ticks and should not exceed "2^32 - 1". This corresponds to a timeout period of 131071 seconds, calculated at the highest rate of 32768 kHz. If the reload value is set to zero, the Watchdog reset is immediately generated.

Watchdog_close() is not supported by this driver implementation. Once started, the Watchdog timer can only be stopped by a hardware reset.

No CC13X4/CC26X4 specific command has been implemented. Any call to Watchdog_control() will receive the return code Watchdog_STATUS_UNDEFINEDCMD.

The Watchdog module available on CC13X4/CC26X4 devices does not support reset masking or interrupt generation. Therefore, the two parameters Watchdog_Params::resetMode and Watchdog_Params::callbackFxn in the Watchdog_Params struct are not supported and will be ignored by the Watchdog driver.

Power Management

Once started, the Watchdog will keep running in Active, Idle and Standby mode.

Supported Functions

| Generic API Function | API Function | Description | |---------------------------— |-------------------------------— |------------------------------------------------— | | Watchdog_init() | WatchdogCC26X4_init() | Initialize Watchdog driver | | Watchdog_open() | WatchdogCC26X4_open() | Initialize Watchdog HW and set system dependencies | | Watchdog_clear() | WatchdogCC26X4_clear() | Reload Watchdog counter | | Watchdog_setReload() | WatchdogCC26X4_setReload() | Update Watchdog timer reload value in clock ticks | | Watchdog_convertMsToTicks() | WatchdogCC26X4_convertMsToTicks() | Converts milliseconds to clock ticks |

Note
All calls should go through the generic API. Please refer to Watchdog.h for a complete description of the generic APIs.

Use Cases

Basic Watchdog

In this basic watchdog example, the application is expected to start the Watchdog timer by calling Watchdog_open(). If needed, Watchdog_setReload() may be called to change the timeout period. If all monitored tasks are doing alright, Watchdog_clear() should be called regularly to reload the counter so as to restart the timeout period and to avoid the Watchdog resetting the device. If the Watchdog_clear() is missed and the Watchdog timer is allowed to timeout, the device will be reset.

The following code example shows how to correctly initialize the driver's parameters, start the Watchdog timer and modify at runtime the timeout period.

uint32_t tickValue;
handle = Watchdog_open(Watchdog_configIndex, &params);
// set timeout period to 100 ms
tickValue = Watchdog_convertMsToTicks(handle, 100);
Watchdog_setReload(handle, tickValue);
#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/Watchdog.h>
#include <ti/drivers/dpl/HwiP.h>
Include dependency graph for WatchdogCC26X4.h:

Go to the source code of this file.

Data Structures

struct  WatchdogCC26X4_HWAttrs
 Watchdog hardware attributes for CC26X4. More...
 
struct  WatchdogCC26X4_Object
 Watchdog Object for CC26X4. More...
 

Variables

const Watchdog_FxnTable WatchdogCC26X4_fxnTable
 Watchdog function table for CC26X4. More...
 

Variable Documentation

§ WatchdogCC26X4_fxnTable

const Watchdog_FxnTable WatchdogCC26X4_fxnTable

Watchdog function table for CC26X4.

© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale