Data Fields
Display_FxnTable Struct Reference

The definition of a Display function table that contains the required set of functions to control a specific Display driver implementation. More...

#include <Display.h>

Collaboration diagram for Display_FxnTable:
Collaboration graph
[legend]

Data Fields

Display_initFxn initFxn
 
Display_openFxn openFxn
 
Display_clearFxn clearFxn
 
Display_clearLinesFxn clearLinesFxn
 
Display_vprintfFxn vprintfFxn
 
Display_closeFxn closeFxn
 
Display_controlFxn controlFxn
 
Display_getTypeFxn getTypeFxn
 

Detailed Description

The definition of a Display function table that contains the required set of functions to control a specific Display driver implementation.

Field Documentation

§ initFxn

Display_initFxn Display_FxnTable::initFxn

§ openFxn

Display_openFxn Display_FxnTable::openFxn

§ clearFxn

Display_clearFxn Display_FxnTable::clearFxn

§ clearLinesFxn

Display_clearLinesFxn Display_FxnTable::clearLinesFxn

§ vprintfFxn

Display_vprintfFxn Display_FxnTable::vprintfFxn

§ closeFxn

Display_closeFxn Display_FxnTable::closeFxn

§ controlFxn

Display_controlFxn Display_FxnTable::controlFxn

§ getTypeFxn

Display_getTypeFxn Display_FxnTable::getTypeFxn

The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale