Data Fields
DisplayUart2_Object Struct Reference

DisplayUart2 Object. More...

#include <DisplayUart2.h>

Collaboration diagram for DisplayUart2_Object:
Collaboration graph
[legend]

Data Fields

UART2_Handle hUart
 
SemaphoreP_Handle mutex
 
char * lineClearSeq
 

Detailed Description

DisplayUart2 Object.

The application must not access any member variables of this structure!

Field Documentation

§ hUart

UART2_Handle DisplayUart2_Object::hUart

§ mutex

SemaphoreP_Handle DisplayUart2_Object::mutex

§ lineClearSeq

char* DisplayUart2_Object::lineClearSeq

The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale