ECDHCC26X1 Hardware Attributes. More...
#include <ECDHCC26X1.h>
Data Fields | |
uint8_t | dummy |
ECDHCC26X1 Hardware Attributes.
ECC26XX hardware attributes should be included in the board file and pointed to by the ECDH_config struct.
uint8_t ECDHCC26X1_HWAttrs::dummy |