![]() |
![]() |
|
rflib
|
|
Macros | |
| #define | RF_convertUsToRatTicks(microseconds) ((microseconds) * (RF_RAT_TICKS_PER_US)) |
| Converts a duration given in microseconds into radio timer (RAT) ticks. More... | |
| #define | RF_convertMsToRatTicks(milliseconds) ((milliseconds) * 1000 * (RF_RAT_TICKS_PER_US)) |
| Converts a duration given in milliseconds into radio timer (RAT) ticks. More... | |
| #define | RF_convertRatTicksToUs(ticks) ((ticks) / (RF_RAT_TICKS_PER_US)) |
| Converts a duration given in radio timer (RAT) ticks into microseconds. More... | |
| #define | RF_convertRatTicksToMs(ticks) ((ticks) / (1000 * (RF_RAT_TICKS_PER_US))) |
| Converts a duration given in radio timer (RAT) ticks into milliseconds. More... | |
RF Core Events | |
Events originating on the RF core and caused during command execution. They are aliases for the corresponding interrupt flags. RF Core Events are command-specific and are explained in the Technical Reference Manual.
| |
| #define | RF_EventCmdDone (1 << 0) |
| A radio operation command in a chain finished. More... | |
| #define | RF_EventLastCmdDone (1 << 1) |
| A stand-alone radio operation command or the last radio operation command in a chain finished. More... | |
| #define | RF_EventFGCmdDone (1 << 2) |
| A IEEE-mode radio operation command in a chain finished. More... | |
| #define | RF_EventLastFGCmdDone (1 << 3) |
| A stand-alone IEEE-mode radio operation command or the last command in a chain finished. More... | |
| #define | RF_EventTxDone (1 << 4) |
| Packet transmitted. More... | |
| #define | RF_EventTXAck (1 << 5) |
| ACK packet transmitted. More... | |
| #define | RF_EventTxCtrl (1 << 6) |
| Control packet transmitted. More... | |
| #define | RF_EventTxCtrlAck (1 << 7) |
| Acknowledgement received on a transmitted control packet. More... | |
| #define | RF_EventTxCtrlAckAck (1 << 8) |
| Acknowledgement received on a transmitted control packet, and acknowledgement transmitted for that packet. More... | |
| #define | RF_EventTxRetrans (1 << 9) |
| Packet retransmitted. More... | |
| #define | RF_EventTxEntryDone (1 << 10) |
| Tx queue data entry state changed to Finished. More... | |
| #define | RF_EventTxBufferChange (1 << 11) |
| A buffer change is complete. More... | |
| #define | RF_EventPaChanged (1 << 14) |
| The PA was reconfigured on the fly. More... | |
| #define | RF_EventSamplesEntryDone (1 << 15) |
| CTE data has been copied, only valid if autocopy feature is enabled. More... | |
| #define | RF_EventRxOk (1 << 16) |
| Packet received with CRC OK, payload, and not to be ignored. More... | |
| #define | RF_EventRxNOk (1 << 17) |
| Packet received with CRC error. More... | |
| #define | RF_EventRxIgnored (1 << 18) |
| Packet received with CRC OK, but to be ignored. More... | |
| #define | RF_EventRxEmpty (1 << 19) |
| Packet received with CRC OK, not to be ignored, no payload. More... | |
| #define | RF_EventRxCtrl (1 << 20) |
| Control packet received with CRC OK, not to be ignored. More... | |
| #define | RF_EventRxCtrlAck (1 << 21) |
| Control packet received with CRC OK, not to be ignored, then ACK sent. More... | |
| #define | RF_EventRxBufFull (1 << 22) |
| Packet received that did not fit in the Rx queue. More... | |
| #define | RF_EventRxEntryDone (1 << 23) |
| Rx queue data entry changing state to Finished. More... | |
| #define | RF_EventDataWritten (1 << 24) |
| Data written to partial read Rx buffer. More... | |
| #define | RF_EventNDataWritten (1 << 25) |
| Specified number of bytes written to partial read Rx buffer. More... | |
| #define | RF_EventRxAborted (1 << 26) |
| Packet reception stopped before packet was done. More... | |
| #define | RF_EventRxCollisionDetected (1 << 27) |
| A collision was indicated during packet reception. More... | |
| #define | RF_EventModulesUnlocked (1 << 29) |
| As part of the boot process, the CM0 has opened access to RF core modules and memories. More... | |
| #define | RF_EventInternalError (uint32_t)(1 << 31) |
| Internal error observed. More... | |
| #define | RF_EventMdmSoft 0x0000002000000000 |
| Synchronization word detected (MDMSOFT interrupt flag) More... | |
RF Driver Events | |
| #define | RF_EventCmdCancelled 0x1000000000000000 |
| Command canceled before it was started. More... | |
| #define | RF_EventCmdAborted 0x2000000000000000 |
| Abrupt command termination caused by RF_cancelCmd() or RF_flushCmd(). More... | |
| #define | RF_EventCmdStopped 0x4000000000000000 |
| Graceful command termination caused by RF_cancelCmd() or RF_flushCmd(). More... | |
| #define | RF_EventRatCh 0x0800000000000000 |
| A user-programmable RAT channel triggered an event. More... | |
| #define | RF_EventPowerUp 0x0400000000000000 |
| RF power up event. More... | |
| #define | RF_EventError 0x0200000000000000 |
| Event flag used for error callback functions to indicate an error. See RF_Params::pErrCb. More... | |
| #define | RF_EventCmdPreempted 0x0100000000000000 |
| Command preempted by another command with higher priority. Applies only to multi-client applications. More... | |
Control codes for driver configuration | |
Control codes are used in RF_control(). | |
| #define | RF_CTRL_SET_INACTIVITY_TIMEOUT 0 |
| Control code used by RF_control to set inactivity timeout. More... | |
| #define | RF_CTRL_UPDATE_SETUP_CMD 1 |
| Control code used by RF_control to update setup command. More... | |
| #define | RF_CTRL_SET_POWERUP_DURATION_MARGIN 2 |
| Control code used by RF_control to set powerup duration margin. More... | |
| #define | RF_CTRL_SET_PHYSWITCHING_DURATION_MARGIN 3 |
| Control code used by RF_control to set the phy switching margin. More... | |
| #define | RF_CTRL_SET_RAT_RTC_ERR_TOL_VAL 4 |
| Control code used by RF_control to set max error tolerance for RAT/RTC. More... | |
| #define | RF_CTRL_SET_POWER_MGMT 5 |
| Control code used by RF_control to set power management. More... | |
| #define | RF_CTRL_SET_HWI_PRIORITY 6 |
| Control code used by RF_control to set the hardware interrupt priority level of the RF driver. More... | |
| #define | RF_CTRL_SET_SWI_PRIORITY 7 |
| Control code used by RF_control to set the software interrupt priority level of the RF driver. More... | |
| #define | RF_CTRL_SET_AVAILABLE_RAT_CHANNELS_MASK 8 |
| Control code used by RF_control to mask the available RAT channels manually. More... | |
| #define | RF_CTRL_COEX_CONTROL 9 |
| Control code used by RF_control to enable or disable the coexistence feature at runtime. More... | |
TX Power Table defines | |
| #define | RF_TxPowerTable_MIN_DBM -128 |
| #define | RF_TxPowerTable_MAX_DBM 126 |
| #define | RF_TxPowerTable_INVALID_DBM 127 |
| #define | RF_TxPowerTable_INVALID_VALUE 0x3fffff |
| #define | RF_TxPowerTable_TERMINATION_ENTRY { .power = RF_TxPowerTable_INVALID_DBM, .value = { .rawValue = RF_TxPowerTable_INVALID_VALUE, .paType = RF_TxPowerTable_DefaultPA } } |
| #define | RF_TxPowerTable_DEFAULT_PA_ENTRY(bias, gain, boost, coefficient) { .rawValue = ((bias) << 0) | ((gain) << 6) | ((boost) << 8) | ((coefficient) << 9), .paType = RF_TxPowerTable_DefaultPA } |
| #define | RF_TxPowerTable_CC13x4Sub1GHz_DEFAULT_PA_ENTRY(bias, gain, boost, coefficient, gain2) { .rawValue = ((bias) << 0) | ((gain) << 6) | ((boost) << 8) | ((coefficient) << 9) | ((gain2) << 16), .paType = RF_TxPowerTable_DefaultPA } |
| #define | RF_TxPowerTable_HIGH_PA_ENTRY(bias, ibboost, boost, coefficient, ldotrim) { .rawValue = ((bias) << 0) | ((ibboost) << 6) | ((boost) << 8) | ((coefficient) << 9) | ((ldotrim) << 16), .paType = RF_TxPowerTable_HighPA } |
Other defines | |
| #define | RF_GET_RSSI_ERROR_VAL (-128) |
| Error return value for RF_getRssi() More... | |
| #define | RF_CMDHANDLE_FLUSH_ALL (-1) |
| RF command handle to flush all RF commands. More... | |
| #define | RF_ALLOC_ERROR (-2) |
| RF command or RAT channel allocation error. More... | |
| #define | RF_SCHEDULE_CMD_ERROR (-3) |
| RF command schedule error. More... | |
| #define | RF_ERROR_RAT_PROG (-255) |
| A rat channel could not be programmed. More... | |
| #define | RF_ERROR_INVALID_RFMODE (-256) |
| Invalid RF_Mode. Used in error callback. More... | |
| #define | RF_ERROR_CMDFS_SYNTH_PROG (-257) |
| Synthesizer error with CMD_FS. Used in error callback. If this error occurred in error callback, user needs to resend CMD_FS to recover. See the device's errata for more details. More... | |
| #define | RF_NUM_SCHEDULE_ACCESS_ENTRIES 2 |
| Number of access request entries. More... | |
| #define | RF_NUM_SCHEDULE_COMMAND_ENTRIES 8 |
| Number of scheduled command entries. More... | |
| #define | RF_NUM_SCHEDULE_MAP_ENTRIES (RF_NUM_SCHEDULE_ACCESS_ENTRIES + RF_NUM_SCHEDULE_COMMAND_ENTRIES) |
| Number of schedule map entries. This is the sum of access request and scheduled command entries. More... | |
| #define | RF_SCH_MAP_CURRENT_CMD_OFFSET RF_NUM_SCHEDULE_ACCESS_ENTRIES |
| Offset of the current command entry in the schedule map. More... | |
| #define | RF_SCH_MAP_PENDING_CMD_OFFSET (RF_SCH_MAP_CURRENT_CMD_OFFSET + 2) |
| Offset of the first pending command entry in the schedule map. More... | |
| #define | RF_ABORT_PREEMPTION (1<<2) |
| Used with RF_cancelCmd() to provoke subscription to RadioFreeCallback. More... | |
| #define | RF_ABORT_GRACEFULLY (1<<0) |
| Used with RF_cancelCmd() for graceful command termination. More... | |
| #define | RF_SCH_CMD_EXECUTION_TIME_UNKNOWN 0 |
| For unknown execution time for RF scheduler. More... | |
| #define | RF_RAT_ANY_CHANNEL (-1) |
| To be used within the channel configuration structure. Allocate any of the available channels. More... | |
| #define | RF_RAT_TICKS_PER_US 4 |
| Radio timer (RAT) ticks per microsecond. More... | |
| #define | RF_LODIVIDER_MASK 0x7F |
| Mask to be used to determine the effective value of the setup command's loDivider field. More... | |
Stack ID defines | |
Reserved values to identify which stack owns an RF_Handle h (stored as h->clientConfig.nID) | |
| #define | RF_STACK_ID_DEFAULT 0x00000000 |
| No value is set. More... | |
| #define | RF_STACK_ID_154 0x8000F154 |
| ID for TI 15.4 Stack. More... | |
| #define | RF_STACK_ID_BLE 0x8000FB1E |
| ID for TI BLE Stack. More... | |
| #define | RF_STACK_ID_EASYLINK 0x8000FEA2 |
| ID for TI EasyLink Stack. More... | |
| #define | RF_STACK_ID_THREAD 0x8000FEAD |
| ID for TI Thread Stack. More... | |
| #define | RF_STACK_ID_TOF 0x8000F00F |
| ID for TI TOF Stack. More... | |
| #define | RF_STACK_ID_CUSTOM 0x0000FC00 |
| ID for Custom Stack. More... | |
| #define RF_EventCmdDone (1 << 0) |
A radio operation command in a chain finished.
| #define RF_EventLastCmdDone (1 << 1) |
A stand-alone radio operation command or the last radio operation command in a chain finished.
| #define RF_EventFGCmdDone (1 << 2) |
A IEEE-mode radio operation command in a chain finished.
| #define RF_EventLastFGCmdDone (1 << 3) |
A stand-alone IEEE-mode radio operation command or the last command in a chain finished.
| #define RF_EventTxDone (1 << 4) |
Packet transmitted.
| #define RF_EventTXAck (1 << 5) |
ACK packet transmitted.
| #define RF_EventTxCtrl (1 << 6) |
Control packet transmitted.
| #define RF_EventTxCtrlAck (1 << 7) |
Acknowledgement received on a transmitted control packet.
| #define RF_EventTxCtrlAckAck (1 << 8) |
Acknowledgement received on a transmitted control packet, and acknowledgement transmitted for that packet.
| #define RF_EventTxRetrans (1 << 9) |
Packet retransmitted.
| #define RF_EventTxEntryDone (1 << 10) |
Tx queue data entry state changed to Finished.
| #define RF_EventTxBufferChange (1 << 11) |
A buffer change is complete.
| #define RF_EventPaChanged (1 << 14) |
The PA was reconfigured on the fly.
| #define RF_EventSamplesEntryDone (1 << 15) |
CTE data has been copied, only valid if autocopy feature is enabled.
| #define RF_EventRxOk (1 << 16) |
Packet received with CRC OK, payload, and not to be ignored.
| #define RF_EventRxNOk (1 << 17) |
Packet received with CRC error.
| #define RF_EventRxIgnored (1 << 18) |
Packet received with CRC OK, but to be ignored.
| #define RF_EventRxEmpty (1 << 19) |
Packet received with CRC OK, not to be ignored, no payload.
| #define RF_EventRxCtrl (1 << 20) |
Control packet received with CRC OK, not to be ignored.
| #define RF_EventRxCtrlAck (1 << 21) |
Control packet received with CRC OK, not to be ignored, then ACK sent.
| #define RF_EventRxBufFull (1 << 22) |
Packet received that did not fit in the Rx queue.
| #define RF_EventRxEntryDone (1 << 23) |
Rx queue data entry changing state to Finished.
| #define RF_EventDataWritten (1 << 24) |
Data written to partial read Rx buffer.
| #define RF_EventNDataWritten (1 << 25) |
Specified number of bytes written to partial read Rx buffer.
| #define RF_EventRxAborted (1 << 26) |
Packet reception stopped before packet was done.
| #define RF_EventRxCollisionDetected (1 << 27) |
A collision was indicated during packet reception.
| #define RF_EventModulesUnlocked (1 << 29) |
As part of the boot process, the CM0 has opened access to RF core modules and memories.
| #define RF_EventInternalError (uint32_t)(1 << 31) |
Internal error observed.
| #define RF_EventMdmSoft 0x0000002000000000 |
Synchronization word detected (MDMSOFT interrupt flag)
| #define RF_EventCmdCancelled 0x1000000000000000 |
Command canceled before it was started.
| #define RF_EventCmdAborted 0x2000000000000000 |
Abrupt command termination caused by RF_cancelCmd() or RF_flushCmd().
| #define RF_EventCmdStopped 0x4000000000000000 |
Graceful command termination caused by RF_cancelCmd() or RF_flushCmd().
| #define RF_EventRatCh 0x0800000000000000 |
A user-programmable RAT channel triggered an event.
| #define RF_EventPowerUp 0x0400000000000000 |
RF power up event.
| #define RF_EventError 0x0200000000000000 |
Event flag used for error callback functions to indicate an error. See RF_Params::pErrCb.
| #define RF_EventCmdPreempted 0x0100000000000000 |
Command preempted by another command with higher priority. Applies only to multi-client applications.
| #define RF_CTRL_SET_INACTIVITY_TIMEOUT 0 |
Control code used by RF_control to set inactivity timeout.
Setting this control allows RF to power down the radio upon completion of a radio command after a specified timeout period (in us) With this control code arg is a pointer to the timeout variable and returns RF_StatSuccess.
| #define RF_CTRL_UPDATE_SETUP_CMD 1 |
Control code used by RF_control to update setup command.
Setting this control notifies RF that the setup command is to be updated, so that RF will take proper actions when executing the next setup command. Note the updated setup command will take effect in the next power up cycle when RF executes the setup command. Prior to updating the setup command, user should make sure all pending commands have completed.
| #define RF_CTRL_SET_POWERUP_DURATION_MARGIN 2 |
Control code used by RF_control to set powerup duration margin.
Setting this control updates the powerup duration margin. Default is RF_DEFAULT_POWER_UP_MARGIN.
| #define RF_CTRL_SET_PHYSWITCHING_DURATION_MARGIN 3 |
Control code used by RF_control to set the phy switching margin.
Setting this control updates the phy switching duration margin, which is used to calculate when run-time conflicts shall be evaluated in case of colliding radio operations issued from two different clients. Default is RF_DEFAULT_PHY_SWITCHING_MARGIN.
| #define RF_CTRL_SET_RAT_RTC_ERR_TOL_VAL 4 |
Control code used by RF_control to set max error tolerance for RAT/RTC.
Setting this control updates the error tol for how frequently the CMD_RAT_SYNC_STOP is sent. Default is RF_DEFAULT_RAT_RTC_ERR_TOL_IN_US (5 us) Client is recommeneded to change this setting before sending any commands.
| #define RF_CTRL_SET_POWER_MGMT 5 |
Control code used by RF_control to set power management.
Setting this control configures RF driver to enable or disable power management. By default power management is enabled. If disabled, once RF core wakes up, RF driver will not go to standby and will not power down RF core. To configure power management, use this control to pass a parameter value of 0 to disable power management, and pass a parameter value of 1 to re-enable power management. This control is valid for dual-mode code only. Setting this control when using single-mode code has no effect (power management always enabled).
| #define RF_CTRL_SET_HWI_PRIORITY 6 |
Control code used by RF_control to set the hardware interrupt priority level of the RF driver.
This control code sets the hardware interrupt priority level that is used by the RF driver. Valid values are INT_PRI_LEVEL1 (highest) until INT_PRI_LEVEL7 (lowest). The default interrupt priority is set in the board support file. The default value is -1 which means "lowest possible priority".
When using the TI-RTOS kernel, INT_PRI_LEVEL0 is reserved for zero-latency interrupts and must not be used.
Execute this control code only while the RF core is powered down and the RF driver command queue is empty. This is usually the case after calling RF_open(). Changing the interrupt priority level while the RF driver is active will result in RF_StatBusyError being returned.
Example:
| #define RF_CTRL_SET_SWI_PRIORITY 7 |
Control code used by RF_control to set the software interrupt priority level of the RF driver.
This control code sets the software interrupt priority level that is used by the RF driver. Valid values are integers starting at 0 (lowest) until Swi_numPriorities - 1 (highest). The default interrupt priority is set in the board support file. The default value is 0 which means means "lowest possible priority".
Execute this control code only while the RF core is powered down and the RF driver command queue is empty. This is usually the case after calling RF_open(). Changing the interrupt priority level while the RF driver is active will result in RF_StatBusyError being returned.
Example:
| #define RF_CTRL_SET_AVAILABLE_RAT_CHANNELS_MASK 8 |
Control code used by RF_control to mask the available RAT channels manually.
This control code can be used to manually disallow/allow access to certain RAT channels from the RAT APIs. A typical use case is when a RAT channel is programmed through chained radio operations, and hence is used outside the scope of the RF driver. By disallowing access to this channel one can prevent collision between the automatic channel allocation through RF_ratCompare()/RF_ratCapture() and the direct configuration through RF_postCmd().
| #define RF_CTRL_COEX_CONTROL 9 |
Control code used by RF_control to enable or disable the coexistence feature at runtime.
This control code can be used to manually override the statically configured setting for global enable/disable of the coexistence feature. It will have no effect if coexistence is not originally enabled and included in the compiled project.
Example:
| #define RF_TxPowerTable_MIN_DBM -128 |
Refers to the the minimum available power in dBm when accessing a power table.
| #define RF_TxPowerTable_MAX_DBM 126 |
Refers to the the maximum available power in dBm when accessing a power table.
| #define RF_TxPowerTable_INVALID_DBM 127 |
Refers to an invalid power level in a TX power table.
| #define RF_TxPowerTable_INVALID_VALUE 0x3fffff |
Refers to an invalid power value in a TX power table.
This is the raw value part of a TX power configuration. In order to check whether a given power configuration is valid, do:
A TX power table is always terminated by an invalid power configuration.
| #define RF_TxPowerTable_TERMINATION_ENTRY { .power = RF_TxPowerTable_INVALID_DBM, .value = { .rawValue = RF_TxPowerTable_INVALID_VALUE, .paType = RF_TxPowerTable_DefaultPA } } |
Marks the last entry in a TX power table.
In order to use RF_TxPowerTable_findValue() and RF_TxPowerTable_findPowerLevel(), every power table must be terminated by a RF_TxPowerTable_TERMINATION_ENTRY:
| #define RF_TxPowerTable_DEFAULT_PA_ENTRY | ( | bias, | |
| gain, | |||
| boost, | |||
| coefficient | |||
| ) | { .rawValue = ((bias) << 0) | ((gain) << 6) | ((boost) << 8) | ((coefficient) << 9), .paType = RF_TxPowerTable_DefaultPA } |
Creates a TX power table entry for the default PA.
The values for bias, gain, boost and coefficient are usually measured by Texas Instruments for a specific front-end configuration. They can then be obtained from SmartRFStudio or SysConfig.
| #define RF_TxPowerTable_CC13x4Sub1GHz_DEFAULT_PA_ENTRY | ( | bias, | |
| gain, | |||
| boost, | |||
| coefficient, | |||
| gain2 | |||
| ) | { .rawValue = ((bias) << 0) | ((gain) << 6) | ((boost) << 8) | ((coefficient) << 9) | ((gain2) << 16), .paType = RF_TxPowerTable_DefaultPA } |
Creates a TX power table Sub1-GHz entry for the default PA.
The values for bias, gain, boost, coefficient and gain2 are usually measured by Texas Instruments for a specific front-end configuration. They can then be obtained from SmartRFStudio or SysConfig.
| #define RF_TxPowerTable_HIGH_PA_ENTRY | ( | bias, | |
| ibboost, | |||
| boost, | |||
| coefficient, | |||
| ldotrim | |||
| ) | { .rawValue = ((bias) << 0) | ((ibboost) << 6) | ((boost) << 8) | ((coefficient) << 9) | ((ldotrim) << 16), .paType = RF_TxPowerTable_HighPA } |
Creates a TX power table entry for the High-power PA.
The values for bias, ibboost, boost, coefficient and ldoTrim are usually measured by Texas Instruments for a specific front-end configuration. They can then be obtained from SmartRFStudio or SysConfig.
| #define RF_GET_RSSI_ERROR_VAL (-128) |
Error return value for RF_getRssi()
| #define RF_CMDHANDLE_FLUSH_ALL (-1) |
RF command handle to flush all RF commands.
| #define RF_ALLOC_ERROR (-2) |
RF command or RAT channel allocation error.
| #define RF_SCHEDULE_CMD_ERROR (-3) |
RF command schedule error.
| #define RF_ERROR_RAT_PROG (-255) |
A rat channel could not be programmed.
| #define RF_ERROR_INVALID_RFMODE (-256) |
Invalid RF_Mode. Used in error callback.
| #define RF_ERROR_CMDFS_SYNTH_PROG (-257) |
Synthesizer error with CMD_FS. Used in error callback. If this error occurred in error callback, user needs to resend CMD_FS to recover. See the device's errata for more details.
| #define RF_NUM_SCHEDULE_ACCESS_ENTRIES 2 |
Number of access request entries.
| #define RF_NUM_SCHEDULE_COMMAND_ENTRIES 8 |
Number of scheduled command entries.
| #define RF_NUM_SCHEDULE_MAP_ENTRIES (RF_NUM_SCHEDULE_ACCESS_ENTRIES + RF_NUM_SCHEDULE_COMMAND_ENTRIES) |
Number of schedule map entries. This is the sum of access request and scheduled command entries.
| #define RF_SCH_MAP_CURRENT_CMD_OFFSET RF_NUM_SCHEDULE_ACCESS_ENTRIES |
Offset of the current command entry in the schedule map.
| #define RF_SCH_MAP_PENDING_CMD_OFFSET (RF_SCH_MAP_CURRENT_CMD_OFFSET + 2) |
Offset of the first pending command entry in the schedule map.
| #define RF_ABORT_PREEMPTION (1<<2) |
Used with RF_cancelCmd() to provoke subscription to RadioFreeCallback.
| #define RF_ABORT_GRACEFULLY (1<<0) |
Used with RF_cancelCmd() for graceful command termination.
| #define RF_SCH_CMD_EXECUTION_TIME_UNKNOWN 0 |
For unknown execution time for RF scheduler.
| #define RF_RAT_ANY_CHANNEL (-1) |
To be used within the channel configuration structure. Allocate any of the available channels.
| #define RF_RAT_TICKS_PER_US 4 |
Radio timer (RAT) ticks per microsecond.
| #define RF_LODIVIDER_MASK 0x7F |
Mask to be used to determine the effective value of the setup command's loDivider field.
| #define RF_STACK_ID_DEFAULT 0x00000000 |
No value is set.
| #define RF_STACK_ID_154 0x8000F154 |
ID for TI 15.4 Stack.
| #define RF_STACK_ID_BLE 0x8000FB1E |
ID for TI BLE Stack.
| #define RF_STACK_ID_EASYLINK 0x8000FEA2 |
ID for TI EasyLink Stack.
| #define RF_STACK_ID_THREAD 0x8000FEAD |
ID for TI Thread Stack.
| #define RF_STACK_ID_TOF 0x8000F00F |
ID for TI TOF Stack.
| #define RF_STACK_ID_CUSTOM 0x0000FC00 |
ID for Custom Stack.
| #define RF_convertUsToRatTicks | ( | microseconds | ) | ((microseconds) * (RF_RAT_TICKS_PER_US)) |
Converts a duration given in microseconds into radio timer (RAT) ticks.
| #define RF_convertMsToRatTicks | ( | milliseconds | ) | ((milliseconds) * 1000 * (RF_RAT_TICKS_PER_US)) |
Converts a duration given in milliseconds into radio timer (RAT) ticks.
| #define RF_convertRatTicksToUs | ( | ticks | ) | ((ticks) / (RF_RAT_TICKS_PER_US)) |
Converts a duration given in radio timer (RAT) ticks into microseconds.
| #define RF_convertRatTicksToMs | ( | ticks | ) | ((ticks) / (1000 * (RF_RAT_TICKS_PER_US))) |
Converts a duration given in radio timer (RAT) ticks into milliseconds.